5 years agoMerge pull request #3 in PROCESSOR-SDK/bcp-lld from PRSDK-4300 to master DEV.BCP_LLD.02.01.00.07A DEV.PROCESSOR-SDK.05.02.00.07 DEV.PROCESSOR-SDK.05.03.00.05 DEV.PROCESSOR-SDK.06.00.00.05
Merge pull request #3 in PROCESSOR-SDK/bcp-lld from PRSDK-4300 to master
* commit '7cfb2617fd64d9b70e3035a6b06b91937dca6c8e':
PRSDK-4300: Corrected XDC package version
* commit '7cfb2617fd64d9b70e3035a6b06b91937dca6c8e':
PRSDK-4300: Corrected XDC package version
PRSDK-4300: Corrected XDC package version
5 years agoMerge pull request #2 in PROCESSOR-SDK/bcp-lld from Doc_ver_update_5.0 to master DEV.BCP_LLD.02.01.00.07 DEV.PROCESSOR-SDK.05.01.00.10 DEV.PROCESSOR-SDK.05.01.00.11
Merge pull request #2 in PROCESSOR-SDK/bcp-lld from Doc_ver_update_5.0 to master
* commit '2be37ab05c841004fc85b24fb40de0263e71f94a':
Updated version in release note
Documentation and version updates for procsdk 5.0 release
* commit '2be37ab05c841004fc85b24fb40de0263e71f94a':
Updated version in release note
Documentation and version updates for procsdk 5.0 release
Updated version in release note
Documentation and version updates for procsdk 5.0 release
Merge pull request #1 in PROCESSOR-SDK/bcp-lld from PRSDK-2194 to master
* commit 'c0210956df08945538350a3da4ecb155727a7acb':
PRSDK-2194 Added RULES_MAKE macro
* commit 'c0210956df08945538350a3da4ecb155727a7acb':
PRSDK-2194 Added RULES_MAKE macro
PRSDK-2194 Added RULES_MAKE macro
Added RULES_MAKE macro to support build based on custom Rules.make
location
Added RULES_MAKE macro to support build based on custom Rules.make
location
update release notes and version number for
processor sdk release
processor sdk release
updated .gitignore
fixed packaging of library size text files and removed the chm from package
support SECTTI and parallel builds
Merge branch 'releases/mcsdk_03.01.03.00'
Release note update for MCSDK 3.1.3.6
Fix SDOCM00115152: set unintitialized queueType in Bcp_rxOpen()
to QMSS_PARAM_NOT_SPECIFIED.
to QMSS_PARAM_NOT_SPECIFIED.
SDOCM00115151 fix. TSC enabled for BCP example and unit
test so that TSCL/TSCH can be used for counting delays.
test so that TSCL/TSCH can be used for counting delays.
Merge branch 'releases/mcsdk_03.01.03.00'
Release document update and version update.
SDOCM00114659
SDOCM00114659
Fix for SDOCM00114659. Break statements added to
each switch statement of this file to ensure
that only the register of interest is accessed
or set.
each switch statement of this file to ensure
that only the register of interest is accessed
or set.
Corrected call in example and test files for LTE
DL to Semaphore_delete() after fix for
SDOCM00112895.
DL to Semaphore_delete() after fix for
SDOCM00112895.
Merge branch 'releases/mcsdk_03.01.01.00'
Release notes update for SDOM00114088.
Fix for SDOCM00114088. In Bcp_rxOpen(), the queueType
is no longer changed when the queueNumber is specified.
Application should set queueType appropriately.
is no longer changed when the queueNumber is specified.
Application should set queueType appropriately.
Fix for SDOCM00114088. In Bcp_rxOpen(), the
queueType is no longer changed when the queueNumber is
specified. Application should set queueType appropriately.
queueType is no longer changed when the queueNumber is
specified. Application should set queueType appropriately.
Merge branch 'releases/mcsdk_03.01.00.00'
Fix for SDOCM00105728. extern "C" construct added
for bcp_osal.h.
for bcp_osal.h.
Update version of LLD to 2.1.0.3.
Fix for SDOCM00112895. Address to semaphore handle
passed to the Semaphore_delete() API call.
passed to the Semaphore_delete() API call.
Merge branch 'releases/mcsdk_03.01.00.00'
9 years agoAddressed SDOCM00107359 and partial SDOCM00108469 (minus compiler DEV.BCP_LLD.02.01.00.02
Addressed SDOCM00107359 and partial SDOCM00108469 (minus compiler
upgrade) for debugging LLD with optimization (to get the call
stack).
upgrade) for debugging LLD with optimization (to get the call
stack).
Merge branch 'releases/mcsdk_03.01.00.00'
9 years ago Added new CSL header file to test and examples after a #define was DEV.BCP_LLD.02.01.00.01
Added new CSL header file to test and examples after a #define was
moved from QMSS to the CSL header file.
moved from QMSS to the CSL header file.
Incorporated new osal functions for QMSS accumulator queues for IR
SDOCM00107127: Separate protection OSALs for QMSS LLD. A new semaphore
was added for QMSS Accumulator queue access in the OSAL, and the BCP
semaphore number was changed in test/src/test_main.c to accommodate the
new semaphore usage.
SDOCM00107127: Separate protection OSALs for QMSS LLD. A new semaphore
was added for QMSS Accumulator queue access in the OSAL, and the BCP
semaphore number was changed in test/src/test_main.c to accommodate the
new semaphore usage.
Update of development build scripts to PDK 3.1.0.1. Also update to
Example projects include path to include local files rather than
PDK files for BCP first.
Example projects include path to include local files rather than
PDK files for BCP first.
10 years agoUpdate to XDC package version and document versions DEV.BCP.02.01.00.00 DEV.BCP_LLD.02.01.00.00
Update to XDC package version and document versions
Update to BCP version number due to example and unit test code changes for Lamarr.
Change to Example and unit test code for BCP to remove SRIO support
K2L device does not have SRIO IP on it, and so the example code
needed changes to remove the dependence. Through the use of
DEVICE_K2L compile-time flag, SRIO function calls were disabled
in the common example and unit test src code files for Keystone2 devices.
SDOCM00105932
K2L device does not have SRIO IP on it, and so the example code
needed changes to remove the dependence. Through the use of
DEVICE_K2L compile-time flag, SRIO function calls were disabled
in the common example and unit test src code files for Keystone2 devices.
SDOCM00105932
update setupenv.bat to be compatible with other LLDs
Merge remote-tracking branch 'origin' into releases/mcsdk_03.01.00.00
Update of version and document
10 years agoFix as per issue reported in SDOCM00102300, BCP driver not compatible with QMSS using...
Fix as per issue reported in SDOCM00102300, BCP driver not compatible with QMSS using RMv2.
Limited validation as RM is not enabled in the example/test for BCP. Fix being included to unblock
Limited validation as RM is not enabled in the example/test for BCP. Fix being included to unblock
Update release note and version
Fix for IR:SDOCM00100869
Modified source to remove hardcoding of QMSS Mgr value from zero to take care of second QMSS instance
Modified source to remove hardcoding of QMSS Mgr value from zero to take care of second QMSS instance
BCP LLD support for Lamarr (K2L)
Fix for IR: SDOCM00098765
MCSDK 3.0: updated docs for Alpha-4
MCSDK 3.0: workaround to fix the compilation issue to use device specific CSL
MCSDK 3.0: device name change for Alpha-4
Commited by migration script
initial commit