PRSDK-3363 Fixed Klocwork issue on EDMA Examples Klocwork error fix for EDMA3 examples
PRSDK-415 Address review comments Removed #ifdef EDMA3_RES_USER_REQ enclosures in EDMA3 driver and examples. Add API in EDMA3 examples to validate the paRAM id allocated is same as the requested DMA channel number.
PRSDK-415 Add support to verify allocated PaRAM Id Add support to verify the requested DMA Channel ID gets the corresponding PaRAM Id. The test can be enabled by adding EDMA3_RES_USER_REQ macro in makefile of driver and AM335x example makefile.
PRSDK-927: additional fix to ensure the far qualifier only applies for C66x compilation Signed-off-by: Ivan Pang <i-pang@ti.com>
PRSDK-927: updated declaration of numEdma3Instances to far, since build mem_model:data=far Signed-off-by: Ivan Pang <i-pang@ti.com>
Following changes done 1. Teardown sequence in standalone example was not proper ie edma3deinit() was called after heartbeats (huge delay) so de-initialization was not happening. 2. Code clean up - Indentation and tab removal changes for only standalone example files.
Fixed warnings in building for tda2xx platform Signed-off-by: Prasad Konnur <prasadkonnur@ti.com>
Removed Busy waiting in edma examples Added a Sem pend while waiting for interrupt and Sem post in ISR servicing the interrupt Signed-off-by: Prasad Konnur <prasadkonnur@ti.com>
Added Vayu support in edma3lld Tested on A15, IPU and DSP cores on Zebu System edma and DSP edma both added Signed-off-by: Prasad Konnur <prasadkonnur@ti.com>
Fix for multi-core execution of examples. - Address would need to be global for EDMA transfer - Testing version querry API added in the EDMA DRV module - Adding of code to test default RM configuration Signed-off-by: Sundaram Raju <sundaram@ti.com>
EDMA3 driver sample example made generic EDMA3 sample application made generic so that it takes the EDMA3 Driver handle now and all the test cases can be run on any EDMA3 controller
Changing dos to unix format
EDMA3: Adding release package 02.00.00.03