fixed build warning Signed-off-by: Prasad Konnur <prasadkonnur@ti.com>
PRSDK-8534: migration to sysbios 6.82 - Updated toolchains - Bios: bios_6_82_00_16 - XDC : xdctools_3_61_00_16_core - TI CGT: ti-cgt-arm_20.2.0.LTS - GCC CGT: gcc-arm-9.2-2019.12-x86_64-arm-none-eabi - C66x TI CGT: ti-cgt-c6000_8.3.2 - Eve CGT: arp32_1.0.8 - Commented example build for platforms not supported in latest Bios - Updated A8 to use GCC toolchains for all platforms - Updated A8 and A15 Rules - Updated to use std libs from gnu\targets\arm\libs\install-native\arm-none-eabi\lib\thumb\v7-a\hard - Removed nano.specs from linker option as the nano libs are not supported under v7-a - Link the libgcc from compiler from lib/gcc/arm-none-eabi/9.2.1/thumb/v7-a+fp/hard Signed-off-by: Prasad Konnur <prasadkonnur@ti.com>
PRSDK-5267 Add support to enable SMP mode Remove platform specifc cache header files from SYSBIOS. Add generic cache header file to allow BIOS to choose appropriate cache APIs based on the RTSC config file.
PRSDK-5267 Add support to enable SMP mode Remove platform specifc cache header files from SYSBIOS. Add generic cache header file to allow BIOS to choose appropriate cache APIs based on the RTSC config file.
Merge pull request #27 in PROCESSOR-SDK/edma3_lld from PRSDK-415 to master * commit '24cc4bc8763902321b368dbd14207ce8af1ee056': Removing Extra lines PRSDK-415 Reverting makefile changes PRSDK-415 Address review comments PRSDK-415 Address review comments. PRSDK-415 Add support to verify allocated PaRAM Id PRSDK-415: Address review comments PRSDK-415: Updated config file to be generic PRSDK-415 Update global cfgparams for AM335x PRSDK-415 Disabled reserved parameters for AM335x
PRSDK-415 Address review comments Removed #ifdef EDMA3_RES_USER_REQ enclosures in EDMA3 driver and examples. Add API in EDMA3 examples to validate the paRAM id allocated is same as the requested DMA channel number.
edma3: PRSDK-3579: Clean up static analysis error in UART/SPI LLD caused by edma3 LLD dmaChannelHwEvtMap is an array of size 2, lCh should be checked before referencing drvObject->gblCfgParams.dmaChannelHwEvtMap[] Signed-off-by: Hao Zhang <hzhang@ti.com>
PRSDK-415 Address review comments. - Removed global variable which is used to get PaRAM ID. - Updated EDMA3_DRV_getAllocatedPARAMId() function to return paRAM id from the EDMA3 driver global variable. - Updated makefile to receive EDMA3_RES_USER_REQ macro as a flag through command line interface. Signed-off-by: Pratap Reddy <x0257344@ti.com>
PRSDK-415 Add support to verify allocated PaRAM Id Add support to verify the requested DMA Channel ID gets the corresponding PaRAM Id. The test can be enabled by adding EDMA3_RES_USER_REQ macro in makefile of driver and AM335x example makefile.
PRSDK-415: Updated config file to be generic Updated AM335x config file generically on all EDMA3 regions to allocate user request PARAM set from any regions.
PRSDK-415 Update global cfgparams for AM335x Reused reserved PARAM set masking code removed previously. Updated Global cfgparams to allocate user request PARAM set.
Merge pull request #20 in PROCESSOR-SDK/edma3_lld from misrac_fix_PRSDK-3354 to master * commit '81e2f425f6bf02b1bf477955a818b76f8a303969': misrac fix 2 for 4.2.0 (PRSDK-3354) misrac fix for 4.2.0 (PRSDK-3354)