1 CSL 2.0 DAT Adapter Reference Implementation Using EDMA3 Low Level Driver\r
2 \r
3 +++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++\r
4 Following directories are part of this package:-\r
5 \r
6 CSL2_DAT_DEMO - Top level directory\r
7 - csl2_legacy_include - Legacy headers of CSL 2.0\r
8 - dat_edma3LLD - Reference implementation of the DAT APIs using \r
9 the EDMA3 Low level driver package\r
10 - demo - Example pjt to run on DM6446 EVM, \r
11 that makes calls DAT APIs\r
12 - bios_adapter - BIOS specific implementation of critical section entry exit APIs required by EDMA3 LLD as well as\r
13 the Dat wrapper\r
14 - Interrupt registration and un-registration code\r
15 required by the application\r
16 - docs - CSL_DAT_Adapter presentation \r
17 +++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++\r
18 Following environment variables need to be set to correctly build the pjt\r
19 EDMA3LLD_INSTALL_DIR Location of EDMA3 Low level driver package\r
20 installation \r
21 (NOTE:- Ensure EDMA3 low level driver package is\r
22 built specifically for DM6446)\r
23 \r
24 +++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++\r
25 Issues:-\r
26 1. Due to a DM6446 Simulation bug, this example does not run on the simulator \r
27 +++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++\r