updated lib path for gcc compiler
[keystone-rtos/edma3_lld.git] / examples / CSL2_DAT_DEMO / docs / readme.txt
1 CSL 2.0 DAT Adapter Reference Implementation Using EDMA3 Low Level Driver\r
2 \r
3 +++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++\r
4 Following directories are part of this package:-\r
5 \r
6 CSL2_DAT_DEMO             - Top level directory\r
7     - demo                    - Platform specific CCSv4 build files.\r
8     - docs                    - CSL_DAT_Adapter presentation \r
9         - src\r
10                 - bios_adapter        - BIOS specific implementation of critical section                                \r
11                                                                 entry exit APIs required by the DAT wrapper.\r
12                 - csl2_legacy_include - Required legacy headers of CSL 2.0\r
13                 - dat_edma3LLD        - Reference implementation of the DAT APIs using \r
14                                 the EDMA3 Low level driver package\r
15 +++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++\r