EDMA3: BIOS6 Release 02.00.01.04
[keystone-rtos/edma3_lld.git] / examples / CSL2_DAT_DEMO / src / csl2_legacy_include / tistdtypes.h
1 /*
2  *  ======== tistdtypes.h ========
3  */
5 /*
6  * These types are also defined by other TI components.  They are bracketed
7  * with _TI_STD_TYPES to avoid warnings for duplicate definition.
8  *
9  * You may get warnings about duplicate type definitions when using this
10  * header file with earlier versions of DSP/BIOS and CSL.
11  *
12  * You can use the '-pds303' compiler option to suppress these warnings.
13  */
14 #ifndef _TI_STD_TYPES
15 #define _TI_STD_TYPES
17 /*
18  * This '#ifndef STD_' is needed to protect from duplicate definitions
19  * of Int, Uns, etc. in DSP/BIOS v4.x (e.g. 4.90, 4.80) since these versions
20  * of DSP/BIOS did not contain the '#ifndef_TI_STD_TYPES' logic.
21  */
22 #ifndef STD_
24 /*
25  * Aliases for standard C types
26  */
27 typedef int                     Int;
28 typedef unsigned                Uns;
29 typedef char                    Char;
31 /* pointer to null-terminated character sequence */
32 typedef char                    *String;
34 typedef void                    *Ptr;           /* pointer to arbitrary type */
36 typedef unsigned short          Bool;           /* boolean */
38 #endif /* STD_ */
40 /*
41  * Uint8, Uint16, Uint32, etc are defined to be "smallest unit of
42  * available storage that is large enough to hold unsigned or integer
43  * of specified size".
44  */
46 /* Handle the 6x ISA */
47 #if defined(_TMS320C6X)
48     /* Unsigned integer definitions (32bit, 16bit, 8bit) follow... */
49     typedef unsigned int        Uint32;
50     typedef unsigned short      Uint16;
51     typedef unsigned char       Uint8;
53     /* Signed integer definitions (32bit, 16bit, 8bit) follow... */
54     typedef int                 Int32;
55     typedef short               Int16;
56     typedef char                Int8;
58 /* Handle the 54x, 55x and 28x ISAs */
59 #elif defined(_TMS320C5XX) || defined(__TMS320C55X__) || defined(_TMS320C28X)
60     /* Unsigned integer definitions (32bit, 16bit, 8bit) follow... */
61     typedef unsigned long       Uint32;
62     typedef unsigned short      Uint16;
63     typedef unsigned char       Uint8;
65     /* Signed integer definitions (32bit, 16bit, 8bit) follow... */
66     typedef long                Int32;
67     typedef short               Int16;
68     typedef char                Int8;
70 #else
71     /* Other ISAs not supported */
72     #error <tistdtypes.h> is not supported for this target
73 #endif  /* defined(_6x_) */
75 #endif  /* _TI_STD_TYPES */