74f80b8f77b69e3994a02986ea1688e8e319490b
[keystone-rtos/edma3_lld.git] / examples / edma3_driver / src / sample.h
1 /*
2  * bios6_edma3_drv_sample.h
3  *
4  * Header file for the Demo application for the EDMA3 Driver.
5  *
6  * Copyright (C) 2009 Texas Instruments Incorporated - http://www.ti.com/
7  *
8  *
9  *  Redistribution and use in source and binary forms, with or without
10  *  modification, are permitted provided that the following conditions
11  *  are met:
12  *
13  *    Redistributions of source code must retain the above copyright
14  *    notice, this list of conditions and the following disclaimer.
15  *
16  *    Redistributions in binary form must reproduce the above copyright
17  *    notice, this list of conditions and the following disclaimer in the
18  *    documentation and/or other materials provided with the
19  *    distribution.
20  *
21  *    Neither the name of Texas Instruments Incorporated nor the names of
22  *    its contributors may be used to endorse or promote products derived
23  *    from this software without specific prior written permission.
24  *
25  *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
26  *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
27  *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
28  *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
29  *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
30  *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
31  *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
32  *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
33  *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
34  *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
35  *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
36  *
37 */
39 #ifndef _SAMPLE_H_
40 #define _SAMPLE_H_
42 #include <stdio.h>
43 #include <xdc/std.h>
44 #include <ti/sysbios/knl/Task.h>
46 /* Include EDMA3 Driver */
47 #include <ti/sdo/edma3/drv/sample/bios6_edma3_drv_sample.h>
49 #ifdef __cplusplus
50 extern "C" {
51 #endif
53 /* MAX ACOUNT */
54 #define MAX_ACOUNT                                      (64u)
55 /* MAX BCOUNT */
56 #define MAX_BCOUNT                                      (1u)
57 /* MAX CCOUNT */
58 #define MAX_CCOUNT                                      (1u)
59 /**
60  * Buffers (src and dest) are needed for mem-2-mem data transfers.
61  * This define is for the MAXIMUM size and hence the maximum data
62  * which could be transferred using the sample test cases below.
63  */
64 #define MAX_BUFFER_SIZE                         (MAX_ACOUNT * MAX_BCOUNT * MAX_CCOUNT)
66 #ifndef BUILD_TDA2XX_MPU
67 /* To enable/disable the cache .*/
68 #define EDMA3_ENABLE_DCACHE                 (1u)
69 #endif
71 /* OPT Field specific defines */
72 #define OPT_SYNCDIM_SHIFT                   (0x00000002u)
73 #define OPT_TCC_MASK                        (0x0003F000u)
74 #define OPT_TCC_SHIFT                       (0x0000000Cu)
75 #define OPT_ITCINTEN_SHIFT                  (0x00000015u)
76 #define OPT_TCINTEN_SHIFT                   (0x00000014u)
78 /**
79  * EDMA3 Driver Handle, which is used to call all the Driver APIs.
80  * It gets initialized during EDMA3 Initialization.
81  */
82 extern EDMA3_DRV_Handle hEdma[];
84 extern void callback1 (unsigned int tcc, EDMA3_RM_TccStatus status,
85                         void *appData);
87 extern void callback2 (unsigned int tcc, EDMA3_RM_TccStatus status,
88                         void *appData);
90 extern signed char*  getGlobalAddr(signed char* addr);
91 /* Flag variable to check transfer completion on channel 1 */
92 extern volatile short irqRaised1;
93 /* Flag variable to check transfer completion on channel 2 */
94 extern volatile short irqRaised2;
96 #define MAX_NUM_EDMA_INSTANCES  5
98 /* Define to verify the default RM config.
99  * Additional configuration required. Update the 
100  * gblCfgReqdArray[] to reflect the master/slave config.
101  * In the case of multiple instances default configuration
102  * may require more than one cores other than core 0 to be master. 
103  * #define EDMA3_DRV_USE_DEF_RM_CFG 
104  */
106 #define GLOBAL_ADDR(addr) (getGlobalAddr(addr))
108 /**
109  *  \brief   EDMA3 mem-to-mem data copy test case, using a DMA channel.
110  *
111  *
112  *  \param  acnt        [IN]      Number of bytes in an array
113  *  \param  bcnt        [IN]      Number of arrays in a frame
114  *  \param  ccnt        [IN]      Number of frames in a block
115  *  \param  syncType    [IN]      Synchronization type (A/AB Sync)
116  *
117  *  \return  EDMA3_DRV_SOK or EDMA3_DRV Error Code
118  */
119 EDMA3_DRV_Result edma3_test(
120                     EDMA3_DRV_Handle hEdma,
121                     unsigned int acnt,
122                     unsigned int bcnt,
123                     unsigned int ccnt,
124                     EDMA3_DRV_SyncType syncType);
128 /**
129  *  \brief   EDMA3 mem-to-mem data copy test case, using two DMA
130  *              channels, linked to each other.
131  *
132  *  \param  acnt        [IN]      Number of bytes in an array
133  *  \param  bcnt        [IN]      Number of arrays in a frame
134  *  \param  ccnt        [IN]      Number of frames in a block
135  *  \param  syncType    [IN]      Synchronization type (A/AB Sync)
136  *
137  *  \return  EDMA3_DRV_SOK or EDMA3_DRV Error Code
138  */
139 EDMA3_DRV_Result edma3_test_with_link(
140                     EDMA3_DRV_Handle hEdma,
141                     unsigned int acnt,
142                     unsigned int bcnt,
143                     unsigned int ccnt,
144                     EDMA3_DRV_SyncType syncType);
148 /**
149  *  \brief   EDMA3 mem-to-mem data copy test case, using a QDMA channel.
150  *
151  *
152  *  \param  acnt        [IN]      Number of bytes in an array
153  *  \param  bcnt        [IN]      Number of arrays in a frame
154  *  \param  ccnt        [IN]      Number of frames in a block
155  *  \param  syncType    [IN]      Synchronization type (A/AB Sync)
156  *
157  *  \return  EDMA3_DRV_SOK or EDMA3_DRV Error Code
158  */
159 EDMA3_DRV_Result qdma_test(
160                     EDMA3_DRV_Handle hEdma,
161                     unsigned int acnt,
162                     unsigned int bcnt,
163                     unsigned int ccnt,
164                     EDMA3_DRV_SyncType syncType);
168 /**
169  *  \brief   EDMA3 misc test cases.
170  *              This test case will read/write to some CC registers.
171  *
172  *  \return  EDMA3_DRV_SOK or EDMA3_DRV Error Code
173  */
174 EDMA3_DRV_Result edma3_misc_test(EDMA3_DRV_Handle hEdma);
177 /**
178  *  \brief   EDMA3 mem-to-mem data copy test case, using a QDMA channel,
179  *              linked to another LINK channel.
180  *
181  *  \param  acnt        [IN]      Number of bytes in an array
182  *  \param  bcnt        [IN]      Number of arrays in a frame
183  *  \param  ccnt        [IN]      Number of frames in a block
184  *  \param  syncType    [IN]      Synchronization type (A/AB Sync)
185  *
186  *  \return  EDMA3_DRV_SOK or EDMA3_DRV Error Code
187  */
188 EDMA3_DRV_Result qdma_test_with_link(
189                     EDMA3_DRV_Handle hEdma,
190                     unsigned int acnt,
191                     unsigned int bcnt,
192                     unsigned int ccnt,
193                     EDMA3_DRV_SyncType syncType);
196 /**
197  *  \brief   EDMA3 mem-to-mem data copy test case, using two DMA channels,
198  *              chained to each other.
199  *
200  *  \param  acnt        [IN]      Number of bytes in an array
201  *  \param  bcnt        [IN]      Number of arrays in a frame
202  *  \param  ccnt        [IN]      Number of frames in a block
203  *  \param  syncType    [IN]      Synchronization type (A/AB Sync)
204  *
205  *  \return  EDMA3_DRV_SOK or EDMA3_DRV Error Code
206  */
207 EDMA3_DRV_Result edma3_test_with_chaining(
208                     EDMA3_DRV_Handle hEdma,
209                                 unsigned int acnt,
210                                 unsigned int bcnt,
211                                 unsigned int ccnt,
212                                 EDMA3_DRV_SyncType syncType);
215 /**
216  *  \brief   EDMA3 mem-to-mem data copy test case, using a DMA channel.
217  *              This test case doesnot rely on the callback mechanism.
218  *              Instead, it Polls the IPR register to check the transfer
219  *              completion status.
220  *
221  *  \param  acnt        [IN]      Number of bytes in an array
222  *  \param  bcnt        [IN]      Number of arrays in a frame
223  *  \param  ccnt        [IN]      Number of frames in a block
224  *  \param  syncType    [IN]      Synchronization type (A/AB Sync)
225  *
226  *  \return  EDMA3_DRV_SOK or EDMA3_DRV Error Code
227  */
228 EDMA3_DRV_Result edma3_test_poll_mode(
229                     EDMA3_DRV_Handle hEdma,
230                                 unsigned int acnt,
231                                 unsigned int bcnt,
232                                 unsigned int ccnt,
233                                 EDMA3_DRV_SyncType syncType);
236 /**
237  *  \brief   EDMA3 ping-pong based data copy test case, using a DMA and
238  *              a link channel.
239  *
240  *  \return  EDMA3_DRV_SOK or EDMA3_DRV Error Code
241  */
242 EDMA3_DRV_Result edma3_test_ping_pong_mode(EDMA3_DRV_Handle hEdma);
244 #ifdef __cplusplus
246 #endif /* extern "C" */
248 #endif  /* _SAMPLE_H_ */