Updated Makerules
[keystone-rtos/edma3_lld.git] / makerules / env.mk
1 # File: env.mk. This file contains all the paths and other ENV variables
3 #
4 # Module paths
5 #
7 # Directory where all internal software packages are located; typically 
8 #  those that are checked into version controlled repository. In this case all
9 #  the OMX components and SDK/OMX demo.
10 INTERNAL_SW_ROOT = E:/EDMA/edma3_lld_02_11_00_01
12 # Directory where all external (imported) software packages are located; typically 
13 #  those that are NOT checked into version controlled repository. In this case,
14 #  compiler tool chains, BIOS, XDC, Syslink, IPC, FC, CE, drivers, codecs, etc.
15 EXTERNAL_SW_ROOT = C:/PROGRA~1/TEXASI~1
17 # Destination root directory.
18 #   - specify the directory where you want to place the object, archive/library,
19 #     binary and other generated files in a different location than source tree
20 #   - or leave it blank to place then in the same tree as the source
21 #DEST_ROOT = E:/Temp/sdk5008_outfiles
23 # Utilities directory. This is required only if the build machine is Windows.
24 #   - specify the installation directory of utility which supports POSIX commands
25 #     (eg: Cygwin installation or MSYS installation).
26 UTILS_INSTALL_DIR = C:/PROGRA~1/TEXASI~1/xdctools_3_20_07_86
28 # Set path separator, etc based on the OS
29 ifeq ($(OS),Windows_NT)
30   PATH_SEPARATOR = ;
31   UTILSPATH = $(UTILS_INSTALL_DIR)/bin/
32 else 
33   # else, assume it is linux
34   PATH_SEPARATOR = :
35 endif
37 # BIOS
38 bios_PATH = $(EXTERNAL_SW_ROOT)/bios_6_31_03_25
39 bios_INCLUDE = $(bios_PATH)/packages
41 # XDC
42 xdc_PATH = $(EXTERNAL_SW_ROOT)/xdctools_3_20_07_86
43 xdc_INCLUDE = $(xdc_PATH)/packages
45 # EDMA3 LLD
46 edma3_lld_PATH = $(INTERNAL_SW_ROOT)
47 include $(edma3_lld_PATH)/packages/component.mk
49 #
50 # Tools paths
51 #
52 # Cortex-M3
53 CODEGEN_PATH_M3 = $(EXTERNAL_SW_ROOT)/TMS470~1.3
55 # Cortex-A8
56 CODEGEN_PATH_A8 = $(EXTERNAL_SW_ROOT)/TMS470~1.3
58 # ARM-9
59 CODEGEN_PATH_ARM9 = $(EXTERNAL_SW_ROOT)/TMS470~1.3
61 # DSP - Since same toolchain does not support COFF and ELF, there are two entries
62 #        This would go away when one version supports both formats
63 CODEGEN_PATH_DSP = $(EXTERNAL_SW_ROOT)/C6000C~1.4
64 CODEGEN_PATH_DSPELF = $(EXTERNAL_SW_ROOT)/C6000C~1.0B2
67 # Commands commonly used within the make files
69 RM = $(UTILSPATH)rm
70 RMDIR = $(UTILSPATH)rm -rf
71 MKDIR = $(UTILSPATH)mkdir
72 ECHO = @$(UTILSPATH)echo
73 # MAKE = $(UTILSPATH)make
74 EGREP = $(UTILSPATH)egrep
75 CP = $(UTILSPATH)cp
77 # This is to avoid using full blown cygwin - chmod is really needed only linux
78 ifeq ($(OS),Windows_NT)
79 CHMOD = @echo
80 else
81 CHMOD = $(UTILSPATH)chmod
82 endif
84 #
85 # XDC specific ENV variables
86 #
88 # XDC Config.bld file (required for configuro) ; Derives from top-level omx_PATH
89 CONFIG_BLD_XDC_674 = $(edma3_lld_PATH)/packages/_config.bld
90 CONFIG_BLD_XDC_64p = $(edma3_lld_PATH)/packages/_config.bld
91 CONFIG_BLD_XDC_a8 = $(edma3_lld_PATH)/packages/_config.bld
92 CONFIG_BLD_XDC_arm9 = $(edma3_lld_PATH)/packages/_config.bld
94 XDCPATH = $(bios_PATH)/packages;$(xdc_PATH)/packages;$(edma3_lld_PATH)/packages;
95 export XDCPATH
97 XDCROOT = $(xdc_PATH)
98 XDCTOOLS = $(xdc_PATH)
99 export XDCROOT
100 export XDCTOOLS
102 TMS470_CGTOOLS = $(CODEGEN_PATH_M3)
103 CGTOOLS = $(CODEGEN_PATH_DSP)
104 CGTOOLS_ELF = $(CODEGEN_PATH_DSPELF)
105 export TMS470CGTOOLPATH
107 CODESOURCERYCGTOOLS = $(CODEGEN_PATH_A8)
108 export CODESOURCERYCGTOOLS
110 PATH += $(PATH_SEPARATOR)$(xdc_PATH)$(PATH_SEPARATOR)$(CODEGEN_PATH_M3)/bin
111 export PATH
113 # Nothing beyond this point