1 # File: env.mk. This file contains all the paths and other ENV variables
3 #
4 # Module paths
5 #
7 # Directory where all internal software packages are located; typically
8 # those that are checked into version controlled repository. In this case all
9 # the OMX components and SDK/OMX demo.
10 INTERNAL_SW_ROOT = E:/EDMA/edma3_lld_02_11_03_01
12 # Directory where all external (imported) software packages are located; typically
13 # those that are NOT checked into version controlled repository. In this case,
14 # compiler tool chains, BIOS, XDC, Syslink, IPC, FC, CE, drivers, codecs, etc.
15 EXTERNAL_SW_ROOT = C:/PROGRA~1/TEXASI~1
17 # Destination root directory.
18 # - specify the directory where you want to place the object, archive/library,
19 # binary and other generated files in a different location than source tree
20 # - or leave it blank to place then in the same tree as the source
21 #DEST_ROOT = E:/Temp/edma3_lld_02_11_02_03
23 # Utilities directory. This is required only if the build machine is Windows.
24 # - specify the installation directory of utility which supports POSIX commands
25 # (eg: Cygwin installation or MSYS installation).
26 UTILS_INSTALL_DIR = C:/PROGRA~1/TEXASI~1/xdctools_3_22_04_46
28 # Set path separator, etc based on the OS
29 ifeq ($(OS),Windows_NT)
30 PATH_SEPARATOR = ;
31 UTILSPATH = $(UTILS_INSTALL_DIR)/bin/
32 else
33 # else, assume it is linux
34 PATH_SEPARATOR = :
35 endif
37 # BIOS
38 bios_PATH = $(EXTERNAL_SW_ROOT)/bios_6_33_02_31
39 bios_INCLUDE = $(bios_PATH)/packages
41 # XDC
42 xdc_PATH = $(EXTERNAL_SW_ROOT)/xdctools_3_23_01_43
43 xdc_INCLUDE = $(xdc_PATH)/packages
45 # EDMA3 LLD
46 edma3_lld_PATH = $(INTERNAL_SW_ROOT)
47 include $(edma3_lld_PATH)/packages/component.mk
49 #
50 # Tools paths
51 #
52 # Cortex-M3
53 CODEGEN_PATH_M3 = $(EXTERNAL_SW_ROOT)/TMS470~1.0
55 # Cortex-A8
56 CODEGEN_PATH_A8 = $(EXTERNAL_SW_ROOT)/TMS470~1.0
58 # Cortex-A15
59 CODEGEN_PATH_A15 = C:\GNUTOO~1\4F700~1.720
61 # ARM-9
62 CODEGEN_PATH_ARM9 = $(EXTERNAL_SW_ROOT)/TMS470~1.0
64 # DSP - Since same toolchain does not support COFF and ELF, there are two entries
65 # This would go away when one version supports both formats
66 CODEGEN_PATH_DSP = $(EXTERNAL_SW_ROOT)/C6000C~1.3
67 CODEGEN_PATH_DSPELF = $(EXTERNAL_SW_ROOT)/C6000C~1.3
70 # Commands commonly used within the make files
72 RM = $(UTILSPATH)rm
73 RMDIR = $(UTILSPATH)rm -rf
74 MKDIR = $(UTILSPATH)mkdir
75 ECHO = @$(UTILSPATH)echo
76 # MAKE = $(UTILSPATH)make
77 EGREP = $(UTILSPATH)egrep
78 CP = $(UTILSPATH)cp
80 # This is to avoid using full blown cygwin - chmod is really needed only linux
81 ifeq ($(OS),Windows_NT)
82 CHMOD = @echo
83 else
84 CHMOD = $(UTILSPATH)chmod
85 endif
87 #
88 # XDC specific ENV variables
89 #
91 # XDC Config.bld file (required for configuro) ; Derives from top-level omx_PATH
92 CONFIG_BLD_XDC_674 = $(edma3_lld_PATH)/packages/_config.bld
93 CONFIG_BLD_XDC_64p = $(edma3_lld_PATH)/packages/_config.bld
94 CONFIG_BLD_XDC_64t = $(edma3_lld_PATH)/packages/_config.bld
95 CONFIG_BLD_XDC_a8 = $(edma3_lld_PATH)/packages/_config.bld
96 CONFIG_BLD_XDC_arm9 = $(edma3_lld_PATH)/packages/_config.bld
97 CONFIG_BLD_XDC_66 = $(edma3_lld_PATH)/packages/_config.bld
98 CONFIG_BLD_XDC_m3 = $(edma3_lld_PATH)/packages/_config.bld
100 XDCPATH = $(bios_PATH)/packages;$(xdc_PATH)/packages;$(edma3_lld_PATH)/packages;
101 export XDCPATH
103 XDCROOT = $(xdc_PATH)
104 XDCTOOLS = $(xdc_PATH)
105 export XDCROOT
106 export XDCTOOLS
108 TMS470_CGTOOLS = $(CODEGEN_PATH_M3)
109 CGTOOLS = $(CODEGEN_PATH_DSP)
110 CGTOOLS_ELF = $(CODEGEN_PATH_DSPELF)
111 export TMS470_CGTOOLS
113 CODESOURCERYCGTOOLS = $(CODEGEN_PATH_A8)
114 export CODESOURCERYCGTOOLS
116 PATH += $(PATH_SEPARATOR)$(xdc_PATH)$(PATH_SEPARATOR)$(CODEGEN_PATH_M3)/bin
117 export PATH
119 # Nothing beyond this point