35dc338ed99fabceefec6c0fb7555f4f63e1ed96
1 # File: component.mk
2 # This file is component include make file of OMX.
4 # List of variables set in this file and their purpose:
5 # <mod>_RELPATH - This is the relative path of the module, typically from
6 # top-level directory of the package
7 # <mod>_PATH - This is the absolute path of the module. It derives from
8 # absolute path of the top-level directory (set in env.mk)
9 # and relative path set above
10 # <mod>_INCLUDE - This is the path that has interface header files of the
11 # module. This can be multiple directories (space separated)
12 # <mod>_PKG_LIST - Names of the modules (and sub-modules) that are a part
13 # part of this module, including itself.
14 # <mod>_PLATFORM_DEPENDENCY - "yes": means the code for this module depends on
15 # platform and the compiled obj/lib has to be kept
16 # under <platform> directory
17 # "no" or "" or if this variable is not defined: means
18 # this module has no platform dependent code and hence
19 # the obj/libs are not kept under <platform> dir.
20 # <mod>_CORE_DEPENDENCY - "yes": means the code for this module depends on
21 # core and the compiled obj/lib has to be kept
22 # under <core> directory
23 # "no" or "" or if this variable is not defined: means
24 # this module has no core dependent code and hence
25 # the obj/libs are not kept under <core> dir.
26 # <mod>_APP_STAGE_FILES - List of source files that belongs to the module
27 # <mod>, but that needs to be compiled at application
28 # build stage (in the context of the app). This is
29 # primarily for link time configurations or if the
30 # source file is dependent on options/defines that are
31 # application dependent. This can be left blank or
32 # not defined at all, in which case, it means there
33 # no source files in the module <mod> that are required
34 # to be compiled in the application build stage.
35 #
37 # List of modules under EDMA3 LLD
38 edma3_lld_COMP_LIST_c6xdsp = edma3_lld_rm edma3_lld_drv
40 # List of examples under EDMA3 LLD
41 edma3_lld_EXAMPLES_LIST = edma3_drv_arm_ti816x_sample edma3_drv_c6472_sample edma3_drv_c6472be_sample edma3_drv_c6748_sample \
42 edma3_drv_da830_sample edma3_drv_omapl138_sample \
43 edma3_drv_tci6486_sample edma3_drv_tci6486be_sample edma3_drv_ti816x_sample \
44 edma3_drv_ti816x_sim_sample \
45 edma3_drv_ti814x_sample edma3_drv_arm_ti814x_sample \
46 edma3_drv_tci6608_sample edma3_drv_tci6608be_sample \
47 edma3_drv_tci6616_sample edma3_drv_tci6616be_sample \
48 edma3_drv_c6670_sample edma3_drv_c6670be_sample \
49 edma3_drv_c6678_sample edma3_drv_c6678be_sample \
50 # edma3_drv_arm_omapl138_sample edma3_drv_omap4_sample
52 # List of libraries
53 edma3_lld_LIBS_ALL = edma3_lld_rm edma3_lld_drv edma3_lld_rm_sample edma3_lld_drv_sample
55 # EDMA3 LLD RM - Resource manager
56 edma3_lld_rm_RELPATH = ti/sdo/edma3/rm
57 edma3_lld_rm_PATH = $(edma3_lld_PATH)/packages/$(edma3_lld_rm_RELPATH)
58 edma3_lld_rm_INCLUDE = $(edma3_lld_rm_PATH) $(edma3_lld_rm_PATH)/src
59 edma3_lld_rm_PKG_LIST = edma3_lld_rm edma3_lld_rm_sample
60 edma3_lld_rm_PLATFORM_DEPENDENCY = yes
62 edma3_lld_rm_sample_RELPATH = ti/sdo/edma3/rm/sample
63 edma3_lld_rm_sample_PATH = $(edma3_lld_PATH)/packages/$(edma3_lld_rm_sample_RELPATH)
64 edma3_lld_rm_sample_INCLUDE = $(edma3_lld_rm_sample_PATH) $(edma3_lld_rm_sample_PATH)/src
65 edma3_lld_rm_sample_PLATFORM_DEPENDENCY = yes
67 # EDMA3 LLD DRV - Driver
68 edma3_lld_drv_RELPATH = ti/sdo/edma3/drv
69 edma3_lld_drv_PATH = $(edma3_lld_PATH)/packages/$(edma3_lld_drv_RELPATH)
70 edma3_lld_drv_INCLUDE = $(edma3_lld_drv_PATH) $(edma3_lld_drv_PATH)/src
71 edma3_lld_drv_PKG_LIST = edma3_lld_drv edma3_lld_drv_sample
72 edma3_lld_drv_PLATFORM_DEPENDENCY = no
74 edma3_lld_drv_sample_RELPATH = ti/sdo/edma3/drv/sample
75 edma3_lld_drv_sample_PATH = $(edma3_lld_PATH)/packages/$(edma3_lld_drv_sample_RELPATH)
76 edma3_lld_drv_sample_INCLUDE = $(edma3_lld_drv_sample_PATH) $(edma3_lld_drv_sample_PATH)/src
77 edma3_lld_drv_sample_PLATFORM_DEPENDENCY = yes
79 # EDMA3 LLD top level
80 edma3_lld_INCLUDE = $(edma3_lld_PATH)/packages $(edma3_lld_rm_INCLUDE) $(edma3_lld_drv_INCLUDE) \
81 $(edma3_lld_rm_sample_INCLUDE) $(edma3_lld_drv_sample_INCLUDE)
83 # EDMA3 LLD examples
84 edma3_drv_c6472_sample_EXAMPLES_RELPATH = examples/edma3_driver/evm6472
85 edma3_drv_c6472_sample_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6472_sample_EXAMPLES_RELPATH)
87 edma3_drv_c6472be_sample_EXAMPLES_RELPATH = examples/edma3_driver/evm6472BE
88 edma3_drv_c6472be_sample_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6472be_sample_EXAMPLES_RELPATH)
90 edma3_drv_c6748_sample_EXAMPLES_RELPATH = examples/edma3_driver/evm6748
91 edma3_drv_c6748_sample_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6748_sample_EXAMPLES_RELPATH)
93 edma3_drv_da830_sample_EXAMPLES_RELPATH = examples/edma3_driver/evmDA830
94 edma3_drv_da830_sample_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_da830_sample_EXAMPLES_RELPATH)
96 edma3_drv_omapl138_sample_EXAMPLES_RELPATH = examples/edma3_driver/evmOMAPL138
97 edma3_drv_omapl138_sample_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_omapl138_sample_EXAMPLES_RELPATH)
99 edma3_drv_omap4_sample_EXAMPLES_RELPATH = examples/edma3_driver/evmOMAP4
100 edma3_drv_omap4_sample_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_omap4_sample_EXAMPLES_RELPATH)
102 edma3_drv_arm_omapl138_sample_EXAMPLES_RELPATH = examples/edma3_driver/evmOMAPL138_ARM
103 edma3_drv_arm_omapl138_sample_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_arm_omapl138_sample_EXAMPLES_RELPATH)
105 edma3_drv_tci6486_sample_EXAMPLES_RELPATH = examples/edma3_driver/evmTCI6486
106 edma3_drv_tci6486_sample_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6486_sample_EXAMPLES_RELPATH)
108 edma3_drv_tci6486be_sample_EXAMPLES_RELPATH = examples/edma3_driver/evmTCI6486BE
109 edma3_drv_tci6486be_sample_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6486be_sample_EXAMPLES_RELPATH)
111 edma3_drv_ti814x_sample_EXAMPLES_RELPATH = examples/edma3_driver/evmTI814x
112 edma3_drv_ti814x_sample_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_ti814x_sample_EXAMPLES_RELPATH)
114 edma3_drv_arm_ti814x_sample_EXAMPLES_RELPATH = examples/edma3_driver/evmTI814x_ARM
115 edma3_drv_arm_ti814x_sample_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_arm_ti814x_sample_EXAMPLES_RELPATH)
117 edma3_drv_ti816x_sample_EXAMPLES_RELPATH = examples/edma3_driver/evmTI816x
118 edma3_drv_ti816x_sample_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_ti816x_sample_EXAMPLES_RELPATH)
120 edma3_drv_arm_ti816x_sample_EXAMPLES_RELPATH = examples/edma3_driver/evmTI816x_ARM
121 edma3_drv_arm_ti816x_sample_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_arm_ti816x_sample_EXAMPLES_RELPATH)
123 edma3_drv_m3_ti814x_sample_EXAMPLES_RELPATH = examples/edma3_driver/evmTI814x_M3
124 edma3_drv_m3_ti814x_sample_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_arm_ti814x_sample_EXAMPLES_RELPATH)
126 edma3_drv_ti816x_sim_sample_EXAMPLES_RELPATH = examples/edma3_driver/simTI816x
127 edma3_drv_ti816x_sim_sample_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_ti816x_sim_sample_EXAMPLES_RELPATH)
129 edma3_drv_tci6608_sample_EXAMPLES_RELPATH = examples/edma3_driver/simTCI6608
130 edma3_drv_tci6608_sample_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6608_sample_EXAMPLES_RELPATH)
132 edma3_drv_tci6608be_sample_EXAMPLES_RELPATH = examples/edma3_driver/simTCI6608BE
133 edma3_drv_tci6608be_sample_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6608be_sample_EXAMPLES_RELPATH)
135 edma3_drv_tci6616_sample_EXAMPLES_RELPATH = examples/edma3_driver/simTCI6616
136 edma3_drv_tci6616_sample_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6616_sample_EXAMPLES_RELPATH)
138 edma3_drv_tci6616be_sample_EXAMPLES_RELPATH = examples/edma3_driver/simTCI6616BE
139 edma3_drv_tci6616be_sample_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6616be_sample_EXAMPLES_RELPATH)
141 edma3_drv_c6670_sample_EXAMPLES_RELPATH = examples/edma3_driver/evm6670
142 edma3_drv_c6670_sample_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6670_sample_EXAMPLES_RELPATH)
144 edma3_drv_c6670be_sample_EXAMPLES_RELPATH = examples/edma3_driver/evm6670BE
145 edma3_drv_c6670be_sample_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6670be_sample_EXAMPLES_RELPATH)
147 edma3_drv_c6678_sample_EXAMPLES_RELPATH = examples/edma3_driver/evm6678
148 edma3_drv_c6678_sample_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6678_sample_EXAMPLES_RELPATH)
150 edma3_drv_c6678be_sample_EXAMPLES_RELPATH = examples/edma3_driver/evm6678BE
151 edma3_drv_c6678be_sample_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6678be_sample_EXAMPLES_RELPATH)
152 # Nothing beyond this point