Merged from master, added a15 support for k2l, c66ak2e
[keystone-rtos/edma3_lld.git] / packages / component.mk
1 # File: component.mk
2 #       This file is component include make file of OMX.
4 # List of variables set in this file and their purpose:
5 # <mod>_RELPATH        - This is the relative path of the module, typically from
6 #                        top-level directory of the package
7 # <mod>_PATH           - This is the absolute path of the module. It derives from
8 #                        absolute path of the top-level directory (set in env.mk)
9 #                        and relative path set above
10 # <mod>_INCLUDE        - This is the path that has interface header files of the
11 #                        module. This can be multiple directories (space separated)
12 # <mod>_PKG_LIST       - Names of the modules (and sub-modules) that are a part
13 #                        part of this module, including itself.
14 # <mod>_PLATFORM_DEPENDENCY - "yes": means the code for this module depends on 
15 #                             platform and the compiled obj/lib has to be kept
16 #                             under <platform> directory
17 #                             "no" or "" or if this variable is not defined: means
18 #                             this module has no platform dependent code and hence
19 #                             the obj/libs are not kept under <platform> dir.
20 # <mod>_CORE_DEPENDENCY     - "yes": means the code for this module depends on 
21 #                             core and the compiled obj/lib has to be kept
22 #                             under <core> directory
23 #                             "no" or "" or if this variable is not defined: means
24 #                             this module has no core dependent code and hence
25 #                             the obj/libs are not kept under <core> dir.
26 # <mod>_APP_STAGE_FILES     - List of source files that belongs to the module
27 #                             <mod>, but that needs to be compiled at application
28 #                             build stage (in the context of the app). This is
29 #                             primarily for link time configurations or if the
30 #                             source file is dependent on options/defines that are
31 #                             application dependent. This can be left blank or
32 #                             not defined at all, in which case, it means there
33 #                             no source files in the module <mod> that are required
34 #                             to be compiled in the application build stage.
35 #
37 # List of modules under EDMA3 LLD
38 edma3_lld_COMP_LIST_c6xdsp = edma3_lld_rm edma3_lld_drv
40 # List of examples under EDMA3 LLD
41 edma3_lld_EXAMPLES_LIST = edma3_drv_ti816x-evm_m3_example edma3_drv_c6472-evm_64p_example edma3_drv_c6472-evm_64p_be_example edma3_drv_c6748-evm_674_example \
42                           edma3_drv_da830-evm_674_example edma3_drv_omapl138-evm_674_example \
43                           edma3_drv_tci6486-evm_64p_example edma3_drv_tci6486-evm_64p_be_example edma3_drv_ti816x-evm_674_example \
44                           edma3_drv_ti816x_sim_sample  \
45                           edma3_drv_ti814x-evm_674_example edma3_drv_ti814x-evm_a8_example \
46                           edma3_drv_tci6608-sim_66_example edma3_drv_tci6608-sim_66_be_example  \
47                           edma3_drv_tci6616-sim_66_example edma3_drv_tci6616-sim_66_be_example  \
48                           edma3_drv_tci6614-sim_66_example edma3_drv_tci6614-sim_66_be_example  \
49                           edma3_drv_c6657-sim_66_example edma3_drv_c6657-sim_66_be_example  \
50                           edma3_drv_tci6638k2k-sim_66_example edma3_drv_tci6638k2k-sim_66_be_example  \
51                           edma3_drv_c6670-evm_66_example edma3_drv_c6670-evm_66_be_example  \
52                           edma3_drv_c6678-evm_66_example edma3_drv_c6678-evm_66_be_example  \
53                           edma3_drv_tci6614-evm_66_example edma3_drv_tci6614-evm_66_be_example  \
54                           edma3_drv_c6657-evm_66_example edma3_drv_c6657-evm_66_be_example  \
55                           edma3_drv_c66ak2e-evm_66_example edma3_drv_c66ak2e-evm_66_be_example  \
56                           edma3_drv_tci6638k2k-evm_66_example edma3_drv_tci6638k2k-evm_66_be_example  \
57                           edma3_drv_tci6630k2l-evm_66_example edma3_drv_tci6630k2l-evm_66_be_example  \
58                           edma3_drv_tci6636k2h-evm_66_example edma3_drv_tci6636k2h-evm_66_be_example  \
59                           edma3_drv_tci6638k2k-evm_a15_example \
60                           edma3_drv_tci6636k2h-evm_a15_example \
61                           edma3_drv_omapl138-evm_arm9_example edma3_drv_omap4-evm_64t_example
63 # List of libraries
67 ifeq ($(PLATFORM),)
68 PLATFORM = tda2xx-evm ti816x-evm ti814x-evm c6a811x-evm c6472-evm c6670-evm c6678-evm c6748-evm da830-evm omapl138-evm tci6486-evm tci6608-sim tci6616-sim tci6614-evm tci6614-sim c6657-evm c66ak2e-evm c6657-sim tci6638k2k-evm tci6630k2l-evm tci6638k2k-sim tci6636k2h-evm
69 endif
71 ifeq ($(TARGET),)
72 TARGET = 674 m3 a8 64p 66 m4 a15 eve
73 edma3_lld_LIBS_ALL = edma3_lld_rm_generic
74 endif
76 #Prepare library list to build from the PLATFORM and TARGET
77 ifeq ($(PLATFORM),generic)
78 edma3_lld_LIBS_ALL = edma3_lld_rm_generic
79 else
80 edma3_lld_LIBS_ALL += $(foreach plat, $(PLATFORM),$(foreach targ,$(TARGET),edma3_lld_$(plat)_$(targ)_libs))
81 endif
83 #Prepare Example list from PLATFORM and TARGET
84 ifeq ($(ENDIAN),big)
85 edma3_lld_EXAMPLES_LIST = $(foreach plat, $(PLATFORM),$(foreach targ,$(TARGET),edma3_drv_$(plat)_$(targ)_be_example))
86 else
87 edma3_lld_EXAMPLES_LIST = $(foreach plat, $(PLATFORM),$(foreach targ,$(TARGET),edma3_drv_$(plat)_$(targ)_example))
88 endif
91 # EDMA3 LLD RM - Resource manager
92 edma3_lld_rm_RELPATH = ti/sdo/edma3/rm
93 edma3_lld_rm_PATH = $(edma3_lld_PATH)/packages/$(edma3_lld_rm_RELPATH)
94 edma3_lld_rm_INCLUDE = $(edma3_lld_rm_PATH) $(edma3_lld_rm_PATH)/src
95 edma3_lld_rm_PKG_LIST = edma3_lld_rm edma3_lld_rm_sample
96 edma3_lld_rm_PLATFORM_DEPENDENCY = yes
98 edma3_lld_rm_sample_RELPATH = ti/sdo/edma3/rm/sample
99 edma3_lld_rm_sample_PATH = $(edma3_lld_PATH)/packages/$(edma3_lld_rm_sample_RELPATH)
100 edma3_lld_rm_sample_INCLUDE = $(edma3_lld_rm_sample_PATH) $(edma3_lld_rm_sample_PATH)/src
101 edma3_lld_rm_sample_PLATFORM_DEPENDENCY = yes
103 # EDMA3 LLD DRV - Driver
104 edma3_lld_drv_RELPATH = ti/sdo/edma3/drv
105 edma3_lld_drv_PATH = $(edma3_lld_PATH)/packages/$(edma3_lld_drv_RELPATH)
106 edma3_lld_drv_INCLUDE = $(edma3_lld_drv_PATH) $(edma3_lld_drv_PATH)/src
107 edma3_lld_drv_PKG_LIST = edma3_lld_drv edma3_lld_drv_sample
108 edma3_lld_drv_PLATFORM_DEPENDENCY = no
110 edma3_lld_drv_sample_RELPATH = ti/sdo/edma3/drv/sample
111 edma3_lld_drv_sample_PATH = $(edma3_lld_PATH)/packages/$(edma3_lld_drv_sample_RELPATH)
112 edma3_lld_drv_sample_INCLUDE = $(edma3_lld_drv_sample_PATH) $(edma3_lld_drv_sample_PATH)/src
113 edma3_lld_drv_sample_PLATFORM_DEPENDENCY = yes
115 # EDMA3 LLD top level
116 edma3_lld_INCLUDE = $(edma3_lld_PATH)/packages $(edma3_lld_rm_INCLUDE) $(edma3_lld_drv_INCLUDE) \
117                     $(edma3_lld_rm_sample_INCLUDE) $(edma3_lld_drv_sample_INCLUDE)
119 # EDMA3 LLD examples
120 edma3_drv_c6472-evm_64p_example_EXAMPLES_RELPATH = examples/edma3_driver/evm6472
121 edma3_drv_c6472-evm_64p_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6472-evm_64p_example_EXAMPLES_RELPATH)
123 edma3_drv_c6472-evm_64p_be_example_EXAMPLES_RELPATH = examples/edma3_driver/evm6472BE
124 edma3_drv_c6472-evm_64p_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6472-evm_64p_be_example_EXAMPLES_RELPATH)
126 edma3_drv_c6748-evm_674_example_EXAMPLES_RELPATH = examples/edma3_driver/evm6748
127 edma3_drv_c6748-evm_674_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6748-evm_674_example_EXAMPLES_RELPATH)
129 edma3_drv_da830-evm_674_example_EXAMPLES_RELPATH = examples/edma3_driver/evmDA830
130 edma3_drv_da830-evm_674_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_da830-evm_674_example_EXAMPLES_RELPATH)
132 edma3_drv_omapl138-evm_674_example_EXAMPLES_RELPATH = examples/edma3_driver/evmOMAPL138
133 edma3_drv_omapl138-evm_674_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_omapl138-evm_674_example_EXAMPLES_RELPATH)
135 edma3_drv_omap4-evm_64t_example_EXAMPLES_RELPATH = examples/edma3_driver/evmOMAP4
136 edma3_drv_omap4-evm_64t_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_omap4-evm_64t_example_EXAMPLES_RELPATH)
138 edma3_drv_omapl138-evm_arm9_example_EXAMPLES_RELPATH = examples/edma3_driver/evmOMAPL138_ARM
139 edma3_drv_omapl138-evm_arm9_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_omapl138-evm_arm9_example_EXAMPLES_RELPATH)
141 edma3_drv_tci6486-evm_64p_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTCI6486
142 edma3_drv_tci6486-evm_64p_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6486-evm_64p_example_EXAMPLES_RELPATH)
144 edma3_drv_tci6486-evm_64p_be_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTCI6486BE
145 edma3_drv_tci6486-evm_64p_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6486-evm_64p_be_example_EXAMPLES_RELPATH)
147 edma3_drv_ti814x-evm_674_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTI814x
148 edma3_drv_ti814x-evm_674_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_ti814x-evm_674_example_EXAMPLES_RELPATH)
150 edma3_drv_ti814x-evm_a8_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTI814x_A8
151 edma3_drv_ti814x-evm_a8_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_ti814x-evm_a8_example_EXAMPLES_RELPATH)
153 edma3_drv_ti814x-evm_m3_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTI814x_M3
154 edma3_drv_ti814x-evm_m3_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_ti814x-evm_m3_example_EXAMPLES_RELPATH)
156 edma3_drv_ti816x-evm_674_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTI816x
157 edma3_drv_ti816x-evm_674_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_ti816x-evm_674_example_EXAMPLES_RELPATH)
159 edma3_drv_ti816x-evm_a8_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTI816x_A8
160 edma3_drv_ti816x-evm_a8_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_ti816x-evm_a8_example_EXAMPLES_RELPATH)
162 edma3_drv_ti816x-evm_m3_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTI816x_M3
163 edma3_drv_ti816x-evm_m3_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_ti816x-evm_m3_example_EXAMPLES_RELPATH)
165 edma3_drv_c6a811x-evm_674_example_EXAMPLES_RELPATH = examples/edma3_driver/evmC6A811x
166 edma3_drv_c6a811x-evm_674_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6a811x-evm_674_example_EXAMPLES_RELPATH)
168 edma3_drv_c6a811x-evm_a8_example_EXAMPLES_RELPATH = examples/edma3_driver/evmC6A811x_A8
169 edma3_drv_c6a811x-evm_a8_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6a811x-evm_a8_example_EXAMPLES_RELPATH)
171 edma3_drv_c6a811x-evm_m3_example_EXAMPLES_RELPATH = examples/edma3_driver/evmC6A811x_M3
172 edma3_drv_c6a811x-evm_m3_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6a811x-evm_m3_example_EXAMPLES_RELPATH)
174 edma3_drv_tci6608-sim_66_example_EXAMPLES_RELPATH = examples/edma3_driver/simTCI6608
175 edma3_drv_tci6608-sim_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6608-sim_66_example_EXAMPLES_RELPATH)
177 edma3_drv_tci6608-sim_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/simTCI6608BE
178 edma3_drv_tci6608-sim_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6608-sim_66_be_example_EXAMPLES_RELPATH)
180 edma3_drv_tci6616-sim_66_example_EXAMPLES_RELPATH = examples/edma3_driver/simTCI6616
181 edma3_drv_tci6616-sim_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6616-sim_66_example_EXAMPLES_RELPATH)
183 edma3_drv_tci6616-sim_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/simTCI6616BE
184 edma3_drv_tci6616-sim_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6616-sim_66_be_example_EXAMPLES_RELPATH)
186 edma3_drv_tci6614-sim_66_example_EXAMPLES_RELPATH = examples/edma3_driver/simTCI6614
187 edma3_drv_tci6614-sim_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6614-sim_66_example_EXAMPLES_RELPATH)
189 edma3_drv_tci6614-sim_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/simTCI6614BE
190 edma3_drv_tci6614-sim_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6614-sim_66_be_example_EXAMPLES_RELPATH)
192 edma3_drv_c6657-sim_66_example_EXAMPLES_RELPATH = examples/edma3_driver/simC6657
193 edma3_drv_c6657-sim_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6657-sim_66_example_EXAMPLES_RELPATH)
195 edma3_drv_c6657-sim_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/simC6657BE
196 edma3_drv_c6657-sim_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6657-sim_66_be_example_EXAMPLES_RELPATH)
198 edma3_drv_tci6638k2k-sim_66_example_EXAMPLES_RELPATH = examples/edma3_driver/simTCI6638K2K
199 edma3_drv_tci6638k2k-sim_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6638k2k-sim_66_example_EXAMPLES_RELPATH)
201 edma3_drv_tci6638k2k-sim_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/simTCI6638K2KBE
202 edma3_drv_tci6638k2k-sim_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6638k2k-sim_66_be_example_EXAMPLES_RELPATH)
204 edma3_drv_c6670-evm_66_example_EXAMPLES_RELPATH = examples/edma3_driver/evm6670
205 edma3_drv_c6670-evm_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6670-evm_66_example_EXAMPLES_RELPATH)
207 edma3_drv_c6670-evm_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/evm6670BE
208 edma3_drv_c6670-evm_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6670-evm_66_be_example_EXAMPLES_RELPATH)
210 edma3_drv_c6678-evm_66_example_EXAMPLES_RELPATH = examples/edma3_driver/evm6678
211 edma3_drv_c6678-evm_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6678-evm_66_example_EXAMPLES_RELPATH)
213 edma3_drv_c6678-evm_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/evm6678BE
214 edma3_drv_c6678-evm_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6678-evm_66_be_example_EXAMPLES_RELPATH)
216 edma3_drv_c66ak2e-evm_66_example_EXAMPLES_RELPATH = examples/edma3_driver/evmC66AK2E
217 edma3_drv_c66ak2e-evm_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c66ak2e-evm_66_example_EXAMPLES_RELPATH)
218 edma3_drv_c66ak2e-evm_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/evmC66AK2EBE
219 edma3_drv_c66ak2e-evm_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c66ak2e-evm_66_be_example_EXAMPLES_RELPATH)
221 edma3_drv_tci6614-evm_66_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTCI6614
222 edma3_drv_tci6614-evm_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6614-evm_66_example_EXAMPLES_RELPATH)
224 edma3_drv_tci6614-evm_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTCI6614BE
225 edma3_drv_tci6614-evm_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6614-evm_66_be_example_EXAMPLES_RELPATH)
227 edma3_drv_c6657-evm_66_example_EXAMPLES_RELPATH = examples/edma3_driver/evm6657
228 edma3_drv_c6657-evm_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6657-evm_66_example_EXAMPLES_RELPATH)
230 edma3_drv_c6657-evm_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/evm6657BE
231 edma3_drv_c6657-evm_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6657-evm_66_be_example_EXAMPLES_RELPATH)
233 edma3_drv_tci6638k2k-evm_66_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTCI6638K2K
234 edma3_drv_tci6638k2k-evm_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6638k2k-evm_66_example_EXAMPLES_RELPATH)
236 edma3_drv_tci6638k2k-evm_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTCI6638K2KBE
237 edma3_drv_tci6638k2k-evm_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6638k2k-evm_66_be_example_EXAMPLES_RELPATH)
239 edma3_drv_tci6630k2l-evm_66_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTCI6630K2L
240 edma3_drv_tci6630k2l-evm_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6630k2l-evm_66_example_EXAMPLES_RELPATH)
242 edma3_drv_tci6630k2l-evm_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTCI6630K2LBE
243 edma3_drv_tci6630k2l-evm_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6630k2l-evm_66_be_example_EXAMPLES_RELPATH)
245 edma3_drv_tci6636k2h-evm_66_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTCI6636K2H
246 edma3_drv_tci6636k2h-evm_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6636k2h-evm_66_example_EXAMPLES_RELPATH)
248 edma3_drv_tci6636k2h-evm_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTCI6636K2HBE
249 edma3_drv_tci6636k2h-evm_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6636k2h-evm_66_be_example_EXAMPLES_RELPATH)
251 edma3_drv_tda2xx-evm_m4_example_EXAMPLES_RELPATH = examples/edma3_driver/evmtda2xx_M4
252 edma3_drv_tda2xx-evm_m4_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tda2xx-evm_m4_example_EXAMPLES_RELPATH)
254 edma3_drv_tda2xx-evm_a15_example_EXAMPLES_RELPATH = examples/edma3_driver/evmtda2xx_A15
255 edma3_drv_tda2xx-evm_a15_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tda2xx-evm_a15_example_EXAMPLES_RELPATH)
257 edma3_drv_tda2xx-evm_66_example_EXAMPLES_RELPATH = examples/edma3_driver/evmtda2xx
258 edma3_drv_tda2xx-evm_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tda2xx-evm_66_example_EXAMPLES_RELPATH)
260 edma3_drv_tci6636k2h-evm_a15_example_EXAMPLES_RELPATH = examples/edma3_user_space_driver/evmTCI6636K2H
261 edma3_drv_tci6636k2h-evm_a15_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6636k2h-evm_a15_example_EXAMPLES_RELPATH)
263 edma3_drv_tci6638k2k-evm_a15_example_EXAMPLES_RELPATH = examples/edma3_user_space_driver/evmTCI6638K2K
264 edma3_drv_tci6638k2k-evm_a15_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6638k2k-evm_a15_example_EXAMPLES_RELPATH)
266 edma3_drv_c66ak2e-evm_a15_example_EXAMPLES_RELPATH = examples/edma3_user_space_driver/evmC66AK2E
267 edma3_drv_c66ak2e-evm_a15_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c66ak2e-evm_a15_example_EXAMPLES_RELPATH)
269 edma3_drv_tci6630k2l-evm_a15_example_EXAMPLES_RELPATH = examples/edma3_user_space_driver/evmTCI6630K2L
270 edma3_drv_tci6630k2l-evm_a15_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6630k2l-evm_a15_example_EXAMPLES_RELPATH)
272 edma3_drv_tda2xx-evm_eve_example_EXAMPLES_RELPATH = examples/edma3_driver/evmtda2xx_EVE
273 edma3_drv_tda2xx-evm_eve_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tda2xx-evm_eve_example_EXAMPLES_RELPATH)
275 # Nothing beyond this point