Documentation changes for version 02.11.02.04
[keystone-rtos/edma3_lld.git] / packages / ti / sdo / edma3 / drv / docs / EDMA3_Driver_Doxygen.cfg
1 # Doxyfile 1.6.1
3 # This file describes the settings to be used by the documentation system
4 # doxygen (www.doxygen.org) for a project
5 #
6 # All text after a hash (#) is considered a comment and will be ignored
7 # The format is:
8 #       TAG = value [value, ...]
9 # For lists items can also be appended using:
10 #       TAG += value [value, ...]
11 # Values that contain spaces should be placed between quotes (" ")
13 #---------------------------------------------------------------------------
14 # Project related configuration options
15 #---------------------------------------------------------------------------
17 # This tag specifies the encoding used for all characters in the config file 
18 # that follow. The default is UTF-8 which is also the encoding used for all 
19 # text before the first occurrence of this tag. Doxygen uses libiconv (or the 
20 # iconv built into libc) for the transcoding. See 
21 # http://www.gnu.org/software/libiconv for the list of possible encodings.
23 DOXYFILE_ENCODING      = UTF-8
25 # The PROJECT_NAME tag is a single word (or a sequence of words surrounded 
26 # by quotes) that should identify the project.
28 PROJECT_NAME           = "EDMA3 Driver"
30 # The PROJECT_NUMBER tag can be used to enter a project or revision number. 
31 # This could be handy for archiving the generated documentation or 
32 # if some version control system is used.
34 PROJECT_NUMBER         = 02.11.02
36 # The OUTPUT_DIRECTORY tag is used to specify the (relative or absolute) 
37 # base path where the generated documentation will be put. 
38 # If a relative path is entered, it will be relative to the location 
39 # where doxygen was started. If left blank the current directory will be used.
41 OUTPUT_DIRECTORY       = .
43 # If the CREATE_SUBDIRS tag is set to YES, then doxygen will create 
44 # 4096 sub-directories (in 2 levels) under the output directory of each output 
45 # format and will distribute the generated files over these directories. 
46 # Enabling this option can be useful when feeding doxygen a huge amount of 
47 # source files, where putting all generated files in the same directory would 
48 # otherwise cause performance problems for the file system.
50 CREATE_SUBDIRS         = NO
52 # The OUTPUT_LANGUAGE tag is used to specify the language in which all 
53 # documentation generated by doxygen is written. Doxygen will use this 
54 # information to generate all constant output in the proper language. 
55 # The default language is English, other supported languages are: 
56 # Afrikaans, Arabic, Brazilian, Catalan, Chinese, Chinese-Traditional, 
57 # Croatian, Czech, Danish, Dutch, Esperanto, Farsi, Finnish, French, German, 
58 # Greek, Hungarian, Italian, Japanese, Japanese-en (Japanese with English 
59 # messages), Korean, Korean-en, Lithuanian, Norwegian, Macedonian, Persian, 
60 # Polish, Portuguese, Romanian, Russian, Serbian, Serbian-Cyrilic, Slovak, 
61 # Slovene, Spanish, Swedish, Ukrainian, and Vietnamese.
63 OUTPUT_LANGUAGE        = English
65 # If the BRIEF_MEMBER_DESC tag is set to YES (the default) Doxygen will 
66 # include brief member descriptions after the members that are listed in 
67 # the file and class documentation (similar to JavaDoc). 
68 # Set to NO to disable this.
70 BRIEF_MEMBER_DESC      = YES
72 # If the REPEAT_BRIEF tag is set to YES (the default) Doxygen will prepend 
73 # the brief description of a member or function before the detailed description. 
74 # Note: if both HIDE_UNDOC_MEMBERS and BRIEF_MEMBER_DESC are set to NO, the 
75 # brief descriptions will be completely suppressed.
77 REPEAT_BRIEF           = YES
79 # This tag implements a quasi-intelligent brief description abbreviator 
80 # that is used to form the text in various listings. Each string 
81 # in this list, if found as the leading text of the brief description, will be 
82 # stripped from the text and the result after processing the whole list, is 
83 # used as the annotated text. Otherwise, the brief description is used as-is. 
84 # If left blank, the following values are used ("$name" is automatically 
85 # replaced with the name of the entity): "The $name class" "The $name widget" 
86 # "The $name file" "is" "provides" "specifies" "contains" 
87 # "represents" "a" "an" "the"
89 ABBREVIATE_BRIEF       = 
91 # If the ALWAYS_DETAILED_SEC and REPEAT_BRIEF tags are both set to YES then 
92 # Doxygen will generate a detailed section even if there is only a brief 
93 # description.
95 ALWAYS_DETAILED_SEC    = NO
97 # If the INLINE_INHERITED_MEMB tag is set to YES, doxygen will show all 
98 # inherited members of a class in the documentation of that class as if those 
99 # members were ordinary class members. Constructors, destructors and assignment 
100 # operators of the base classes will not be shown.
102 INLINE_INHERITED_MEMB  = NO
104 # If the FULL_PATH_NAMES tag is set to YES then Doxygen will prepend the full 
105 # path before files name in the file list and in the header files. If set 
106 # to NO the shortest path that makes the file name unique will be used.
108 FULL_PATH_NAMES        = NO
110 # If the FULL_PATH_NAMES tag is set to YES then the STRIP_FROM_PATH tag 
111 # can be used to strip a user-defined part of the path. Stripping is 
112 # only done if one of the specified strings matches the left-hand part of 
113 # the path. The tag can be used to show relative paths in the file list. 
114 # If left blank the directory from which doxygen is run is used as the 
115 # path to strip.
117 STRIP_FROM_PATH        = 
119 # The STRIP_FROM_INC_PATH tag can be used to strip a user-defined part of 
120 # the path mentioned in the documentation of a class, which tells 
121 # the reader which header file to include in order to use a class. 
122 # If left blank only the name of the header file containing the class 
123 # definition is used. Otherwise one should specify the include paths that 
124 # are normally passed to the compiler using the -I flag.
126 STRIP_FROM_INC_PATH    = 
128 # If the SHORT_NAMES tag is set to YES, doxygen will generate much shorter 
129 # (but less readable) file names. This can be useful is your file systems 
130 # doesn't support long names like on DOS, Mac, or CD-ROM.
132 SHORT_NAMES            = NO
134 # If the JAVADOC_AUTOBRIEF tag is set to YES then Doxygen 
135 # will interpret the first line (until the first dot) of a JavaDoc-style 
136 # comment as the brief description. If set to NO, the JavaDoc 
137 # comments will behave just like regular Qt-style comments 
138 # (thus requiring an explicit @brief command for a brief description.)
140 JAVADOC_AUTOBRIEF      = NO
142 # If the QT_AUTOBRIEF tag is set to YES then Doxygen will 
143 # interpret the first line (until the first dot) of a Qt-style 
144 # comment as the brief description. If set to NO, the comments 
145 # will behave just like regular Qt-style comments (thus requiring 
146 # an explicit \brief command for a brief description.)
148 QT_AUTOBRIEF           = NO
150 # The MULTILINE_CPP_IS_BRIEF tag can be set to YES to make Doxygen 
151 # treat a multi-line C++ special comment block (i.e. a block of //! or /// 
152 # comments) as a brief description. This used to be the default behaviour. 
153 # The new default is to treat a multi-line C++ comment block as a detailed 
154 # description. Set this tag to YES if you prefer the old behaviour instead.
156 MULTILINE_CPP_IS_BRIEF = NO
158 # If the INHERIT_DOCS tag is set to YES (the default) then an undocumented 
159 # member inherits the documentation from any documented member that it 
160 # re-implements.
162 INHERIT_DOCS           = YES
164 # If the SEPARATE_MEMBER_PAGES tag is set to YES, then doxygen will produce 
165 # a new page for each member. If set to NO, the documentation of a member will 
166 # be part of the file/class/namespace that contains it.
168 SEPARATE_MEMBER_PAGES  = NO
170 # The TAB_SIZE tag can be used to set the number of spaces in a tab. 
171 # Doxygen uses this value to replace tabs by spaces in code fragments.
173 TAB_SIZE               = 8
175 # This tag can be used to specify a number of aliases that acts 
176 # as commands in the documentation. An alias has the form "name=value". 
177 # For example adding "sideeffect=\par Side Effects:\n" will allow you to 
178 # put the command \sideeffect (or @sideeffect) in the documentation, which 
179 # will result in a user-defined paragraph with heading "Side Effects:". 
180 # You can put \n's in the value part of an alias to insert newlines.
182 ALIASES                = 
184 # Set the OPTIMIZE_OUTPUT_FOR_C tag to YES if your project consists of C 
185 # sources only. Doxygen will then generate output that is more tailored for C. 
186 # For instance, some of the names that are used will be different. The list 
187 # of all members will be omitted, etc.
189 OPTIMIZE_OUTPUT_FOR_C  = YES
191 # Set the OPTIMIZE_OUTPUT_JAVA tag to YES if your project consists of Java 
192 # sources only. Doxygen will then generate output that is more tailored for 
193 # Java. For instance, namespaces will be presented as packages, qualified 
194 # scopes will look different, etc.
196 OPTIMIZE_OUTPUT_JAVA   = NO
198 # Set the OPTIMIZE_FOR_FORTRAN tag to YES if your project consists of Fortran 
199 # sources only. Doxygen will then generate output that is more tailored for 
200 # Fortran.
202 OPTIMIZE_FOR_FORTRAN   = NO
204 # Set the OPTIMIZE_OUTPUT_VHDL tag to YES if your project consists of VHDL 
205 # sources. Doxygen will then generate output that is tailored for 
206 # VHDL.
208 OPTIMIZE_OUTPUT_VHDL   = NO
210 # Doxygen selects the parser to use depending on the extension of the files it parses. 
211 # With this tag you can assign which parser to use for a given extension. 
212 # Doxygen has a built-in mapping, but you can override or extend it using this tag. 
213 # The format is ext=language, where ext is a file extension, and language is one of 
214 # the parsers supported by doxygen: IDL, Java, Javascript, C#, C, C++, D, PHP, 
215 # Objective-C, Python, Fortran, VHDL, C, C++. For instance to make doxygen treat 
216 # .inc files as Fortran files (default is PHP), and .f files as C (default is Fortran), 
217 # use: inc=Fortran f=C. Note that for custom extensions you also need to set
218 # FILE_PATTERNS otherwise the files are not read by doxygen.
220 EXTENSION_MAPPING      = 
222 # If you use STL classes (i.e. std::string, std::vector, etc.) but do not want 
223 # to include (a tag file for) the STL sources as input, then you should 
224 # set this tag to YES in order to let doxygen match functions declarations and 
225 # definitions whose arguments contain STL classes (e.g. func(std::string); v.s. 
226 # func(std::string) {}). This also make the inheritance and collaboration 
227 # diagrams that involve STL classes more complete and accurate.
229 BUILTIN_STL_SUPPORT    = NO
231 # If you use Microsoft's C++/CLI language, you should set this option to YES to 
232 # enable parsing support.
234 CPP_CLI_SUPPORT        = NO
236 # Set the SIP_SUPPORT tag to YES if your project consists of sip sources only. 
237 # Doxygen will parse them like normal C++ but will assume all classes use public 
238 # instead of private inheritance when no explicit protection keyword is present.
240 SIP_SUPPORT            = NO
242 # For Microsoft's IDL there are propget and propput attributes to indicate getter 
243 # and setter methods for a property. Setting this option to YES (the default) 
244 # will make doxygen to replace the get and set methods by a property in the 
245 # documentation. This will only work if the methods are indeed getting or 
246 # setting a simple type. If this is not the case, or you want to show the 
247 # methods anyway, you should set this option to NO.
249 IDL_PROPERTY_SUPPORT   = YES
251 # If member grouping is used in the documentation and the DISTRIBUTE_GROUP_DOC 
252 # tag is set to YES, then doxygen will reuse the documentation of the first 
253 # member in the group (if any) for the other members of the group. By default 
254 # all members of a group must be documented explicitly.
256 DISTRIBUTE_GROUP_DOC   = NO
258 # Set the SUBGROUPING tag to YES (the default) to allow class member groups of 
259 # the same type (for instance a group of public functions) to be put as a 
260 # subgroup of that type (e.g. under the Public Functions section). Set it to 
261 # NO to prevent subgrouping. Alternatively, this can be done per class using 
262 # the \nosubgrouping command.
264 SUBGROUPING            = YES
266 # When TYPEDEF_HIDES_STRUCT is enabled, a typedef of a struct, union, or enum 
267 # is documented as struct, union, or enum with the name of the typedef. So 
268 # typedef struct TypeS {} TypeT, will appear in the documentation as a struct 
269 # with name TypeT. When disabled the typedef will appear as a member of a file, 
270 # namespace, or class. And the struct will be named TypeS. This can typically 
271 # be useful for C code in case the coding convention dictates that all compound 
272 # types are typedef'ed and only the typedef is referenced, never the tag name.
274 TYPEDEF_HIDES_STRUCT   = NO
276 # The SYMBOL_CACHE_SIZE determines the size of the internal cache use to 
277 # determine which symbols to keep in memory and which to flush to disk. 
278 # When the cache is full, less often used symbols will be written to disk. 
279 # For small to medium size projects (<1000 input files) the default value is 
280 # probably good enough. For larger projects a too small cache size can cause 
281 # doxygen to be busy swapping symbols to and from disk most of the time 
282 # causing a significant performance penality. 
283 # If the system has enough physical memory increasing the cache will improve the 
284 # performance by keeping more symbols in memory. Note that the value works on 
285 # a logarithmic scale so increasing the size by one will rougly double the 
286 # memory usage. The cache size is given by this formula: 
287 # 2^(16+SYMBOL_CACHE_SIZE). The valid range is 0..9, the default is 0, 
288 # corresponding to a cache size of 2^16 = 65536 symbols
290 SYMBOL_CACHE_SIZE      = 0
292 #---------------------------------------------------------------------------
293 # Build related configuration options
294 #---------------------------------------------------------------------------
296 # If the EXTRACT_ALL tag is set to YES doxygen will assume all entities in 
297 # documentation are documented, even if no documentation was available. 
298 # Private class members and static file members will be hidden unless 
299 # the EXTRACT_PRIVATE and EXTRACT_STATIC tags are set to YES
301 EXTRACT_ALL            = NO
303 # If the EXTRACT_PRIVATE tag is set to YES all private members of a class 
304 # will be included in the documentation.
306 EXTRACT_PRIVATE        = NO
308 # If the EXTRACT_STATIC tag is set to YES all static members of a file 
309 # will be included in the documentation.
311 EXTRACT_STATIC         = YES
313 # If the EXTRACT_LOCAL_CLASSES tag is set to YES classes (and structs) 
314 # defined locally in source files will be included in the documentation. 
315 # If set to NO only classes defined in header files are included.
317 EXTRACT_LOCAL_CLASSES  = YES
319 # This flag is only useful for Objective-C code. When set to YES local 
320 # methods, which are defined in the implementation section but not in 
321 # the interface are included in the documentation. 
322 # If set to NO (the default) only methods in the interface are included.
324 EXTRACT_LOCAL_METHODS  = NO
326 # If this flag is set to YES, the members of anonymous namespaces will be 
327 # extracted and appear in the documentation as a namespace called 
328 # 'anonymous_namespace{file}', where file will be replaced with the base 
329 # name of the file that contains the anonymous namespace. By default 
330 # anonymous namespace are hidden.
332 EXTRACT_ANON_NSPACES   = NO
334 # If the HIDE_UNDOC_MEMBERS tag is set to YES, Doxygen will hide all 
335 # undocumented members of documented classes, files or namespaces. 
336 # If set to NO (the default) these members will be included in the 
337 # various overviews, but no documentation section is generated. 
338 # This option has no effect if EXTRACT_ALL is enabled.
340 HIDE_UNDOC_MEMBERS     = YES
342 # If the HIDE_UNDOC_CLASSES tag is set to YES, Doxygen will hide all 
343 # undocumented classes that are normally visible in the class hierarchy. 
344 # If set to NO (the default) these classes will be included in the various 
345 # overviews. This option has no effect if EXTRACT_ALL is enabled.
347 HIDE_UNDOC_CLASSES     = YES
349 # If the HIDE_FRIEND_COMPOUNDS tag is set to YES, Doxygen will hide all 
350 # friend (class|struct|union) declarations. 
351 # If set to NO (the default) these declarations will be included in the 
352 # documentation.
354 HIDE_FRIEND_COMPOUNDS  = NO
356 # If the HIDE_IN_BODY_DOCS tag is set to YES, Doxygen will hide any 
357 # documentation blocks found inside the body of a function. 
358 # If set to NO (the default) these blocks will be appended to the 
359 # function's detailed documentation block.
361 HIDE_IN_BODY_DOCS      = YES
363 # The INTERNAL_DOCS tag determines if documentation 
364 # that is typed after a \internal command is included. If the tag is set 
365 # to NO (the default) then the documentation will be excluded. 
366 # Set it to YES to include the internal documentation.
368 INTERNAL_DOCS          = NO
370 # If the CASE_SENSE_NAMES tag is set to NO then Doxygen will only generate 
371 # file names in lower-case letters. If set to YES upper-case letters are also 
372 # allowed. This is useful if you have classes or files whose names only differ 
373 # in case and if your file system supports case sensitive file names. Windows 
374 # and Mac users are advised to set this option to NO.
376 CASE_SENSE_NAMES       = NO
378 # If the HIDE_SCOPE_NAMES tag is set to NO (the default) then Doxygen 
379 # will show members with their full class and namespace scopes in the 
380 # documentation. If set to YES the scope will be hidden.
382 HIDE_SCOPE_NAMES       = NO
384 # If the SHOW_INCLUDE_FILES tag is set to YES (the default) then Doxygen 
385 # will put a list of the files that are included by a file in the documentation 
386 # of that file.
388 SHOW_INCLUDE_FILES     = YES
390 # If the INLINE_INFO tag is set to YES (the default) then a tag [inline] 
391 # is inserted in the documentation for inline members.
393 INLINE_INFO            = YES
395 # If the SORT_MEMBER_DOCS tag is set to YES (the default) then doxygen 
396 # will sort the (detailed) documentation of file and class members 
397 # alphabetically by member name. If set to NO the members will appear in 
398 # declaration order.
400 SORT_MEMBER_DOCS       = NO
402 # If the SORT_BRIEF_DOCS tag is set to YES then doxygen will sort the 
403 # brief documentation of file, namespace and class members alphabetically 
404 # by member name. If set to NO (the default) the members will appear in 
405 # declaration order.
407 SORT_BRIEF_DOCS        = NO
409 # If the SORT_MEMBERS_CTORS_1ST tag is set to YES then doxygen
410 # will sort the (brief and detailed) documentation of class members so that
411 # constructors and destructors are listed first. If set to NO (the default)
412 # the constructors will appear in the respective orders defined by
413 # SORT_MEMBER_DOCS and SORT_BRIEF_DOCS.
414 # This tag will be ignored for brief docs if SORT_BRIEF_DOCS is set to NO
415 # and ignored for detailed docs if SORT_MEMBER_DOCS is set to NO.
417 SORT_MEMBERS_CTORS_1ST = NO
419 # If the SORT_GROUP_NAMES tag is set to YES then doxygen will sort the 
420 # hierarchy of group names into alphabetical order. If set to NO (the default) 
421 # the group names will appear in their defined order.
423 SORT_GROUP_NAMES       = NO
425 # If the SORT_BY_SCOPE_NAME tag is set to YES, the class list will be 
426 # sorted by fully-qualified names, including namespaces. If set to 
427 # NO (the default), the class list will be sorted only by class name, 
428 # not including the namespace part. 
429 # Note: This option is not very useful if HIDE_SCOPE_NAMES is set to YES. 
430 # Note: This option applies only to the class list, not to the 
431 # alphabetical list.
433 SORT_BY_SCOPE_NAME     = NO
435 # The GENERATE_TODOLIST tag can be used to enable (YES) or 
436 # disable (NO) the todo list. This list is created by putting \todo 
437 # commands in the documentation.
439 GENERATE_TODOLIST      = YES
441 # The GENERATE_TESTLIST tag can be used to enable (YES) or 
442 # disable (NO) the test list. This list is created by putting \test 
443 # commands in the documentation.
445 GENERATE_TESTLIST      = YES
447 # The GENERATE_BUGLIST tag can be used to enable (YES) or 
448 # disable (NO) the bug list. This list is created by putting \bug 
449 # commands in the documentation.
451 GENERATE_BUGLIST       = YES
453 # The GENERATE_DEPRECATEDLIST tag can be used to enable (YES) or 
454 # disable (NO) the deprecated list. This list is created by putting 
455 # \deprecated commands in the documentation.
457 GENERATE_DEPRECATEDLIST= YES
459 # The ENABLED_SECTIONS tag can be used to enable conditional 
460 # documentation sections, marked by \if sectionname ... \endif.
462 ENABLED_SECTIONS       = 
464 # The MAX_INITIALIZER_LINES tag determines the maximum number of lines 
465 # the initial value of a variable or define consists of for it to appear in 
466 # the documentation. If the initializer consists of more lines than specified 
467 # here it will be hidden. Use a value of 0 to hide initializers completely. 
468 # The appearance of the initializer of individual variables and defines in the 
469 # documentation can be controlled using \showinitializer or \hideinitializer 
470 # command in the documentation regardless of this setting.
472 MAX_INITIALIZER_LINES  = 30
474 # Set the SHOW_USED_FILES tag to NO to disable the list of files generated 
475 # at the bottom of the documentation of classes and structs. If set to YES the 
476 # list will mention the files that were used to generate the documentation.
478 SHOW_USED_FILES        = YES
480 # If the sources in your project are distributed over multiple directories 
481 # then setting the SHOW_DIRECTORIES tag to YES will show the directory hierarchy 
482 # in the documentation. The default is NO.
484 SHOW_DIRECTORIES       = NO
486 # Set the SHOW_FILES tag to NO to disable the generation of the Files page. 
487 # This will remove the Files entry from the Quick Index and from the 
488 # Folder Tree View (if specified). The default is YES.
490 SHOW_FILES             = YES
492 # Set the SHOW_NAMESPACES tag to NO to disable the generation of the 
493 # Namespaces page.  This will remove the Namespaces entry from the Quick Index 
494 # and from the Folder Tree View (if specified). The default is YES.
496 SHOW_NAMESPACES        = YES
498 # The FILE_VERSION_FILTER tag can be used to specify a program or script that 
499 # doxygen should invoke to get the current version for each file (typically from 
500 # the version control system). Doxygen will invoke the program by executing (via 
501 # popen()) the command <command> <input-file>, where <command> is the value of 
502 # the FILE_VERSION_FILTER tag, and <input-file> is the name of an input file 
503 # provided by doxygen. Whatever the program writes to standard output 
504 # is used as the file version. See the manual for examples.
506 FILE_VERSION_FILTER    = 
508 # The LAYOUT_FILE tag can be used to specify a layout file which will be parsed by 
509 # doxygen. The layout file controls the global structure of the generated output files 
510 # in an output format independent way. The create the layout file that represents 
511 # doxygen's defaults, run doxygen with the -l option. You can optionally specify a 
512 # file name after the option, if omitted DoxygenLayout.xml will be used as the name 
513 # of the layout file.
515 LAYOUT_FILE            = 
517 #---------------------------------------------------------------------------
518 # configuration options related to warning and progress messages
519 #---------------------------------------------------------------------------
521 # The QUIET tag can be used to turn on/off the messages that are generated 
522 # by doxygen. Possible values are YES and NO. If left blank NO is used.
524 QUIET                  = NO
526 # The WARNINGS tag can be used to turn on/off the warning messages that are 
527 # generated by doxygen. Possible values are YES and NO. If left blank 
528 # NO is used.
530 WARNINGS               = YES
532 # If WARN_IF_UNDOCUMENTED is set to YES, then doxygen will generate warnings 
533 # for undocumented members. If EXTRACT_ALL is set to YES then this flag will 
534 # automatically be disabled.
536 WARN_IF_UNDOCUMENTED   = YES
538 # If WARN_IF_DOC_ERROR is set to YES, doxygen will generate warnings for 
539 # potential errors in the documentation, such as not documenting some 
540 # parameters in a documented function, or documenting parameters that 
541 # don't exist or using markup commands wrongly.
543 WARN_IF_DOC_ERROR      = YES
545 # This WARN_NO_PARAMDOC option can be abled to get warnings for 
546 # functions that are documented, but have no documentation for their parameters 
547 # or return value. If set to NO (the default) doxygen will only warn about 
548 # wrong or incomplete parameter documentation, but not about the absence of 
549 # documentation.
551 WARN_NO_PARAMDOC       = NO
553 # The WARN_FORMAT tag determines the format of the warning messages that 
554 # doxygen can produce. The string should contain the $file, $line, and $text 
555 # tags, which will be replaced by the file and line number from which the 
556 # warning originated and the warning text. Optionally the format may contain 
557 # $version, which will be replaced by the version of the file (if it could 
558 # be obtained via FILE_VERSION_FILTER)
560 WARN_FORMAT            = "$file:$line: $text"
562 # The WARN_LOGFILE tag can be used to specify a file to which warning 
563 # and error messages should be written. If left blank the output is written 
564 # to stderr.
566 WARN_LOGFILE           = 
568 #---------------------------------------------------------------------------
569 # configuration options related to the input files
570 #---------------------------------------------------------------------------
572 # The INPUT tag can be used to specify the files and/or directories that contain 
573 # documented source files. You may enter file names like "myfile.cpp" or 
574 # directories like "/usr/src/myproject". Separate the files or directories 
575 # with spaces.
577 INPUT                  = ..\edma3_drv.h \
578                          ..\src
580 # This tag can be used to specify the character encoding of the source files 
581 # that doxygen parses. Internally doxygen uses the UTF-8 encoding, which is 
582 # also the default input encoding. Doxygen uses libiconv (or the iconv built 
583 # into libc) for the transcoding. See http://www.gnu.org/software/libiconv for 
584 # the list of possible encodings.
586 INPUT_ENCODING         = UTF-8
588 # If the value of the INPUT tag contains directories, you can use the 
589 # FILE_PATTERNS tag to specify one or more wildcard pattern (like *.cpp 
590 # and *.h) to filter out the source-files in the directories. If left 
591 # blank the following patterns are tested: 
592 # *.c *.cc *.cxx *.cpp *.c++ *.java *.ii *.ixx *.ipp *.i++ *.inl *.h *.hh *.hxx 
593 # *.hpp *.h++ *.idl *.odl *.cs *.php *.php3 *.inc *.m *.mm *.py *.f90
595 FILE_PATTERNS          = *.c \
596                          *.h
598 # The RECURSIVE tag can be used to turn specify whether or not subdirectories 
599 # should be searched for input files as well. Possible values are YES and NO. 
600 # If left blank NO is used.
602 RECURSIVE              = YES
604 # The EXCLUDE tag can be used to specify files and/or directories that should 
605 # excluded from the INPUT source files. This way you can easily exclude a 
606 # subdirectory from a directory tree whose root is specified with the INPUT tag.
608 EXCLUDE                = 
610 # The EXCLUDE_SYMLINKS tag can be used select whether or not files or 
611 # directories that are symbolic links (a Unix filesystem feature) are excluded 
612 # from the input.
614 EXCLUDE_SYMLINKS       = NO
616 # If the value of the INPUT tag contains directories, you can use the 
617 # EXCLUDE_PATTERNS tag to specify one or more wildcard patterns to exclude 
618 # certain files from those directories. Note that the wildcards are matched 
619 # against the file with absolute path, so to exclude all test directories 
620 # for example use the pattern */test/*
622 EXCLUDE_PATTERNS       = 
624 # The EXCLUDE_SYMBOLS tag can be used to specify one or more symbol names 
625 # (namespaces, classes, functions, etc.) that should be excluded from the 
626 # output. The symbol name can be a fully qualified name, a word, or if the 
627 # wildcard * is used, a substring. Examples: ANamespace, AClass, 
628 # AClass::ANamespace, ANamespace::*Test
630 EXCLUDE_SYMBOLS        = 
632 # The EXAMPLE_PATH tag can be used to specify one or more files or 
633 # directories that contain example code fragments that are included (see 
634 # the \include command).
636 EXAMPLE_PATH           = 
638 # If the value of the EXAMPLE_PATH tag contains directories, you can use the 
639 # EXAMPLE_PATTERNS tag to specify one or more wildcard pattern (like *.cpp 
640 # and *.h) to filter out the source-files in the directories. If left 
641 # blank all files are included.
643 EXAMPLE_PATTERNS       = 
645 # If the EXAMPLE_RECURSIVE tag is set to YES then subdirectories will be 
646 # searched for input files to be used with the \include or \dontinclude 
647 # commands irrespective of the value of the RECURSIVE tag. 
648 # Possible values are YES and NO. If left blank NO is used.
650 EXAMPLE_RECURSIVE      = NO
652 # The IMAGE_PATH tag can be used to specify one or more files or 
653 # directories that contain image that are included in the documentation (see 
654 # the \image command).
656 IMAGE_PATH             = 
658 # The INPUT_FILTER tag can be used to specify a program that doxygen should 
659 # invoke to filter for each input file. Doxygen will invoke the filter program 
660 # by executing (via popen()) the command <filter> <input-file>, where <filter> 
661 # is the value of the INPUT_FILTER tag, and <input-file> is the name of an 
662 # input file. Doxygen will then use the output that the filter program writes 
663 # to standard output.  If FILTER_PATTERNS is specified, this tag will be 
664 # ignored.
666 INPUT_FILTER           = 
668 # The FILTER_PATTERNS tag can be used to specify filters on a per file pattern 
669 # basis.  Doxygen will compare the file name with each pattern and apply the 
670 # filter if there is a match.  The filters are a list of the form: 
671 # pattern=filter (like *.cpp=my_cpp_filter). See INPUT_FILTER for further 
672 # info on how filters are used. If FILTER_PATTERNS is empty, INPUT_FILTER 
673 # is applied to all files.
675 FILTER_PATTERNS        = 
677 # If the FILTER_SOURCE_FILES tag is set to YES, the input filter (if set using 
678 # INPUT_FILTER) will be used to filter the input files when producing source 
679 # files to browse (i.e. when SOURCE_BROWSER is set to YES).
681 FILTER_SOURCE_FILES    = NO
683 #---------------------------------------------------------------------------
684 # configuration options related to source browsing
685 #---------------------------------------------------------------------------
687 # If the SOURCE_BROWSER tag is set to YES then a list of source files will 
688 # be generated. Documented entities will be cross-referenced with these sources. 
689 # Note: To get rid of all source code in the generated output, make sure also 
690 # VERBATIM_HEADERS is set to NO.
692 SOURCE_BROWSER         = NO
694 # Setting the INLINE_SOURCES tag to YES will include the body 
695 # of functions and classes directly in the documentation.
697 INLINE_SOURCES         = NO
699 # Setting the STRIP_CODE_COMMENTS tag to YES (the default) will instruct 
700 # doxygen to hide any special comment blocks from generated source code 
701 # fragments. Normal C and C++ comments will always remain visible.
703 STRIP_CODE_COMMENTS    = YES
705 # If the REFERENCED_BY_RELATION tag is set to YES 
706 # then for each documented function all documented 
707 # functions referencing it will be listed.
709 REFERENCED_BY_RELATION = NO
711 # If the REFERENCES_RELATION tag is set to YES 
712 # then for each documented function all documented entities 
713 # called/used by that function will be listed.
715 REFERENCES_RELATION    = NO
717 # If the REFERENCES_LINK_SOURCE tag is set to YES (the default) 
718 # and SOURCE_BROWSER tag is set to YES, then the hyperlinks from 
719 # functions in REFERENCES_RELATION and REFERENCED_BY_RELATION lists will 
720 # link to the source code.  Otherwise they will link to the documentation.
722 REFERENCES_LINK_SOURCE = YES
724 # If the USE_HTAGS tag is set to YES then the references to source code 
725 # will point to the HTML generated by the htags(1) tool instead of doxygen 
726 # built-in source browser. The htags tool is part of GNU's global source 
727 # tagging system (see http://www.gnu.org/software/global/global.html). You 
728 # will need version 4.8.6 or higher.
730 USE_HTAGS              = NO
732 # If the VERBATIM_HEADERS tag is set to YES (the default) then Doxygen 
733 # will generate a verbatim copy of the header file for each class for 
734 # which an include is specified. Set to NO to disable this.
736 VERBATIM_HEADERS       = NO
738 #---------------------------------------------------------------------------
739 # configuration options related to the alphabetical class index
740 #---------------------------------------------------------------------------
742 # If the ALPHABETICAL_INDEX tag is set to YES, an alphabetical index 
743 # of all compounds will be generated. Enable this if the project 
744 # contains a lot of classes, structs, unions or interfaces.
746 ALPHABETICAL_INDEX     = YES
748 # If the alphabetical index is enabled (see ALPHABETICAL_INDEX) then 
749 # the COLS_IN_ALPHA_INDEX tag can be used to specify the number of columns 
750 # in which this list will be split (can be a number in the range [1..20])
752 COLS_IN_ALPHA_INDEX    = 4
754 # In case all classes in a project start with a common prefix, all 
755 # classes will be put under the same header in the alphabetical index. 
756 # The IGNORE_PREFIX tag can be used to specify one or more prefixes that 
757 # should be ignored while generating the index headers.
759 IGNORE_PREFIX          = 
761 #---------------------------------------------------------------------------
762 # configuration options related to the HTML output
763 #---------------------------------------------------------------------------
765 # If the GENERATE_HTML tag is set to YES (the default) Doxygen will 
766 # generate HTML output.
768 GENERATE_HTML          = YES
770 # The HTML_OUTPUT tag is used to specify where the HTML docs will be put. 
771 # If a relative path is entered the value of OUTPUT_DIRECTORY will be 
772 # put in front of it. If left blank `html' will be used as the default path.
774 HTML_OUTPUT            = html
776 # The HTML_FILE_EXTENSION tag can be used to specify the file extension for 
777 # each generated HTML page (for example: .htm,.php,.asp). If it is left blank 
778 # doxygen will generate files with .html extension.
780 HTML_FILE_EXTENSION    = .html
782 # The HTML_HEADER tag can be used to specify a personal HTML header for 
783 # each generated HTML page. If it is left blank doxygen will generate a 
784 # standard header.
786 HTML_HEADER            = 
788 # The HTML_FOOTER tag can be used to specify a personal HTML footer for 
789 # each generated HTML page. If it is left blank doxygen will generate a 
790 # standard footer.
792 HTML_FOOTER            = 
794 # The HTML_STYLESHEET tag can be used to specify a user-defined cascading 
795 # style sheet that is used by each HTML page. It can be used to 
796 # fine-tune the look of the HTML output. If the tag is left blank doxygen 
797 # will generate a default style sheet. Note that doxygen will try to copy 
798 # the style sheet file to the HTML output directory, so don't put your own 
799 # stylesheet in the HTML output directory as well, or it will be erased!
801 HTML_STYLESHEET        = 
803 # If the HTML_ALIGN_MEMBERS tag is set to YES, the members of classes, 
804 # files or namespaces will be aligned in HTML using tables. If set to 
805 # NO a bullet list will be used.
807 HTML_ALIGN_MEMBERS     = YES
809 # If the HTML_DYNAMIC_SECTIONS tag is set to YES then the generated HTML 
810 # documentation will contain sections that can be hidden and shown after the 
811 # page has loaded. For this to work a browser that supports 
812 # JavaScript and DHTML is required (for instance Mozilla 1.0+, Firefox 
813 # Netscape 6.0+, Internet explorer 5.0+, Konqueror, or Safari).
815 HTML_DYNAMIC_SECTIONS  = NO
817 # If the GENERATE_DOCSET tag is set to YES, additional index files 
818 # will be generated that can be used as input for Apple's Xcode 3 
819 # integrated development environment, introduced with OSX 10.5 (Leopard). 
820 # To create a documentation set, doxygen will generate a Makefile in the 
821 # HTML output directory. Running make will produce the docset in that 
822 # directory and running "make install" will install the docset in 
823 # ~/Library/Developer/Shared/Documentation/DocSets so that Xcode will find 
824 # it at startup. 
825 # See http://developer.apple.com/tools/creatingdocsetswithdoxygen.html for more information.
827 GENERATE_DOCSET        = NO
829 # When GENERATE_DOCSET tag is set to YES, this tag determines the name of the 
830 # feed. A documentation feed provides an umbrella under which multiple 
831 # documentation sets from a single provider (such as a company or product suite) 
832 # can be grouped.
834 DOCSET_FEEDNAME        = "Doxygen generated docs"
836 # When GENERATE_DOCSET tag is set to YES, this tag specifies a string that 
837 # should uniquely identify the documentation set bundle. This should be a 
838 # reverse domain-name style string, e.g. com.mycompany.MyDocSet. Doxygen 
839 # will append .docset to the name.
841 DOCSET_BUNDLE_ID       = org.doxygen.Project
843 # If the GENERATE_HTMLHELP tag is set to YES, additional index files 
844 # will be generated that can be used as input for tools like the 
845 # Microsoft HTML help workshop to generate a compiled HTML help file (.chm) 
846 # of the generated HTML documentation.
848 GENERATE_HTMLHELP      = YES
850 # If the GENERATE_HTMLHELP tag is set to YES, the CHM_FILE tag can 
851 # be used to specify the file name of the resulting .chm file. You 
852 # can add a path in front of the file if the result should not be 
853 # written to the html output directory.
855 CHM_FILE               = ..\EDMA3_Driver.chm
857 # If the GENERATE_HTMLHELP tag is set to YES, the HHC_LOCATION tag can 
858 # be used to specify the location (absolute path including file name) of 
859 # the HTML help compiler (hhc.exe). If non-empty doxygen will try to run 
860 # the HTML help compiler on the generated index.hhp.
862 HHC_LOCATION           = "C:\Program Files\HTML Help Workshop\hhc.exe"
864 # If the GENERATE_HTMLHELP tag is set to YES, the GENERATE_CHI flag 
865 # controls if a separate .chi index file is generated (YES) or that 
866 # it should be included in the master .chm file (NO).
868 GENERATE_CHI           = NO
870 # If the GENERATE_HTMLHELP tag is set to YES, the CHM_INDEX_ENCODING 
871 # is used to encode HtmlHelp index (hhk), content (hhc) and project file 
872 # content.
874 CHM_INDEX_ENCODING     = 
876 # If the GENERATE_HTMLHELP tag is set to YES, the BINARY_TOC flag 
877 # controls whether a binary table of contents is generated (YES) or a 
878 # normal table of contents (NO) in the .chm file.
880 BINARY_TOC             = NO
882 # The TOC_EXPAND flag can be set to YES to add extra items for group members 
883 # to the contents of the HTML help documentation and to the tree view.
885 TOC_EXPAND             = NO
887 # If the GENERATE_QHP tag is set to YES and both QHP_NAMESPACE and QHP_VIRTUAL_FOLDER 
888 # are set, an additional index file will be generated that can be used as input for 
889 # Qt's qhelpgenerator to generate a Qt Compressed Help (.qch) of the generated 
890 # HTML documentation.
892 GENERATE_QHP           = NO
894 # If the QHG_LOCATION tag is specified, the QCH_FILE tag can 
895 # be used to specify the file name of the resulting .qch file. 
896 # The path specified is relative to the HTML output folder.
898 QCH_FILE               = 
900 # The QHP_NAMESPACE tag specifies the namespace to use when generating 
901 # Qt Help Project output. For more information please see 
902 # http://doc.trolltech.com/qthelpproject.html#namespace
904 QHP_NAMESPACE          = 
906 # The QHP_VIRTUAL_FOLDER tag specifies the namespace to use when generating 
907 # Qt Help Project output. For more information please see 
908 # http://doc.trolltech.com/qthelpproject.html#virtual-folders
910 QHP_VIRTUAL_FOLDER     = doc
912 # If QHP_CUST_FILTER_NAME is set, it specifies the name of a custom filter to add. 
913 # For more information please see 
914 # http://doc.trolltech.com/qthelpproject.html#custom-filters
916 QHP_CUST_FILTER_NAME   = 
918 # The QHP_CUST_FILT_ATTRS tag specifies the list of the attributes of the custom filter to add.For more information please see 
919 # <a href="http://doc.trolltech.com/qthelpproject.html#custom-filters">Qt Help Project / Custom Filters</a>.
921 QHP_CUST_FILTER_ATTRS  = 
923 # The QHP_SECT_FILTER_ATTRS tag specifies the list of the attributes this project's 
924 # filter section matches. 
925 # <a href="http://doc.trolltech.com/qthelpproject.html#filter-attributes">Qt Help Project / Filter Attributes</a>.
927 QHP_SECT_FILTER_ATTRS  = 
929 # If the GENERATE_QHP tag is set to YES, the QHG_LOCATION tag can 
930 # be used to specify the location of Qt's qhelpgenerator. 
931 # If non-empty doxygen will try to run qhelpgenerator on the generated 
932 # .qhp file.
934 QHG_LOCATION           = 
936 # The DISABLE_INDEX tag can be used to turn on/off the condensed index at 
937 # top of each HTML page. The value NO (the default) enables the index and 
938 # the value YES disables it.
940 DISABLE_INDEX          = NO
942 # This tag can be used to set the number of enum values (range [1..20]) 
943 # that doxygen will group on one line in the generated HTML documentation.
945 ENUM_VALUES_PER_LINE   = 1
947 # The GENERATE_TREEVIEW tag is used to specify whether a tree-like index 
948 # structure should be generated to display hierarchical information. 
949 # If the tag value is set to YES, a side panel will be generated 
950 # containing a tree-like index structure (just like the one that 
951 # is generated for HTML Help). For this to work a browser that supports 
952 # JavaScript, DHTML, CSS and frames is required (i.e. any modern browser). 
953 # Windows users are probably better off using the HTML help feature.
955 GENERATE_TREEVIEW      = NO
957 # By enabling USE_INLINE_TREES, doxygen will generate the Groups, Directories, 
958 # and Class Hierarchy pages using a tree view instead of an ordered list.
960 USE_INLINE_TREES       = NO
962 # If the treeview is enabled (see GENERATE_TREEVIEW) then this tag can be 
963 # used to set the initial width (in pixels) of the frame in which the tree 
964 # is shown.
966 TREEVIEW_WIDTH         = 250
968 # Use this tag to change the font size of Latex formulas included 
969 # as images in the HTML documentation. The default is 10. Note that 
970 # when you change the font size after a successful doxygen run you need 
971 # to manually remove any form_*.png images from the HTML output directory 
972 # to force them to be regenerated.
974 FORMULA_FONTSIZE       = 10
976 # When the SEARCHENGINE tag is enable doxygen will generate a search box
977 # for the HTML output. The underlying search engine uses javascript 
978 # and DHTML and should work on any modern browser. Note that when using
979 # HTML help (GENERATE_HTMLHELP) or Qt help (GENERATE_QHP) 
980 # there is already a search function so this one should typically 
981 # be disabled.
983 SEARCHENGINE           = NO
985 #---------------------------------------------------------------------------
986 # configuration options related to the LaTeX output
987 #---------------------------------------------------------------------------
989 # If the GENERATE_LATEX tag is set to YES (the default) Doxygen will 
990 # generate Latex output.
992 GENERATE_LATEX         = NO
994 # The LATEX_OUTPUT tag is used to specify where the LaTeX docs will be put. 
995 # If a relative path is entered the value of OUTPUT_DIRECTORY will be 
996 # put in front of it. If left blank `latex' will be used as the default path.
998 LATEX_OUTPUT           = latex
1000 # The LATEX_CMD_NAME tag can be used to specify the LaTeX command name to be 
1001 # invoked. If left blank `latex' will be used as the default command name.
1003 LATEX_CMD_NAME         = latex
1005 # The MAKEINDEX_CMD_NAME tag can be used to specify the command name to 
1006 # generate index for LaTeX. If left blank `makeindex' will be used as the 
1007 # default command name.
1009 MAKEINDEX_CMD_NAME     = makeindex
1011 # If the COMPACT_LATEX tag is set to YES Doxygen generates more compact 
1012 # LaTeX documents. This may be useful for small projects and may help to 
1013 # save some trees in general.
1015 COMPACT_LATEX          = NO
1017 # The PAPER_TYPE tag can be used to set the paper type that is used 
1018 # by the printer. Possible values are: a4, a4wide, letter, legal and 
1019 # executive. If left blank a4wide will be used.
1021 PAPER_TYPE             = a4wide
1023 # The EXTRA_PACKAGES tag can be to specify one or more names of LaTeX 
1024 # packages that should be included in the LaTeX output.
1026 EXTRA_PACKAGES         = 
1028 # The LATEX_HEADER tag can be used to specify a personal LaTeX header for 
1029 # the generated latex document. The header should contain everything until 
1030 # the first chapter. If it is left blank doxygen will generate a 
1031 # standard header. Notice: only use this tag if you know what you are doing!
1033 LATEX_HEADER           = 
1035 # If the PDF_HYPERLINKS tag is set to YES, the LaTeX that is generated 
1036 # is prepared for conversion to pdf (using ps2pdf). The pdf file will 
1037 # contain links (just like the HTML output) instead of page references 
1038 # This makes the output suitable for online browsing using a pdf viewer.
1040 PDF_HYPERLINKS         = NO
1042 # If the USE_PDFLATEX tag is set to YES, pdflatex will be used instead of 
1043 # plain latex in the generated Makefile. Set this option to YES to get a 
1044 # higher quality PDF documentation.
1046 USE_PDFLATEX           = NO
1048 # If the LATEX_BATCHMODE tag is set to YES, doxygen will add the \\batchmode. 
1049 # command to the generated LaTeX files. This will instruct LaTeX to keep 
1050 # running if errors occur, instead of asking the user for help. 
1051 # This option is also used when generating formulas in HTML.
1053 LATEX_BATCHMODE        = NO
1055 # If LATEX_HIDE_INDICES is set to YES then doxygen will not 
1056 # include the index chapters (such as File Index, Compound Index, etc.) 
1057 # in the output.
1059 LATEX_HIDE_INDICES     = NO
1061 # If LATEX_SOURCE_CODE is set to YES then doxygen will include
1062 # source code with syntax highlighting in the LaTeX output.
1063 # Note that which sources are shown also depends on other settings
1064 # such as SOURCE_BROWSER.
1066 LATEX_SOURCE_CODE      = NO
1068 #---------------------------------------------------------------------------
1069 # configuration options related to the RTF output
1070 #---------------------------------------------------------------------------
1072 # If the GENERATE_RTF tag is set to YES Doxygen will generate RTF output 
1073 # The RTF output is optimized for Word 97 and may not look very pretty with 
1074 # other RTF readers or editors.
1076 GENERATE_RTF           = NO
1078 # The RTF_OUTPUT tag is used to specify where the RTF docs will be put. 
1079 # If a relative path is entered the value of OUTPUT_DIRECTORY will be 
1080 # put in front of it. If left blank `rtf' will be used as the default path.
1082 RTF_OUTPUT             = rtf
1084 # If the COMPACT_RTF tag is set to YES Doxygen generates more compact 
1085 # RTF documents. This may be useful for small projects and may help to 
1086 # save some trees in general.
1088 COMPACT_RTF            = NO
1090 # If the RTF_HYPERLINKS tag is set to YES, the RTF that is generated 
1091 # will contain hyperlink fields. The RTF file will 
1092 # contain links (just like the HTML output) instead of page references. 
1093 # This makes the output suitable for online browsing using WORD or other 
1094 # programs which support those fields. 
1095 # Note: wordpad (write) and others do not support links.
1097 RTF_HYPERLINKS         = NO
1099 # Load stylesheet definitions from file. Syntax is similar to doxygen's 
1100 # config file, i.e. a series of assignments. You only have to provide 
1101 # replacements, missing definitions are set to their default value.
1103 RTF_STYLESHEET_FILE    = 
1105 # Set optional variables used in the generation of an rtf document. 
1106 # Syntax is similar to doxygen's config file.
1108 RTF_EXTENSIONS_FILE    = 
1110 #---------------------------------------------------------------------------
1111 # configuration options related to the man page output
1112 #---------------------------------------------------------------------------
1114 # If the GENERATE_MAN tag is set to YES (the default) Doxygen will 
1115 # generate man pages
1117 GENERATE_MAN           = NO
1119 # The MAN_OUTPUT tag is used to specify where the man pages will be put. 
1120 # If a relative path is entered the value of OUTPUT_DIRECTORY will be 
1121 # put in front of it. If left blank `man' will be used as the default path.
1123 MAN_OUTPUT             = man
1125 # The MAN_EXTENSION tag determines the extension that is added to 
1126 # the generated man pages (default is the subroutine's section .3)
1128 MAN_EXTENSION          = .3
1130 # If the MAN_LINKS tag is set to YES and Doxygen generates man output, 
1131 # then it will generate one additional man file for each entity 
1132 # documented in the real man page(s). These additional files 
1133 # only source the real man page, but without them the man command 
1134 # would be unable to find the correct page. The default is NO.
1136 MAN_LINKS              = NO
1138 #---------------------------------------------------------------------------
1139 # configuration options related to the XML output
1140 #---------------------------------------------------------------------------
1142 # If the GENERATE_XML tag is set to YES Doxygen will 
1143 # generate an XML file that captures the structure of 
1144 # the code including all documentation.
1146 GENERATE_XML           = NO
1148 # The XML_OUTPUT tag is used to specify where the XML pages will be put. 
1149 # If a relative path is entered the value of OUTPUT_DIRECTORY will be 
1150 # put in front of it. If left blank `xml' will be used as the default path.
1152 XML_OUTPUT             = xml
1154 # The XML_SCHEMA tag can be used to specify an XML schema, 
1155 # which can be used by a validating XML parser to check the 
1156 # syntax of the XML files.
1158 XML_SCHEMA             = 
1160 # The XML_DTD tag can be used to specify an XML DTD, 
1161 # which can be used by a validating XML parser to check the 
1162 # syntax of the XML files.
1164 XML_DTD                = 
1166 # If the XML_PROGRAMLISTING tag is set to YES Doxygen will 
1167 # dump the program listings (including syntax highlighting 
1168 # and cross-referencing information) to the XML output. Note that 
1169 # enabling this will significantly increase the size of the XML output.
1171 XML_PROGRAMLISTING     = YES
1173 #---------------------------------------------------------------------------
1174 # configuration options for the AutoGen Definitions output
1175 #---------------------------------------------------------------------------
1177 # If the GENERATE_AUTOGEN_DEF tag is set to YES Doxygen will 
1178 # generate an AutoGen Definitions (see autogen.sf.net) file 
1179 # that captures the structure of the code including all 
1180 # documentation. Note that this feature is still experimental 
1181 # and incomplete at the moment.
1183 GENERATE_AUTOGEN_DEF   = NO
1185 #---------------------------------------------------------------------------
1186 # configuration options related to the Perl module output
1187 #---------------------------------------------------------------------------
1189 # If the GENERATE_PERLMOD tag is set to YES Doxygen will 
1190 # generate a Perl module file that captures the structure of 
1191 # the code including all documentation. Note that this 
1192 # feature is still experimental and incomplete at the 
1193 # moment.
1195 GENERATE_PERLMOD       = NO
1197 # If the PERLMOD_LATEX tag is set to YES Doxygen will generate 
1198 # the necessary Makefile rules, Perl scripts and LaTeX code to be able 
1199 # to generate PDF and DVI output from the Perl module output.
1201 PERLMOD_LATEX          = NO
1203 # If the PERLMOD_PRETTY tag is set to YES the Perl module output will be 
1204 # nicely formatted so it can be parsed by a human reader.  This is useful 
1205 # if you want to understand what is going on.  On the other hand, if this 
1206 # tag is set to NO the size of the Perl module output will be much smaller 
1207 # and Perl will parse it just the same.
1209 PERLMOD_PRETTY         = YES
1211 # The names of the make variables in the generated doxyrules.make file 
1212 # are prefixed with the string contained in PERLMOD_MAKEVAR_PREFIX. 
1213 # This is useful so different doxyrules.make files included by the same 
1214 # Makefile don't overwrite each other's variables.
1216 PERLMOD_MAKEVAR_PREFIX = 
1218 #---------------------------------------------------------------------------
1219 # Configuration options related to the preprocessor
1220 #---------------------------------------------------------------------------
1222 # If the ENABLE_PREPROCESSING tag is set to YES (the default) Doxygen will 
1223 # evaluate all C-preprocessor directives found in the sources and include 
1224 # files.
1226 ENABLE_PREPROCESSING   = YES
1228 # If the MACRO_EXPANSION tag is set to YES Doxygen will expand all macro 
1229 # names in the source code. If set to NO (the default) only conditional 
1230 # compilation will be performed. Macro expansion can be done in a controlled 
1231 # way by setting EXPAND_ONLY_PREDEF to YES.
1233 MACRO_EXPANSION        = NO
1235 # If the EXPAND_ONLY_PREDEF and MACRO_EXPANSION tags are both set to YES 
1236 # then the macro expansion is limited to the macros specified with the 
1237 # PREDEFINED and EXPAND_AS_DEFINED tags.
1239 EXPAND_ONLY_PREDEF     = NO
1241 # If the SEARCH_INCLUDES tag is set to YES (the default) the includes files 
1242 # in the INCLUDE_PATH (see below) will be search if a #include is found.
1244 SEARCH_INCLUDES        = YES
1246 # The INCLUDE_PATH tag can be used to specify one or more directories that 
1247 # contain include files that are not input files but should be processed by 
1248 # the preprocessor.
1250 INCLUDE_PATH           = 
1252 # You can use the INCLUDE_FILE_PATTERNS tag to specify one or more wildcard 
1253 # patterns (like *.h and *.hpp) to filter out the header-files in the 
1254 # directories. If left blank, the patterns specified with FILE_PATTERNS will 
1255 # be used.
1257 INCLUDE_FILE_PATTERNS  = 
1259 # The PREDEFINED tag can be used to specify one or more macro names that 
1260 # are defined before the preprocessor is started (similar to the -D option of 
1261 # gcc). The argument of the tag is a list of macros of the form: name 
1262 # or name=definition (no spaces). If the definition and the = are 
1263 # omitted =1 is assumed. To prevent a macro definition from being 
1264 # undefined via #undef or recursively expanded use the := operator 
1265 # instead of the = operator.
1267 PREDEFINED             = 
1269 # If the MACRO_EXPANSION and EXPAND_ONLY_PREDEF tags are set to YES then 
1270 # this tag can be used to specify a list of macro names that should be expanded. 
1271 # The macro definition that is found in the sources will be used. 
1272 # Use the PREDEFINED tag if you want to use a different macro definition.
1274 EXPAND_AS_DEFINED      = 
1276 # If the SKIP_FUNCTION_MACROS tag is set to YES (the default) then 
1277 # doxygen's preprocessor will remove all function-like macros that are alone 
1278 # on a line, have an all uppercase name, and do not end with a semicolon. Such 
1279 # function macros are typically used for boiler-plate code, and will confuse 
1280 # the parser if not removed.
1282 SKIP_FUNCTION_MACROS   = YES
1284 #---------------------------------------------------------------------------
1285 # Configuration::additions related to external references
1286 #---------------------------------------------------------------------------
1288 # The TAGFILES option can be used to specify one or more tagfiles. 
1289 # Optionally an initial location of the external documentation 
1290 # can be added for each tagfile. The format of a tag file without 
1291 # this location is as follows: 
1292 #   TAGFILES = file1 file2 ... 
1293 # Adding location for the tag files is done as follows: 
1294 #   TAGFILES = file1=loc1 "file2 = loc2" ... 
1295 # where "loc1" and "loc2" can be relative or absolute paths or 
1296 # URLs. If a location is present for each tag, the installdox tool 
1297 # does not have to be run to correct the links. 
1298 # Note that each tag file must have a unique name 
1299 # (where the name does NOT include the path) 
1300 # If a tag file is not located in the directory in which doxygen 
1301 # is run, you must also specify the path to the tagfile here.
1303 TAGFILES               = 
1305 # When a file name is specified after GENERATE_TAGFILE, doxygen will create 
1306 # a tag file that is based on the input files it reads.
1308 GENERATE_TAGFILE       = 
1310 # If the ALLEXTERNALS tag is set to YES all external classes will be listed 
1311 # in the class index. If set to NO only the inherited external classes 
1312 # will be listed.
1314 ALLEXTERNALS           = NO
1316 # If the EXTERNAL_GROUPS tag is set to YES all external groups will be listed 
1317 # in the modules index. If set to NO, only the current project's groups will 
1318 # be listed.
1320 EXTERNAL_GROUPS        = YES
1322 # The PERL_PATH should be the absolute path and name of the perl script 
1323 # interpreter (i.e. the result of `which perl').
1325 PERL_PATH              = /usr/bin/perl
1327 #---------------------------------------------------------------------------
1328 # Configuration options related to the dot tool
1329 #---------------------------------------------------------------------------
1331 # If the CLASS_DIAGRAMS tag is set to YES (the default) Doxygen will 
1332 # generate a inheritance diagram (in HTML, RTF and LaTeX) for classes with base 
1333 # or super classes. Setting the tag to NO turns the diagrams off. Note that 
1334 # this option is superseded by the HAVE_DOT option below. This is only a 
1335 # fallback. It is recommended to install and use dot, since it yields more 
1336 # powerful graphs.
1338 CLASS_DIAGRAMS         = NO
1340 # You can define message sequence charts within doxygen comments using the \msc 
1341 # command. Doxygen will then run the mscgen tool (see 
1342 # http://www.mcternan.me.uk/mscgen/) to produce the chart and insert it in the 
1343 # documentation. The MSCGEN_PATH tag allows you to specify the directory where 
1344 # the mscgen tool resides. If left empty the tool is assumed to be found in the 
1345 # default search path.
1347 MSCGEN_PATH            = 
1349 # If set to YES, the inheritance and collaboration graphs will hide 
1350 # inheritance and usage relations if the target is undocumented 
1351 # or is not a class.
1353 HIDE_UNDOC_RELATIONS   = YES
1355 # If you set the HAVE_DOT tag to YES then doxygen will assume the dot tool is 
1356 # available from the path. This tool is part of Graphviz, a graph visualization 
1357 # toolkit from AT&T and Lucent Bell Labs. The other options in this section 
1358 # have no effect if this option is set to NO (the default)
1360 HAVE_DOT               = NO
1362 # By default doxygen will write a font called FreeSans.ttf to the output 
1363 # directory and reference it in all dot files that doxygen generates. This 
1364 # font does not include all possible unicode characters however, so when you need 
1365 # these (or just want a differently looking font) you can specify the font name 
1366 # using DOT_FONTNAME. You need need to make sure dot is able to find the font, 
1367 # which can be done by putting it in a standard location or by setting the 
1368 # DOTFONTPATH environment variable or by setting DOT_FONTPATH to the directory 
1369 # containing the font.
1371 DOT_FONTNAME           = FreeSans
1373 # The DOT_FONTSIZE tag can be used to set the size of the font of dot graphs. 
1374 # The default size is 10pt.
1376 DOT_FONTSIZE           = 10
1378 # By default doxygen will tell dot to use the output directory to look for the 
1379 # FreeSans.ttf font (which doxygen will put there itself). If you specify a 
1380 # different font using DOT_FONTNAME you can set the path where dot 
1381 # can find it using this tag.
1383 DOT_FONTPATH           = 
1385 # If the CLASS_GRAPH and HAVE_DOT tags are set to YES then doxygen 
1386 # will generate a graph for each documented class showing the direct and 
1387 # indirect inheritance relations. Setting this tag to YES will force the 
1388 # the CLASS_DIAGRAMS tag to NO.
1390 CLASS_GRAPH            = YES
1392 # If the COLLABORATION_GRAPH and HAVE_DOT tags are set to YES then doxygen 
1393 # will generate a graph for each documented class showing the direct and 
1394 # indirect implementation dependencies (inheritance, containment, and 
1395 # class references variables) of the class with other documented classes.
1397 COLLABORATION_GRAPH    = YES
1399 # If the GROUP_GRAPHS and HAVE_DOT tags are set to YES then doxygen 
1400 # will generate a graph for groups, showing the direct groups dependencies
1402 GROUP_GRAPHS           = YES
1404 # If the UML_LOOK tag is set to YES doxygen will generate inheritance and 
1405 # collaboration diagrams in a style similar to the OMG's Unified Modeling 
1406 # Language.
1408 UML_LOOK               = NO
1410 # If set to YES, the inheritance and collaboration graphs will show the 
1411 # relations between templates and their instances.
1413 TEMPLATE_RELATIONS     = NO
1415 # If the ENABLE_PREPROCESSING, SEARCH_INCLUDES, INCLUDE_GRAPH, and HAVE_DOT 
1416 # tags are set to YES then doxygen will generate a graph for each documented 
1417 # file showing the direct and indirect include dependencies of the file with 
1418 # other documented files.
1420 INCLUDE_GRAPH          = YES
1422 # If the ENABLE_PREPROCESSING, SEARCH_INCLUDES, INCLUDED_BY_GRAPH, and 
1423 # HAVE_DOT tags are set to YES then doxygen will generate a graph for each 
1424 # documented header file showing the documented files that directly or 
1425 # indirectly include this file.
1427 INCLUDED_BY_GRAPH      = YES
1429 # If the CALL_GRAPH and HAVE_DOT options are set to YES then 
1430 # doxygen will generate a call dependency graph for every global function 
1431 # or class method. Note that enabling this option will significantly increase 
1432 # the time of a run. So in most cases it will be better to enable call graphs 
1433 # for selected functions only using the \callgraph command.
1435 CALL_GRAPH             = NO
1437 # If the CALLER_GRAPH and HAVE_DOT tags are set to YES then 
1438 # doxygen will generate a caller dependency graph for every global function 
1439 # or class method. Note that enabling this option will significantly increase 
1440 # the time of a run. So in most cases it will be better to enable caller 
1441 # graphs for selected functions only using the \callergraph command.
1443 CALLER_GRAPH           = NO
1445 # If the GRAPHICAL_HIERARCHY and HAVE_DOT tags are set to YES then doxygen 
1446 # will graphical hierarchy of all classes instead of a textual one.
1448 GRAPHICAL_HIERARCHY    = YES
1450 # If the DIRECTORY_GRAPH, SHOW_DIRECTORIES and HAVE_DOT tags are set to YES 
1451 # then doxygen will show the dependencies a directory has on other directories 
1452 # in a graphical way. The dependency relations are determined by the #include 
1453 # relations between the files in the directories.
1455 DIRECTORY_GRAPH        = YES
1457 # The DOT_IMAGE_FORMAT tag can be used to set the image format of the images 
1458 # generated by dot. Possible values are png, jpg, or gif 
1459 # If left blank png will be used.
1461 DOT_IMAGE_FORMAT       = png
1463 # The tag DOT_PATH can be used to specify the path where the dot tool can be 
1464 # found. If left blank, it is assumed the dot tool can be found in the path.
1466 DOT_PATH               = 
1468 # The DOTFILE_DIRS tag can be used to specify one or more directories that 
1469 # contain dot files that are included in the documentation (see the 
1470 # \dotfile command).
1472 DOTFILE_DIRS           = 
1474 # The DOT_GRAPH_MAX_NODES tag can be used to set the maximum number of 
1475 # nodes that will be shown in the graph. If the number of nodes in a graph 
1476 # becomes larger than this value, doxygen will truncate the graph, which is 
1477 # visualized by representing a node as a red box. Note that doxygen if the 
1478 # number of direct children of the root node in a graph is already larger than 
1479 # DOT_GRAPH_MAX_NODES then the graph will not be shown at all. Also note 
1480 # that the size of a graph can be further restricted by MAX_DOT_GRAPH_DEPTH.
1482 DOT_GRAPH_MAX_NODES    = 50
1484 # The MAX_DOT_GRAPH_DEPTH tag can be used to set the maximum depth of the 
1485 # graphs generated by dot. A depth value of 3 means that only nodes reachable 
1486 # from the root by following a path via at most 3 edges will be shown. Nodes 
1487 # that lay further from the root node will be omitted. Note that setting this 
1488 # option to 1 or 2 may greatly reduce the computation time needed for large 
1489 # code bases. Also note that the size of a graph can be further restricted by 
1490 # DOT_GRAPH_MAX_NODES. Using a depth of 0 means no depth restriction.
1492 MAX_DOT_GRAPH_DEPTH    = 0
1494 # Set the DOT_TRANSPARENT tag to YES to generate images with a transparent 
1495 # background. This is disabled by default, because dot on Windows does not 
1496 # seem to support this out of the box. Warning: Depending on the platform used, 
1497 # enabling this option may lead to badly anti-aliased labels on the edges of 
1498 # a graph (i.e. they become hard to read).
1500 DOT_TRANSPARENT        = NO
1502 # Set the DOT_MULTI_TARGETS tag to YES allow dot to generate multiple output 
1503 # files in one run (i.e. multiple -o and -T options on the command line). This 
1504 # makes dot run faster, but since only newer versions of dot (>1.8.10) 
1505 # support this, this feature is disabled by default.
1507 DOT_MULTI_TARGETS      = NO
1509 # If the GENERATE_LEGEND tag is set to YES (the default) Doxygen will 
1510 # generate a legend page explaining the meaning of the various boxes and 
1511 # arrows in the dot generated graphs.
1513 GENERATE_LEGEND        = YES
1515 # If the DOT_CLEANUP tag is set to YES (the default) Doxygen will 
1516 # remove the intermediate dot files that are used to generate 
1517 # the various graphs.
1519 DOT_CLEANUP            = YES