Moved SoC specific config files in rm/src/configs
[keystone-rtos/edma3_lld.git] / packages / ti / sdo / edma3 / drv / sample / src / sample_cs.c
1 /*
2  * bios6_edma3_drv_sample_cs.c
3  *
4  * Sample functions showing the implementation of critical section entry/exit
5  * routines and various semaphore related routines (all BIOS6 depenedent).
6  * These implementations MUST be provided by the user / application, using the
7  * EDMA3 driver, for its correct functioning.
8  *
9  * Copyright (C) 2009 Texas Instruments Incorporated - http://www.ti.com/
10  *
11  *
12  *  Redistribution and use in source and binary forms, with or without
13  *  modification, are permitted provided that the following conditions
14  *  are met:
15  *
16  *    Redistributions of source code must retain the above copyright
17  *    notice, this list of conditions and the following disclaimer.
18  *
19  *    Redistributions in binary form must reproduce the above copyright
20  *    notice, this list of conditions and the following disclaimer in the
21  *    documentation and/or other materials provided with the
22  *    distribution.
23  *
24  *    Neither the name of Texas Instruments Incorporated nor the names of
25  *    its contributors may be used to endorse or promote products derived
26  *    from this software without specific prior written permission.
27  *
28  *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
29  *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
30  *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
31  *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
32  *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
33  *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
34  *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
35  *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
36  *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
37  *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
38  *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
39  *
40 */
42 #include <ti/sysbios/family/c64p/EventCombiner.h>
43 #include <ti/sysbios/hal/Cache.h>
44 #include <ti/sysbios/hal/Hwi.h>
45 #include <ti/sysbios/knl/Task.h>
46 #include <ti/sysbios/ipc/Semaphore.h>
48 #include <ti/sdo/edma3/drv/sample/bios6_edma3_drv_sample.h>
50 extern unsigned int ccXferCompInt[][EDMA3_MAX_REGIONS];
51 extern unsigned int ccErrorInt[];
52 extern unsigned int tcErrorInt[][EDMA3_MAX_TC];
54 /**
55  * DSP instance number on which the executable is running. Its value is
56  * determined by reading the processor specific register DNUM.
57  */
58 extern unsigned int dsp_num;
60 /**
61  * \brief   EDMA3 OS Protect Entry
62  *
63  *      This function saves the current state of protection in 'intState'
64  *      variable passed by caller, if the protection level is
65  *      EDMA3_OS_PROTECT_INTERRUPT. It then applies the requested level of
66  *      protection.
67  *      For EDMA3_OS_PROTECT_INTERRUPT_XFER_COMPLETION and
68  *      EDMA3_OS_PROTECT_INTERRUPT_CC_ERROR, variable 'intState' is ignored,
69  *      and the requested interrupt is disabled.
70  *      For EDMA3_OS_PROTECT_INTERRUPT_TC_ERROR, '*intState' specifies the
71  *      Transfer Controller number whose interrupt needs to be disabled.
72  *
73  * \param   level is numeric identifier of the desired degree of protection.
74  * \param   intState is memory location where current state of protection is
75  *      saved for future use while restoring it via edma3OsProtectExit() (Only
76  *      for EDMA3_OS_PROTECT_INTERRUPT protection level).
77  * \return  None
78  */
79 void edma3OsProtectEntry (unsigned int edma3InstanceId, 
80                                                         int level, unsigned int *intState)
81     {    
82     if (((level == EDMA3_OS_PROTECT_INTERRUPT)
83         || (level == EDMA3_OS_PROTECT_INTERRUPT_TC_ERROR))
84         && (intState == NULL))
85         {
86         return;
87         }
88     else
89         {
90         switch (level)
91             {
92             /* Disable all (global) interrupts */
93             case EDMA3_OS_PROTECT_INTERRUPT :
94                 *intState = Hwi_disable();
95                 break;
97             /* Disable scheduler */
98             case EDMA3_OS_PROTECT_SCHEDULER :
99                                         Task_disable();
100                 break;
102             /* Disable EDMA3 transfer completion interrupt only */
103             case EDMA3_OS_PROTECT_INTERRUPT_XFER_COMPLETION :
104                 EventCombiner_disableEvent(ccXferCompInt[edma3InstanceId][dsp_num]);
105                 break;
107             /* Disable EDMA3 CC error interrupt only */
108             case EDMA3_OS_PROTECT_INTERRUPT_CC_ERROR :
109                 EventCombiner_disableEvent(ccErrorInt[edma3InstanceId]);
110                 break;
112             /* Disable EDMA3 TC error interrupt only */
113             case EDMA3_OS_PROTECT_INTERRUPT_TC_ERROR :
114                 switch (*intState)
115                     {
116                     case 0:
117                     case 1:
118                     case 2:
119                     case 3:
120                     case 4:
121                     case 5:
122                     case 6:
123                     case 7:
124                         /* Fall through... */
125                         /* Disable the corresponding interrupt */
126                         EventCombiner_disableEvent(tcErrorInt[edma3InstanceId][*intState]);
127                         break;
129                      default:
130                         break;
131                     }
133                 break;
135             default:
136                 break;
137             }
138         }
139     }
142 /**
143  * \brief   EDMA3 OS Protect Exit
144  *
145  *      This function undoes the protection enforced to original state
146  *      as is specified by the variable 'intState' passed, if the protection
147  *      level is EDMA3_OS_PROTECT_INTERRUPT.
148  *      For EDMA3_OS_PROTECT_INTERRUPT_XFER_COMPLETION and
149  *      EDMA3_OS_PROTECT_INTERRUPT_CC_ERROR, variable 'intState' is ignored,
150  *      and the requested interrupt is enabled.
151  *      For EDMA3_OS_PROTECT_INTERRUPT_TC_ERROR, 'intState' specifies the
152  *      Transfer Controller number whose interrupt needs to be enabled.
153  * \param   level is numeric identifier of the desired degree of protection.
154  * \param   intState is original state of protection at time when the
155  *      corresponding edma3OsProtectEntry() was called (Only
156  *      for EDMA3_OS_PROTECT_INTERRUPT protection level).
157  * \return  None
158  */
159 void edma3OsProtectExit (unsigned int edma3InstanceId,
160                         int level, unsigned int intState)
161     {
162     switch (level)
163         {
164         /* Enable all (global) interrupts */
165         case EDMA3_OS_PROTECT_INTERRUPT :
166             Hwi_restore(intState);
167             break;
169         /* Enable scheduler */
170         case EDMA3_OS_PROTECT_SCHEDULER :
171             Task_enable();
172             break;
174         /* Enable EDMA3 transfer completion interrupt only */
175         case EDMA3_OS_PROTECT_INTERRUPT_XFER_COMPLETION :
176             EventCombiner_enableEvent(ccXferCompInt[edma3InstanceId][dsp_num]);
177             break;
179         /* Enable EDMA3 CC error interrupt only */
180         case EDMA3_OS_PROTECT_INTERRUPT_CC_ERROR :
181             EventCombiner_enableEvent(ccErrorInt[edma3InstanceId]);
182             break;
184         /* Enable EDMA3 TC error interrupt only */
185         case EDMA3_OS_PROTECT_INTERRUPT_TC_ERROR :
186             switch (intState)
187                 {
188                 case 0:
189                 case 1:
190                 case 2:
191                 case 3:
192                 case 4:
193                 case 5:
194                 case 6:
195                 case 7:
196                     /* Fall through... */
197                     /* Enable the corresponding interrupt */
198                     EventCombiner_enableEvent(tcErrorInt[edma3InstanceId][intState]);
199                     break;
201                  default:
202                     break;
203                 }
205             break;
207         default:
208             break;
209         }
210     }
213 /**
214  *  \brief   EDMA3 Cache Invalidate
215  *
216  *  This function invalidates the D cache.
217  *
218  *  \param  mem_start_ptr [IN]      Starting address of memory.
219  *                                  Please note that this should be
220  *                                  aligned according to the cache line size.
221  *  \param  num_bytes [IN]          length of buffer
222  *  \return  EDMA3_DRV_SOK if success, else error code in case of error
223  *          or non-alignment of buffers.
224  *
225  * Note: This function is required if the buffer is in DDR.
226  * For other cases, where buffer is NOT in DDR, user
227  * may or may not require the below implementation and
228  * should modify it according to her need.
229  */
230 EDMA3_DRV_Result Edma3_CacheInvalidate(unsigned int mem_start_ptr,
231                            unsigned int    num_bytes)
232     {
233     EDMA3_DRV_Result cacheInvResult = EDMA3_DRV_SOK;
235     /* Verify whether the start address is cache aligned or not */
236     if((mem_start_ptr & (EDMA3_CACHE_LINE_SIZE_IN_BYTES-1u))    !=    0)
237         {
238 #ifdef EDMA3_DRV_DEBUG
239         EDMA3_DRV_PRINTF("\r\n Cache : Memory is not %d bytes alinged\r\n",
240                             EDMA3_CACHE_LINE_SIZE_IN_BYTES);
241 #endif
242         cacheInvResult = EDMA3_NON_ALIGNED_BUFFERS_ERROR;
243         }
244     else
245         {
246                 Cache_inv((Ptr)mem_start_ptr, num_bytes, Cache_Type_ALL, TRUE);
247         }
249     return cacheInvResult;
254 /**
255  * \brief   EDMA3 Cache Flush
256  *
257  *  This function flushes (cleans) the Cache
258  *
259  *  \param  mem_start_ptr [IN]      Starting address of memory.
260  *                                  Please note that this should be
261  *                                  aligned according to the cache line size.
262  *  \param  num_bytes [IN]          length of buffer
263  *  \return  EDMA3_DRV_SOK if success, else error code in case of error
264  *          or non-alignment of buffers.
265  *
266  * Note: This function is required if the buffer is in DDR.
267  * For other cases, where buffer is NOT in DDR, user
268  * may or may not require the below implementation and
269  * should modify it according to her need.
270  */
271 EDMA3_DRV_Result Edma3_CacheFlush(unsigned int mem_start_ptr,
272                       unsigned int num_bytes)
273     {
274     EDMA3_DRV_Result cacheFlushResult = EDMA3_DRV_SOK;
276     /* Verify whether the start address is cache aligned or not */
277     if((mem_start_ptr & (EDMA3_CACHE_LINE_SIZE_IN_BYTES-1u))    !=    0)
278         {
279 #ifdef EDMA3_DRV_DEBUG
280         EDMA3_DRV_PRINTF("\r\n Cache : Memory is not %d bytes alinged\r\n",
281                             EDMA3_CACHE_LINE_SIZE_IN_BYTES);
282 #endif
283         cacheFlushResult = EDMA3_NON_ALIGNED_BUFFERS_ERROR;
284         }
285     else
286         {
287                 Cache_wb((Ptr)mem_start_ptr, num_bytes, Cache_Type_ALL, TRUE);
288         }
290     return cacheFlushResult;
294 /**
295   * Counting Semaphore related functions (OS dependent) should be
296   * called/implemented by the application. A handle to the semaphore
297   * is required while opening the driver/resource manager instance.
298   */
300 /**
301  * \brief   EDMA3 OS Semaphore Create
302  *
303  *      This function creates a counting semaphore with specified
304  *      attributes and initial value. It should be used to create a semaphore
305  *      with initial value as '1'. The semaphore is then passed by the user
306  *      to the EDMA3 driver/RM for proper sharing of resources.
307  * \param   initVal [IN] is initial value for semaphore
308  * \param   semParams [IN] is the semaphore attributes.
309  * \param   hSem [OUT] is location to recieve the handle to just created
310  *      semaphore
311  * \return  EDMA3_DRV_SOK if succesful, else a suitable error code.
312  */
313 EDMA3_DRV_Result edma3OsSemCreate(int initVal,
314                                                         const Semaphore_Params *semParams,
315                                 EDMA3_OS_Sem_Handle *hSem)
316     {
317     EDMA3_DRV_Result semCreateResult = EDMA3_DRV_SOK;
319     if(NULL == hSem)
320         {
321         semCreateResult = EDMA3_DRV_E_INVALID_PARAM;
322         }
323     else
324         {
325         *hSem = (EDMA3_OS_Sem_Handle)Semaphore_create(initVal, semParams, NULL);
326         if ( (*hSem) == NULL )
327             {
328             semCreateResult = EDMA3_DRV_E_SEMAPHORE;
329             }
330         }
332     return semCreateResult;
333     }
336 /**
337  * \brief   EDMA3 OS Semaphore Delete
338  *
339  *      This function deletes or removes the specified semaphore
340  *      from the system. Associated dynamically allocated memory
341  *      if any is also freed up.
342  * \param   hSem [IN] handle to the semaphore to be deleted
343  * \return  EDMA3_DRV_SOK if succesful else a suitable error code
344  */
345 EDMA3_DRV_Result edma3OsSemDelete(EDMA3_OS_Sem_Handle hSem)
346     {
347     EDMA3_DRV_Result semDeleteResult = EDMA3_DRV_SOK;
349     if(NULL == hSem)
350         {
351         semDeleteResult = EDMA3_DRV_E_INVALID_PARAM;
352         }
353     else
354         {
355                 Semaphore_delete((Semaphore_Handle *)&hSem);
356         }
358     return semDeleteResult;
359     }
362 /**
363  * \brief   EDMA3 OS Semaphore Take
364  *
365  *      This function takes a semaphore token if available.
366  *      If a semaphore is unavailable, it blocks currently
367  *      running thread in wait (for specified duration) for
368  *      a free semaphore.
369  * \param   hSem [IN] is the handle of the specified semaphore
370  * \param   mSecTimeout [IN] is wait time in milliseconds
371  * \return  EDMA3_DRV_Result if successful else a suitable error code
372  */
373 EDMA3_DRV_Result edma3OsSemTake(EDMA3_OS_Sem_Handle hSem, int mSecTimeout)
374     {
375     EDMA3_DRV_Result semTakeResult = EDMA3_DRV_SOK;
376     unsigned short semPendResult;
378     if(NULL == hSem)
379         {
380         semTakeResult = EDMA3_DRV_E_INVALID_PARAM;
381         }
382     else
383         {
384         semPendResult = Semaphore_pend(hSem, mSecTimeout);
385         if (semPendResult == FALSE)
386             {
387             semTakeResult = EDMA3_DRV_E_SEMAPHORE;
388             }
389         }
391     return semTakeResult;
392     }
395 /**
396  * \brief   EDMA3 OS Semaphore Give
397  *
398  *      This function gives or relinquishes an already
399  *      acquired semaphore token
400  * \param   hSem [IN] is the handle of the specified semaphore
401  * \return  EDMA3_DRV_Result if successful else a suitable error code
402  */
403 EDMA3_DRV_Result edma3OsSemGive(EDMA3_OS_Sem_Handle hSem)
404     {
405     EDMA3_DRV_Result semGiveResult = EDMA3_DRV_SOK;
407     if(NULL == hSem)
408         {
409         semGiveResult = EDMA3_DRV_E_INVALID_PARAM;
410         }
411     else
412         {
413                 Semaphore_post(hSem);
414         }
416     return semGiveResult;
417     }