Misra C Fixes for dra72x
[keystone-rtos/edma3_lld.git] / packages / ti / sdo / edma3 / rm / sample / bios6_edma3_rm_sample.h
1 /*
2  * bios6_edma3_rm_sample.h
3  *
4  * Header file for the Demo application for the EDMA3 Resource Manager.
5  *
6  * Copyright (C) 2009 Texas Instruments Incorporated - http://www.ti.com/
7  *
8  *
9  *  Redistribution and use in source and binary forms, with or without
10  *  modification, are permitted provided that the following conditions
11  *  are met:
12  *
13  *    Redistributions of source code must retain the above copyright
14  *    notice, this list of conditions and the following disclaimer.
15  *
16  *    Redistributions in binary form must reproduce the above copyright
17  *    notice, this list of conditions and the following disclaimer in the
18  *    documentation and/or other materials provided with the
19  *    distribution.
20  *
21  *    Neither the name of Texas Instruments Incorporated nor the names of
22  *    its contributors may be used to endorse or promote products derived
23  *    from this software without specific prior written permission.
24  *
25  *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
26  *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
27  *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
28  *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
29  *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
30  *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
31  *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
32  *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
33  *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
34  *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
35  *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
36  *
37 */
39 #ifndef BIOS6_EDMA3_RM_SAMPLE_H_
40 #define BIOS6_EDMA3_RM_SAMPLE_H_
42 #include <ti/sysbios/knl/Semaphore.h>
44 #include <ti/sdo/edma3/rm/edma3_rm.h>
46 #ifdef __cplusplus
47 extern "C" {
48 #endif
50 /* To enable debug traces in the EDMA3 sample app */
51 /* Nowhere this macro is used, undefined to remove Misra C warning */
53 /* #define EDMA3_DEBUG_PRINT  */
55 #ifdef EDMA3_DEBUG_PRINT
56 #include <stdio.h>
57 #define EDMA3_DEBUG_PRINTF printf
58 #endif /* EDMA3_DEBUG_PRINT */
60 /**
61  * Cache line size on the underlying SoC. It needs to be modified
62  * for different cache line sizes, if the Cache is Enabled.
63  */
64 #define EDMA3_CACHE_LINE_SIZE_IN_BYTES      (128u)
66 /* Error returned in case of buffers are not aligned on the cache boundary */
67 #define EDMA3_NON_ALIGNED_BUFFERS_ERROR     (-1)
69 /* Error returned in case of data mismatch */
70 #define EDMA3_DATA_MISMATCH_ERROR           (-2)
72 /**
73  * \brief   EDMA3 Initialization
74  *
75  * This function initializes the EDMA3 Resource Manager for the given EDMA3 controller
76  * and opens a EDMA3 RM instance. It internally calls EDMA3_RM_create() and
77  * EDMA3_RM_open(), in that order.
78  *
79  * It also registers interrupt handlers for various EDMA3 interrupts like 
80  * transfer completion or error interrupts.
81  *
82  *  \param  edma3Id     [IN]            EDMA3 Controller Instance Id (Hardware
83  *                                                                      instance id, starting from 0)
84  *  \param  errorCode   [IN/OUT]        Error code while opening RM instance
85  *  \return EDMA3_RM_Handle: If successfully opened, the API will return the
86  *                            associated RM's instance handle.
87  */
88 EDMA3_RM_Handle edma3init (uint32_t edma3Id, EDMA3_RM_Result *errorCode);
90 /**
91  * \brief   EDMA3 De-initialization
92  *
93  * This function de-initializes the EDMA3 RM for the given EDMA3 controller
94  * and closes the previously opened EDMA3 RM instance. It internally calls 
95  * EDMA3_RM_close and EDMA3_RM_delete(), in that order.
96  *
97  * It also un-registers the previously registered interrupt handlers for various 
98  * EDMA3 interrupts.
99  *
100  *  \param  edma3Id     [IN]            EDMA3 Controller Instance Id (Hardware
101  *                                                                      instance id, starting from 0)
102  *  \param  hEdma               [IN]            EDMA3 RM handle, returned while using
103  *                                                                      edma3init().
104  *  \return  EDMA3_RM_SOK if success, else error code
105  */
106 EDMA3_RM_Result edma3deinit (uint32_t edma3Id, EDMA3_RM_Handle hEdma);
108 /**
109  * Counting Semaphore related functions (OS dependent) should be
110  * called/implemented by the application. A handle to the semaphore
111  * is required while opening the driver/resource manager instance.
112  */
114 /**
115  * \brief   EDMA3 OS Semaphore Create
116  *
117  *      This function creates a counting semaphore with specified
118  *      attributes and initial value. It should be used to create a semaphore
119  *      with initial value as '1'. The semaphore is then passed by the user
120  *      to the EDMA3 RM for proper sharing of resources.
121  * \param   initVal [IN] is initial value for semaphore
122  * \param   attrs [IN] is the semaphore attributes ex: Fifo type
123  * \param   hSem [OUT] is location to recieve the handle to just created
124  *      semaphore
125  * \return  EDMA3_RM_SOK if succesful, else a suitable error code.
126  */
127 EDMA3_RM_Result edma3OsSemCreate(int32_t initVal,
128                                                         const Semaphore_Params *semParams,
129                                 EDMA3_OS_Sem_Handle *hSem);
131 /**
132  * \brief   EDMA3 OS Semaphore Delete
133  *
134  *      This function deletes or removes the specified semaphore
135  *      from the system. Associated dynamically allocated memory
136  *      if any is also freed up.
137  * \warning OsSEM services run in client context and not in a thread
138  *      of their own. If there exist threads pended on a semaphore
139  *      that is being deleted, results are undefined.
140  * \param   hSem [IN] handle to the semaphore to be deleted
141  * \return  EDMA3_RM_SOK if succesful else a suitable error code
142  */
143 EDMA3_RM_Result edma3OsSemDelete(EDMA3_OS_Sem_Handle hSem);
145 #ifdef __cplusplus
147 #endif /* extern "C" */
149 #endif