PRSDK-3125: Update remainig
[keystone-rtos/edma3_lld.git] / packages / ti / sdo / edma3 / rm / sample / src / sample_arm_init.c
1 /*
2  * sample_init.c
3  *
4  * Sample Initialization for the EDMA3 RM for BIOS 6 based applications. It
5  * should be MANDATORILY done once before EDMA3 usage.
6  *
7  * Copyright (C) 2009 Texas Instruments Incorporated - http://www.ti.com/
8  *
9  *
10  *  Redistribution and use in source and binary forms, with or without
11  *  modification, are permitted provided that the following conditions
12  *  are met:
13  *
14  *    Redistributions of source code must retain the above copyright
15  *    notice, this list of conditions and the following disclaimer.
16  *
17  *    Redistributions in binary form must reproduce the above copyright
18  *    notice, this list of conditions and the following disclaimer in the
19  *    documentation and/or other materials provided with the
20  *    distribution.
21  *
22  *    Neither the name of Texas Instruments Incorporated nor the names of
23  *    its contributors may be used to endorse or promote products derived
24  *    from this software without specific prior written permission.
25  *
26  *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
27  *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
28  *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
29  *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
30  *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
31  *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
32  *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
33  *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
34  *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
35  *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
36  *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
37  *
38 */
40 #include <ti/sysbios/hal/Hwi.h>
41 #include <ti/sysbios/knl/Semaphore.h>
43 #include <ti/sdo/edma3/rm/sample/bios6_edma3_rm_sample.h>
45 /** @brief EDMA3 Driver Instance specific Semaphore handle */
46 extern EDMA3_OS_Sem_Handle SemHandle[EDMA3_MAX_EDMA3_INSTANCES];
48 /**  To Register the ISRs with the underlying OS, if required. */
49 extern void registerEdma3Interrupts (uint32_t edma3Id);
50 /**  To Unregister the ISRs with the underlying OS, if previously registered. */
51 extern void unregisterEdma3Interrupts (uint32_t edma3Id);
53 /* To find out the DSP# */
54 extern uint16_t determineProcId(void);
56 /**
57  * To check whether the global EDMA3 configuration is required or not.
58  * It should be done ONCE by any of the masters present in the system.
59  * This function checks whether the global configuration is required by the
60  * current master or not. In case of many masters, it should be done only
61  * by one of the masters. Hence this function will return TRUE only once
62  * and FALSE for all other masters. 
63  */
64 extern uint16_t isGblConfigRequired(uint32_t dspNum);
66 /**
67  * DSP instance number on which the executable is running. Its value is
68  * determined by reading the processor specific register DNUM.
69  */
70 uint32_t dsp_num;
72 /**
73  * Shadow Region on which the executable is runnig. Its value is populated
74  * with the dsp_num here in this case.
75  */
76 uint32_t region_id;
78 /* Number of EDMA3 controllers present in the system */
79 extern const uint32_t numEdma3Instances;
81 /* External Global Configuration Structure */
82 extern EDMA3_RM_GblConfigParams sampleEdma3GblCfgParams[EDMA3_MAX_EDMA3_INSTANCES];
84 /* External Instance Specific Configuration Structure */
85 extern EDMA3_RM_InstanceInitConfig sampleInstInitConfig[EDMA3_MAX_EDMA3_INSTANCES][EDMA3_MAX_REGIONS];
87 #ifdef DMA_XBAR_AVAILABLE
88 extern EDMA3_DRV_Result sampleInitXbarEvt(EDMA3_DRV_Handle hEdma, uint32_t edma3Id);
89 #endif
91 /**
92  * \brief   EDMA3 Initialization
93  *
94  * This function initializes the EDMA3 RM and registers the
95  * interrupt handlers.
96  *
97   * \return  EDMA3_RM_SOK if success, else error code
98  */
99 EDMA3_RM_Handle edma3init (uint32_t edma3Id, EDMA3_RM_Result *errorCode)
100     {
101     EDMA3_RM_Param initParam;
102     EDMA3_RM_Result edma3Result = EDMA3_RM_SOK;
103     Semaphore_Params semParams;
104     EDMA3_RM_MiscParam miscParam;
105     EDMA3_RM_GblConfigParams *globalConfig = NULL;
106     EDMA3_RM_InstanceInitConfig *instanceConfig = NULL;
107         EDMA3_RM_Handle hEdmaResMgr = NULL;
109         if ((edma3Id >= numEdma3Instances) || (errorCode == NULL))
110     {
111                 hEdmaResMgr = NULL;
112     }
113     else
114     {
115     /* DSP instance number */
116     dsp_num = determineProcId();
118         globalConfig = &sampleEdma3GblCfgParams[edma3Id];
120         /* Configure it as master, if required */
121         miscParam.isSlave = isGblConfigRequired(dsp_num);
122         
123         edma3Result = EDMA3_RM_create (edma3Id, globalConfig ,
124                                                                         (void *)&miscParam);
126         if (edma3Result == EDMA3_DRV_SOK)
127                 {
128                 /**
129                 * Driver Object created successfully.
130                 * Create a semaphore now for driver instance.
131                 */
132                 Semaphore_Params_init(&semParams);
134                 initParam.rmSemHandle = NULL;
135                 edma3Result = edma3OsSemCreate((int32_t)1, &semParams, &initParam.rmSemHandle);
136                 }
138         if (edma3Result == EDMA3_DRV_SOK)
139                 {
140                 /* Save the semaphore handle for future use */
141                 SemHandle[edma3Id] = initParam.rmSemHandle;
143                 /* configuration structure for the Driver */
144                 instanceConfig = &sampleInstInitConfig[edma3Id][dsp_num];
146                 initParam.isMaster = TRUE;
147                 /* Choose shadow region according to the DSP# */
148                 initParam.regionId = (EDMA3_RM_RegionId)dsp_num;
149                 /*Saving the regionId for using it in the sample_cs.c file */
150                 region_id = (EDMA3_RM_RegionId)dsp_num;
151                 /* Driver instance specific config NULL */
152                 initParam.rmInstInitConfig = instanceConfig;
154         initParam.regionInitEnable = TRUE;
155         initParam.gblerrCbParams.gblerrCb = (EDMA3_RM_GblErrCallback)NULL;
156         initParam.gblerrCbParams.gblerrData = (void *)NULL;
158                 /* Open the Driver Instance */
159                 hEdmaResMgr = EDMA3_RM_open (edma3Id, (EDMA3_RM_Param *)&initParam, 
160                                                                                 &edma3Result);
161                 }
163 #ifdef DMA_XBAR_AVAILABLE
164         {
165         if((hEdmaResMgr != NULL) && (edma3Result == EDMA3_RM_SOK))
166                 {
167                 edma3Result = sampleInitXbarEvt(hEdmaResMgr, edma3Id);
168                 }
169         }
170 #endif
171         if((hEdmaResMgr != NULL) && (edma3Result == EDMA3_DRV_SOK))
172                 {
173                 /**
174                 * Register Interrupt Handlers for various interrupts
175                 * like transfer completion interrupt, CC error
176                 * interrupt, TC error interrupts etc, if required.
177                 */
178                 registerEdma3Interrupts(edma3Id);
179                 }
181         *errorCode = edma3Result;
182     }
183         return hEdmaResMgr;
184     }
186 /**
187  * \brief   EDMA3 De-initialization
188  *
189  * This function removes the EDMA3 RM Instance and unregisters the
190  * interrupt handlers. It also deletes the RM  Object.
191  *
192   * \return  EDMA3_RM_SOK if success, else error code
193  */
194 EDMA3_RM_Result edma3deinit (uint32_t edma3Id, EDMA3_RM_Handle hEdma)
195     {
196     EDMA3_RM_Result edma3Result = EDMA3_RM_SOK;
198     /* Unregister Interrupt Handlers first */
199     unregisterEdma3Interrupts(edma3Id);
201     /* Delete the semaphore */
202     edma3Result = edma3OsSemDelete (SemHandle[edma3Id]);
204     if (EDMA3_RM_SOK == edma3Result)
205         {
206         /* Make the semaphore handle as NULL. */
207         SemHandle[edma3Id] = NULL;
209         /* Now, close the EDMA3 RM Instance */
210         edma3Result = EDMA3_RM_close (hEdma, NULL);
211         }
212         
213     if (EDMA3_RM_SOK == edma3Result)
214         {
215         /* Now, delete the EDMA3 RM Object */
216         edma3Result = EDMA3_RM_delete (edma3Id, NULL);
217         }
219     return edma3Result;
220     }
222 /* End of File */