Adding TCI6498 support in RM sample init lib
[keystone-rtos/edma3_lld.git] / packages / ti / sdo / edma3 / rm / sample / src / sample_cs.c
1 /*\r
2  * sample_cs.c\r
3  *\r
4  * Sample functions showing the implementation of critical section entry/exit\r
5  * routines and various semaphore related routines (all OS depenedent). These\r
6  * implementations MUST be provided by the user / application, using the EDMA3\r
7  * Resource Manager, for its correct functioning.\r
8  *\r
9  * Copyright (C) 2009 Texas Instruments Incorporated - http://www.ti.com/\r
10  *\r
11  *\r
12  *  Redistribution and use in source and binary forms, with or without\r
13  *  modification, are permitted provided that the following conditions\r
14  *  are met:\r
15  *\r
16  *    Redistributions of source code must retain the above copyright\r
17  *    notice, this list of conditions and the following disclaimer.\r
18  *\r
19  *    Redistributions in binary form must reproduce the above copyright\r
20  *    notice, this list of conditions and the following disclaimer in the\r
21  *    documentation and/or other materials provided with the\r
22  *    distribution.\r
23  *\r
24  *    Neither the name of Texas Instruments Incorporated nor the names of\r
25  *    its contributors may be used to endorse or promote products derived\r
26  *    from this software without specific prior written permission.\r
27  *\r
28  *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS\r
29  *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT\r
30  *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR\r
31  *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT\r
32  *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,\r
33  *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT\r
34  *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,\r
35  *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY\r
36  *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT\r
37  *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE\r
38  *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.\r
39  *\r
40 */\r
41 \r
42 #include <ti/sysbios/family/c64p/EventCombiner.h>\r
43 #include <ti/sysbios/hal/Hwi.h>\r
44 #include <ti/sysbios/knl/Task.h>\r
45 #include <ti/sysbios/ipc/Semaphore.h>\r
46 \r
47 #include <ti/sdo/edma3/rm/sample/bios6_edma3_rm_sample.h>\r
48 \r
49 extern unsigned int ccXferCompInt[][EDMA3_MAX_REGIONS];\r
50 extern unsigned int ccErrorInt[];\r
51 extern unsigned int tcErrorInt[][EDMA3_MAX_TC];\r
52 \r
53 /**\r
54  * DSP instance number on which the executable is running. Its value is\r
55  * determined by reading the processor specific register DNUM.\r
56  */\r
57 extern unsigned int dsp_num;\r
58 \r
59 /**\r
60  * \brief   EDMA3 OS Protect Entry\r
61  *\r
62  *      This function saves the current state of protection in 'intState'\r
63  *      variable passed by caller, if the protection level is\r
64  *      EDMA3_OS_PROTECT_INTERRUPT. It then applies the requested level of\r
65  *      protection.\r
66  *      For EDMA3_OS_PROTECT_INTERRUPT_XFER_COMPLETION and\r
67  *      EDMA3_OS_PROTECT_INTERRUPT_CC_ERROR, variable 'intState' is ignored,\r
68  *      and the requested interrupt is disabled.\r
69  *      For EDMA3_OS_PROTECT_INTERRUPT_TC_ERROR, '*intState' specifies the\r
70  *      Transfer Controller number whose interrupt needs to be disabled.\r
71  *\r
72  * \param   level is numeric identifier of the desired degree of protection.\r
73  * \param   intState is memory location where current state of protection is\r
74  *      saved for future use while restoring it via edma3OsProtectExit() (Only\r
75  *      for EDMA3_OS_PROTECT_INTERRUPT protection level).\r
76  * \return  None\r
77  */\r
78 void edma3OsProtectEntry (unsigned int edma3InstanceId, \r
79                                                         int level, unsigned int *intState)\r
80     {\r
81     if (((level == EDMA3_OS_PROTECT_INTERRUPT)\r
82         || (level == EDMA3_OS_PROTECT_INTERRUPT_TC_ERROR))\r
83         && (intState == NULL))\r
84         {\r
85         return;\r
86         }\r
87     else\r
88         {\r
89         switch (level)\r
90             {\r
91             /* Disable all (global) interrupts */\r
92             case EDMA3_OS_PROTECT_INTERRUPT :\r
93                 *intState = Hwi_disable();\r
94                 break;\r
95 \r
96             /* Disable scheduler */\r
97             case EDMA3_OS_PROTECT_SCHEDULER :\r
98                                 Task_disable();\r
99                 break;\r
100 \r
101             /* Disable EDMA3 transfer completion interrupt only */\r
102             case EDMA3_OS_PROTECT_INTERRUPT_XFER_COMPLETION :\r
103                 EventCombiner_disableEvent(ccXferCompInt[edma3InstanceId][dsp_num]);\r
104                 break;\r
105 \r
106             /* Disable EDMA3 CC error interrupt only */\r
107             case EDMA3_OS_PROTECT_INTERRUPT_CC_ERROR :\r
108                 EventCombiner_disableEvent(ccErrorInt[edma3InstanceId]);\r
109                 break;\r
110 \r
111             /* Disable EDMA3 TC error interrupt only */\r
112             case EDMA3_OS_PROTECT_INTERRUPT_TC_ERROR :\r
113                 switch (*intState)\r
114                     {\r
115                     case 0:\r
116                     case 1:\r
117                     case 2:\r
118                     case 3:\r
119                     case 4:\r
120                     case 5:\r
121                     case 6:\r
122                     case 7:\r
123                         /* Fall through... */\r
124                         /* Disable the corresponding interrupt */\r
125                         EventCombiner_disableEvent(tcErrorInt[edma3InstanceId][*intState]);\r
126                         break;\r
127 \r
128                      default:\r
129                         break;\r
130                     }\r
131 \r
132                 break;\r
133 \r
134             default:\r
135                 break;\r
136             }\r
137         }\r
138     }\r
139 \r
140 \r
141 /**\r
142  * \brief   EDMA3 OS Protect Exit\r
143  *\r
144  *      This function undoes the protection enforced to original state\r
145  *      as is specified by the variable 'intState' passed, if the protection\r
146  *      level is EDMA3_OS_PROTECT_INTERRUPT.\r
147  *      For EDMA3_OS_PROTECT_INTERRUPT_XFER_COMPLETION and\r
148  *      EDMA3_OS_PROTECT_INTERRUPT_CC_ERROR, variable 'intState' is ignored,\r
149  *      and the requested interrupt is enabled.\r
150  *      For EDMA3_OS_PROTECT_INTERRUPT_TC_ERROR, 'intState' specifies the\r
151  *      Transfer Controller number whose interrupt needs to be enabled.\r
152  * \param   level is numeric identifier of the desired degree of protection.\r
153  * \param   intState is original state of protection at time when the\r
154  *      corresponding edma3OsProtectEntry() was called (Only\r
155  *      for EDMA3_OS_PROTECT_INTERRUPT protection level).\r
156  * \return  None\r
157  */\r
158 void edma3OsProtectExit (unsigned int edma3InstanceId,\r
159                         int level, unsigned int intState)\r
160     {\r
161     switch (level)\r
162         {\r
163         /* Enable all (global) interrupts */\r
164         case EDMA3_OS_PROTECT_INTERRUPT :\r
165             Hwi_restore(intState);\r
166             break;\r
167 \r
168         /* Enable scheduler */\r
169         case EDMA3_OS_PROTECT_SCHEDULER :\r
170             Task_enable();\r
171             break;\r
172 \r
173         /* Enable EDMA3 transfer completion interrupt only */\r
174         case EDMA3_OS_PROTECT_INTERRUPT_XFER_COMPLETION :\r
175             EventCombiner_enableEvent(ccXferCompInt[edma3InstanceId][dsp_num]);\r
176             break;\r
177 \r
178         /* Enable EDMA3 CC error interrupt only */\r
179         case EDMA3_OS_PROTECT_INTERRUPT_CC_ERROR :\r
180             EventCombiner_enableEvent(ccErrorInt[edma3InstanceId]);\r
181             break;\r
182 \r
183         /* Enable EDMA3 TC error interrupt only */\r
184         case EDMA3_OS_PROTECT_INTERRUPT_TC_ERROR :\r
185             switch (intState)\r
186                 {\r
187                 case 0:\r
188                 case 1:\r
189                 case 2:\r
190                 case 3:\r
191                 case 4:\r
192                 case 5:\r
193                 case 6:\r
194                 case 7:\r
195                     /* Fall through... */\r
196                     /* Enable the corresponding interrupt */\r
197                     EventCombiner_enableEvent(tcErrorInt[edma3InstanceId][intState]);\r
198                     break;\r
199 \r
200                  default:\r
201                     break;\r
202                 }\r
203 \r
204             break;\r
205 \r
206         default:\r
207             break;\r
208         }\r
209     }\r
210 \r
211 \r
212 /**\r
213   * Counting Semaphore related functions (OS dependent) should be\r
214   * called/implemented by the application. A handle to the semaphore\r
215   * is required while opening the resource manager instance.\r
216   */\r
217 \r
218 /**\r
219  * \brief   EDMA3 OS Semaphore Create\r
220  *\r
221  *      This function creates a counting semaphore with specified\r
222  *      attributes and initial value. It should be used to create a semaphore\r
223  *      with initial value as '1'. The semaphore is then passed by the user\r
224  *      to the EDMA3 RM for proper sharing of resources.\r
225  * \param   initVal [IN] is initial value for semaphore\r
226  * \param   semParams [IN] is the semaphore attributes.\r
227  * \param   hSem [OUT] is location to recieve the handle to just created\r
228  *      semaphore\r
229  * \return  EDMA3_RM_SOK if succesful, else a suitable error code.\r
230  */\r
231 EDMA3_RM_Result edma3OsSemCreate(int initVal,\r
232                                                         const Semaphore_Params *semParams,\r
233                                 EDMA3_OS_Sem_Handle *hSem)\r
234     {\r
235     EDMA3_RM_Result semCreateResult = EDMA3_RM_SOK;\r
236 \r
237     if(NULL == hSem)\r
238         {\r
239         semCreateResult = EDMA3_RM_E_INVALID_PARAM;\r
240         }\r
241     else\r
242         {\r
243         *hSem = (EDMA3_OS_Sem_Handle)Semaphore_create(initVal, semParams, NULL);\r
244         if ( (*hSem) == NULL )\r
245             {\r
246             semCreateResult = EDMA3_RM_E_SEMAPHORE;\r
247             }\r
248         }\r
249 \r
250     return semCreateResult;\r
251     }\r
252 \r
253 \r
254 /**\r
255  * \brief   EDMA3 OS Semaphore Delete\r
256  *\r
257  *      This function deletes or removes the specified semaphore\r
258  *      from the system. Associated dynamically allocated memory\r
259  *      if any is also freed up.\r
260  * \param   hSem [IN] handle to the semaphore to be deleted\r
261  * \return  EDMA3_RM_SOK if succesful else a suitable error code\r
262  */\r
263 EDMA3_RM_Result edma3OsSemDelete(EDMA3_OS_Sem_Handle hSem)\r
264     {\r
265     EDMA3_RM_Result semDeleteResult = EDMA3_RM_SOK;\r
266 \r
267     if(NULL == hSem)\r
268         {\r
269         semDeleteResult = EDMA3_RM_E_INVALID_PARAM;\r
270         }\r
271     else\r
272         {\r
273                 Semaphore_delete(hSem);\r
274         }\r
275 \r
276     return semDeleteResult;\r
277     }\r
278 \r
279 \r
280 /**\r
281  * \brief   EDMA3 OS Semaphore Take\r
282  *\r
283  *      This function takes a semaphore token if available.\r
284  *      If a semaphore is unavailable, it blocks currently\r
285  *      running thread in wait (for specified duration) for\r
286  *      a free semaphore.\r
287  * \param   hSem [IN] is the handle of the specified semaphore\r
288  * \param   mSecTimeout [IN] is wait time in milliseconds\r
289  * \return  EDMA3_RM_Result if successful else a suitable error code\r
290  */\r
291 EDMA3_RM_Result edma3OsSemTake(EDMA3_OS_Sem_Handle hSem, int mSecTimeout)\r
292     {\r
293     EDMA3_RM_Result semTakeResult = EDMA3_RM_SOK;\r
294     unsigned short semPendResult;\r
295 \r
296     if(NULL == hSem)\r
297         {\r
298         semTakeResult = EDMA3_RM_E_INVALID_PARAM;\r
299         }\r
300     else\r
301         {\r
302         semPendResult = Semaphore_pend(hSem, mSecTimeout);\r
303         if (semPendResult == FALSE)\r
304             {\r
305             semTakeResult = EDMA3_RM_E_SEMAPHORE;\r
306             }\r
307         }\r
308 \r
309     return semTakeResult;\r
310     }\r
311 \r
312 \r
313 /**\r
314  * \brief   EDMA3 OS Semaphore Give\r
315  *\r
316  *      This function gives or relinquishes an already\r
317  *      acquired semaphore token\r
318  * \param   hSem [IN] is the handle of the specified semaphore\r
319  * \return  EDMA3_RM_Result if successful else a suitable error code\r
320  */\r
321 EDMA3_RM_Result edma3OsSemGive(EDMA3_OS_Sem_Handle hSem)\r
322     {\r
323     EDMA3_RM_Result semGiveResult = EDMA3_RM_SOK;\r
324 \r
325     if(NULL == hSem)\r
326         {\r
327         semGiveResult = EDMA3_RM_E_INVALID_PARAM;\r
328         }\r
329     else\r
330         {\r
331                 Semaphore_post(hSem);\r
332         }\r
333 \r
334     return semGiveResult;\r
335     }\r
336 \r
337 /* End of File */\r
338 \r