/* * ======== tistdtypes.h ======== */ /* * These types are also defined by other TI components. They are bracketed * with _TI_STD_TYPES to avoid warnings for duplicate definition. * * You may get warnings about duplicate type definitions when using this * header file with earlier versions of DSP/BIOS and CSL. * * You can use the '-pds303' compiler option to suppress these warnings. */ #ifndef _TI_STD_TYPES #define _TI_STD_TYPES /* * This '#ifndef STD_' is needed to protect from duplicate definitions * of Int, Uns, etc. in DSP/BIOS v4.x (e.g. 4.90, 4.80) since these versions * of DSP/BIOS did not contain the '#ifndef_TI_STD_TYPES' logic. */ #ifndef STD_ /* * Aliases for standard C types */ typedef int Int; typedef unsigned Uns; typedef char Char; /* pointer to null-terminated character sequence */ typedef char *String; typedef void *Ptr; /* pointer to arbitrary type */ typedef unsigned short Bool; /* boolean */ #endif /* STD_ */ /* * Uint8, Uint16, Uint32, etc are defined to be "smallest unit of * available storage that is large enough to hold unsigned or integer * of specified size". */ /* Handle the 6x ISA */ #if defined(_TMS320C6X) /* Unsigned integer definitions (32bit, 16bit, 8bit) follow... */ typedef unsigned int Uint32; typedef unsigned short Uint16; typedef unsigned char Uint8; /* Signed integer definitions (32bit, 16bit, 8bit) follow... */ typedef int Int32; typedef short Int16; typedef char Int8; /* Handle the 54x, 55x and 28x ISAs */ #elif defined(_TMS320C5XX) || defined(__TMS320C55X__) || defined(_TMS320C28X) /* Unsigned integer definitions (32bit, 16bit, 8bit) follow... */ typedef unsigned long Uint32; typedef unsigned short Uint16; typedef unsigned char Uint8; /* Signed integer definitions (32bit, 16bit, 8bit) follow... */ typedef long Int32; typedef short Int16; typedef char Int8; #else /* Other ISAs not supported */ #error is not supported for this target #endif /* defined(_6x_) */ #endif /* _TI_STD_TYPES */