# File: env.mk. This file contains all the paths and other ENV variables # # Module paths # # Directory where all internal software packages are located; typically # those that are checked into version controlled repository. In this case all # the OMX components and SDK/OMX demo. INTERNAL_SW_ROOT = E:/EDMA/edma3_lld_02_11_00_01 # Directory where all external (imported) software packages are located; typically # those that are NOT checked into version controlled repository. In this case, # compiler tool chains, BIOS, XDC, Syslink, IPC, FC, CE, drivers, codecs, etc. EXTERNAL_SW_ROOT = C:/PROGRA~1/TEXASI~1 # Destination root directory. # - specify the directory where you want to place the object, archive/library, # binary and other generated files in a different location than source tree # - or leave it blank to place then in the same tree as the source #DEST_ROOT = E:/Temp/sdk5008_outfiles # Utilities directory. This is required only if the build machine is Windows. # - specify the installation directory of utility which supports POSIX commands # (eg: Cygwin installation or MSYS installation). UTILS_INSTALL_DIR = C:/PROGRA~1/TEXASI~1/xdctools_3_20_07_86 # Set path separator, etc based on the OS ifeq ($(OS),Windows_NT) PATH_SEPARATOR = ; UTILSPATH = $(UTILS_INSTALL_DIR)/bin/ else # else, assume it is linux PATH_SEPARATOR = : endif # BIOS bios_PATH = $(EXTERNAL_SW_ROOT)/bios_6_31_04_27 bios_INCLUDE = $(bios_PATH)/packages # XDC xdc_PATH = $(EXTERNAL_SW_ROOT)/xdctools_3_20_07_86 xdc_INCLUDE = $(xdc_PATH)/packages # EDMA3 LLD edma3_lld_PATH = $(INTERNAL_SW_ROOT) include $(edma3_lld_PATH)/packages/component.mk # # Tools paths # # Cortex-M3 CODEGEN_PATH_M3 = $(EXTERNAL_SW_ROOT)/TMS470~1.3 # Cortex-A8 CODEGEN_PATH_A8 = $(EXTERNAL_SW_ROOT)/TMS470~1.3 # ARM-9 CODEGEN_PATH_ARM9 = $(EXTERNAL_SW_ROOT)/TMS470~1.3 # DSP - Since same toolchain does not support COFF and ELF, there are two entries # This would go away when one version supports both formats CODEGEN_PATH_DSP = $(EXTERNAL_SW_ROOT)/C6000C~1.4 CODEGEN_PATH_DSPELF = $(EXTERNAL_SW_ROOT)/C6000C~1.0 # Commands commonly used within the make files RM = $(UTILSPATH)rm RMDIR = $(UTILSPATH)rm -rf MKDIR = $(UTILSPATH)mkdir ECHO = @$(UTILSPATH)echo # MAKE = $(UTILSPATH)make EGREP = $(UTILSPATH)egrep CP = $(UTILSPATH)cp # This is to avoid using full blown cygwin - chmod is really needed only linux ifeq ($(OS),Windows_NT) CHMOD = @echo else CHMOD = $(UTILSPATH)chmod endif # # XDC specific ENV variables # # XDC Config.bld file (required for configuro) ; Derives from top-level omx_PATH CONFIG_BLD_XDC_674 = $(edma3_lld_PATH)/packages/_config.bld CONFIG_BLD_XDC_64p = $(edma3_lld_PATH)/packages/_config.bld CONFIG_BLD_XDC_a8 = $(edma3_lld_PATH)/packages/_config.bld CONFIG_BLD_XDC_arm9 = $(edma3_lld_PATH)/packages/_config.bld CONFIG_BLD_XDC_66 = $(edma3_lld_PATH)/packages/_config.bld XDCPATH = $(bios_PATH)/packages;$(xdc_PATH)/packages;$(edma3_lld_PATH)/packages; export XDCPATH XDCROOT = $(xdc_PATH) XDCTOOLS = $(xdc_PATH) export XDCROOT export XDCTOOLS TMS470_CGTOOLS = $(CODEGEN_PATH_M3) CGTOOLS = $(CODEGEN_PATH_DSP) CGTOOLS_ELF = $(CODEGEN_PATH_DSPELF) export TMS470CGTOOLPATH CODESOURCERYCGTOOLS = $(CODEGEN_PATH_A8) export CODESOURCERYCGTOOLS PATH += $(PATH_SEPARATOR)$(xdc_PATH)$(PATH_SEPARATOR)$(CODEGEN_PATH_M3)/bin export PATH # Nothing beyond this point