# Filename: rules_a8.mk # # Make rules for A8 - This file has all the common rules and defines required # for Cortex-A8 ISA # # This file needs to change when: # 1. Code generation tool chain changes (currently it uses CodeSourcery) # 2. Internal switches (which are normally not touched) has to change # 3. XDC specific switches change # 4. a rule common for A8 ISA has to be added or modified # Set compiler/archiver/linker commands and include paths CODEGEN_INCLUDE = $(CODEGEN_PATH_A8) CC = $(CODEGEN_PATH_A8)/bin/arm-none-linux-gnueabi-gcc AR = $(CODEGEN_PATH_A8)/bin/arm-none-linux-gnueabi-ar LNK = $(CODEGEN_PATH_A8)/bin/arm-none-linux-gnueabi-ld # Internal CFLAGS - normally doesn't change CFLAGS_INTERNAL = -fPIC -fno-strict-aliasing -MD -MF $(DEPFILE).P -march=armv5t -Dfar= -D_DEBUG_=1 -DMULTICHANNEL_OPT=1 CFLAGS_DIROPTS = # XDC specific CFLAGS CFLAGS_XDCINTERNAL = -Dxdc_target_name__=GCArmv5T -Dxdc_target_types__=gnu/targets/arm/std.h -Dxdc_bld__profile_$(PROFILE_$(CORE)) -Dxdc_bld__vers_1_0_4_3_3 LNKFLAGS_INTERNAL_PROFILE = # Following 'if...' block is for an application; to add a #define for each # component in the build. This is required to know - at compile time - which # components are on which core. ifndef MODULE_NAME # Derive list of all packages from each of the components needed by the app PKG_LIST_LOCAL = $(foreach COMP,$(COMP_LIST_$(CORE)),$($(COMP)_PKG_LIST)) # Defines for the app and cfg source code to know which components/packages # are included in the build for the local CORE... CFLAGS_APP_DEFINES = $(foreach PKG,$(PKG_LIST_LOCAL),-D_LOCAL_$(PKG)_) CFLAGS_APP_DEFINES += $(foreach PKG,$(PKG_LIST_LOCAL),-D_BUILD_$(PKG)_) ifeq ($(CORE),m3vpss) PKG_LIST_REMOTE = $(foreach COMP,$(COMP_LIST_m3video),$($(COMP)_PKG_LIST)) CFLAGS_APP_DEFINES += -D_LOCAL_CORE_m3vpss_ endif ifeq ($(CORE),m3video) PKG_LIST_REMOTE = $(foreach COMP,$(COMP_LIST_m3vpss),$($(COMP)_PKG_LIST)) CFLAGS_APP_DEFINES += -D_LOCAL_CORE_m3video_ endif ifeq ($(CORE),a8host) PKG_LIST_REMOTE = $(foreach COMP,$(COMP_LIST_m3video),$($(COMP)_PKG_LIST)) PKG_LIST_REMOTE += $(foreach COMP,$(COMP_LIST_m3vpss),$($(COMP)_PKG_LIST)) CFLAGS_APP_DEFINES += -D_LOCAL_CORE_a8host_ endif # Defines for the app and cfg source code to know which components/packages # are included in the build for the remote CORE... CFLAGS_APP_DEFINES += $(foreach PKG,$(PKG_LIST_REMOTE),-D_REMOTE_$(PKG)_) CFLAGS_APP_DEFINES += $(foreach PKG,$(PKG_LIST_REMOTE),-D_BUILD_$(PKG)_) endif # Assemble CFLAGS from all other CFLAGS definitions _CFLAGS = $(CFLAGS_GLOBAL_$(CORE)) $(CFLAGS_INTERNAL) $(CFLAGS_XDCINTERNAL) $(CFLAGS_LOCAL_COMMON) $(CFLAGS_LOCAL_$(CORE)) $(CFLAGS_LOCAL_$(PLATFORM)) $(CFLAGS_LOCAL_$(SOC)) $(CFLAGS_APP_DEFINES) $(CFLAGS_COMP_COMMON) $(CFLAGS_GLOBAL_$(PLATFORM)) # Object file creation # The first $(CC) generates the dependency make files for each of the objects # The second $(CC) compiles the source to generate object $(OBJ_PATHS): $(OBJDIR)/%.$(OBJEXT): %.c $(ECHO) \# Compiling $< to $@ ... $(CC) $(_CFLAGS) $(INCLUDES) $(CFLAGS_DIROPTS) -o $(OBJDIR)/$(basename $(notdir $<)).$(OBJEXT) $< # Archive flags - normally doesn't change ARFLAGS = cr # Archive/library file creation $(LIBDIR)/$(MODULE_NAME).$(LIBEXT) : $(OBJ_PATHS) $(ECHO) \# $(ECHO) \# Archiving $(OBJ_PATHS) into $@... $(ECHO) \# $(AR) $(ARFLAGS) $@ $(OBJ_PATHS) # Linker options and rules LNKFLAGS_INTERNAL_COMMON = -lpthread -lrt -L$(CODEGEN_PATH_A8)/arm-none-linux-gnueabi/lib # Assemble Linker flags from all other LNKFLAGS definitions _LNKFLAGS = $(LNKFLAGS_INTERNAL_COMMON) $(LNKFLAGS_INTERNAL_PROFILE) $(LNKFLAGS_GLOBAL_$(CORE)) $(LNKFLAGS_LOCAL_COMMON) $(LNKFLAGS_LOCAL_$(CORE)) # Path of the RTS library - normally doesn't change for a given tool-chain RTSLIB_PATH = LIB_PATHS += LNK_LIBS = $(addprefix -l,$(LIB_PATHS)) # Linker - to create executable file $(BINDIR)/$(APP_NAME)_$(CORE)_$(PROFILE_$(CORE)).$(EXEEXT) : $(OBJ_PATHS) $(LIB_PATHS) $(LNKCMD_FILE) $(OBJDIR)/$(CFG_COBJ_XDC) $(ECHO) \# Linking into $@ $(ECHO) \# # $(LNK) $(OBJ_PATHS) $(OBJDIR)/$(CFG_COBJ_XDC) $(LNKCMD_FILE) $(_LNKFLAGS) -o $@ -Map $@.map $(LNK_LIBS) $(CC) $(OBJ_PATHS) $(OBJDIR)/$(CFG_COBJ_XDC) $(LIB_PATHS) $(LNKCMD_FILE) $(_LNKFLAGS) -o $@ $(ECHO) \# $(ECHO) \# $@ created. $(ECHO) \# # XDC specific - assemble XDC-Configuro command CONFIGURO_CMD = $(xdc_PATH)/xs xdc.tools.configuro --generationOnly -o $(CONFIGURO_DIR) -t $(TARGET_XDC) -p $(PLATFORM_XDC) \ --cfgArgs $(CFGARGS_XDC) -r $(PROFILE_$(CORE)) -b $(CONFIG_BLD_XDC_$(ISA)) $(XDC_CFG_FILE_NAME) _XDC_GREP_STRING = \"$(XDC_GREP_STRING)\" EGREP_CMD = $(EGREP) -ivw $(XDC_GREP_STRING) $(XDCLNKCMD_FILE) # Invoke configuro for the rest of the components # NOTE: 1. String handling is having issues with various make versions when the # cammand is directly tried to be given below. Hence, as a work-around, # the command is re-directed to a file (shell or batch file) and then # executed # 2. The linker.cmd file generated, includes the libraries generated by # XDC. An egrep to search for these and omit in the .cmd file is added # after configuro is done #$(CFG_CFILE_XDC) : $(XDC_CFG_FILE) xdc_configuro : $(XDC_CFG_FILE) $(ECHO) \# Invoking configuro... $(ECHO) -e $(CONFIGURO_CMD) > $(DEST_ROOT)/maketemp_configuro_cmd_$(CORE).bat $(CHMOD) a+x $(DEST_ROOT)/maketemp_configuro_cmd_$(CORE).bat $(DEST_ROOT)/maketemp_configuro_cmd_$(CORE).bat # $(CP) $(XDCLNKCMD_FILE) $(LNKCMD_FILE) # $(ECHO) @ $(EGREP_CMD) > maketemp_egrep_cmd.bat # ./maketemp_egrep_cmd.bat | $(CYGWINPATH)/bin/tail -n+3 > $(LNKCMD_FILE) $(EGREP_CMD) > $(LNKCMD_FILE) # $(EGREP) -iv "$(XDC_GREP_STRING)" $(XDCLNKCMD_FILE) > $(LNKCMD_FILE) $(ECHO) \# Configuro done! $(LNKCMD_FILE) : # $(CP) $(XDCLNKCMD_FILE) $(LNKCMD_FILE) # $(ECHO) @ $(EGREP_CMD) > maketemp_egrep_cmd.bat # ./maketemp_egrep_cmd.bat | $(CYGWINPATH)/bin/tail -n+3 > $(LNKCMD_FILE) # $(EGREP_CMD) > $(LNKCMD_FILE) ifndef MODULE_NAME $(OBJDIR)/$(CFG_COBJ_XDC) : $(CFG_C_XDC) $(ECHO) \# Compiling generated $< to $@ ... $(CC) $(_CFLAGS) $(INCLUDES) $(CFLAGS_DIROPTS) -o $(OBJDIR)/$(CFG_COBJ_XDC) $(CFG_C_XDC) endif # Include dependency make files that were generated by $(CC) -include $(SRCS:%.c=$(DEPDIR)/%.P) # Nothing beyond this point