# Filename: rules_GCC_arm9.mk # # Make rules for A9 - This file has all the common rules and defines required # for Cortex-A9 ISA # # This file needs to change when: # 1. Code generation tool chain changes # 2. Internal switches (which are normally not touched) has to change # 3. XDC specific switches change # 4. a rule common for A9 ISA has to be added or modified # Set compiler/archiver/linker commands and include paths CODEGEN_INCLUDE = $(CODEGEN_PATH_A9_GCC)/arm-none-eabi/include $(CODEGEN_PATH_A9_GCC)/arm-none-eabi/include/newlib-nano CC = $(CODEGEN_PATH_A9_GCC)/bin/arm-none-eabi-gcc AR = $(CODEGEN_PATH_A9_GCC)/bin/arm-none-eabi-ar LNK = $(CODEGEN_PATH_A9_GCC)/bin/arm-none-eabi-gcc # XDC Specific defines ifneq ($(XDC_CFG_FILE_$(CORE)),) ifeq ($(PROFILE_$(CORE)),debug) CFG_CFILENAMEPART_XDC =pa9fg endif ifeq ($(PROFILE_$(CORE)),release) CFG_CFILENAMEPART_XDC =pa9fg endif ifeq ($(PROFILE_$(CORE)),whole_program_debug) CFG_CFILENAMEPART_XDC =p$(FORMAT_EXT)a9f$(ENDIAN_EXT) CFG_LNKFILENAMEPART_XDC=_x endif CFG_CFILE_XDC =$(patsubst %.cfg,%_$(CFG_CFILENAMEPART_XDC).c,$(notdir $(XDC_CFG_FILE_$(CORE)))) CFG_C_XDC = $(addprefix $(CONFIGURO_DIR)/package/cfg/,$(CFG_CFILE_XDC)) XDCLNKCMD_FILE =$(patsubst %.c, %$(CFG_LNKFILENAMEPART_XDC)_x.xdl, $(CFG_C_XDC)) CFG_COBJ_XDC = $(patsubst %.c,%.oa9fg,$(CFG_CFILE_XDC)) LNKCMD_FILE = $(CONFIGURO_DIR)/linker.cmd SPACE := SPACE += XDC_GREP_STRING = $(CONFIGURO_DIRNAME) # XDC_GREP_STRING = $(subst $(SPACE),\|,$(COMP_LIST_$(CORE))) # XDC_GREP_STRING += \|$(CONFIGURO_DIRNAME) endif # Internal CFLAGS - normally doesn't change CFLAGS_INTERNAL = -Wall -Wunknown-pragmas -c -mcpu=cortex-a9 -g -mfpu=neon -mfloat-abi=hard -mabi=aapcs -mapcs-frame -Wswitch CFLAGS_DIROPTS = LNKFLAGS_INTERNAL = -nostartfiles -static -Wl,--gc-sections -mfloat-abi=hard --specs=nano.specs # CFLAGS based on profile selected CFLAGS_XDCINTERNAL = -Dxdc_target_name__=A9F -Dxdc_target_types__=gnu/targets/arm/std.h -Dxdc_cfg__header__='$(CONFIGURO_DIR)/package/cfg/$(XDC_CFG_BASE_FILE_NAME)_xem3.h' -Dxdc_bld__profile_$(PROFILE_$(CORE)) -Dxdc_bld__vers_1_0_4_3_3 # Following 'if...' block is for an application; to add a #define for each # component in the build. This is required to know - at compile time - which # components are on which core. ifndef MODULE_NAME # Derive list of all packages from each of the components needed by the app PKG_LIST_LOCAL = $(foreach COMP,$(COMP_LIST_$(CORE)),$($(COMP)_PKG_LIST)) # Defines for the app and cfg source code to know which components/packages # are included in the build for the local CORE... CFLAGS_APP_DEFINES = $(foreach PKG,$(PKG_LIST_LOCAL),-D_LOCAL_$(PKG)_) CFLAGS_APP_DEFINES += $(foreach PKG,$(PKG_LIST_LOCAL),-D_BUILD_$(PKG)_) ifeq ($(CORE),arm9) PKG_LIST_REMOTE = $(foreach COMP,$(COMP_LIST_arm9),$($(COMP)_PKG_LIST)) CFLAGS_APP_DEFINES += -D_LOCAL_CORE_arm9_ endif # Defines for the app and cfg source code to know which components/packages # are included in the build for the remote CORE... CFLAGS_APP_DEFINES += $(foreach PKG,$(PKG_LIST_REMOTE),-D_REMOTE_$(PKG)_) CFLAGS_APP_DEFINES += $(foreach PKG,$(PKG_LIST_REMOTE),-D_BUILD_$(PKG)_) endif ifeq ($(PROFILE_$(CORE)), debug) CFLAGS_INTERNAL += -D_DEBUG_=1 endif ifeq ($(PROFILE_$(CORE)), release) CFLAGS_INTERNAL += -O2 -s -DNDEBUG LNKFLAGS_INTERNAL_PROFILE = -O2 endif # Assemble CFLAGS from all other CFLAGS definitions _CFLAGS = $(CFLAGS_INTERNAL) $(CFLAGS_XDCINTERNAL) $(CFLAGS_GLOBAL_$(CORE)) $(CFLAGS_LOCAL_COMMON) $(CFLAGS_LOCAL_$(CORE)) $(CFLAGS_LOCAL_$(PLATFORM)) $(CFLAGS_LOCAL_$(SOC)) $(CFLAGS_APP_DEFINES) $(CFLAGS_COMP_COMMON) $(CFLAGS_GLOBAL_$(PLATFORM)) # Object file creation # The second $(CC) compiles the source to generate object $(OBJ_PATHS): $(OBJDIR)/%.$(OBJEXT): %.c $(ECHO) \# Compiling $< to $@ ... $(CC) -c -MD -MF $@.dep $(_CFLAGS) $(INCLUDES) -o $(OBJDIR)/$(basename $(notdir $<)).$(OBJEXT) $< ASMFLAGS = # Object file creation $(OBJ_PATHS_ASM): $(OBJDIR)/%.$(OBJEXT): %.asm $(ECHO) \# Compiling $(PLATFORM):$(CORE):$(PROFILE_$(CORE)):$(APP_NAME)$(MODULE_NAME): $< $(CC) -c -x assembler-with-cpp $(_CFLAGS) $(ASMFLAGS) $(INCLUDES) -o $(OBJDIR)/$(basename $(notdir $<)).$(OBJEXT) $< $(PACKAGE_PATHS): $(PACKAGEDIR)/%: % $(ECHO) \# Copying $(PACKAGE_NAME)/$($(MODULE_NAME)_RELPATH)/$< $(MKDIR) -p $(DEST_ROOT)/package/$(PACKAGE_SELECT)/$(PACKAGE_NAME)/$($(MODULE_NAME)_RELPATH) $(CP) --parents -rf $< $(DEST_ROOT)/package/$(PACKAGE_SELECT)/$(PACKAGE_NAME)/$($(MODULE_NAME)_RELPATH) # Archive flags - normally doesn't change ARFLAGS = cr # Archive/library file creation $(LIBDIR)/$(MODULE_NAME).$(LIBEXT) : $(OBJ_PATHS_ASM) $(OBJ_PATHS) $(ECHO) \# $(ECHO) \# Archiving $(OBJ_PATHS) into $@... $(ECHO) \# $(AR) $(ARFLAGS) $@ $(OBJ_PATHS_ASM) $(OBJ_PATHS) # Linker options and rules LNKFLAGS_INTERNAL_COMMON = # Assemble Linker flags from all other LNKFLAGS definitions _LNKFLAGS = $(LNKFLAGS_INTERNAL) $(LNKFLAGS_INTERNAL_COMMON) $(LNKFLAGS_INTERNAL_PROFILE) $(LNKFLAGS_GLOBAL_$(CORE)) $(LNKFLAGS_LOCAL_COMMON) $(LNKFLAGS_LOCAL_$(CORE)) # Path of the RTS library - normally doesn't change for a given tool-chain RTSLIB_PATH = BIOS_RUNTIME_PATH = $(bios_PATH)/packages/gnu/targets/arm/libs/install-native/arm-none-eabi/lib/hard LIB_PATHS += $(BIOS_RUNTIME_PATH)/libc_nano.a $(BIOS_RUNTIME_PATH)/libm.a $(BIOS_RUNTIME_PATH)/librdimon_nano.a $(BIOS_RUNTIME_PATH)/libg_nano.a LNK_LIBS = $(addprefix -l,$(LIB_PATHS)) # Linker - to create executable file $(BINDIR)/$(APP_NAME)_$(CORE)_$(PROFILE_$(CORE)).$(EXEEXT) : $(OBJ_PATHS) $(LIB_PATHS) $(LNKCMD_FILE) $(CONFIGURO_DIR)/package/cfg/$(CFG_COBJ_XDC) $(ECHO) \# Linking into $@ $(ECHO) \# $(LNK) $(_LNKFLAGS) $(OBJ_PATHS_ASM) $(OBJ_PATHS) -Wl,-T,$(LNKCMD_FILE) -Wl,-Map,$@.map $(LIB_PATHS) -o $@ $(ECHO) \# $(ECHO) \# $@ created. $(ECHO) \# # XDC specific - assemble XDC-Configuro command CONFIGURO_CMD = $(xdc_PATH)/xs xdc.tools.configuro -o $(CONFIGURO_DIR) -t $(TARGET_XDC) -p $(PLATFORM_XDC) \ -r $(PROFILE_$(CORE)) -c $(CODEGEN_PATH_A9_GCC) -b $(CONFIG_BLD_XDC_$(ISA)) $(XDC_CFG_FILE_NAME) _XDC_GREP_STRING = \"$(XDC_GREP_STRING)\" EGREP_CMD = $(EGREP) -ivw $(XDC_GREP_STRING) $(XDCLNKCMD_FILE) # Invoke configuro for the rest of the components # NOTE: 1. String handling is having issues with various make versions when the # cammand is directly tried to be given below. Hence, as a work-around, # the command is re-directed to a file (shell or batch file) and then # executed # 2. The linker.cmd file generated, includes the libraries generated by # XDC. An egrep to search for these and omit in the .cmd file is added # after configuro is done #$(CFG_CFILE_XDC) : $(XDC_CFG_FILE) xdc_configuro : $(XDC_CFG_FILE) $(ECHO) \# Invoking configuro... $(ECHO) -e $(CONFIGURO_CMD) > $(DEST_ROOT)maketemp_configuro_cmd_$(CORE).bat ifeq ($(OS),Windows_NT) CACLS $(DEST_ROOT)maketemp_configuro_cmd_$(CORE).bat /E /P Everyone:F $(DEST_ROOT)maketemp_configuro_cmd_$(CORE).bat else $(CHMOD) a+x $(DEST_ROOT)maketemp_configuro_cmd_$(CORE).bat ./$(DEST_ROOT)maketemp_configuro_cmd_$(CORE).bat endif # $(CP) $(XDCLNKCMD_FILE) $(LNKCMD_FILE) # $(ECHO) @ $(EGREP_CMD) > maketemp_egrep_cmd.bat # ./maketemp_egrep_cmd.bat | $(CYGWINPATH)/bin/tail -n+3 > $(LNKCMD_FILE) # $(EGREP_CMD) > $(LNKCMD_FILE) # $(EGREP) -iv "$(XDC_GREP_STRING)" $(XDCLNKCMD_FILE) > $(LNKCMD_FILE) $(ECHO) \# Configuro done! $(LNKCMD_FILE) : # $(CP) $(XDCLNKCMD_FILE) $(LNKCMD_FILE) # $(ECHO) @ $(EGREP_CMD) > maketemp_egrep_cmd.bat # ./maketemp_egrep_cmd.bat | $(CYGWINPATH)/bin/tail -n+3 > $(LNKCMD_FILE) # $(EGREP_CMD) > $(LNKCMD_FILE) ifndef MODULE_NAME $(CONFIGURO_DIR)/package/cfg/$(CFG_COBJ_XDC) : $(CFG_C_XDC) $(ECHO) \# Compiling generated $< to $@ ... $(CC) $(_CFLAGS) $(INCLUDES) $(CFLAGS_DIROPTS) -o $(CONFIGURO_DIR)/package/cfg/$(CFG_COBJ_XDC) $(CFG_C_XDC) endif # Include dependency make files that were generated by $(CC) -include $(SRCS:%.c=$(DEPDIR)/%.P) # Nothing beyond this point