# Filename: rules_m3.mk # # Make rules for M3 - This file has all the common rules and defines required # for Cortex-M3 ISA # # This file needs to change when: # 1. Code generation tool chain changes (currently it uses TMS470) # 2. Internal switches (which are normally not touched) has to change # 3. XDC specific switches change # 4. a rule common for M3 ISA has to be added or modified # Set compiler/archiver/linker commands and include paths CODEGEN_INCLUDE = $(CODEGEN_PATH_M3)/include CC = $(CODEGEN_PATH_M3)/bin/cl470 AR = $(CODEGEN_PATH_M3)/bin/ar470 LNK = $(CODEGEN_PATH_M3)/bin/lnk470 # Derive a part of RTS Library name based on ENDIAN: little/big ifeq ($(ENDIAN),little) RTSLIB_ENDIAN = le else RTSLIB_ENDIAN = be endif # Derive compiler switch and part of RTS Library name based on FORMAT: COFF/ELF ifeq ($(FORMAT),COFF) CSWITCH_FORMAT = ti_arm9_abi RTSLIB_FORMAT = tiarm9 endif ifeq ($(FORMAT),ELF) CSWITCH_FORMAT = eabi RTSLIB_FORMAT = eabi endif # Internal CFLAGS - normally doesn't change CFLAGS_INTERNAL = -c -qq -pdsw225 --endian=$(ENDIAN) -mv7M3 --abi=$(CSWITCH_FORMAT) -eo.$(OBJEXT) -ea.$(ASMEXT) --symdebug:dwarf CFLAGS_DIROPTS = -fr=$(OBJDIR) -fs=$(OBJDIR) # CFLAGS based on profile selected ifeq ($(PROFILE_$(CORE)), debug) CFLAGS_XDCINTERNAL = -Dxdc_target_name__=M3 -Dxdc_target_types__=ti/targets/arm/elf/std.h -Dxdc_bld__profile_debug -Dxdc_bld__vers_1_0_4_6_1 -D_DEBUG_=1 ifndef MODULE_NAME CFLAGS_XDCINTERNAL += -Dxdc_cfg__header__='$(CONFIGURO_DIR)/package/cfg/$(XDC_CFG_BASE_FILE_NAME)_xem3.h' endif LNKFLAGS_INTERNAL_PROFILE = endif ifeq ($(PROFILE_$(CORE)), whole_program_debug) CFLAGS_XDCINTERNAL = -Dxdc_target_name__=M3 -Dxdc_target_types__=ti/targets/arm/elf/std.h -Dxdc_bld__profile_whole_program_debug -Dxdc_bld__vers_1_0_4_6_1 -ms -oe ifndef MODULE_NAME CFLAGS_XDCINTERNAL += -Dxdc_cfg__header__='$(CONFIGURO_DIR)/package/cfg/$(XDC_CFG_BASE_FILE_NAME)_pem3.h' endif LNKFLAGS_INTERNAL_PROFILE = --opt='--endian=$(ENDIAN) -mv7M3 --abi=$(CSWITCH_FORMAT) -qq -pdsw225 $(CFLAGS_GLOBAL_$(CORE)) -oe --symdebug:dwarf -ms -op2 -O3 -k -os --optimize_with_debug --inline_recursion_limit=20' --strict_compatibility=on # LNKFLAGS_INTERNAL_PROFILE = endif ifeq ($(PROFILE_$(CORE)), release) CFLAGS_XDCINTERNAL = -Dxdc_target_name__=M3 -Dxdc_target_types__=ti/targets/arm/elf/std.h -Dxdc_bld__profile_debug -Dxdc_bld__vers_1_0_4_6_1 -O2 ifndef MODULE_NAME CFLAGS_XDCINTERNAL += -Dxdc_cfg__header__='$(CONFIGURO_DIR)/package/cfg/$(XDC_CFG_BASE_FILE_NAME)_xem3.h' endif LNKFLAGS_INTERNAL_PROFILE = -o2 endif # Following 'if...' block is for an application; to add a #define for each # component in the build. This is required to know - at compile time - which # components are on which core. ifndef MODULE_NAME # Derive list of all packages from each of the components needed by the app PKG_LIST_M3_LOCAL = $(foreach COMP,$(COMP_LIST_$(CORE)),$($(COMP)_PKG_LIST)) # Defines for the app and cfg source code to know which components/packages # are included in the build for the local CORE... CFLAGS_APP_DEFINES = $(foreach PKG,$(PKG_LIST_M3_LOCAL),-D_LOCAL_$(PKG)_) CFLAGS_APP_DEFINES += $(foreach PKG,$(PKG_LIST_M3_LOCAL),-D_BUILD_$(PKG)_) ifeq ($(CORE),m3vpss) PKG_LIST_M3_REMOTE = $(foreach COMP,$(COMP_LIST_m3video),$($(COMP)_PKG_LIST)) CFLAGS_APP_DEFINES += -D_LOCAL_CORE_m3vpss_ endif ifeq ($(CORE),m3video) PKG_LIST_M3_REMOTE = $(foreach COMP,$(COMP_LIST_m3vpss),$($(COMP)_PKG_LIST)) CFLAGS_APP_DEFINES += -D_LOCAL_CORE_m3video_ endif PKG_LIST_A8_REMOTE = $(foreach COMP,$(COMP_LIST_a8host),$($(COMP)_PKG_LIST)) # Defines for the app and cfg source code to know which components/packages # are included in the build for the remote CORE... CFLAGS_APP_DEFINES += $(foreach PKG,$(PKG_LIST_M3_REMOTE),-D_REMOTE_$(PKG)_) CFLAGS_APP_DEFINES += $(foreach PKG,$(PKG_LIST_M3_REMOTE),-D_BUILD_$(PKG)_) CFLAGS_APP_DEFINES += $(foreach PKG,$(PKG_LIST_A8_REMOTE),-D_REMOTE_$(PKG)_) CFLAGS_APP_DEFINES += $(foreach PKG,$(PKG_LIST_A8_REMOTE),-D_BUILD_$(PKG)_) endif # Assemble CFLAGS from all other CFLAGS definitions _CFLAGS = $(CFLAGS_INTERNAL) $(CFLAGS_GLOBAL_$(CORE)) $(CFLAGS_XDCINTERNAL) $(CFLAGS_LOCAL_COMMON) $(CFLAGS_LOCAL_$(CORE)) $(CFLAGS_LOCAL_$(PLATFORM)) $(CFLAGS_LOCAL_$(SOC)) $(CFLAGS_APP_DEFINES) $(CFLAGS_COMP_COMMON) $(CFLAGS_GLOBAL_$(PLATFORM)) # Object file creation # The first $(CC) generates the dependency make files for each of the objects # The second $(CC) compiles the source to generate object $(OBJ_PATHS): $(OBJDIR)/%.$(OBJEXT): %.c $(ECHO) \# Compiling $< to $@ ... $(CC) -ppd=$(DEPFILE).P $(_CFLAGS) $(INCLUDES) $(CFLAGS_DIROPTS) -fc $< $(CC) $(_CFLAGS) $(INCLUDES) $(CFLAGS_DIROPTS) -fc $< # Archive flags - normally doesn't change ARFLAGS = rq # Archive/library file creation $(LIBDIR)/$(MODULE_NAME).$(LIBEXT) : $(OBJ_PATHS) $(ECHO) \# $(ECHO) \# Archiving $(OBJ_PATHS) into $@... $(ECHO) \# $(AR) $(ARFLAGS) $@ $(OBJ_PATHS) # Linker options and rules LNKFLAGS_INTERNAL_COMMON = -w -q -u _c_int00 --silicon_version=7M3 -c --dynamic # Assemble Linker flags from all other LNKFLAGS definitions _LNKFLAGS = $(LNKFLAGS_INTERNAL_COMMON) $(LNKFLAGS_INTERNAL_PROFILE) $(LNKFLAGS_GLOBAL_$(CORE)) $(LNKFLAGS_LOCAL_COMMON) $(LNKFLAGS_LOCAL_$(CORE)) # Path of the RTS library - normally doesn't change for a given tool-chain RTSLIB_PATH = $(CODEGEN_PATH_M3)/lib/rtsv7M3_T_$(RTSLIB_ENDIAN)_$(RTSLIB_FORMAT).lib LIB_PATHS += $(RTSLIB_PATH) LNK_LIBS = $(addprefix -l,$(LIB_PATHS)) ifeq ($(DEST_ROOT),) TMPOBJDIR = . else TMPOBJDIR = $(OBJDIR) endif # Linker - to create executable file $(BINDIR)/$(APP_NAME)_$(CORE)_$(PROFILE_$(CORE)).$(EXEEXT) : $(OBJ_PATHS) $(LIB_PATHS) $(LNKCMD_FILE) $(OBJDIR)/$(CFG_COBJ_XDC) $(ECHO) \# Linking into $@ $(ECHO) \# cd $(TMPOBJDIR) && $(LNK) $(_LNKFLAGS) $(OBJ_PATHS) $(OBJDIR)/$(CFG_COBJ_XDC) $(LNKCMD_FILE) -o $@ -m $@.map $(LNK_LIBS) $(ECHO) \# $(ECHO) \# $@ created. $(ECHO) \# # XDC specific - assemble XDC-Configuro command CONFIGURO_CMD = $(xdc_PATH)/xs xdc.tools.configuro --generationOnly -o $(CONFIGURO_DIR) -t $(TARGET_XDC) -p $(PLATFORM_XDC) \ $(CFGARGS_XDC) -r $(PROFILE_$(CORE)) -b $(CONFIG_BLD_XDC_$(ISA)) $(XDC_CFG_FILE_NAME) _XDC_GREP_STRING = \"$(XDC_GREP_STRING)\" EGREP_CMD = $(EGREP) -ivw $(XDC_GREP_STRING) $(XDCLNKCMD_FILE) ifneq ($(DEST_ROOT),) DEST_ROOT += / endif # Invoke configuro for the rest of the components # NOTE: 1. String handling is having issues with various make versions when the # cammand is directly tried to be given below. Hence, as a work-around, # the command is re-directed to a file (shell or batch file) and then # executed # 2. The linker.cmd file generated, includes the libraries generated by # XDC. An egrep to search for these and omit in the .cmd file is added # after configuro is done #$(CFG_CFILE_XDC) : $(XDC_CFG_FILE) xdc_configuro : $(XDC_CFG_FILE) $(ECHO) \# Invoking configuro... $(ECHO) -e $(CONFIGURO_CMD) > $(DEST_ROOT)maketemp_configuro_cmd_$(CORE).bat $(CHMOD) a+x $(DEST_ROOT)maketemp_configuro_cmd_$(CORE).bat $(DEST_ROOT)maketemp_configuro_cmd_$(CORE).bat $(CP) $(XDCLNKCMD_FILE) $(LNKCMD_FILE) # $(ECHO) @ $(EGREP_CMD) > maketemp_egrep_cmd.bat # ./maketemp_egrep_cmd.bat | $(CYGWINPATH)/bin/tail -n+3 > $(LNKCMD_FILE) # $(EGREP_CMD) > $(LNKCMD_FILE) # $(EGREP) -iv "$(XDC_GREP_STRING)" $(XDCLNKCMD_FILE) > $(LNKCMD_FILE) $(ECHO) \# Configuro done! $(LNKCMD_FILE) : # $(CP) $(XDCLNKCMD_FILE) $(LNKCMD_FILE) # $(ECHO) @ $(EGREP_CMD) > maketemp_egrep_cmd.bat # ./maketemp_egrep_cmd.bat | $(CYGWINPATH)/bin/tail -n+3 > $(LNKCMD_FILE) # $(EGREP_CMD) > $(LNKCMD_FILE) ifndef MODULE_NAME $(OBJDIR)/$(CFG_COBJ_XDC) : $(CFG_C_XDC) $(ECHO) \# Compiling generated $< to $@ ... $(CC) -ppd=$(DEPFILE).P $(_CFLAGS) $(INCLUDES) $(CFLAGS_DIROPTS) -fc $(CFG_C_XDC) $(CC) $(_CFLAGS) $(INCLUDES) $(CFLAGS_DIROPTS) -fc $(CFG_C_XDC) endif # Include dependency make files that were generated by $(CC) -include $(SRCS:%.c=$(DEPDIR)/%.P) # Nothing beyond this point