# File: component.mk # This file is component include make file of OMX. # List of variables set in this file and their purpose: # _RELPATH - This is the relative path of the module, typically from # top-level directory of the package # _PATH - This is the absolute path of the module. It derives from # absolute path of the top-level directory (set in env.mk) # and relative path set above # _INCLUDE - This is the path that has interface header files of the # module. This can be multiple directories (space separated) # _PKG_LIST - Names of the modules (and sub-modules) that are a part # part of this module, including itself. # _PLATFORM_DEPENDENCY - "yes": means the code for this module depends on # platform and the compiled obj/lib has to be kept # under directory # "no" or "" or if this variable is not defined: means # this module has no platform dependent code and hence # the obj/libs are not kept under dir. # _CORE_DEPENDENCY - "yes": means the code for this module depends on # core and the compiled obj/lib has to be kept # under directory # "no" or "" or if this variable is not defined: means # this module has no core dependent code and hence # the obj/libs are not kept under dir. # _APP_STAGE_FILES - List of source files that belongs to the module # , but that needs to be compiled at application # build stage (in the context of the app). This is # primarily for link time configurations or if the # source file is dependent on options/defines that are # application dependent. This can be left blank or # not defined at all, in which case, it means there # no source files in the module that are required # to be compiled in the application build stage. # # List of modules under EDMA3 LLD edma3_lld_COMP_LIST_c6xdsp = edma3_lld_rm edma3_lld_drv # List of examples under EDMA3 LLD edma3_lld_EXAMPLES_LIST = edma3_drv_ti816x-evm_m3_example edma3_drv_c6472-evm_64p_example edma3_drv_c6472-evm_64p_be_example edma3_drv_c6748-evm_674_example \ edma3_drv_da830-evm_674_example edma3_drv_omapl138-evm_674_example \ edma3_drv_tci6486-evm_64p_example edma3_drv_tci6486-evm_64p_be_example edma3_drv_ti816x-evm_674_example \ edma3_drv_ti816x_sim_sample \ edma3_drv_ti814x-evm_674_example edma3_drv_ti814x-evm_a8_example \ edma3_drv_tci6608-sim_66_example edma3_drv_tci6608-sim_66_be_example \ edma3_drv_tci6616-sim_66_example edma3_drv_tci6616-sim_66_be_example \ edma3_drv_tci6614-sim_66_example edma3_drv_tci6614-sim_66_be_example \ edma3_drv_c6657-sim_66_example edma3_drv_c6657-sim_66_be_example \ edma3_drv_tci6638k2k-sim_66_example edma3_drv_tci6638k2k-sim_66_be_example \ edma3_drv_c6670-evm_66_example edma3_drv_c6670-evm_66_be_example \ edma3_drv_c6678-evm_66_example edma3_drv_c6678-evm_66_be_example \ edma3_drv_tci6614-evm_66_example edma3_drv_tci6614-evm_66_be_example \ edma3_drv_c6657-evm_66_example edma3_drv_c6657-evm_66_be_example \ edma3_drv_c66ak2e-evm_66_example edma3_drv_c66ak2e-evm_66_be_example \ edma3_drv_tci6638k2k-evm_66_example edma3_drv_tci6638k2k-evm_66_be_example \ edma3_drv_tci6630k2l-evm_66_example edma3_drv_tci6630k2l-evm_66_be_example \ edma3_drv_tci6636k2h-evm_66_example edma3_drv_tci6636k2h-evm_66_be_example \ edma3_drv_tci6638k2k-evm_a15_example \ edma3_drv_tci6636k2h-evm_a15_example \ edma3_drv_omapl138-evm_arm9_example edma3_drv_omap4-evm_64t_example # List of libraries ifeq ($(PLATFORM),) PLATFORM = tda2xx-evm ti816x-evm ti814x-evm c6a811x-evm c6472-evm c6670-evm c6678-evm c6748-evm da830-evm omapl138-evm tci6486-evm tci6608-sim tci6616-sim tci6614-evm tci6614-sim c6657-evm c66ak2e-evm c6657-sim tci6638k2k-evm tci6630k2l-evm tci6638k2k-sim tci6636k2h-evm endif ifeq ($(TARGET),) TARGET = 674 m3 a8 64p 66 m4 a15 eve edma3_lld_LIBS_ALL = edma3_lld_rm_generic endif #Prepare library list to build from the PLATFORM and TARGET ifeq ($(PLATFORM),generic) edma3_lld_LIBS_ALL = edma3_lld_rm_generic else edma3_lld_LIBS_ALL += $(foreach plat, $(PLATFORM),$(foreach targ,$(TARGET),edma3_lld_$(plat)_$(targ)_libs)) endif #Prepare Example list from PLATFORM and TARGET ifeq ($(ENDIAN),big) edma3_lld_EXAMPLES_LIST = $(foreach plat, $(PLATFORM),$(foreach targ,$(TARGET),edma3_drv_$(plat)_$(targ)_be_example)) else edma3_lld_EXAMPLES_LIST = $(foreach plat, $(PLATFORM),$(foreach targ,$(TARGET),edma3_drv_$(plat)_$(targ)_example)) endif # EDMA3 LLD RM - Resource manager edma3_lld_rm_RELPATH = ti/sdo/edma3/rm edma3_lld_rm_PATH = $(edma3_lld_PATH)/packages/$(edma3_lld_rm_RELPATH) edma3_lld_rm_INCLUDE = $(edma3_lld_rm_PATH) $(edma3_lld_rm_PATH)/src edma3_lld_rm_PKG_LIST = edma3_lld_rm edma3_lld_rm_sample edma3_lld_rm_PLATFORM_DEPENDENCY = yes edma3_lld_rm_sample_RELPATH = ti/sdo/edma3/rm/sample edma3_lld_rm_sample_PATH = $(edma3_lld_PATH)/packages/$(edma3_lld_rm_sample_RELPATH) edma3_lld_rm_sample_INCLUDE = $(edma3_lld_rm_sample_PATH) $(edma3_lld_rm_sample_PATH)/src edma3_lld_rm_sample_PLATFORM_DEPENDENCY = yes # EDMA3 LLD DRV - Driver edma3_lld_drv_RELPATH = ti/sdo/edma3/drv edma3_lld_drv_PATH = $(edma3_lld_PATH)/packages/$(edma3_lld_drv_RELPATH) edma3_lld_drv_INCLUDE = $(edma3_lld_drv_PATH) $(edma3_lld_drv_PATH)/src edma3_lld_drv_PKG_LIST = edma3_lld_drv edma3_lld_drv_sample edma3_lld_drv_PLATFORM_DEPENDENCY = no edma3_lld_drv_sample_RELPATH = ti/sdo/edma3/drv/sample edma3_lld_drv_sample_PATH = $(edma3_lld_PATH)/packages/$(edma3_lld_drv_sample_RELPATH) edma3_lld_drv_sample_INCLUDE = $(edma3_lld_drv_sample_PATH) $(edma3_lld_drv_sample_PATH)/src edma3_lld_drv_sample_PLATFORM_DEPENDENCY = yes # EDMA3 LLD top level edma3_lld_INCLUDE = $(edma3_lld_PATH)/packages $(edma3_lld_rm_INCLUDE) $(edma3_lld_drv_INCLUDE) \ $(edma3_lld_rm_sample_INCLUDE) $(edma3_lld_drv_sample_INCLUDE) # EDMA3 LLD examples edma3_drv_c6472-evm_64p_example_EXAMPLES_RELPATH = examples/edma3_driver/evm6472 edma3_drv_c6472-evm_64p_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6472-evm_64p_example_EXAMPLES_RELPATH) edma3_drv_c6472-evm_64p_be_example_EXAMPLES_RELPATH = examples/edma3_driver/evm6472BE edma3_drv_c6472-evm_64p_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6472-evm_64p_be_example_EXAMPLES_RELPATH) edma3_drv_c6748-evm_674_example_EXAMPLES_RELPATH = examples/edma3_driver/evm6748 edma3_drv_c6748-evm_674_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6748-evm_674_example_EXAMPLES_RELPATH) edma3_drv_da830-evm_674_example_EXAMPLES_RELPATH = examples/edma3_driver/evmDA830 edma3_drv_da830-evm_674_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_da830-evm_674_example_EXAMPLES_RELPATH) edma3_drv_omapl138-evm_674_example_EXAMPLES_RELPATH = examples/edma3_driver/evmOMAPL138 edma3_drv_omapl138-evm_674_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_omapl138-evm_674_example_EXAMPLES_RELPATH) edma3_drv_omap4-evm_64t_example_EXAMPLES_RELPATH = examples/edma3_driver/evmOMAP4 edma3_drv_omap4-evm_64t_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_omap4-evm_64t_example_EXAMPLES_RELPATH) edma3_drv_omapl138-evm_arm9_example_EXAMPLES_RELPATH = examples/edma3_driver/evmOMAPL138_ARM edma3_drv_omapl138-evm_arm9_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_omapl138-evm_arm9_example_EXAMPLES_RELPATH) edma3_drv_tci6486-evm_64p_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTCI6486 edma3_drv_tci6486-evm_64p_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6486-evm_64p_example_EXAMPLES_RELPATH) edma3_drv_tci6486-evm_64p_be_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTCI6486BE edma3_drv_tci6486-evm_64p_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6486-evm_64p_be_example_EXAMPLES_RELPATH) edma3_drv_ti814x-evm_674_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTI814x edma3_drv_ti814x-evm_674_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_ti814x-evm_674_example_EXAMPLES_RELPATH) edma3_drv_ti814x-evm_a8_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTI814x_A8 edma3_drv_ti814x-evm_a8_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_ti814x-evm_a8_example_EXAMPLES_RELPATH) edma3_drv_ti814x-evm_m3_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTI814x_M3 edma3_drv_ti814x-evm_m3_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_ti814x-evm_m3_example_EXAMPLES_RELPATH) edma3_drv_ti816x-evm_674_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTI816x edma3_drv_ti816x-evm_674_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_ti816x-evm_674_example_EXAMPLES_RELPATH) edma3_drv_ti816x-evm_a8_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTI816x_A8 edma3_drv_ti816x-evm_a8_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_ti816x-evm_a8_example_EXAMPLES_RELPATH) edma3_drv_ti816x-evm_m3_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTI816x_M3 edma3_drv_ti816x-evm_m3_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_ti816x-evm_m3_example_EXAMPLES_RELPATH) edma3_drv_c6a811x-evm_674_example_EXAMPLES_RELPATH = examples/edma3_driver/evmC6A811x edma3_drv_c6a811x-evm_674_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6a811x-evm_674_example_EXAMPLES_RELPATH) edma3_drv_c6a811x-evm_a8_example_EXAMPLES_RELPATH = examples/edma3_driver/evmC6A811x_A8 edma3_drv_c6a811x-evm_a8_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6a811x-evm_a8_example_EXAMPLES_RELPATH) edma3_drv_c6a811x-evm_m3_example_EXAMPLES_RELPATH = examples/edma3_driver/evmC6A811x_M3 edma3_drv_c6a811x-evm_m3_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6a811x-evm_m3_example_EXAMPLES_RELPATH) edma3_drv_tci6608-sim_66_example_EXAMPLES_RELPATH = examples/edma3_driver/simTCI6608 edma3_drv_tci6608-sim_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6608-sim_66_example_EXAMPLES_RELPATH) edma3_drv_tci6608-sim_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/simTCI6608BE edma3_drv_tci6608-sim_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6608-sim_66_be_example_EXAMPLES_RELPATH) edma3_drv_tci6616-sim_66_example_EXAMPLES_RELPATH = examples/edma3_driver/simTCI6616 edma3_drv_tci6616-sim_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6616-sim_66_example_EXAMPLES_RELPATH) edma3_drv_tci6616-sim_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/simTCI6616BE edma3_drv_tci6616-sim_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6616-sim_66_be_example_EXAMPLES_RELPATH) edma3_drv_tci6614-sim_66_example_EXAMPLES_RELPATH = examples/edma3_driver/simTCI6614 edma3_drv_tci6614-sim_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6614-sim_66_example_EXAMPLES_RELPATH) edma3_drv_tci6614-sim_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/simTCI6614BE edma3_drv_tci6614-sim_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6614-sim_66_be_example_EXAMPLES_RELPATH) edma3_drv_c6657-sim_66_example_EXAMPLES_RELPATH = examples/edma3_driver/simC6657 edma3_drv_c6657-sim_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6657-sim_66_example_EXAMPLES_RELPATH) edma3_drv_c6657-sim_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/simC6657BE edma3_drv_c6657-sim_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6657-sim_66_be_example_EXAMPLES_RELPATH) edma3_drv_tci6638k2k-sim_66_example_EXAMPLES_RELPATH = examples/edma3_driver/simTCI6638K2K edma3_drv_tci6638k2k-sim_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6638k2k-sim_66_example_EXAMPLES_RELPATH) edma3_drv_tci6638k2k-sim_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/simTCI6638K2KBE edma3_drv_tci6638k2k-sim_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6638k2k-sim_66_be_example_EXAMPLES_RELPATH) edma3_drv_c6670-evm_66_example_EXAMPLES_RELPATH = examples/edma3_driver/evm6670 edma3_drv_c6670-evm_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6670-evm_66_example_EXAMPLES_RELPATH) edma3_drv_c6670-evm_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/evm6670BE edma3_drv_c6670-evm_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6670-evm_66_be_example_EXAMPLES_RELPATH) edma3_drv_c6678-evm_66_example_EXAMPLES_RELPATH = examples/edma3_driver/evm6678 edma3_drv_c6678-evm_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6678-evm_66_example_EXAMPLES_RELPATH) edma3_drv_c6678-evm_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/evm6678BE edma3_drv_c6678-evm_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6678-evm_66_be_example_EXAMPLES_RELPATH) edma3_drv_c66ak2e-evm_66_example_EXAMPLES_RELPATH = examples/edma3_driver/evmC66AK2E edma3_drv_c66ak2e-evm_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c66ak2e-evm_66_example_EXAMPLES_RELPATH) edma3_drv_c66ak2e-evm_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/evmC66AK2EBE edma3_drv_c66ak2e-evm_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c66ak2e-evm_66_be_example_EXAMPLES_RELPATH) edma3_drv_tci6614-evm_66_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTCI6614 edma3_drv_tci6614-evm_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6614-evm_66_example_EXAMPLES_RELPATH) edma3_drv_tci6614-evm_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTCI6614BE edma3_drv_tci6614-evm_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6614-evm_66_be_example_EXAMPLES_RELPATH) edma3_drv_c6657-evm_66_example_EXAMPLES_RELPATH = examples/edma3_driver/evm6657 edma3_drv_c6657-evm_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6657-evm_66_example_EXAMPLES_RELPATH) edma3_drv_c6657-evm_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/evm6657BE edma3_drv_c6657-evm_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c6657-evm_66_be_example_EXAMPLES_RELPATH) edma3_drv_tci6638k2k-evm_66_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTCI6638K2K edma3_drv_tci6638k2k-evm_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6638k2k-evm_66_example_EXAMPLES_RELPATH) edma3_drv_tci6638k2k-evm_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTCI6638K2KBE edma3_drv_tci6638k2k-evm_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6638k2k-evm_66_be_example_EXAMPLES_RELPATH) edma3_drv_tci6630k2l-evm_66_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTCI6630K2L edma3_drv_tci6630k2l-evm_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6630k2l-evm_66_example_EXAMPLES_RELPATH) edma3_drv_tci6630k2l-evm_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTCI6630K2LBE edma3_drv_tci6630k2l-evm_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6630k2l-evm_66_be_example_EXAMPLES_RELPATH) edma3_drv_tci6636k2h-evm_66_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTCI6636K2H edma3_drv_tci6636k2h-evm_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6636k2h-evm_66_example_EXAMPLES_RELPATH) edma3_drv_tci6636k2h-evm_66_be_example_EXAMPLES_RELPATH = examples/edma3_driver/evmTCI6636K2HBE edma3_drv_tci6636k2h-evm_66_be_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6636k2h-evm_66_be_example_EXAMPLES_RELPATH) edma3_drv_tda2xx-evm_m4_example_EXAMPLES_RELPATH = examples/edma3_driver/evmtda2xx_M4 edma3_drv_tda2xx-evm_m4_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tda2xx-evm_m4_example_EXAMPLES_RELPATH) edma3_drv_tda2xx-evm_a15_example_EXAMPLES_RELPATH = examples/edma3_driver/evmtda2xx_A15 edma3_drv_tda2xx-evm_a15_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tda2xx-evm_a15_example_EXAMPLES_RELPATH) edma3_drv_tda2xx-evm_66_example_EXAMPLES_RELPATH = examples/edma3_driver/evmtda2xx edma3_drv_tda2xx-evm_66_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tda2xx-evm_66_example_EXAMPLES_RELPATH) edma3_drv_tci6636k2h-evm_a15_example_EXAMPLES_RELPATH = examples/edma3_user_space_driver/evmTCI6636K2H edma3_drv_tci6636k2h-evm_a15_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6636k2h-evm_a15_example_EXAMPLES_RELPATH) edma3_drv_tci6638k2k-evm_a15_example_EXAMPLES_RELPATH = examples/edma3_user_space_driver/evmTCI6638K2K edma3_drv_tci6638k2k-evm_a15_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6638k2k-evm_a15_example_EXAMPLES_RELPATH) edma3_drv_c66ak2e-evm_a15_example_EXAMPLES_RELPATH = examples/edma3_user_space_driver/evmC66AK2E edma3_drv_c66ak2e-evm_a15_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_c66ak2e-evm_a15_example_EXAMPLES_RELPATH) edma3_drv_tci6630k2l-evm_a15_example_EXAMPLES_RELPATH = examples/edma3_user_space_driver/evmTCI6630K2L edma3_drv_tci6630k2l-evm_a15_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tci6630k2l-evm_a15_example_EXAMPLES_RELPATH) edma3_drv_tda2xx-evm_eve_example_EXAMPLES_RELPATH = examples/edma3_driver/evmtda2xx_EVE edma3_drv_tda2xx-evm_eve_example_EXAMPLES_PATH = $(edma3_lld_PATH)/$(edma3_drv_tda2xx-evm_eve_example_EXAMPLES_RELPATH) # Nothing beyond this point