# Doxyfile 1.6.1 # This file describes the settings to be used by the documentation system # doxygen (www.doxygen.org) for a project # # All text after a hash (#) is considered a comment and will be ignored # The format is: # TAG = value [value, ...] # For lists items can also be appended using: # TAG += value [value, ...] # Values that contain spaces should be placed between quotes (" ") #--------------------------------------------------------------------------- # Project related configuration options #--------------------------------------------------------------------------- # This tag specifies the encoding used for all characters in the config file # that follow. The default is UTF-8 which is also the encoding used for all # text before the first occurrence of this tag. Doxygen uses libiconv (or the # iconv built into libc) for the transcoding. See # http://www.gnu.org/software/libiconv for the list of possible encodings. DOXYFILE_ENCODING = UTF-8 # The PROJECT_NAME tag is a single word (or a sequence of words surrounded # by quotes) that should identify the project. PROJECT_NAME = "EDMA3 Driver" # The PROJECT_NUMBER tag can be used to enter a project or revision number. # This could be handy for archiving the generated documentation or # if some version control system is used. PROJECT_NUMBER = 02.11.04 # The OUTPUT_DIRECTORY tag is used to specify the (relative or absolute) # base path where the generated documentation will be put. # If a relative path is entered, it will be relative to the location # where doxygen was started. If left blank the current directory will be used. OUTPUT_DIRECTORY = . # If the CREATE_SUBDIRS tag is set to YES, then doxygen will create # 4096 sub-directories (in 2 levels) under the output directory of each output # format and will distribute the generated files over these directories. # Enabling this option can be useful when feeding doxygen a huge amount of # source files, where putting all generated files in the same directory would # otherwise cause performance problems for the file system. CREATE_SUBDIRS = NO # The OUTPUT_LANGUAGE tag is used to specify the language in which all # documentation generated by doxygen is written. Doxygen will use this # information to generate all constant output in the proper language. # The default language is English, other supported languages are: # Afrikaans, Arabic, Brazilian, Catalan, Chinese, Chinese-Traditional, # Croatian, Czech, Danish, Dutch, Esperanto, Farsi, Finnish, French, German, # Greek, Hungarian, Italian, Japanese, Japanese-en (Japanese with English # messages), Korean, Korean-en, Lithuanian, Norwegian, Macedonian, Persian, # Polish, Portuguese, Romanian, Russian, Serbian, Serbian-Cyrilic, Slovak, # Slovene, Spanish, Swedish, Ukrainian, and Vietnamese. OUTPUT_LANGUAGE = English # If the BRIEF_MEMBER_DESC tag is set to YES (the default) Doxygen will # include brief member descriptions after the members that are listed in # the file and class documentation (similar to JavaDoc). # Set to NO to disable this. BRIEF_MEMBER_DESC = YES # If the REPEAT_BRIEF tag is set to YES (the default) Doxygen will prepend # the brief description of a member or function before the detailed description. # Note: if both HIDE_UNDOC_MEMBERS and BRIEF_MEMBER_DESC are set to NO, the # brief descriptions will be completely suppressed. REPEAT_BRIEF = YES # This tag implements a quasi-intelligent brief description abbreviator # that is used to form the text in various listings. Each string # in this list, if found as the leading text of the brief description, will be # stripped from the text and the result after processing the whole list, is # used as the annotated text. Otherwise, the brief description is used as-is. # If left blank, the following values are used ("$name" is automatically # replaced with the name of the entity): "The $name class" "The $name widget" # "The $name file" "is" "provides" "specifies" "contains" # "represents" "a" "an" "the" ABBREVIATE_BRIEF = # If the ALWAYS_DETAILED_SEC and REPEAT_BRIEF tags are both set to YES then # Doxygen will generate a detailed section even if there is only a brief # description. ALWAYS_DETAILED_SEC = NO # If the INLINE_INHERITED_MEMB tag is set to YES, doxygen will show all # inherited members of a class in the documentation of that class as if those # members were ordinary class members. Constructors, destructors and assignment # operators of the base classes will not be shown. INLINE_INHERITED_MEMB = NO # If the FULL_PATH_NAMES tag is set to YES then Doxygen will prepend the full # path before files name in the file list and in the header files. If set # to NO the shortest path that makes the file name unique will be used. FULL_PATH_NAMES = NO # If the FULL_PATH_NAMES tag is set to YES then the STRIP_FROM_PATH tag # can be used to strip a user-defined part of the path. Stripping is # only done if one of the specified strings matches the left-hand part of # the path. The tag can be used to show relative paths in the file list. # If left blank the directory from which doxygen is run is used as the # path to strip. STRIP_FROM_PATH = # The STRIP_FROM_INC_PATH tag can be used to strip a user-defined part of # the path mentioned in the documentation of a class, which tells # the reader which header file to include in order to use a class. # If left blank only the name of the header file containing the class # definition is used. Otherwise one should specify the include paths that # are normally passed to the compiler using the -I flag. STRIP_FROM_INC_PATH = # If the SHORT_NAMES tag is set to YES, doxygen will generate much shorter # (but less readable) file names. This can be useful is your file systems # doesn't support long names like on DOS, Mac, or CD-ROM. SHORT_NAMES = NO # If the JAVADOC_AUTOBRIEF tag is set to YES then Doxygen # will interpret the first line (until the first dot) of a JavaDoc-style # comment as the brief description. If set to NO, the JavaDoc # comments will behave just like regular Qt-style comments # (thus requiring an explicit @brief command for a brief description.) JAVADOC_AUTOBRIEF = NO # If the QT_AUTOBRIEF tag is set to YES then Doxygen will # interpret the first line (until the first dot) of a Qt-style # comment as the brief description. If set to NO, the comments # will behave just like regular Qt-style comments (thus requiring # an explicit \brief command for a brief description.) QT_AUTOBRIEF = NO # The MULTILINE_CPP_IS_BRIEF tag can be set to YES to make Doxygen # treat a multi-line C++ special comment block (i.e. a block of //! or /// # comments) as a brief description. This used to be the default behaviour. # The new default is to treat a multi-line C++ comment block as a detailed # description. Set this tag to YES if you prefer the old behaviour instead. MULTILINE_CPP_IS_BRIEF = NO # If the INHERIT_DOCS tag is set to YES (the default) then an undocumented # member inherits the documentation from any documented member that it # re-implements. INHERIT_DOCS = YES # If the SEPARATE_MEMBER_PAGES tag is set to YES, then doxygen will produce # a new page for each member. If set to NO, the documentation of a member will # be part of the file/class/namespace that contains it. SEPARATE_MEMBER_PAGES = NO # The TAB_SIZE tag can be used to set the number of spaces in a tab. # Doxygen uses this value to replace tabs by spaces in code fragments. TAB_SIZE = 8 # This tag can be used to specify a number of aliases that acts # as commands in the documentation. An alias has the form "name=value". # For example adding "sideeffect=\par Side Effects:\n" will allow you to # put the command \sideeffect (or @sideeffect) in the documentation, which # will result in a user-defined paragraph with heading "Side Effects:". # You can put \n's in the value part of an alias to insert newlines. ALIASES = # Set the OPTIMIZE_OUTPUT_FOR_C tag to YES if your project consists of C # sources only. Doxygen will then generate output that is more tailored for C. # For instance, some of the names that are used will be different. The list # of all members will be omitted, etc. OPTIMIZE_OUTPUT_FOR_C = YES # Set the OPTIMIZE_OUTPUT_JAVA tag to YES if your project consists of Java # sources only. Doxygen will then generate output that is more tailored for # Java. For instance, namespaces will be presented as packages, qualified # scopes will look different, etc. OPTIMIZE_OUTPUT_JAVA = NO # Set the OPTIMIZE_FOR_FORTRAN tag to YES if your project consists of Fortran # sources only. Doxygen will then generate output that is more tailored for # Fortran. OPTIMIZE_FOR_FORTRAN = NO # Set the OPTIMIZE_OUTPUT_VHDL tag to YES if your project consists of VHDL # sources. Doxygen will then generate output that is tailored for # VHDL. OPTIMIZE_OUTPUT_VHDL = NO # Doxygen selects the parser to use depending on the extension of the files it parses. # With this tag you can assign which parser to use for a given extension. # Doxygen has a built-in mapping, but you can override or extend it using this tag. # The format is ext=language, where ext is a file extension, and language is one of # the parsers supported by doxygen: IDL, Java, Javascript, C#, C, C++, D, PHP, # Objective-C, Python, Fortran, VHDL, C, C++. For instance to make doxygen treat # .inc files as Fortran files (default is PHP), and .f files as C (default is Fortran), # use: inc=Fortran f=C. Note that for custom extensions you also need to set # FILE_PATTERNS otherwise the files are not read by doxygen. EXTENSION_MAPPING = # If you use STL classes (i.e. std::string, std::vector, etc.) but do not want # to include (a tag file for) the STL sources as input, then you should # set this tag to YES in order to let doxygen match functions declarations and # definitions whose arguments contain STL classes (e.g. func(std::string); v.s. # func(std::string) {}). This also make the inheritance and collaboration # diagrams that involve STL classes more complete and accurate. BUILTIN_STL_SUPPORT = NO # If you use Microsoft's C++/CLI language, you should set this option to YES to # enable parsing support. CPP_CLI_SUPPORT = NO # Set the SIP_SUPPORT tag to YES if your project consists of sip sources only. # Doxygen will parse them like normal C++ but will assume all classes use public # instead of private inheritance when no explicit protection keyword is present. SIP_SUPPORT = NO # For Microsoft's IDL there are propget and propput attributes to indicate getter # and setter methods for a property. Setting this option to YES (the default) # will make doxygen to replace the get and set methods by a property in the # documentation. This will only work if the methods are indeed getting or # setting a simple type. If this is not the case, or you want to show the # methods anyway, you should set this option to NO. IDL_PROPERTY_SUPPORT = YES # If member grouping is used in the documentation and the DISTRIBUTE_GROUP_DOC # tag is set to YES, then doxygen will reuse the documentation of the first # member in the group (if any) for the other members of the group. By default # all members of a group must be documented explicitly. DISTRIBUTE_GROUP_DOC = NO # Set the SUBGROUPING tag to YES (the default) to allow class member groups of # the same type (for instance a group of public functions) to be put as a # subgroup of that type (e.g. under the Public Functions section). Set it to # NO to prevent subgrouping. Alternatively, this can be done per class using # the \nosubgrouping command. SUBGROUPING = YES # When TYPEDEF_HIDES_STRUCT is enabled, a typedef of a struct, union, or enum # is documented as struct, union, or enum with the name of the typedef. So # typedef struct TypeS {} TypeT, will appear in the documentation as a struct # with name TypeT. When disabled the typedef will appear as a member of a file, # namespace, or class. And the struct will be named TypeS. This can typically # be useful for C code in case the coding convention dictates that all compound # types are typedef'ed and only the typedef is referenced, never the tag name. TYPEDEF_HIDES_STRUCT = NO # The SYMBOL_CACHE_SIZE determines the size of the internal cache use to # determine which symbols to keep in memory and which to flush to disk. # When the cache is full, less often used symbols will be written to disk. # For small to medium size projects (<1000 input files) the default value is # probably good enough. For larger projects a too small cache size can cause # doxygen to be busy swapping symbols to and from disk most of the time # causing a significant performance penality. # If the system has enough physical memory increasing the cache will improve the # performance by keeping more symbols in memory. Note that the value works on # a logarithmic scale so increasing the size by one will rougly double the # memory usage. The cache size is given by this formula: # 2^(16+SYMBOL_CACHE_SIZE). The valid range is 0..9, the default is 0, # corresponding to a cache size of 2^16 = 65536 symbols SYMBOL_CACHE_SIZE = 0 #--------------------------------------------------------------------------- # Build related configuration options #--------------------------------------------------------------------------- # If the EXTRACT_ALL tag is set to YES doxygen will assume all entities in # documentation are documented, even if no documentation was available. # Private class members and static file members will be hidden unless # the EXTRACT_PRIVATE and EXTRACT_STATIC tags are set to YES EXTRACT_ALL = NO # If the EXTRACT_PRIVATE tag is set to YES all private members of a class # will be included in the documentation. EXTRACT_PRIVATE = NO # If the EXTRACT_STATIC tag is set to YES all static members of a file # will be included in the documentation. EXTRACT_STATIC = YES # If the EXTRACT_LOCAL_CLASSES tag is set to YES classes (and structs) # defined locally in source files will be included in the documentation. # If set to NO only classes defined in header files are included. EXTRACT_LOCAL_CLASSES = YES # This flag is only useful for Objective-C code. When set to YES local # methods, which are defined in the implementation section but not in # the interface are included in the documentation. # If set to NO (the default) only methods in the interface are included. EXTRACT_LOCAL_METHODS = NO # If this flag is set to YES, the members of anonymous namespaces will be # extracted and appear in the documentation as a namespace called # 'anonymous_namespace{file}', where file will be replaced with the base # name of the file that contains the anonymous namespace. By default # anonymous namespace are hidden. EXTRACT_ANON_NSPACES = NO # If the HIDE_UNDOC_MEMBERS tag is set to YES, Doxygen will hide all # undocumented members of documented classes, files or namespaces. # If set to NO (the default) these members will be included in the # various overviews, but no documentation section is generated. # This option has no effect if EXTRACT_ALL is enabled. HIDE_UNDOC_MEMBERS = YES # If the HIDE_UNDOC_CLASSES tag is set to YES, Doxygen will hide all # undocumented classes that are normally visible in the class hierarchy. # If set to NO (the default) these classes will be included in the various # overviews. This option has no effect if EXTRACT_ALL is enabled. HIDE_UNDOC_CLASSES = YES # If the HIDE_FRIEND_COMPOUNDS tag is set to YES, Doxygen will hide all # friend (class|struct|union) declarations. # If set to NO (the default) these declarations will be included in the # documentation. HIDE_FRIEND_COMPOUNDS = NO # If the HIDE_IN_BODY_DOCS tag is set to YES, Doxygen will hide any # documentation blocks found inside the body of a function. # If set to NO (the default) these blocks will be appended to the # function's detailed documentation block. HIDE_IN_BODY_DOCS = YES # The INTERNAL_DOCS tag determines if documentation # that is typed after a \internal command is included. If the tag is set # to NO (the default) then the documentation will be excluded. # Set it to YES to include the internal documentation. INTERNAL_DOCS = NO # If the CASE_SENSE_NAMES tag is set to NO then Doxygen will only generate # file names in lower-case letters. If set to YES upper-case letters are also # allowed. This is useful if you have classes or files whose names only differ # in case and if your file system supports case sensitive file names. Windows # and Mac users are advised to set this option to NO. CASE_SENSE_NAMES = NO # If the HIDE_SCOPE_NAMES tag is set to NO (the default) then Doxygen # will show members with their full class and namespace scopes in the # documentation. If set to YES the scope will be hidden. HIDE_SCOPE_NAMES = NO # If the SHOW_INCLUDE_FILES tag is set to YES (the default) then Doxygen # will put a list of the files that are included by a file in the documentation # of that file. SHOW_INCLUDE_FILES = YES # If the INLINE_INFO tag is set to YES (the default) then a tag [inline] # is inserted in the documentation for inline members. INLINE_INFO = YES # If the SORT_MEMBER_DOCS tag is set to YES (the default) then doxygen # will sort the (detailed) documentation of file and class members # alphabetically by member name. If set to NO the members will appear in # declaration order. SORT_MEMBER_DOCS = NO # If the SORT_BRIEF_DOCS tag is set to YES then doxygen will sort the # brief documentation of file, namespace and class members alphabetically # by member name. If set to NO (the default) the members will appear in # declaration order. SORT_BRIEF_DOCS = NO # If the SORT_MEMBERS_CTORS_1ST tag is set to YES then doxygen # will sort the (brief and detailed) documentation of class members so that # constructors and destructors are listed first. If set to NO (the default) # the constructors will appear in the respective orders defined by # SORT_MEMBER_DOCS and SORT_BRIEF_DOCS. # This tag will be ignored for brief docs if SORT_BRIEF_DOCS is set to NO # and ignored for detailed docs if SORT_MEMBER_DOCS is set to NO. SORT_MEMBERS_CTORS_1ST = NO # If the SORT_GROUP_NAMES tag is set to YES then doxygen will sort the # hierarchy of group names into alphabetical order. If set to NO (the default) # the group names will appear in their defined order. SORT_GROUP_NAMES = NO # If the SORT_BY_SCOPE_NAME tag is set to YES, the class list will be # sorted by fully-qualified names, including namespaces. If set to # NO (the default), the class list will be sorted only by class name, # not including the namespace part. # Note: This option is not very useful if HIDE_SCOPE_NAMES is set to YES. # Note: This option applies only to the class list, not to the # alphabetical list. SORT_BY_SCOPE_NAME = NO # The GENERATE_TODOLIST tag can be used to enable (YES) or # disable (NO) the todo list. This list is created by putting \todo # commands in the documentation. GENERATE_TODOLIST = YES # The GENERATE_TESTLIST tag can be used to enable (YES) or # disable (NO) the test list. This list is created by putting \test # commands in the documentation. GENERATE_TESTLIST = YES # The GENERATE_BUGLIST tag can be used to enable (YES) or # disable (NO) the bug list. This list is created by putting \bug # commands in the documentation. GENERATE_BUGLIST = YES # The GENERATE_DEPRECATEDLIST tag can be used to enable (YES) or # disable (NO) the deprecated list. This list is created by putting # \deprecated commands in the documentation. GENERATE_DEPRECATEDLIST= YES # The ENABLED_SECTIONS tag can be used to enable conditional # documentation sections, marked by \if sectionname ... \endif. ENABLED_SECTIONS = # The MAX_INITIALIZER_LINES tag determines the maximum number of lines # the initial value of a variable or define consists of for it to appear in # the documentation. If the initializer consists of more lines than specified # here it will be hidden. Use a value of 0 to hide initializers completely. # The appearance of the initializer of individual variables and defines in the # documentation can be controlled using \showinitializer or \hideinitializer # command in the documentation regardless of this setting. MAX_INITIALIZER_LINES = 30 # Set the SHOW_USED_FILES tag to NO to disable the list of files generated # at the bottom of the documentation of classes and structs. If set to YES the # list will mention the files that were used to generate the documentation. SHOW_USED_FILES = YES # If the sources in your project are distributed over multiple directories # then setting the SHOW_DIRECTORIES tag to YES will show the directory hierarchy # in the documentation. The default is NO. SHOW_DIRECTORIES = NO # Set the SHOW_FILES tag to NO to disable the generation of the Files page. # This will remove the Files entry from the Quick Index and from the # Folder Tree View (if specified). The default is YES. SHOW_FILES = YES # Set the SHOW_NAMESPACES tag to NO to disable the generation of the # Namespaces page. This will remove the Namespaces entry from the Quick Index # and from the Folder Tree View (if specified). The default is YES. SHOW_NAMESPACES = YES # The FILE_VERSION_FILTER tag can be used to specify a program or script that # doxygen should invoke to get the current version for each file (typically from # the version control system). Doxygen will invoke the program by executing (via # popen()) the command , where is the value of # the FILE_VERSION_FILTER tag, and is the name of an input file # provided by doxygen. Whatever the program writes to standard output # is used as the file version. See the manual for examples. FILE_VERSION_FILTER = # The LAYOUT_FILE tag can be used to specify a layout file which will be parsed by # doxygen. The layout file controls the global structure of the generated output files # in an output format independent way. The create the layout file that represents # doxygen's defaults, run doxygen with the -l option. You can optionally specify a # file name after the option, if omitted DoxygenLayout.xml will be used as the name # of the layout file. LAYOUT_FILE = #--------------------------------------------------------------------------- # configuration options related to warning and progress messages #--------------------------------------------------------------------------- # The QUIET tag can be used to turn on/off the messages that are generated # by doxygen. Possible values are YES and NO. If left blank NO is used. QUIET = NO # The WARNINGS tag can be used to turn on/off the warning messages that are # generated by doxygen. Possible values are YES and NO. If left blank # NO is used. WARNINGS = YES # If WARN_IF_UNDOCUMENTED is set to YES, then doxygen will generate warnings # for undocumented members. If EXTRACT_ALL is set to YES then this flag will # automatically be disabled. WARN_IF_UNDOCUMENTED = YES # If WARN_IF_DOC_ERROR is set to YES, doxygen will generate warnings for # potential errors in the documentation, such as not documenting some # parameters in a documented function, or documenting parameters that # don't exist or using markup commands wrongly. WARN_IF_DOC_ERROR = YES # This WARN_NO_PARAMDOC option can be abled to get warnings for # functions that are documented, but have no documentation for their parameters # or return value. If set to NO (the default) doxygen will only warn about # wrong or incomplete parameter documentation, but not about the absence of # documentation. WARN_NO_PARAMDOC = NO # The WARN_FORMAT tag determines the format of the warning messages that # doxygen can produce. The string should contain the $file, $line, and $text # tags, which will be replaced by the file and line number from which the # warning originated and the warning text. Optionally the format may contain # $version, which will be replaced by the version of the file (if it could # be obtained via FILE_VERSION_FILTER) WARN_FORMAT = "$file:$line: $text" # The WARN_LOGFILE tag can be used to specify a file to which warning # and error messages should be written. If left blank the output is written # to stderr. WARN_LOGFILE = #--------------------------------------------------------------------------- # configuration options related to the input files #--------------------------------------------------------------------------- # The INPUT tag can be used to specify the files and/or directories that contain # documented source files. You may enter file names like "myfile.cpp" or # directories like "/usr/src/myproject". Separate the files or directories # with spaces. INPUT = ..\edma3_drv.h \ ..\src # This tag can be used to specify the character encoding of the source files # that doxygen parses. Internally doxygen uses the UTF-8 encoding, which is # also the default input encoding. Doxygen uses libiconv (or the iconv built # into libc) for the transcoding. See http://www.gnu.org/software/libiconv for # the list of possible encodings. INPUT_ENCODING = UTF-8 # If the value of the INPUT tag contains directories, you can use the # FILE_PATTERNS tag to specify one or more wildcard pattern (like *.cpp # and *.h) to filter out the source-files in the directories. If left # blank the following patterns are tested: # *.c *.cc *.cxx *.cpp *.c++ *.java *.ii *.ixx *.ipp *.i++ *.inl *.h *.hh *.hxx # *.hpp *.h++ *.idl *.odl *.cs *.php *.php3 *.inc *.m *.mm *.py *.f90 FILE_PATTERNS = *.c \ *.h # The RECURSIVE tag can be used to turn specify whether or not subdirectories # should be searched for input files as well. Possible values are YES and NO. # If left blank NO is used. RECURSIVE = YES # The EXCLUDE tag can be used to specify files and/or directories that should # excluded from the INPUT source files. This way you can easily exclude a # subdirectory from a directory tree whose root is specified with the INPUT tag. EXCLUDE = # The EXCLUDE_SYMLINKS tag can be used select whether or not files or # directories that are symbolic links (a Unix filesystem feature) are excluded # from the input. EXCLUDE_SYMLINKS = NO # If the value of the INPUT tag contains directories, you can use the # EXCLUDE_PATTERNS tag to specify one or more wildcard patterns to exclude # certain files from those directories. Note that the wildcards are matched # against the file with absolute path, so to exclude all test directories # for example use the pattern */test/* EXCLUDE_PATTERNS = # The EXCLUDE_SYMBOLS tag can be used to specify one or more symbol names # (namespaces, classes, functions, etc.) that should be excluded from the # output. The symbol name can be a fully qualified name, a word, or if the # wildcard * is used, a substring. Examples: ANamespace, AClass, # AClass::ANamespace, ANamespace::*Test EXCLUDE_SYMBOLS = # The EXAMPLE_PATH tag can be used to specify one or more files or # directories that contain example code fragments that are included (see # the \include command). EXAMPLE_PATH = # If the value of the EXAMPLE_PATH tag contains directories, you can use the # EXAMPLE_PATTERNS tag to specify one or more wildcard pattern (like *.cpp # and *.h) to filter out the source-files in the directories. If left # blank all files are included. EXAMPLE_PATTERNS = # If the EXAMPLE_RECURSIVE tag is set to YES then subdirectories will be # searched for input files to be used with the \include or \dontinclude # commands irrespective of the value of the RECURSIVE tag. # Possible values are YES and NO. If left blank NO is used. EXAMPLE_RECURSIVE = NO # The IMAGE_PATH tag can be used to specify one or more files or # directories that contain image that are included in the documentation (see # the \image command). IMAGE_PATH = # The INPUT_FILTER tag can be used to specify a program that doxygen should # invoke to filter for each input file. Doxygen will invoke the filter program # by executing (via popen()) the command , where # is the value of the INPUT_FILTER tag, and is the name of an # input file. Doxygen will then use the output that the filter program writes # to standard output. If FILTER_PATTERNS is specified, this tag will be # ignored. INPUT_FILTER = # The FILTER_PATTERNS tag can be used to specify filters on a per file pattern # basis. Doxygen will compare the file name with each pattern and apply the # filter if there is a match. The filters are a list of the form: # pattern=filter (like *.cpp=my_cpp_filter). See INPUT_FILTER for further # info on how filters are used. If FILTER_PATTERNS is empty, INPUT_FILTER # is applied to all files. FILTER_PATTERNS = # If the FILTER_SOURCE_FILES tag is set to YES, the input filter (if set using # INPUT_FILTER) will be used to filter the input files when producing source # files to browse (i.e. when SOURCE_BROWSER is set to YES). FILTER_SOURCE_FILES = NO #--------------------------------------------------------------------------- # configuration options related to source browsing #--------------------------------------------------------------------------- # If the SOURCE_BROWSER tag is set to YES then a list of source files will # be generated. Documented entities will be cross-referenced with these sources. # Note: To get rid of all source code in the generated output, make sure also # VERBATIM_HEADERS is set to NO. SOURCE_BROWSER = NO # Setting the INLINE_SOURCES tag to YES will include the body # of functions and classes directly in the documentation. INLINE_SOURCES = NO # Setting the STRIP_CODE_COMMENTS tag to YES (the default) will instruct # doxygen to hide any special comment blocks from generated source code # fragments. Normal C and C++ comments will always remain visible. STRIP_CODE_COMMENTS = YES # If the REFERENCED_BY_RELATION tag is set to YES # then for each documented function all documented # functions referencing it will be listed. REFERENCED_BY_RELATION = NO # If the REFERENCES_RELATION tag is set to YES # then for each documented function all documented entities # called/used by that function will be listed. REFERENCES_RELATION = NO # If the REFERENCES_LINK_SOURCE tag is set to YES (the default) # and SOURCE_BROWSER tag is set to YES, then the hyperlinks from # functions in REFERENCES_RELATION and REFERENCED_BY_RELATION lists will # link to the source code. Otherwise they will link to the documentation. REFERENCES_LINK_SOURCE = YES # If the USE_HTAGS tag is set to YES then the references to source code # will point to the HTML generated by the htags(1) tool instead of doxygen # built-in source browser. The htags tool is part of GNU's global source # tagging system (see http://www.gnu.org/software/global/global.html). You # will need version 4.8.6 or higher. USE_HTAGS = NO # If the VERBATIM_HEADERS tag is set to YES (the default) then Doxygen # will generate a verbatim copy of the header file for each class for # which an include is specified. Set to NO to disable this. VERBATIM_HEADERS = NO #--------------------------------------------------------------------------- # configuration options related to the alphabetical class index #--------------------------------------------------------------------------- # If the ALPHABETICAL_INDEX tag is set to YES, an alphabetical index # of all compounds will be generated. Enable this if the project # contains a lot of classes, structs, unions or interfaces. ALPHABETICAL_INDEX = YES # If the alphabetical index is enabled (see ALPHABETICAL_INDEX) then # the COLS_IN_ALPHA_INDEX tag can be used to specify the number of columns # in which this list will be split (can be a number in the range [1..20]) COLS_IN_ALPHA_INDEX = 4 # In case all classes in a project start with a common prefix, all # classes will be put under the same header in the alphabetical index. # The IGNORE_PREFIX tag can be used to specify one or more prefixes that # should be ignored while generating the index headers. IGNORE_PREFIX = #--------------------------------------------------------------------------- # configuration options related to the HTML output #--------------------------------------------------------------------------- # If the GENERATE_HTML tag is set to YES (the default) Doxygen will # generate HTML output. GENERATE_HTML = YES # The HTML_OUTPUT tag is used to specify where the HTML docs will be put. # If a relative path is entered the value of OUTPUT_DIRECTORY will be # put in front of it. If left blank `html' will be used as the default path. HTML_OUTPUT = html # The HTML_FILE_EXTENSION tag can be used to specify the file extension for # each generated HTML page (for example: .htm,.php,.asp). If it is left blank # doxygen will generate files with .html extension. HTML_FILE_EXTENSION = .html # The HTML_HEADER tag can be used to specify a personal HTML header for # each generated HTML page. If it is left blank doxygen will generate a # standard header. HTML_HEADER = # The HTML_FOOTER tag can be used to specify a personal HTML footer for # each generated HTML page. If it is left blank doxygen will generate a # standard footer. HTML_FOOTER = # The HTML_STYLESHEET tag can be used to specify a user-defined cascading # style sheet that is used by each HTML page. It can be used to # fine-tune the look of the HTML output. If the tag is left blank doxygen # will generate a default style sheet. Note that doxygen will try to copy # the style sheet file to the HTML output directory, so don't put your own # stylesheet in the HTML output directory as well, or it will be erased! HTML_STYLESHEET = # If the HTML_ALIGN_MEMBERS tag is set to YES, the members of classes, # files or namespaces will be aligned in HTML using tables. If set to # NO a bullet list will be used. HTML_ALIGN_MEMBERS = YES # If the HTML_DYNAMIC_SECTIONS tag is set to YES then the generated HTML # documentation will contain sections that can be hidden and shown after the # page has loaded. For this to work a browser that supports # JavaScript and DHTML is required (for instance Mozilla 1.0+, Firefox # Netscape 6.0+, Internet explorer 5.0+, Konqueror, or Safari). HTML_DYNAMIC_SECTIONS = NO # If the GENERATE_DOCSET tag is set to YES, additional index files # will be generated that can be used as input for Apple's Xcode 3 # integrated development environment, introduced with OSX 10.5 (Leopard). # To create a documentation set, doxygen will generate a Makefile in the # HTML output directory. Running make will produce the docset in that # directory and running "make install" will install the docset in # ~/Library/Developer/Shared/Documentation/DocSets so that Xcode will find # it at startup. # See http://developer.apple.com/tools/creatingdocsetswithdoxygen.html for more information. GENERATE_DOCSET = NO # When GENERATE_DOCSET tag is set to YES, this tag determines the name of the # feed. A documentation feed provides an umbrella under which multiple # documentation sets from a single provider (such as a company or product suite) # can be grouped. DOCSET_FEEDNAME = "Doxygen generated docs" # When GENERATE_DOCSET tag is set to YES, this tag specifies a string that # should uniquely identify the documentation set bundle. This should be a # reverse domain-name style string, e.g. com.mycompany.MyDocSet. Doxygen # will append .docset to the name. DOCSET_BUNDLE_ID = org.doxygen.Project # If the GENERATE_HTMLHELP tag is set to YES, additional index files # will be generated that can be used as input for tools like the # Microsoft HTML help workshop to generate a compiled HTML help file (.chm) # of the generated HTML documentation. GENERATE_HTMLHELP = YES # If the GENERATE_HTMLHELP tag is set to YES, the CHM_FILE tag can # be used to specify the file name of the resulting .chm file. You # can add a path in front of the file if the result should not be # written to the html output directory. CHM_FILE = ..\EDMA3_Driver.chm # If the GENERATE_HTMLHELP tag is set to YES, the HHC_LOCATION tag can # be used to specify the location (absolute path including file name) of # the HTML help compiler (hhc.exe). If non-empty doxygen will try to run # the HTML help compiler on the generated index.hhp. HHC_LOCATION = "C:\Program Files\HTML Help Workshop\hhc.exe" # If the GENERATE_HTMLHELP tag is set to YES, the GENERATE_CHI flag # controls if a separate .chi index file is generated (YES) or that # it should be included in the master .chm file (NO). GENERATE_CHI = NO # If the GENERATE_HTMLHELP tag is set to YES, the CHM_INDEX_ENCODING # is used to encode HtmlHelp index (hhk), content (hhc) and project file # content. CHM_INDEX_ENCODING = # If the GENERATE_HTMLHELP tag is set to YES, the BINARY_TOC flag # controls whether a binary table of contents is generated (YES) or a # normal table of contents (NO) in the .chm file. BINARY_TOC = NO # The TOC_EXPAND flag can be set to YES to add extra items for group members # to the contents of the HTML help documentation and to the tree view. TOC_EXPAND = NO # If the GENERATE_QHP tag is set to YES and both QHP_NAMESPACE and QHP_VIRTUAL_FOLDER # are set, an additional index file will be generated that can be used as input for # Qt's qhelpgenerator to generate a Qt Compressed Help (.qch) of the generated # HTML documentation. GENERATE_QHP = NO # If the QHG_LOCATION tag is specified, the QCH_FILE tag can # be used to specify the file name of the resulting .qch file. # The path specified is relative to the HTML output folder. QCH_FILE = # The QHP_NAMESPACE tag specifies the namespace to use when generating # Qt Help Project output. For more information please see # http://doc.trolltech.com/qthelpproject.html#namespace QHP_NAMESPACE = # The QHP_VIRTUAL_FOLDER tag specifies the namespace to use when generating # Qt Help Project output. For more information please see # http://doc.trolltech.com/qthelpproject.html#virtual-folders QHP_VIRTUAL_FOLDER = doc # If QHP_CUST_FILTER_NAME is set, it specifies the name of a custom filter to add. # For more information please see # http://doc.trolltech.com/qthelpproject.html#custom-filters QHP_CUST_FILTER_NAME = # The QHP_CUST_FILT_ATTRS tag specifies the list of the attributes of the custom filter to add.For more information please see # Qt Help Project / Custom Filters. QHP_CUST_FILTER_ATTRS = # The QHP_SECT_FILTER_ATTRS tag specifies the list of the attributes this project's # filter section matches. # Qt Help Project / Filter Attributes. QHP_SECT_FILTER_ATTRS = # If the GENERATE_QHP tag is set to YES, the QHG_LOCATION tag can # be used to specify the location of Qt's qhelpgenerator. # If non-empty doxygen will try to run qhelpgenerator on the generated # .qhp file. QHG_LOCATION = # The DISABLE_INDEX tag can be used to turn on/off the condensed index at # top of each HTML page. The value NO (the default) enables the index and # the value YES disables it. DISABLE_INDEX = NO # This tag can be used to set the number of enum values (range [1..20]) # that doxygen will group on one line in the generated HTML documentation. ENUM_VALUES_PER_LINE = 1 # The GENERATE_TREEVIEW tag is used to specify whether a tree-like index # structure should be generated to display hierarchical information. # If the tag value is set to YES, a side panel will be generated # containing a tree-like index structure (just like the one that # is generated for HTML Help). For this to work a browser that supports # JavaScript, DHTML, CSS and frames is required (i.e. any modern browser). # Windows users are probably better off using the HTML help feature. GENERATE_TREEVIEW = NO # By enabling USE_INLINE_TREES, doxygen will generate the Groups, Directories, # and Class Hierarchy pages using a tree view instead of an ordered list. USE_INLINE_TREES = NO # If the treeview is enabled (see GENERATE_TREEVIEW) then this tag can be # used to set the initial width (in pixels) of the frame in which the tree # is shown. TREEVIEW_WIDTH = 250 # Use this tag to change the font size of Latex formulas included # as images in the HTML documentation. The default is 10. Note that # when you change the font size after a successful doxygen run you need # to manually remove any form_*.png images from the HTML output directory # to force them to be regenerated. FORMULA_FONTSIZE = 10 # When the SEARCHENGINE tag is enable doxygen will generate a search box # for the HTML output. The underlying search engine uses javascript # and DHTML and should work on any modern browser. Note that when using # HTML help (GENERATE_HTMLHELP) or Qt help (GENERATE_QHP) # there is already a search function so this one should typically # be disabled. SEARCHENGINE = NO #--------------------------------------------------------------------------- # configuration options related to the LaTeX output #--------------------------------------------------------------------------- # If the GENERATE_LATEX tag is set to YES (the default) Doxygen will # generate Latex output. GENERATE_LATEX = NO # The LATEX_OUTPUT tag is used to specify where the LaTeX docs will be put. # If a relative path is entered the value of OUTPUT_DIRECTORY will be # put in front of it. If left blank `latex' will be used as the default path. LATEX_OUTPUT = latex # The LATEX_CMD_NAME tag can be used to specify the LaTeX command name to be # invoked. If left blank `latex' will be used as the default command name. LATEX_CMD_NAME = latex # The MAKEINDEX_CMD_NAME tag can be used to specify the command name to # generate index for LaTeX. If left blank `makeindex' will be used as the # default command name. MAKEINDEX_CMD_NAME = makeindex # If the COMPACT_LATEX tag is set to YES Doxygen generates more compact # LaTeX documents. This may be useful for small projects and may help to # save some trees in general. COMPACT_LATEX = NO # The PAPER_TYPE tag can be used to set the paper type that is used # by the printer. Possible values are: a4, a4wide, letter, legal and # executive. If left blank a4wide will be used. PAPER_TYPE = a4wide # The EXTRA_PACKAGES tag can be to specify one or more names of LaTeX # packages that should be included in the LaTeX output. EXTRA_PACKAGES = # The LATEX_HEADER tag can be used to specify a personal LaTeX header for # the generated latex document. The header should contain everything until # the first chapter. If it is left blank doxygen will generate a # standard header. Notice: only use this tag if you know what you are doing! LATEX_HEADER = # If the PDF_HYPERLINKS tag is set to YES, the LaTeX that is generated # is prepared for conversion to pdf (using ps2pdf). The pdf file will # contain links (just like the HTML output) instead of page references # This makes the output suitable for online browsing using a pdf viewer. PDF_HYPERLINKS = NO # If the USE_PDFLATEX tag is set to YES, pdflatex will be used instead of # plain latex in the generated Makefile. Set this option to YES to get a # higher quality PDF documentation. USE_PDFLATEX = NO # If the LATEX_BATCHMODE tag is set to YES, doxygen will add the \\batchmode. # command to the generated LaTeX files. This will instruct LaTeX to keep # running if errors occur, instead of asking the user for help. # This option is also used when generating formulas in HTML. LATEX_BATCHMODE = NO # If LATEX_HIDE_INDICES is set to YES then doxygen will not # include the index chapters (such as File Index, Compound Index, etc.) # in the output. LATEX_HIDE_INDICES = NO # If LATEX_SOURCE_CODE is set to YES then doxygen will include # source code with syntax highlighting in the LaTeX output. # Note that which sources are shown also depends on other settings # such as SOURCE_BROWSER. LATEX_SOURCE_CODE = NO #--------------------------------------------------------------------------- # configuration options related to the RTF output #--------------------------------------------------------------------------- # If the GENERATE_RTF tag is set to YES Doxygen will generate RTF output # The RTF output is optimized for Word 97 and may not look very pretty with # other RTF readers or editors. GENERATE_RTF = NO # The RTF_OUTPUT tag is used to specify where the RTF docs will be put. # If a relative path is entered the value of OUTPUT_DIRECTORY will be # put in front of it. If left blank `rtf' will be used as the default path. RTF_OUTPUT = rtf # If the COMPACT_RTF tag is set to YES Doxygen generates more compact # RTF documents. This may be useful for small projects and may help to # save some trees in general. COMPACT_RTF = NO # If the RTF_HYPERLINKS tag is set to YES, the RTF that is generated # will contain hyperlink fields. The RTF file will # contain links (just like the HTML output) instead of page references. # This makes the output suitable for online browsing using WORD or other # programs which support those fields. # Note: wordpad (write) and others do not support links. RTF_HYPERLINKS = NO # Load stylesheet definitions from file. Syntax is similar to doxygen's # config file, i.e. a series of assignments. You only have to provide # replacements, missing definitions are set to their default value. RTF_STYLESHEET_FILE = # Set optional variables used in the generation of an rtf document. # Syntax is similar to doxygen's config file. RTF_EXTENSIONS_FILE = #--------------------------------------------------------------------------- # configuration options related to the man page output #--------------------------------------------------------------------------- # If the GENERATE_MAN tag is set to YES (the default) Doxygen will # generate man pages GENERATE_MAN = NO # The MAN_OUTPUT tag is used to specify where the man pages will be put. # If a relative path is entered the value of OUTPUT_DIRECTORY will be # put in front of it. If left blank `man' will be used as the default path. MAN_OUTPUT = man # The MAN_EXTENSION tag determines the extension that is added to # the generated man pages (default is the subroutine's section .3) MAN_EXTENSION = .3 # If the MAN_LINKS tag is set to YES and Doxygen generates man output, # then it will generate one additional man file for each entity # documented in the real man page(s). These additional files # only source the real man page, but without them the man command # would be unable to find the correct page. The default is NO. MAN_LINKS = NO #--------------------------------------------------------------------------- # configuration options related to the XML output #--------------------------------------------------------------------------- # If the GENERATE_XML tag is set to YES Doxygen will # generate an XML file that captures the structure of # the code including all documentation. GENERATE_XML = NO # The XML_OUTPUT tag is used to specify where the XML pages will be put. # If a relative path is entered the value of OUTPUT_DIRECTORY will be # put in front of it. If left blank `xml' will be used as the default path. XML_OUTPUT = xml # The XML_SCHEMA tag can be used to specify an XML schema, # which can be used by a validating XML parser to check the # syntax of the XML files. XML_SCHEMA = # The XML_DTD tag can be used to specify an XML DTD, # which can be used by a validating XML parser to check the # syntax of the XML files. XML_DTD = # If the XML_PROGRAMLISTING tag is set to YES Doxygen will # dump the program listings (including syntax highlighting # and cross-referencing information) to the XML output. Note that # enabling this will significantly increase the size of the XML output. XML_PROGRAMLISTING = YES #--------------------------------------------------------------------------- # configuration options for the AutoGen Definitions output #--------------------------------------------------------------------------- # If the GENERATE_AUTOGEN_DEF tag is set to YES Doxygen will # generate an AutoGen Definitions (see autogen.sf.net) file # that captures the structure of the code including all # documentation. Note that this feature is still experimental # and incomplete at the moment. GENERATE_AUTOGEN_DEF = NO #--------------------------------------------------------------------------- # configuration options related to the Perl module output #--------------------------------------------------------------------------- # If the GENERATE_PERLMOD tag is set to YES Doxygen will # generate a Perl module file that captures the structure of # the code including all documentation. Note that this # feature is still experimental and incomplete at the # moment. GENERATE_PERLMOD = NO # If the PERLMOD_LATEX tag is set to YES Doxygen will generate # the necessary Makefile rules, Perl scripts and LaTeX code to be able # to generate PDF and DVI output from the Perl module output. PERLMOD_LATEX = NO # If the PERLMOD_PRETTY tag is set to YES the Perl module output will be # nicely formatted so it can be parsed by a human reader. This is useful # if you want to understand what is going on. On the other hand, if this # tag is set to NO the size of the Perl module output will be much smaller # and Perl will parse it just the same. PERLMOD_PRETTY = YES # The names of the make variables in the generated doxyrules.make file # are prefixed with the string contained in PERLMOD_MAKEVAR_PREFIX. # This is useful so different doxyrules.make files included by the same # Makefile don't overwrite each other's variables. PERLMOD_MAKEVAR_PREFIX = #--------------------------------------------------------------------------- # Configuration options related to the preprocessor #--------------------------------------------------------------------------- # If the ENABLE_PREPROCESSING tag is set to YES (the default) Doxygen will # evaluate all C-preprocessor directives found in the sources and include # files. ENABLE_PREPROCESSING = YES # If the MACRO_EXPANSION tag is set to YES Doxygen will expand all macro # names in the source code. If set to NO (the default) only conditional # compilation will be performed. Macro expansion can be done in a controlled # way by setting EXPAND_ONLY_PREDEF to YES. MACRO_EXPANSION = NO # If the EXPAND_ONLY_PREDEF and MACRO_EXPANSION tags are both set to YES # then the macro expansion is limited to the macros specified with the # PREDEFINED and EXPAND_AS_DEFINED tags. EXPAND_ONLY_PREDEF = NO # If the SEARCH_INCLUDES tag is set to YES (the default) the includes files # in the INCLUDE_PATH (see below) will be search if a #include is found. SEARCH_INCLUDES = YES # The INCLUDE_PATH tag can be used to specify one or more directories that # contain include files that are not input files but should be processed by # the preprocessor. INCLUDE_PATH = # You can use the INCLUDE_FILE_PATTERNS tag to specify one or more wildcard # patterns (like *.h and *.hpp) to filter out the header-files in the # directories. If left blank, the patterns specified with FILE_PATTERNS will # be used. INCLUDE_FILE_PATTERNS = # The PREDEFINED tag can be used to specify one or more macro names that # are defined before the preprocessor is started (similar to the -D option of # gcc). The argument of the tag is a list of macros of the form: name # or name=definition (no spaces). If the definition and the = are # omitted =1 is assumed. To prevent a macro definition from being # undefined via #undef or recursively expanded use the := operator # instead of the = operator. PREDEFINED = # If the MACRO_EXPANSION and EXPAND_ONLY_PREDEF tags are set to YES then # this tag can be used to specify a list of macro names that should be expanded. # The macro definition that is found in the sources will be used. # Use the PREDEFINED tag if you want to use a different macro definition. EXPAND_AS_DEFINED = # If the SKIP_FUNCTION_MACROS tag is set to YES (the default) then # doxygen's preprocessor will remove all function-like macros that are alone # on a line, have an all uppercase name, and do not end with a semicolon. Such # function macros are typically used for boiler-plate code, and will confuse # the parser if not removed. SKIP_FUNCTION_MACROS = YES #--------------------------------------------------------------------------- # Configuration::additions related to external references #--------------------------------------------------------------------------- # The TAGFILES option can be used to specify one or more tagfiles. # Optionally an initial location of the external documentation # can be added for each tagfile. The format of a tag file without # this location is as follows: # TAGFILES = file1 file2 ... # Adding location for the tag files is done as follows: # TAGFILES = file1=loc1 "file2 = loc2" ... # where "loc1" and "loc2" can be relative or absolute paths or # URLs. If a location is present for each tag, the installdox tool # does not have to be run to correct the links. # Note that each tag file must have a unique name # (where the name does NOT include the path) # If a tag file is not located in the directory in which doxygen # is run, you must also specify the path to the tagfile here. TAGFILES = # When a file name is specified after GENERATE_TAGFILE, doxygen will create # a tag file that is based on the input files it reads. GENERATE_TAGFILE = # If the ALLEXTERNALS tag is set to YES all external classes will be listed # in the class index. If set to NO only the inherited external classes # will be listed. ALLEXTERNALS = NO # If the EXTERNAL_GROUPS tag is set to YES all external groups will be listed # in the modules index. If set to NO, only the current project's groups will # be listed. EXTERNAL_GROUPS = YES # The PERL_PATH should be the absolute path and name of the perl script # interpreter (i.e. the result of `which perl'). PERL_PATH = /usr/bin/perl #--------------------------------------------------------------------------- # Configuration options related to the dot tool #--------------------------------------------------------------------------- # If the CLASS_DIAGRAMS tag is set to YES (the default) Doxygen will # generate a inheritance diagram (in HTML, RTF and LaTeX) for classes with base # or super classes. Setting the tag to NO turns the diagrams off. Note that # this option is superseded by the HAVE_DOT option below. This is only a # fallback. It is recommended to install and use dot, since it yields more # powerful graphs. CLASS_DIAGRAMS = NO # You can define message sequence charts within doxygen comments using the \msc # command. Doxygen will then run the mscgen tool (see # http://www.mcternan.me.uk/mscgen/) to produce the chart and insert it in the # documentation. The MSCGEN_PATH tag allows you to specify the directory where # the mscgen tool resides. If left empty the tool is assumed to be found in the # default search path. MSCGEN_PATH = # If set to YES, the inheritance and collaboration graphs will hide # inheritance and usage relations if the target is undocumented # or is not a class. HIDE_UNDOC_RELATIONS = YES # If you set the HAVE_DOT tag to YES then doxygen will assume the dot tool is # available from the path. This tool is part of Graphviz, a graph visualization # toolkit from AT&T and Lucent Bell Labs. The other options in this section # have no effect if this option is set to NO (the default) HAVE_DOT = NO # By default doxygen will write a font called FreeSans.ttf to the output # directory and reference it in all dot files that doxygen generates. This # font does not include all possible unicode characters however, so when you need # these (or just want a differently looking font) you can specify the font name # using DOT_FONTNAME. You need need to make sure dot is able to find the font, # which can be done by putting it in a standard location or by setting the # DOTFONTPATH environment variable or by setting DOT_FONTPATH to the directory # containing the font. DOT_FONTNAME = FreeSans # The DOT_FONTSIZE tag can be used to set the size of the font of dot graphs. # The default size is 10pt. DOT_FONTSIZE = 10 # By default doxygen will tell dot to use the output directory to look for the # FreeSans.ttf font (which doxygen will put there itself). If you specify a # different font using DOT_FONTNAME you can set the path where dot # can find it using this tag. DOT_FONTPATH = # If the CLASS_GRAPH and HAVE_DOT tags are set to YES then doxygen # will generate a graph for each documented class showing the direct and # indirect inheritance relations. Setting this tag to YES will force the # the CLASS_DIAGRAMS tag to NO. CLASS_GRAPH = YES # If the COLLABORATION_GRAPH and HAVE_DOT tags are set to YES then doxygen # will generate a graph for each documented class showing the direct and # indirect implementation dependencies (inheritance, containment, and # class references variables) of the class with other documented classes. COLLABORATION_GRAPH = YES # If the GROUP_GRAPHS and HAVE_DOT tags are set to YES then doxygen # will generate a graph for groups, showing the direct groups dependencies GROUP_GRAPHS = YES # If the UML_LOOK tag is set to YES doxygen will generate inheritance and # collaboration diagrams in a style similar to the OMG's Unified Modeling # Language. UML_LOOK = NO # If set to YES, the inheritance and collaboration graphs will show the # relations between templates and their instances. TEMPLATE_RELATIONS = NO # If the ENABLE_PREPROCESSING, SEARCH_INCLUDES, INCLUDE_GRAPH, and HAVE_DOT # tags are set to YES then doxygen will generate a graph for each documented # file showing the direct and indirect include dependencies of the file with # other documented files. INCLUDE_GRAPH = YES # If the ENABLE_PREPROCESSING, SEARCH_INCLUDES, INCLUDED_BY_GRAPH, and # HAVE_DOT tags are set to YES then doxygen will generate a graph for each # documented header file showing the documented files that directly or # indirectly include this file. INCLUDED_BY_GRAPH = YES # If the CALL_GRAPH and HAVE_DOT options are set to YES then # doxygen will generate a call dependency graph for every global function # or class method. Note that enabling this option will significantly increase # the time of a run. So in most cases it will be better to enable call graphs # for selected functions only using the \callgraph command. CALL_GRAPH = NO # If the CALLER_GRAPH and HAVE_DOT tags are set to YES then # doxygen will generate a caller dependency graph for every global function # or class method. Note that enabling this option will significantly increase # the time of a run. So in most cases it will be better to enable caller # graphs for selected functions only using the \callergraph command. CALLER_GRAPH = NO # If the GRAPHICAL_HIERARCHY and HAVE_DOT tags are set to YES then doxygen # will graphical hierarchy of all classes instead of a textual one. GRAPHICAL_HIERARCHY = YES # If the DIRECTORY_GRAPH, SHOW_DIRECTORIES and HAVE_DOT tags are set to YES # then doxygen will show the dependencies a directory has on other directories # in a graphical way. The dependency relations are determined by the #include # relations between the files in the directories. DIRECTORY_GRAPH = YES # The DOT_IMAGE_FORMAT tag can be used to set the image format of the images # generated by dot. Possible values are png, jpg, or gif # If left blank png will be used. DOT_IMAGE_FORMAT = png # The tag DOT_PATH can be used to specify the path where the dot tool can be # found. If left blank, it is assumed the dot tool can be found in the path. DOT_PATH = # The DOTFILE_DIRS tag can be used to specify one or more directories that # contain dot files that are included in the documentation (see the # \dotfile command). DOTFILE_DIRS = # The DOT_GRAPH_MAX_NODES tag can be used to set the maximum number of # nodes that will be shown in the graph. If the number of nodes in a graph # becomes larger than this value, doxygen will truncate the graph, which is # visualized by representing a node as a red box. Note that doxygen if the # number of direct children of the root node in a graph is already larger than # DOT_GRAPH_MAX_NODES then the graph will not be shown at all. Also note # that the size of a graph can be further restricted by MAX_DOT_GRAPH_DEPTH. DOT_GRAPH_MAX_NODES = 50 # The MAX_DOT_GRAPH_DEPTH tag can be used to set the maximum depth of the # graphs generated by dot. A depth value of 3 means that only nodes reachable # from the root by following a path via at most 3 edges will be shown. Nodes # that lay further from the root node will be omitted. Note that setting this # option to 1 or 2 may greatly reduce the computation time needed for large # code bases. Also note that the size of a graph can be further restricted by # DOT_GRAPH_MAX_NODES. Using a depth of 0 means no depth restriction. MAX_DOT_GRAPH_DEPTH = 0 # Set the DOT_TRANSPARENT tag to YES to generate images with a transparent # background. This is disabled by default, because dot on Windows does not # seem to support this out of the box. Warning: Depending on the platform used, # enabling this option may lead to badly anti-aliased labels on the edges of # a graph (i.e. they become hard to read). DOT_TRANSPARENT = NO # Set the DOT_MULTI_TARGETS tag to YES allow dot to generate multiple output # files in one run (i.e. multiple -o and -T options on the command line). This # makes dot run faster, but since only newer versions of dot (>1.8.10) # support this, this feature is disabled by default. DOT_MULTI_TARGETS = NO # If the GENERATE_LEGEND tag is set to YES (the default) Doxygen will # generate a legend page explaining the meaning of the various boxes and # arrows in the dot generated graphs. GENERATE_LEGEND = YES # If the DOT_CLEANUP tag is set to YES (the default) Doxygen will # remove the intermediate dot files that are used to generate # the various graphs. DOT_CLEANUP = YES