/* * bios6_edma3_drv_sample.h * * Header file for the sample application for the EDMA3 Driver. * * Copyright (C) 2009 Texas Instruments Incorporated - http://www.ti.com/ * * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * */ #ifndef _BIOS6_EDMA3_DRV_SAMPLE_H_ #define _BIOS6_EDMA3_DRV_SAMPLE_H_ #include #include /* Include EDMA3 Driver */ #include #ifdef __cplusplus extern "C" { #endif /** * Cache line size on the underlying SoC. It needs to be modified * for different cache line sizes, if the Cache is Enabled. */ #define EDMA3_CACHE_LINE_SIZE_IN_BYTES (128u) /* Error returned in case of buffers are not aligned on the cache boundary */ #define EDMA3_NON_ALIGNED_BUFFERS_ERROR (-1) /* Error returned in case of data mismatch */ #define EDMA3_DATA_MISMATCH_ERROR (-2) /** * \brief EDMA3 Initialization * * This function initializes the EDMA3 Driver for the given EDMA3 controller * and opens a EDMA3 driver instance. It internally calls EDMA3_DRV_create() and * EDMA3_DRV_open(), in that order. * * It also registers interrupt handlers for various EDMA3 interrupts like * transfer completion or error interrupts. * * \param edma3Id [IN] EDMA3 Controller Instance Id (Hardware * instance id, starting from 0) * \param errorCode [IN/OUT] Error code while opening DRV instance * \return EDMA3_DRV_Handle: If successfully opened, the API will return the * associated driver's instance handle. */ EDMA3_DRV_Handle edma3init (unsigned int edma3Id, EDMA3_DRV_Result *errorCode); /** * \brief EDMA3 De-initialization * * This function de-initializes the EDMA3 Driver for the given EDMA3 controller * and closes the previously opened EDMA3 driver instance. It internally calls * EDMA3_DRV_close and EDMA3_DRV_delete(), in that order. * * It also un-registers the previously registered interrupt handlers for various * EDMA3 interrupts. * * \param edma3Id [IN] EDMA3 Controller Instance Id (Hardware * instance id, starting from 0) * \param hEdma [IN] EDMA3 Driver handle, returned while using * edma3init(). * \return EDMA3_DRV_SOK if success, else error code */ EDMA3_DRV_Result edma3deinit (unsigned int edma3Id, EDMA3_DRV_Handle hEdma); /** * \brief EDMA3 Cache Invalidate * * This function invalidates the D cache. * * \param mem_start_ptr [IN] Starting address of memory. * Please note that this should be * aligned according to the cache line size. * \param num_bytes [IN] length of buffer * \return EDMA3_DRV_SOK if success, else error code in case of error * or non-alignment of buffers. * * Note: This function is required if the buffer is in DDR. * For other cases, where buffer is NOT in DDR, user * may or may not require the below implementation and * should modify it according to her need. */ EDMA3_DRV_Result Edma3_CacheInvalidate(unsigned int mem_start_ptr, unsigned int num_bytes); /** * \brief EDMA3 Cache Flush * * This function flushes (cleans) the Cache * * \param mem_start_ptr [IN] Starting address of memory. * Please note that this should be * aligned according to the cache line size. * \param num_bytes [IN] length of buffer * \return EDMA3_DRV_SOK if success, else error code in case of error * or non-alignment of buffers. * * Note: This function is required if the buffer is in DDR. * For other cases, where buffer is NOT in DDR, user * may or may not require the below implementation and * should modify it according to her need. */ EDMA3_DRV_Result Edma3_CacheFlush(unsigned int mem_start_ptr, unsigned int num_bytes); /** * Counting Semaphore related functions (OS dependent) should be * called/implemented by the application. A handle to the semaphore * is required while opening the driver/resource manager instance. */ /** * \brief EDMA3 OS Semaphore Create * * This function creates a counting semaphore with specified * attributes and initial value. It should be used to create a semaphore * with initial value as '1'. The semaphore is then passed by the user * to the EDMA3 driver/RM for proper sharing of resources. * \param initVal [IN] is initial value for semaphore * \param semParams [IN] is the semaphore attributes. * \param hSem [OUT] is location to receive the handle to just created * semaphore. * \return EDMA3_DRV_SOK if successful, else a suitable error code. */ EDMA3_DRV_Result edma3OsSemCreate(int initVal, const Semaphore_Params *semParams, EDMA3_OS_Sem_Handle *hSem); /** * \brief EDMA3 OS Semaphore Delete * * This function deletes or removes the specified semaphore * from the system. Associated dynamically allocated memory * if any is also freed up. * \param hSem [IN] handle to the semaphore to be deleted * \return EDMA3_DRV_SOK if successful else a suitable error code */ EDMA3_DRV_Result edma3OsSemDelete(EDMA3_OS_Sem_Handle hSem); #ifdef __cplusplus } #endif /* extern "C" */ #endif /* _BIOS6_EDMA3_DRV_SAMPLE_H_ */