/* * sample_am335x_arm_int_reg.c * * Platform specific interrupt registration and un-registration routines. * * Copyright (C) 2015 Texas Instruments Incorporated - http://www.ti.com/ * * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * */ #include #include #include #include #include // #include /** * EDMA3 TC ISRs which need to be registered with the underlying OS by the user * (Not all TC error ISRs need to be registered, register only for the * available Transfer Controllers). */ void (*ptrEdma3TcIsrHandler[EDMA3_MAX_TC])(uint32_t arg) = { &lisrEdma3TC0ErrHandler0, &lisrEdma3TC1ErrHandler0, &lisrEdma3TC2ErrHandler0, &lisrEdma3TC3ErrHandler0, &lisrEdma3TC4ErrHandler0, &lisrEdma3TC5ErrHandler0, &lisrEdma3TC6ErrHandler0, &lisrEdma3TC7ErrHandler0, }; extern uint32_t ccXferCompInt[][EDMA3_MAX_REGIONS]; extern uint32_t ccErrorInt[]; extern uint32_t tcErrorInt[][EDMA3_MAX_TC]; extern uint32_t numEdma3Tc[]; /** * Variables which will be used internally for referring the hardware interrupt * for various EDMA3 interrupts. */ extern uint32_t hwIntXferComp; extern uint32_t hwIntCcErr; extern uint32_t hwIntTcErr; extern uint32_t dsp_num; /* This variable has to be used as an extern */ //uint32_t gpp_num = 4; Hwi_Handle hwiCCXferCompInt; Hwi_Handle hwiCCErrInt; Hwi_Handle hwiTCErrInt[EDMA3_MAX_TC]; /** To Register the ISRs with the underlying OS, if required. */ void registerEdma3Interrupts (uint32_t edma3Id) { static UInt32 cookie = 0; uint32_t numTc = 0; Hwi_Params hwiParams; Error_Block eb; /* Initialize the Error Block */ Error_init(&eb); /* Disabling the global interrupts */ cookie = Hwi_disable(); /* Initialize the HWI parameters with user specified values */ Hwi_Params_init(&hwiParams); /* argument for the ISR */ hwiParams.arg = edma3Id; /* set the priority ID */ hwiParams.priority = hwIntXferComp; //hwiParams.enableInt = TRUE; hwiCCXferCompInt = Hwi_create( ccXferCompInt[edma3Id][dsp_num], (&lisrEdma3ComplHandler0), (const Hwi_Params *) (&hwiParams), &eb); if (TRUE == Error_check(&eb)) { System_printf("HWI Create Failed\n",Error_getCode(&eb)); } /* Initialize the HWI parameters with user specified values */ Hwi_Params_init(&hwiParams); /* argument for the ISR */ hwiParams.arg = edma3Id; /* set the priority ID */ hwiParams.priority = hwIntCcErr; //hwiParams.enableInt = TRUE; hwiCCErrInt = Hwi_create( ccErrorInt[edma3Id], (&lisrEdma3CCErrHandler0), (const Hwi_Params *) (&hwiParams), &eb); if (TRUE == Error_check(&eb)) { System_printf("HWI Create Failed\n",Error_getCode(&eb)); } while (numTc < numEdma3Tc[edma3Id]) { /* Initialize the HWI parameters with user specified values */ Hwi_Params_init(&hwiParams); /* argument for the ISR */ hwiParams.arg = edma3Id; /* set the priority ID */ hwiParams.priority = hwIntTcErr; //hwiParams.enableInt = TRUE; hwiTCErrInt[numTc] = Hwi_create( tcErrorInt[edma3Id][numTc], (ptrEdma3TcIsrHandler[numTc]), (const Hwi_Params *) (&hwiParams), &eb); if (TRUE == Error_check(&eb)) { System_printf("HWI Create Failed\n",Error_getCode(&eb)); } numTc++; } /** * Enabling the HWI_ID. * EDMA3 interrupts (transfer completion, CC error etc.) * correspond to different ECM events (SoC specific). These ECM events come * under ECM block XXX (handling those specific ECM events). Normally, block * 0 handles events 4-31 (events 0-3 are reserved), block 1 handles events * 32-63 and so on. This ECM block XXX (or interrupt selection number XXX) * is mapped to a specific HWI_INT YYY in the tcf file. So to enable this * mapped HWI_INT YYY, one should use the corresponding bitmask in the * API C64_enableIER(), in which the YYY bit is SET. */ Hwi_enableInterrupt(ccErrorInt[edma3Id]); Hwi_enableInterrupt(ccXferCompInt[edma3Id][dsp_num]); numTc = 0; while (numTc < numEdma3Tc[edma3Id]) { Hwi_enableInterrupt(tcErrorInt[edma3Id][numTc]); numTc++; } /* Restore interrupts */ Hwi_restore(cookie); } /** To Unregister the ISRs with the underlying OS, if previously registered. */ void unregisterEdma3Interrupts (uint32_t edma3Id) { static UInt32 cookie = 0; uint32_t numTc = 0; /* Disabling the global interrupts */ cookie = Hwi_disable(); Hwi_delete(&hwiCCXferCompInt); Hwi_delete(&hwiCCErrInt); while (numTc < numEdma3Tc[edma3Id]) { Hwi_delete(&hwiTCErrInt[numTc]); numTc++; } /* Restore interrupts */ Hwi_restore(cookie); }