/* * sample_tda2xx_int_reg.c * * Platform specific interrupt registration and un-registration routines. * * Copyright (C) 2009 Texas Instruments Incorporated - http://www.ti.com/ * * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * */ #include #include #include #include #include /** * EDMA3 TC ISRs which need to be registered with the underlying OS by the user * (Not all TC error ISRs need to be registered, register only for the * available Transfer Controllers). */ void (*ptrEdma3TcIsrHandler[EDMA3_MAX_TC])(uint32_t arg) = { (void (*)(uint32_t))&lisrEdma3TC0ErrHandler0, (void (*)(uint32_t))&lisrEdma3TC1ErrHandler0, (void (*)(uint32_t))&lisrEdma3TC2ErrHandler0, (void (*)(uint32_t))&lisrEdma3TC3ErrHandler0, (void (*)(uint32_t))&lisrEdma3TC4ErrHandler0, (void (*)(uint32_t))&lisrEdma3TC5ErrHandler0, (void (*)(uint32_t))&lisrEdma3TC6ErrHandler0, (void (*)(uint32_t))&lisrEdma3TC7ErrHandler0, }; extern unsigned int ccXferCompInt[][EDMA3_MAX_REGIONS]; extern unsigned int ccErrorInt[]; extern unsigned int tcErrorInt[][EDMA3_MAX_TC]; extern unsigned int numEdma3Tc[]; /** * Variables which will be used internally for referring the hardware interrupt * for various EDMA3 interrupts. */ extern unsigned int hwIntXferComp[]; extern unsigned int hwIntCcErr[]; extern unsigned int hwIntTcErr[]; extern unsigned int dsp_num; /* This variable has to be used as an extern */ unsigned int gpp_num = 0; Hwi_Handle hwiCCXferCompInt; Hwi_Handle hwiCCErrInt; Hwi_Handle hwiTCErrInt[EDMA3_MAX_TC]; /* External Instance Specific Configuration Structure */ extern EDMA3_DRV_GblXbarToChanConfigParams sampleXbarChanInitConfig[][EDMA3_MAX_REGIONS]; typedef struct { volatile Uint32 TPCC_EVTMUX[32]; } CSL_IntmuxRegs; typedef volatile CSL_IntmuxRegs *CSL_IntmuxRegsOvly; #define CSL_INTMUX_TPCC_EVTMUX_TPCCEVT_MUX_1_MASK (0x00FF0000u) #define CSL_INTMUX_TPCC_EVTMUX_TPCCEVT_MUX_1_SHIFT (0x00000010u) #define CSL_INTMUX_TPCC_EVTMUX_TPCCEVT_MUX_1_RESETVAL (0x00000000u) #define CSL_INTMUX_TPCC_EVTMUX_TPCCEVT_MUX_0_MASK (0x000000FFu) #define CSL_INTMUX_TPCC_EVTMUX_TPCCEVT_MUX_0_SHIFT (0x00000000u) #define CSL_INTMUX_TPCC_EVTMUX_TPCCEVT_MUX_0_RESETVAL (0x00000000u) #define EDMA3_MAX_CROSS_BAR_EVENTS_DRA72X (127u) #define EDMA3_NUM_TCC (64u) #define EDMA3_EVENT_MUX_REG_BASE_ADDR (0x4a002c78) /* * Forward decleration */ EDMA3_DRV_Result sampleMapXbarEvtToChan (unsigned int eventNum, unsigned int *chanNum, const EDMA3_DRV_GblXbarToChanConfigParams * edmaGblXbarConfig); EDMA3_DRV_Result sampleConfigScr (unsigned int eventNum, unsigned int chanNum); void Edma3MemProtectionHandler(unsigned int edma3InstanceId); /** To Register the ISRs with the underlying OS, if required. */ void registerEdma3Interrupts (unsigned int edma3Id) { static UInt32 cookie = 0; unsigned int numTc = 0; Hwi_Params hwiParams; Error_Block eb; /* Initialize the Error Block */ Error_init(&eb); /* Disabling the global interrupts */ cookie = Hwi_disable(); /* Initialize the HWI parameters with user specified values */ Hwi_Params_init(&hwiParams); /* argument for the ISR */ hwiParams.arg = edma3Id; /* set the priority ID */ hwiParams.priority = hwIntXferComp[edma3Id]; hwiCCXferCompInt = Hwi_create( ccXferCompInt[edma3Id][gpp_num], ((Hwi_FuncPtr)&lisrEdma3ComplHandler0), (const Hwi_Params *) (&hwiParams), &eb); if (TRUE == Error_check(&eb)) { System_printf("HWI Create Failed\n",Error_getCode(&eb)); } /* Initialize the HWI parameters with user specified values */ Hwi_Params_init(&hwiParams); /* argument for the ISR */ hwiParams.arg = edma3Id; /* set the priority ID */ hwiParams.priority = hwIntCcErr[edma3Id]; hwiCCErrInt = Hwi_create( ccErrorInt[edma3Id], ((Hwi_FuncPtr)&lisrEdma3CCErrHandler0), (const Hwi_Params *) (&hwiParams), &eb); if (TRUE == Error_check(&eb)) { System_printf("HWI Create Failed\n",Error_getCode(&eb)); } while (numTc < numEdma3Tc[edma3Id]) { /* Initialize the HWI parameters with user specified values */ Hwi_Params_init(&hwiParams); /* argument for the ISR */ hwiParams.arg = edma3Id; /* set the priority ID */ hwiParams.priority = hwIntTcErr[edma3Id]; hwiTCErrInt[numTc] = Hwi_create( tcErrorInt[edma3Id][numTc], (ptrEdma3TcIsrHandler[numTc]), (const Hwi_Params *) (&hwiParams), &eb); if (TRUE == Error_check(&eb)) { System_printf("HWI Create Failed\n",Error_getCode(&eb)); } numTc++; } /** * Enabling the HWI_ID. * EDMA3 interrupts (transfer completion, CC error etc.) * correspond to different ECM events (SoC specific). These ECM events come * under ECM block XXX (handling those specific ECM events). Normally, block * 0 handles events 4-31 (events 0-3 are reserved), block 1 handles events * 32-63 and so on. This ECM block XXX (or interrupt selection number XXX) * is mapped to a specific HWI_INT YYY in the tcf file. So to enable this * mapped HWI_INT YYY, one should use the corresponding bitmask in the * API C64_enableIER(), in which the YYY bit is SET. */ Hwi_enableInterrupt(ccErrorInt[edma3Id]); #if 0 Hwi_enableInterrupt(13); #endif Hwi_enableInterrupt(ccXferCompInt[edma3Id][gpp_num]); numTc = 0; while (numTc < numEdma3Tc[edma3Id]) { Hwi_enableInterrupt(tcErrorInt[edma3Id][numTc]); numTc++; } /* Restore interrupts */ Hwi_restore(cookie); } /** To Unregister the ISRs with the underlying OS, if previously registered. */ void unregisterEdma3Interrupts (unsigned int edma3Id) { static UInt32 cookie = 0; unsigned int numTc = 0; /* Disabling the global interrupts */ cookie = Hwi_disable(); Hwi_delete(&hwiCCXferCompInt); Hwi_delete(&hwiCCErrInt); while (numTc < numEdma3Tc[edma3Id]) { Hwi_delete(&hwiTCErrInt[numTc]); numTc++; } /* Restore interrupts */ Hwi_restore(cookie); } /** * \brief sampleMapXbarEvtToChan * * This function reads from the sample configuration structure which specifies * cross bar events mapped to DMA channel. * * \return EDMA3_DRV_SOK if success, else error code */ EDMA3_DRV_Result sampleMapXbarEvtToChan (unsigned int eventNum, unsigned int *chanNum, const EDMA3_DRV_GblXbarToChanConfigParams * edmaGblXbarConfig) { EDMA3_DRV_Result edma3Result = EDMA3_DRV_E_INVALID_PARAM; unsigned int xbarEvtNum = 0; int edmaChanNum = 0; if ((eventNum < EDMA3_MAX_CROSS_BAR_EVENTS_DRA72X) && (chanNum != NULL) && (edmaGblXbarConfig != NULL)) { xbarEvtNum = eventNum - EDMA3_NUM_TCC; edmaChanNum = edmaGblXbarConfig->dmaMapXbarToChan[xbarEvtNum]; if (edmaChanNum != -1) { *chanNum = edmaChanNum; edma3Result = EDMA3_DRV_SOK; } } return (edma3Result); } /** * \brief sampleConfigScr * * This function configures control config registers for the cross bar events * mapped to the EDMA channel. * * \return EDMA3_DRV_SOK if success, else error code */ EDMA3_DRV_Result sampleConfigScr (unsigned int eventNum, unsigned int chanNum) { EDMA3_DRV_Result edma3Result = EDMA3_DRV_SOK; unsigned int scrChanOffset = 0; unsigned int scrRegOffset = 0; unsigned int xBarEvtNum = 0; CSL_IntmuxRegsOvly scrEvtMux = (CSL_IntmuxRegsOvly)(EDMA3_EVENT_MUX_REG_BASE_ADDR); if ((eventNum < EDMA3_MAX_CROSS_BAR_EVENTS_DRA72X) && (chanNum < EDMA3_NUM_TCC)) { scrRegOffset = chanNum / 2; scrChanOffset = chanNum - (scrRegOffset * 2); xBarEvtNum = eventNum + 1; switch(scrChanOffset) { case 0: scrEvtMux->TPCC_EVTMUX[scrRegOffset] |= (xBarEvtNum & CSL_INTMUX_TPCC_EVTMUX_TPCCEVT_MUX_0_MASK); break; case 1: scrEvtMux->TPCC_EVTMUX[scrRegOffset] |= ((xBarEvtNum << CSL_INTMUX_TPCC_EVTMUX_TPCCEVT_MUX_1_SHIFT) & (CSL_INTMUX_TPCC_EVTMUX_TPCCEVT_MUX_1_MASK)); break; default: edma3Result = EDMA3_DRV_E_INVALID_PARAM; break; } } else { edma3Result = EDMA3_DRV_E_INVALID_PARAM; } return edma3Result; } EDMA3_DRV_Result sampleInitXbarEvt(EDMA3_DRV_Handle hEdma, unsigned int edma3Id) { EDMA3_DRV_Result retVal = EDMA3_DRV_SOK; const EDMA3_DRV_GblXbarToChanConfigParams *sampleXbarToChanConfig = &(sampleXbarChanInitConfig[edma3Id][dsp_num]); if (hEdma != NULL) { retVal = EDMA3_DRV_initXbarEventMap(hEdma, sampleXbarToChanConfig, (EDMA3_DRV_mapXbarEvtToChan)&sampleMapXbarEvtToChan, (EDMA3_DRV_xbarConfigScr)&sampleConfigScr); } return retVal; } void Edma3MemProtectionHandler(unsigned int edma3InstanceId) { printf("memory Protection error"); }