Texas Instruments Technology for Innovators(tm)

EDMA3 LLD 02.10.00 Release Notes

Sept 14, 2009

This EDMA3 Low Level Driver Release is targeted to the users (device drivers and applications) for submitting and synchronizing with EDMA3 based DMA transfers. This release supports DA830 & TCI6498 platforms, on DSP/BIOS 6 side. Porting instructions are also provided to use the package for different platforms and Operating Systems.

Introduction, Documentation, What's New, Upgrade Info, Device Support, Compatibility Information, Validation Info, Known Issues, Examples, Version Information, Technical Support


Introduction

EDMA3 LLD is a single product package containing the following stand-alone software components:

EDMA3 Resource Manager can be used independently whereas the EDMA3 Driver requires the Resource Manager services internally.

EDMA3 LLD (both Resource Manager and the Driver) is a platform independent package. Hence it can be used across multiple platforms. Porting instructions are provided for both the components to do the same.

It is also an OS-agnostic package and thus can be used across multiple operating systems. OS-adaptation layer needs to be provided by the user (in case it is needed) for OS customization. Instructions to do the same are also provided along with the package.

The Low Level Driver has already been ported (DSP/BIOS Operating Systems) and tested on various platforms mentioned below. Sample initialization libraries, which configure the EDMA3 hardware and provide the necessary OS abstraction layer, are also a part of the package. These libraries are available both for the EDMA3 Resource Manager and EDMA3 Driver. These could be used for proper initialization of the software component(s) along with the OS adaptation layer for the same.

The Low Level Driver consists of the following packages:

Documentation

The following documentation is available:


What's New

The following significant changes have been made since 02.00.01:

02.10.00 - This release

The following ECNs are implemented:

ID Headline
TIDSP00012004 Migration to new BSD license
TIDSP00012060 Add TCI6498 support on BIOS6
TIDSP00012061 Support for Big Endian platforms
TIDSP00012062 Specific link channel can be requested using requestChannel API
TIDSP00012063 Link channels can have TCC code
TIDSP00012064 New API to register callback function in EDMA3 driver
TIDSP00012065 New API to check the status of a given DMA/QDMA channel
TIDSP00012079 Signature change for EDMA3 initialization API present in the sample example
TIDSP00012080 API required to enable error interrupts for EDMA3 Transfer Controller
TIDSP00012081 DRAE registers programmed for TCCs while registering callback functions
TIDSP00012094 Linux installer of EDMA3 LLD

The following IRs are closed:

ID Headline
SDOCM00060737 EDMA3 needs to show up as RTSC product in CCSv4

Upgrade Information

The EDMA3 LLD packages are available in the "packages/" subdirectory of the product. If you have a previous release of the EDMA3 LLD product, you can install this release next to it, and modify your application and/or server builds to use this newer release.


Device Support

This release supports and has been tested on the following devices:


Compatibility Information

Compatibility Key Definitions

Compatibility keys are intentionally independent of Marketing product numbers and are intended to:

  1. Enable tooling to identify incompatibilities between components, and
  2. Convey a level of compatibility between different releases to set end user expectations.

Compatibility keys are composed of 3 comma-delimited numbers - M, S, R - where:


Validation

This release was built and validated against using the following components:

This release was validated in the following configurations:


Known Issues

The following are known issues with the current EDMA3 LLD release:

Pre-built instrumented libraries for DA830 not provided initially.

Pre-built instrumented EDMA3 libraries for DA830 will not be provided initially. XDC does not support the same and hence the limitation. See IR# SDOCM00036738 for more details.

EDMA3 hardware does not work properly in FIFO mode with all the controllers.

Very few peripherals support EDMA3 FIFO mode. EMIF controller doesn't support the same. So EDMA3 CANNOT be used in FIFO mode for doing a memory-to-memory data transfers, EDMA3 being configured in the FIFO mode. Applications trying to use EDMA3 in FIFO mode should first check their respective peripheral-controller document for this mode support.


Examples

EDMA3 LLD sample initialization libraries / OS abstraction layers (for different platforms) are located in:

EDMA3 LLD stand-alone applications (for different platforms) are located in:


Version Information

This product's version follows a version format, M.mm.pp.bb, where M is a 2 digit major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.

To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. edma3_lld_02_10_00_XX.

Subsequent releases of patch upgrades will be identified by the patch number, ex. EDMA3 LLD 02.10.01 with directory edma3_lld_02_10_01_YY. Typically, these patches only include critical bug fixes.


Technical Support

For technical support, contact softwaresupport@ti.com


Last updated: Sept 14, 2009