fixed build warning
[keystone-rtos/edma3_lld.git] / examples / edma3_driver / src / dma_poll_test.c
old mode 100644 (file)
new mode 100755 (executable)
index 948dc1a..efd308c
@@ -7,7 +7,7 @@
 * to check the status of ongoing transfer. Interrupt will NOT occur in this 
 * case.
 *
-* Copyright (C) 2009 Texas Instruments Incorporated - http://www.ti.com/ 
+* Copyright (C) 2009-2018 Texas Instruments Incorporated - http://www.ti.com/
 * 
 * 
 *  Redistribution and use in source and binary forms, with or without 
@@ -48,6 +48,7 @@ extern signed char   _dstBuff1[MAX_BUFFER_SIZE];
 extern signed char *srcBuff1;
 extern signed char *dstBuff1;
 
+#define EDMA3_DRV_DMA_CHANNEL_USR_REQ     (10)
 /**
 *  \brief   EDMA3 mem-to-mem data copy test case, using a DMA channel.
 *              This test case doesnot rely on the callback mechanism.
@@ -78,6 +79,9 @@ EDMA3_DRV_Result edma3_test_poll_mode(
     uint32_t BRCnt = 0;
     int srcbidx = 0, desbidx = 0;
     int srccidx = 0, descidx = 0;
+#ifdef EDMA3_RES_USER_REQ
+    uint32_t paRAMId = 0;
+#endif
 
 
     srcBuff1 = (signed char*) GLOBAL_ADDR(_srcBuff1);
@@ -139,7 +143,6 @@ EDMA3_DRV_Result edma3_test_poll_mode(
     tcc = EDMA3_DRV_TCC_ANY;
     chId = EDMA3_DRV_DMA_CHANNEL_ANY;
 
-
     /* Request any DMA channel and any TCC */
     if (result == EDMA3_DRV_SOK)
     {
@@ -298,3 +301,276 @@ EDMA3_DRV_Result edma3_test_poll_mode(
     }
     return result;
 }
+
+
+/**
+*  \brief   EDMA3 mem-to-mem data copy test case with user requested paRAMId
+*           using a DMA channel.
+*           This test case doesnot rely on the callback mechanism.
+*           Instead, it Polls the IPR register to check the transfer
+*           completion status.
+*
+*  \param  edma3Instance [IN]    EDMA3 Instance number
+*  \param  acnt        [IN]      Number of bytes in an array
+*  \param  bcnt        [IN]      Number of arrays in a frame
+*  \param  ccnt        [IN]      Number of frames in a block
+*  \param  syncType    [IN]      Synchronization type (A/AB Sync)
+*
+*  \return  EDMA3_DRV_SOK or EDMA3_DRV Error Code
+*/
+EDMA3_DRV_Result edma3_test_user_req_paRAMId(
+                                      EDMA3_DRV_Handle hEdma,
+                                      uint32_t edmaInstance,
+                                      uint32_t acnt,
+                                      uint32_t bcnt,
+                                      uint32_t ccnt,
+                                      EDMA3_DRV_SyncType syncType)
+{
+    EDMA3_DRV_Result result = EDMA3_DRV_SOK;
+    uint32_t chId = 0;
+    uint32_t tcc = 0;
+    int i;
+    uint32_t count;
+    uint32_t Istestpassed = 0u;
+    uint32_t numenabled = 0;
+    uint32_t BRCnt = 0;
+    int srcbidx = 0, desbidx = 0;
+    int srccidx = 0, descidx = 0;
+    uint32_t paRAMId = 0;
+
+
+    srcBuff1 = (signed char*) GLOBAL_ADDR(_srcBuff1);
+    dstBuff1 = (signed char*) GLOBAL_ADDR(_dstBuff1);
+
+    /* Initalize source and destination buffers */
+    for (count = 0u; count < (acnt*bcnt*ccnt); count++)
+    {
+        srcBuff1[count] = (int)count+5;
+        /**
+        * No need to initialize the destination buffer as it is being invalidated.
+        dstBuff1[count] = initval;
+        */
+    }
+
+#ifdef EDMA3_ENABLE_DCACHE
+    /*
+    * Note: These functions are required if the buffer is in DDR.
+    * For other cases, where buffer is NOT in DDR, user
+    * may or may not require the below functions.
+    */
+    /* Flush the Source Buffer */
+    if (result == EDMA3_DRV_SOK)
+    {
+        result = Edma3_CacheFlush((uint32_t)srcBuff1, (acnt*bcnt*ccnt));
+    }
+
+    /* Invalidate the Destination Buffer */
+    if (result == EDMA3_DRV_SOK)
+    {
+        result = Edma3_CacheInvalidate((uint32_t)dstBuff1, (acnt*bcnt*ccnt));
+    }
+#endif  /* EDMA3_ENABLE_DCACHE */
+
+
+    /* Set B count reload as B count. */
+    BRCnt = bcnt;
+
+    /* Setting up the SRC/DES Index */
+    srcbidx = (int)acnt;
+    desbidx = (int)acnt;
+
+    if (syncType == EDMA3_DRV_SYNC_A)
+    {
+        /* A Sync Transfer Mode */
+        srccidx = (int)acnt;
+        descidx = (int)acnt;
+    }
+    else
+    {
+        /* AB Sync Transfer Mode */
+        srccidx = ((int)acnt * (int)bcnt);
+        descidx = ((int)acnt * (int)bcnt);
+    }
+
+
+    /* Setup for Channel 1*/
+    tcc = EDMA3_DRV_TCC_ANY;
+
+    chId = EDMA3_DRV_DMA_CHANNEL_USR_REQ;
+
+    /* Request any DMA channel and any TCC */
+    if (result == EDMA3_DRV_SOK)
+    {
+        result = EDMA3_DRV_requestChannel (hEdma, &chId, &tcc,
+            (EDMA3_RM_EventQueue)0,
+            NULL, NULL);
+
+        result = EDMA3_DRV_getAllocatedPARAMId(hEdma, chId, &paRAMId);
+        if(result == EDMA3_DRV_SOK)
+        {
+            printf("\nReserved Channel ID Test\n");
+            printf ("The Requested Channel ID: %d \nThe allocated PARAM Id:%d\n", (int)chId, (int)paRAMId);
+
+            if (chId == paRAMId)
+            {
+                printf("The Requested Param ID is allocated for the given Channel\n");
+            }
+            else
+            {
+                printf("The Requested Param ID is not allocated as same as the DMA channel\n");
+                result = EDMA3_DATA_MISMATCH_ERROR;
+            }
+            printf("\n");
+        }
+    }
+
+    if (result == EDMA3_DRV_SOK)
+    {
+        result = EDMA3_DRV_setSrcParams (hEdma, chId, (uint32_t)(srcBuff1),
+            EDMA3_DRV_ADDR_MODE_INCR,
+            EDMA3_DRV_W8BIT);
+    }
+
+    if (result == EDMA3_DRV_SOK)
+    {
+        result = EDMA3_DRV_setDestParams (hEdma, chId, (uint32_t)(dstBuff1),
+            EDMA3_DRV_ADDR_MODE_INCR,
+            EDMA3_DRV_W8BIT);
+    }
+
+    if (result == EDMA3_DRV_SOK)
+    {
+        result = EDMA3_DRV_setSrcIndex (hEdma, chId, srcbidx, srccidx);
+    }
+
+    if (result == EDMA3_DRV_SOK)
+    {
+        result =  EDMA3_DRV_setDestIndex (hEdma, chId, desbidx, descidx);
+    }
+
+    if (result == EDMA3_DRV_SOK)
+    {
+        if (syncType == EDMA3_DRV_SYNC_A)
+        {
+            result = EDMA3_DRV_setTransferParams (hEdma, chId, acnt, bcnt, ccnt,
+                BRCnt, EDMA3_DRV_SYNC_A);
+        }
+        else
+        {
+            result = EDMA3_DRV_setTransferParams (hEdma, chId, acnt, bcnt, ccnt,
+                BRCnt, EDMA3_DRV_SYNC_AB);
+        }
+    }
+
+    if (result == EDMA3_DRV_SOK)
+    {
+        result = EDMA3_DRV_setOptField (hEdma, chId,
+            EDMA3_DRV_OPT_FIELD_TCINTEN, 1u);
+    }
+
+    if (result == EDMA3_DRV_SOK)
+    {
+        result = EDMA3_DRV_setOptField (hEdma, chId,
+            EDMA3_DRV_OPT_FIELD_ITCINTEN, 1u);
+    }
+
+    /*
+    * Since the transfer is going to happen in Manual mode of EDMA3
+    * operation, we have to 'Enable the Transfer' multiple times.
+    * Number of times depends upon the Mode (A/AB Sync)
+    * and the different counts.
+    */
+    if (result == EDMA3_DRV_SOK)
+    {
+        /*Need to activate next param*/
+        if (syncType == EDMA3_DRV_SYNC_A)
+        {
+            numenabled = bcnt * ccnt;
+        }
+        else
+        {
+            /* AB Sync Transfer Mode */
+            numenabled = ccnt;
+        }
+
+
+        for (i = 0; i < numenabled; i++)
+        {
+            /*
+            * Now enable the transfer as many times as calculated above.
+            */
+            result = EDMA3_DRV_enableTransfer (hEdma, chId,
+                EDMA3_DRV_TRIG_MODE_MANUAL);
+            if (result != EDMA3_DRV_SOK)
+            {
+#ifdef EDMA3_DRV_DEBUG
+                EDMA3_DRV_PRINTF ("edma3_test_user_req_paRAMId: EDMA3_DRV_enableTransfer " \
+                    "Failed, error code: %d\r\n", result);
+#endif  /* EDMA3_DRV_DEBUG */
+                break;
+            }
+
+
+            /* Wait for the Completion Bit to be SET in the IPR/IPRH register. */
+            result = EDMA3_DRV_waitAndClearTcc (hEdma, tcc);
+            if (result != EDMA3_DRV_SOK)
+            {
+#ifdef EDMA3_DRV_DEBUG
+                EDMA3_DRV_PRINTF ("edma3_test_user_req_paRAMId: EDMA3_DRV_waitAndClearTcc " \
+                    "Failed, error code: %d\r\n", result);
+#endif  /* EDMA3_DRV_DEBUG */
+                break;
+            }
+        }
+    }
+
+
+    /* Match the Source and Destination Buffers. */
+    if (EDMA3_DRV_SOK == result)
+    {
+        for (i = 0; i < (acnt*bcnt*ccnt); i++)
+        {
+            if (srcBuff1[i] != dstBuff1[i])
+            {
+                Istestpassed = 0u;
+#ifdef EDMA3_DRV_DEBUG
+                EDMA3_DRV_PRINTF("edma3_test_user_req_paRAMId: Data write-read matching" \
+                    "FAILED at i = %d\r\n", i);
+#endif  /* EDMA3_DRV_DEBUG */
+                break;
+            }
+        }
+        if (i == (acnt*bcnt*ccnt))
+        {
+            Istestpassed = 1u;
+        }
+
+
+        /* Free the previously allocated channel. */
+        result = EDMA3_DRV_freeChannel (hEdma, chId);
+        if (result != EDMA3_DRV_SOK)
+        {
+#ifdef EDMA3_DRV_DEBUG
+            EDMA3_DRV_PRINTF("edma3_test_user_req_paRAMId: EDMA3_DRV_freeChannel() FAILED, " \
+                "error code: %d\r\n", result);
+#endif  /* EDMA3_DRV_DEBUG */
+        }
+    }
+
+
+    if(Istestpassed == 1u)
+    {
+#ifdef EDMA3_DRV_DEBUG
+        EDMA3_DRV_PRINTF("edma3_test_user_req_paRAMId PASSED\r\n");
+#endif  /* EDMA3_DRV_DEBUG */
+    }
+    else
+    {
+#ifdef EDMA3_DRV_DEBUG
+        EDMA3_DRV_PRINTF("edma3_test_user_req_paRAMId FAILED\r\n");
+#endif  /* EDMA3_DRV_DEBUG */
+        result = ((EDMA3_DRV_SOK == result) ?
+                    EDMA3_DATA_MISMATCH_ERROR : result);
+    }
+    return result;
+}