uint32_t BRCnt = 0;
int srcbidx = 0, desbidx = 0;
int srccidx = 0, descidx = 0;
+#ifdef EDMA3_RES_USER_REQ
+ uint32_t paRAMId = 0;
+#endif
srcBuff1 = (signed char*) GLOBAL_ADDR(_srcBuff1);
/* Setup for Channel 1*/
tcc = EDMA3_DRV_TCC_ANY;
-#ifdef EDMA3_RES_USER_REQ
- chId = EDMA3_DRV_DMA_CHANNEL_USR_REQ;
-#else
chId = EDMA3_DRV_DMA_CHANNEL_ANY;
-#endif
-
/* Request any DMA channel and any TCC */
if (result == EDMA3_DRV_SOK)
result = EDMA3_DRV_requestChannel (hEdma, &chId, &tcc,
(EDMA3_RM_EventQueue)0,
NULL, NULL);
-#ifdef EDMA3_RES_USER_REQ
- printf("\nReserved Channel ID Test\n");
- printf ("The Requested Channel ID: %d \nThe allocated PARAM Id:%d\n",chId,EDMA3_DRV_getAllocatedPARAMId());
-
- if (chId == EDMA3_DRV_getAllocatedPARAMId())
- {
- printf("The Requested Param ID is allocated for the given Channel\n");
- }
- printf("\n");
-#endif
}
if (result == EDMA3_DRV_SOK)
}
return result;
}
+
+
+/**
+* \brief EDMA3 mem-to-mem data copy test case with user requested paRAMId
+* using a DMA channel.
+* This test case doesnot rely on the callback mechanism.
+* Instead, it Polls the IPR register to check the transfer
+* completion status.
+*
+* \param edma3Instance [IN] EDMA3 Instance number
+* \param acnt [IN] Number of bytes in an array
+* \param bcnt [IN] Number of arrays in a frame
+* \param ccnt [IN] Number of frames in a block
+* \param syncType [IN] Synchronization type (A/AB Sync)
+*
+* \return EDMA3_DRV_SOK or EDMA3_DRV Error Code
+*/
+EDMA3_DRV_Result edma3_test_user_req_paRAMId(
+ EDMA3_DRV_Handle hEdma,
+ uint32_t edmaInstance,
+ uint32_t acnt,
+ uint32_t bcnt,
+ uint32_t ccnt,
+ EDMA3_DRV_SyncType syncType)
+{
+ EDMA3_DRV_Result result = EDMA3_DRV_SOK;
+ uint32_t chId = 0;
+ uint32_t tcc = 0;
+ int i;
+ uint32_t count;
+ uint32_t Istestpassed = 0u;
+ uint32_t numenabled = 0;
+ uint32_t BRCnt = 0;
+ int srcbidx = 0, desbidx = 0;
+ int srccidx = 0, descidx = 0;
+ uint32_t paRAMId = 0;
+
+
+ srcBuff1 = (signed char*) GLOBAL_ADDR(_srcBuff1);
+ dstBuff1 = (signed char*) GLOBAL_ADDR(_dstBuff1);
+
+ /* Initalize source and destination buffers */
+ for (count = 0u; count < (acnt*bcnt*ccnt); count++)
+ {
+ srcBuff1[count] = (int)count+5;
+ /**
+ * No need to initialize the destination buffer as it is being invalidated.
+ dstBuff1[count] = initval;
+ */
+ }
+
+#ifdef EDMA3_ENABLE_DCACHE
+ /*
+ * Note: These functions are required if the buffer is in DDR.
+ * For other cases, where buffer is NOT in DDR, user
+ * may or may not require the below functions.
+ */
+ /* Flush the Source Buffer */
+ if (result == EDMA3_DRV_SOK)
+ {
+ result = Edma3_CacheFlush((uint32_t)srcBuff1, (acnt*bcnt*ccnt));
+ }
+
+ /* Invalidate the Destination Buffer */
+ if (result == EDMA3_DRV_SOK)
+ {
+ result = Edma3_CacheInvalidate((uint32_t)dstBuff1, (acnt*bcnt*ccnt));
+ }
+#endif /* EDMA3_ENABLE_DCACHE */
+
+
+ /* Set B count reload as B count. */
+ BRCnt = bcnt;
+
+ /* Setting up the SRC/DES Index */
+ srcbidx = (int)acnt;
+ desbidx = (int)acnt;
+
+ if (syncType == EDMA3_DRV_SYNC_A)
+ {
+ /* A Sync Transfer Mode */
+ srccidx = (int)acnt;
+ descidx = (int)acnt;
+ }
+ else
+ {
+ /* AB Sync Transfer Mode */
+ srccidx = ((int)acnt * (int)bcnt);
+ descidx = ((int)acnt * (int)bcnt);
+ }
+
+
+ /* Setup for Channel 1*/
+ tcc = EDMA3_DRV_TCC_ANY;
+
+ chId = EDMA3_DRV_DMA_CHANNEL_USR_REQ;
+
+ /* Request any DMA channel and any TCC */
+ if (result == EDMA3_DRV_SOK)
+ {
+ result = EDMA3_DRV_requestChannel (hEdma, &chId, &tcc,
+ (EDMA3_RM_EventQueue)0,
+ NULL, NULL);
+
+ result = EDMA3_DRV_getAllocatedPARAMId(hEdma, chId, &paRAMId);
+ if(result == EDMA3_DRV_SOK)
+ {
+ printf("\nReserved Channel ID Test\n");
+ printf ("The Requested Channel ID: %d \nThe allocated PARAM Id:%d\n", (int)chId, (int)paRAMId);
+
+ if (chId == paRAMId)
+ {
+ printf("The Requested Param ID is allocated for the given Channel\n");
+ }
+ else
+ {
+ printf("The Requested Param ID is not allocated as same as the DMA channel\n");
+ result = EDMA3_DATA_MISMATCH_ERROR;
+ }
+ printf("\n");
+ }
+ }
+
+ if (result == EDMA3_DRV_SOK)
+ {
+ result = EDMA3_DRV_setSrcParams (hEdma, chId, (uint32_t)(srcBuff1),
+ EDMA3_DRV_ADDR_MODE_INCR,
+ EDMA3_DRV_W8BIT);
+ }
+
+ if (result == EDMA3_DRV_SOK)
+ {
+ result = EDMA3_DRV_setDestParams (hEdma, chId, (uint32_t)(dstBuff1),
+ EDMA3_DRV_ADDR_MODE_INCR,
+ EDMA3_DRV_W8BIT);
+ }
+
+ if (result == EDMA3_DRV_SOK)
+ {
+ result = EDMA3_DRV_setSrcIndex (hEdma, chId, srcbidx, srccidx);
+ }
+
+ if (result == EDMA3_DRV_SOK)
+ {
+ result = EDMA3_DRV_setDestIndex (hEdma, chId, desbidx, descidx);
+ }
+
+ if (result == EDMA3_DRV_SOK)
+ {
+ if (syncType == EDMA3_DRV_SYNC_A)
+ {
+ result = EDMA3_DRV_setTransferParams (hEdma, chId, acnt, bcnt, ccnt,
+ BRCnt, EDMA3_DRV_SYNC_A);
+ }
+ else
+ {
+ result = EDMA3_DRV_setTransferParams (hEdma, chId, acnt, bcnt, ccnt,
+ BRCnt, EDMA3_DRV_SYNC_AB);
+ }
+ }
+
+ if (result == EDMA3_DRV_SOK)
+ {
+ result = EDMA3_DRV_setOptField (hEdma, chId,
+ EDMA3_DRV_OPT_FIELD_TCINTEN, 1u);
+ }
+
+ if (result == EDMA3_DRV_SOK)
+ {
+ result = EDMA3_DRV_setOptField (hEdma, chId,
+ EDMA3_DRV_OPT_FIELD_ITCINTEN, 1u);
+ }
+
+ /*
+ * Since the transfer is going to happen in Manual mode of EDMA3
+ * operation, we have to 'Enable the Transfer' multiple times.
+ * Number of times depends upon the Mode (A/AB Sync)
+ * and the different counts.
+ */
+ if (result == EDMA3_DRV_SOK)
+ {
+ /*Need to activate next param*/
+ if (syncType == EDMA3_DRV_SYNC_A)
+ {
+ numenabled = bcnt * ccnt;
+ }
+ else
+ {
+ /* AB Sync Transfer Mode */
+ numenabled = ccnt;
+ }
+
+
+ for (i = 0; i < numenabled; i++)
+ {
+ /*
+ * Now enable the transfer as many times as calculated above.
+ */
+ result = EDMA3_DRV_enableTransfer (hEdma, chId,
+ EDMA3_DRV_TRIG_MODE_MANUAL);
+ if (result != EDMA3_DRV_SOK)
+ {
+#ifdef EDMA3_DRV_DEBUG
+ EDMA3_DRV_PRINTF ("edma3_test_user_req_paRAMId: EDMA3_DRV_enableTransfer " \
+ "Failed, error code: %d\r\n", result);
+#endif /* EDMA3_DRV_DEBUG */
+ break;
+ }
+
+
+ /* Wait for the Completion Bit to be SET in the IPR/IPRH register. */
+ result = EDMA3_DRV_waitAndClearTcc (hEdma, tcc);
+ if (result != EDMA3_DRV_SOK)
+ {
+#ifdef EDMA3_DRV_DEBUG
+ EDMA3_DRV_PRINTF ("edma3_test_user_req_paRAMId: EDMA3_DRV_waitAndClearTcc " \
+ "Failed, error code: %d\r\n", result);
+#endif /* EDMA3_DRV_DEBUG */
+ break;
+ }
+ }
+ }
+
+
+ /* Match the Source and Destination Buffers. */
+ if (EDMA3_DRV_SOK == result)
+ {
+ for (i = 0; i < (acnt*bcnt*ccnt); i++)
+ {
+ if (srcBuff1[i] != dstBuff1[i])
+ {
+ Istestpassed = 0u;
+#ifdef EDMA3_DRV_DEBUG
+ EDMA3_DRV_PRINTF("edma3_test_user_req_paRAMId: Data write-read matching" \
+ "FAILED at i = %d\r\n", i);
+#endif /* EDMA3_DRV_DEBUG */
+ break;
+ }
+ }
+ if (i == (acnt*bcnt*ccnt))
+ {
+ Istestpassed = 1u;
+ }
+
+
+ /* Free the previously allocated channel. */
+ result = EDMA3_DRV_freeChannel (hEdma, chId);
+ if (result != EDMA3_DRV_SOK)
+ {
+#ifdef EDMA3_DRV_DEBUG
+ EDMA3_DRV_PRINTF("edma3_test_user_req_paRAMId: EDMA3_DRV_freeChannel() FAILED, " \
+ "error code: %d\r\n", result);
+#endif /* EDMA3_DRV_DEBUG */
+ }
+ }
+
+
+ if(Istestpassed == 1u)
+ {
+#ifdef EDMA3_DRV_DEBUG
+ EDMA3_DRV_PRINTF("edma3_test_user_req_paRAMId PASSED\r\n");
+#endif /* EDMA3_DRV_DEBUG */
+ }
+ else
+ {
+#ifdef EDMA3_DRV_DEBUG
+ EDMA3_DRV_PRINTF("edma3_test_user_req_paRAMId FAILED\r\n");
+#endif /* EDMA3_DRV_DEBUG */
+ result = ((EDMA3_DRV_SOK == result) ?
+ EDMA3_DATA_MISMATCH_ERROR : result);
+ }
+ return result;
+}