]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - keystone-rtos/edma3_lld.git/blobdiff - makerules/env.mk
updated lib path for gcc compiler
[keystone-rtos/edma3_lld.git] / makerules / env.mk
index 3a80e41f29a77de2d338dcf023962b1c58655b61..99b698e19918dff405883fcd0c562d5d341fa783 100755 (executable)
@@ -7,7 +7,7 @@
 # Directory where all internal software packages are located; typically 
 #  those that are checked into version controlled repository. In this case all
 #  the OMX components and SDK/OMX demo.
-INTERNAL_SW_ROOT ?= E:/EDMA/edma3_lld_02_12_01_23
+INTERNAL_SW_ROOT ?= E:/EDMA/edma3_lld_02_12_01_25
 
 # Directory where all external (imported) software packages are located; typically 
 #  those that are NOT checked into version controlled repository. In this case,
@@ -23,7 +23,7 @@ EXTERNAL_SW_ROOT ?= C:/PROGRA~2/TEXASI~1
 # Utilities directory. This is required only if the build machine is Windows.
 #   - specify the installation directory of utility which supports POSIX commands
 #     (eg: Cygwin installation or MSYS installation).
-UTILS_INSTALL_DIR = $(EXTERNAL_SW_ROOT)/xdctools_3_31_02_38_core
+UTILS_INSTALL_DIR = $(EXTERNAL_SW_ROOT)/xdctools_3_61_00_16_core
 
 # Set path separator, etc based on the OS
 # On windows if sh.exe is installed (cygwin installs) make will execute
@@ -44,11 +44,11 @@ else
 endif
 
 # BIOS
-bios_PATH = $(EXTERNAL_SW_ROOT)/bios_6_42_02_29
+bios_PATH = $(EXTERNAL_SW_ROOT)/bios_6_82_00_16
 bios_INCLUDE = $(bios_PATH)/packages
 
 # XDC
-xdc_PATH = $(EXTERNAL_SW_ROOT)/xdctools_3_31_02_38
+xdc_PATH = $(EXTERNAL_SW_ROOT)/xdctools_3_61_00_16_core
 xdc_INCLUDE = $(xdc_PATH)/packages
 
 # EDMA3 LLD
@@ -59,31 +59,31 @@ include $(edma3_lld_PATH)/packages/component.mk
 # Tools paths
 #
 # Cortex-M3
-CODEGEN_PATH_M3 = $(EXTERNAL_SW_ROOT)/TIARMC~1.5
+CODEGEN_PATH_M3 = $(EXTERNAL_SW_ROOT)/ti-cgt-arm_20.2.0.LTS
 # Cortex-M4
-CODEGEN_PATH_M4 = $(EXTERNAL_SW_ROOT)/ti-cgt-arm_5.2.2
+CODEGEN_PATH_M4 = $(EXTERNAL_SW_ROOT)/ti-cgt-arm_20.2.0.LTS
 # Cortex-A8
-CODEGEN_PATH_A8 = $(EXTERNAL_SW_ROOT)/TIARMC~1.5
+CODEGEN_PATH_A8 = $(EXTERNAL_SW_ROOT)/ti-cgt-arm_20.2.0.LTS
 # Cortex-A8 GCC
-CODEGEN_PATH_A8_GCC = $(EXTERNAL_SW_ROOT)/gcc-arm-none-eabi-4_8-2014q3
+CODEGEN_PATH_A8_GCC = $(EXTERNAL_SW_ROOT)/gcc-arm-none-eabi-9-2019-q4-major
 
 # Cortex-A15
-CODEGEN_PATH_A15 = $(EXTERNAL_SW_ROOT)/gcc-arm-none-eabi-4_8-2014q3
+CODEGEN_PATH_A15 = $(EXTERNAL_SW_ROOT)/gcc-arm-none-eabi-9-2019-q4-major
 # Cortex-A15_GCC
-CODEGEN_PATH_A15_GCC = $(EXTERNAL_SW_ROOT)/gcc-arm-none-eabi-4_8-2014q3
+CODEGEN_PATH_A15_GCC = $(EXTERNAL_SW_ROOT)/gcc-arm-none-eabi-6-2017-q1-update
 
 # ARM-9
-CODEGEN_PATH_ARM9 = $(EXTERNAL_SW_ROOT)/TIARMC~1.5
+CODEGEN_PATH_ARM9 = $(EXTERNAL_SW_ROOT)/ti-cgt-arm_20.2.0.LTS
 # ARM-9 GCC
-CODEGEN_PATH_A9_GCC = $(EXTERNAL_SW_ROOT)/gcc-arm-none-eabi-4_8-2014q3
+CODEGEN_PATH_A9_GCC = $(EXTERNAL_SW_ROOT)/gcc-arm-none-eabi-6-2017-q1-update
 
 # DSP - Since same toolchain does not support COFF and ELF, there are two entries
 #        This would go away when one version supports both formats
-CODEGEN_PATH_DSP = $(EXTERNAL_SW_ROOT)/c6000_7.4.12
-CODEGEN_PATH_DSPELF = $(EXTERNAL_SW_ROOT)/c6000_7.4.12
+CODEGEN_PATH_DSP = $(EXTERNAL_SW_ROOT)/ti-cgt-c6000_8.3.2
+CODEGEN_PATH_DSPELF = $(EXTERNAL_SW_ROOT)/ti-cgt-c6000_8.3.2
 
 # ARP32
-CODEGEN_PATH_ARP32 = $(EXTERNAL_SW_ROOT)/ARP32_1.0.2
+CODEGEN_PATH_ARP32 = /datalocal/ti_components/cg_tools/linux/arp32_1.0.8
 
 # Commands commonly used within the make files
 
@@ -133,7 +133,4 @@ export TMS470_CGTOOLS
 CODESOURCERYCGTOOLS = $(CODEGEN_PATH_A8)
 export CODESOURCERYCGTOOLS
 
-PATH += $(PATH_SEPARATOR)$(xdc_PATH)$(PATH_SEPARATOR)$(CODEGEN_PATH_M3)/bin
-export PATH
-
 # Nothing beyond this point