Updated the tools used for building the package in env.mk
[keystone-rtos/edma3_lld.git] / makerules / env.mk
old mode 100644 (file)
new mode 100755 (executable)
index fccbab9..b498f8a
@@ -7,12 +7,12 @@
 # Directory where all internal software packages are located; typically 
 #  those that are checked into version controlled repository. In this case all
 #  the OMX components and SDK/OMX demo.
-INTERNAL_SW_ROOT = E:/EDMA/MAKEFI~1/WITHMA~1/testinghis/edma/edma3_lld_02_10_04_01
+INTERNAL_SW_ROOT = E:/EDMA/edma3_lld_02_11_00_01
 
 # Directory where all external (imported) software packages are located; typically 
 #  those that are NOT checked into version controlled repository. In this case,
 #  compiler tool chains, BIOS, XDC, Syslink, IPC, FC, CE, drivers, codecs, etc.
-EXTERNAL_SW_ROOT = E:/EDMA/MAKEFI~1/WITHMA~1/testinghis/edma/tools
+EXTERNAL_SW_ROOT = C:/PROGRA~1/TEXASI~1
 
 # Destination root directory.
 #   - specify the directory where you want to place the object, archive/library,
@@ -23,7 +23,7 @@ EXTERNAL_SW_ROOT = E:/EDMA/MAKEFI~1/WITHMA~1/testinghis/edma/tools
 # Utilities directory. This is required only if the build machine is Windows.
 #   - specify the installation directory of utility which supports POSIX commands
 #     (eg: Cygwin installation or MSYS installation).
-UTILS_INSTALL_DIR = E:/EDMA/MAKEFI~1/WITHMA~1/testinghis/edma/tools/xdctools_3_20_02_59
+UTILS_INSTALL_DIR = C:/PROGRA~1/TEXASI~1/xdctools_3_20_07_86
 
 # Set path separator, etc based on the OS
 ifeq ($(OS),Windows_NT)
@@ -35,11 +35,11 @@ else
 endif
 
 # BIOS
-bios_PATH = $(EXTERNAL_SW_ROOT)/bios_6_30_02_42
+bios_PATH = $(EXTERNAL_SW_ROOT)/bios_6_31_04_27
 bios_INCLUDE = $(bios_PATH)/packages
 
 # XDC
-xdc_PATH = $(EXTERNAL_SW_ROOT)/xdctools_3_20_02_59
+xdc_PATH = $(EXTERNAL_SW_ROOT)/xdctools_3_20_07_86
 xdc_INCLUDE = $(xdc_PATH)/packages
 
 # EDMA3 LLD
@@ -50,16 +50,18 @@ include $(edma3_lld_PATH)/packages/component.mk
 # Tools paths
 #
 # Cortex-M3
-
 CODEGEN_PATH_M3 = $(EXTERNAL_SW_ROOT)/TMS470~1.3
 
 # Cortex-A8
-CODEGEN_PATH_A8 = $(EXTERNAL_SW_ROOT)/CodeSourcery/2009q1-203
+CODEGEN_PATH_A8 = $(EXTERNAL_SW_ROOT)/TMS470~1.3
+
+# ARM-9
+CODEGEN_PATH_ARM9 = $(EXTERNAL_SW_ROOT)/TMS470~1.3
 
 # DSP - Since same toolchain does not support COFF and ELF, there are two entries
 #        This would go away when one version supports both formats
-CODEGEN_PATH_DSP = $(EXTERNAL_SW_ROOT)/C6000C~1.0
-CODEGEN_PATH_DSPELF = $(EXTERNAL_SW_ROOT)/C6000C~1.0A1
+CODEGEN_PATH_DSP = $(EXTERNAL_SW_ROOT)/C6000C~1.4
+CODEGEN_PATH_DSPELF = $(EXTERNAL_SW_ROOT)/C6000C~1.0
 
 
 # Commands commonly used within the make files
@@ -84,8 +86,11 @@ endif
 #
 
 # XDC Config.bld file (required for configuro) ; Derives from top-level omx_PATH
-CONFIG_BLD_XDC_c674 = $(edma3_lld_PATH)/packages/_config.bld
-CONFIG_BLD_XDC_c64p = $(edma3_lld_PATH)/packages/_config.bld
+CONFIG_BLD_XDC_674 = $(edma3_lld_PATH)/packages/_config.bld
+CONFIG_BLD_XDC_64p = $(edma3_lld_PATH)/packages/_config.bld
+CONFIG_BLD_XDC_a8 = $(edma3_lld_PATH)/packages/_config.bld
+CONFIG_BLD_XDC_arm9 = $(edma3_lld_PATH)/packages/_config.bld
+CONFIG_BLD_XDC_66 = $(edma3_lld_PATH)/packages/_config.bld
 
 XDCPATH = $(bios_PATH)/packages;$(xdc_PATH)/packages;$(edma3_lld_PATH)/packages;
 export XDCPATH