Misra C fixes:
[keystone-rtos/edma3_lld.git] / packages / ti / sdo / edma3 / rm / sample / src / sample_arm_init.c
index e89cb0e9487abdcc04fe65f2bd736625d6683bf2..e25564bebea9a819ca5dae49875c5c023c237c02 100644 (file)
 #include <ti/sdo/edma3/rm/sample/bios6_edma3_rm_sample.h>
 
 /** @brief EDMA3 Driver Instance specific Semaphore handle */
 #include <ti/sdo/edma3/rm/sample/bios6_edma3_rm_sample.h>
 
 /** @brief EDMA3 Driver Instance specific Semaphore handle */
-extern EDMA3_OS_Sem_Handle rmSemHandle[];
+extern EDMA3_OS_Sem_Handle rmSemHandle[EDMA3_MAX_EDMA3_INSTANCES];
 
 /**  To Register the ISRs with the underlying OS, if required. */
 
 /**  To Register the ISRs with the underlying OS, if required. */
-extern void registerEdma3Interrupts (unsigned int edma3Id);
+extern void registerEdma3Interrupts (uint32_t edma3Id);
 /**  To Unregister the ISRs with the underlying OS, if previously registered. */
 /**  To Unregister the ISRs with the underlying OS, if previously registered. */
-extern void unregisterEdma3Interrupts (unsigned int edma3Id);
+extern void unregisterEdma3Interrupts (uint32_t edma3Id);
 
 /* To find out the DSP# */
 
 /* To find out the DSP# */
-extern unsigned short determineProcId();
+extern uint16_t determineProcId(void);
 
 /**
  * To check whether the global EDMA3 configuration is required or not.
 
 /**
  * To check whether the global EDMA3 configuration is required or not.
@@ -61,31 +61,31 @@ extern unsigned short determineProcId();
  * by one of the masters. Hence this function will return TRUE only once
  * and FALSE for all other masters. 
  */
  * by one of the masters. Hence this function will return TRUE only once
  * and FALSE for all other masters. 
  */
-extern unsigned short isGblConfigRequired(unsigned int dspNum);
+extern uint16_t isGblConfigRequired(uint32_t dspNum);
 
 /**
  * DSP instance number on which the executable is running. Its value is
  * determined by reading the processor specific register DNUM.
  */
 
 /**
  * DSP instance number on which the executable is running. Its value is
  * determined by reading the processor specific register DNUM.
  */
-unsigned int dsp_num;
+uint32_t dsp_num;
 
 /**
  * Shadow Region on which the executable is runnig. Its value is populated
  * with the dsp_num here in this case.
  */
 
 /**
  * Shadow Region on which the executable is runnig. Its value is populated
  * with the dsp_num here in this case.
  */
-unsigned int region_id;
+uint32_t region_id;
 
 /* Number of EDMA3 controllers present in the system */
 
 /* Number of EDMA3 controllers present in the system */
-extern const unsigned int numEdma3Instances;
+extern const uint32_t numEdma3Instances;
 
 /* External Global Configuration Structure */
 
 /* External Global Configuration Structure */
-extern EDMA3_RM_GblConfigParams sampleEdma3GblCfgParams[];
+extern EDMA3_RM_GblConfigParams sampleEdma3GblCfgParams[EDMA3_MAX_EDMA3_INSTANCES];
 
 /* External Instance Specific Configuration Structure */
 
 /* External Instance Specific Configuration Structure */
-extern EDMA3_RM_InstanceInitConfig sampleInstInitConfig[][EDMA3_MAX_REGIONS];
+extern EDMA3_RM_InstanceInitConfig sampleInstInitConfig[EDMA3_MAX_EDMA3_INSTANCES][EDMA3_MAX_REGIONS];
 
 #ifdef DMA_XBAR_AVAILABLE
 
 #ifdef DMA_XBAR_AVAILABLE
-extern EDMA3_DRV_Result sampleInitXbarEvt(EDMA3_DRV_Handle hEdma, unsigned int edma3Id);
+extern EDMA3_DRV_Result sampleInitXbarEvt(EDMA3_DRV_Handle hEdma, uint32_t edma3Id);
 #endif
 
 /**
 #endif
 
 /**
@@ -96,7 +96,7 @@ extern EDMA3_DRV_Result sampleInitXbarEvt(EDMA3_DRV_Handle hEdma, unsigned int e
  *
   * \return  EDMA3_RM_SOK if success, else error code
  */
  *
   * \return  EDMA3_RM_SOK if success, else error code
  */
-EDMA3_RM_Handle edma3init (unsigned int edma3Id, EDMA3_RM_Result *errorCode)
+EDMA3_RM_Handle edma3init (uint32_t edma3Id, EDMA3_RM_Result *errorCode)
     {
     EDMA3_RM_Param initParam;
     EDMA3_RM_Result edma3Result = EDMA3_RM_SOK;
     {
     EDMA3_RM_Param initParam;
     EDMA3_RM_Result edma3Result = EDMA3_RM_SOK;
@@ -107,8 +107,11 @@ EDMA3_RM_Handle edma3init (unsigned int edma3Id, EDMA3_RM_Result *errorCode)
        EDMA3_RM_Handle hEdmaResMgr = NULL;
 
        if ((edma3Id >= numEdma3Instances) || (errorCode == NULL))
        EDMA3_RM_Handle hEdmaResMgr = NULL;
 
        if ((edma3Id >= numEdma3Instances) || (errorCode == NULL))
-               return hEdmaResMgr;
-
+    {
+               hEdmaResMgr = NULL;
+    }
+    else
+    {
     /* DSP instance number */
     dsp_num = determineProcId();
 
     /* DSP instance number */
     dsp_num = determineProcId();
 
@@ -129,7 +132,7 @@ EDMA3_RM_Handle edma3init (unsigned int edma3Id, EDMA3_RM_Result *errorCode)
                Semaphore_Params_init(&semParams);
 
                initParam.rmSemHandle = NULL;
                Semaphore_Params_init(&semParams);
 
                initParam.rmSemHandle = NULL;
-               edma3Result = edma3OsSemCreate(1, &semParams, &initParam.rmSemHandle);
+               edma3Result = edma3OsSemCreate((int32_t)1, &semParams, &initParam.rmSemHandle);
                }
 
        if (edma3Result == EDMA3_DRV_SOK)
                }
 
        if (edma3Result == EDMA3_DRV_SOK)
@@ -159,13 +162,13 @@ EDMA3_RM_Handle edma3init (unsigned int edma3Id, EDMA3_RM_Result *errorCode)
 
 #ifdef DMA_XBAR_AVAILABLE
        {
 
 #ifdef DMA_XBAR_AVAILABLE
        {
-       if(hEdmaResMgr && (edma3Result == EDMA3_RM_SOK))
+       if((hEdmaResMgr != NULL) && (edma3Result == EDMA3_RM_SOK))
                {
                edma3Result = sampleInitXbarEvt(hEdmaResMgr, edma3Id);
                }
        }
 #endif
                {
                edma3Result = sampleInitXbarEvt(hEdmaResMgr, edma3Id);
                }
        }
 #endif
-       if(hEdmaResMgr && (edma3Result == EDMA3_DRV_SOK))
+       if((hEdmaResMgr != NULL) && (edma3Result == EDMA3_DRV_SOK))
                {
                /**
                * Register Interrupt Handlers for various interrupts
                {
                /**
                * Register Interrupt Handlers for various interrupts
@@ -175,7 +178,8 @@ EDMA3_RM_Handle edma3init (unsigned int edma3Id, EDMA3_RM_Result *errorCode)
                registerEdma3Interrupts(edma3Id);
                }
 
                registerEdma3Interrupts(edma3Id);
                }
 
-       *errorCode = edma3Result;       
+       *errorCode = edma3Result;
+    }
        return hEdmaResMgr;
     }
 
        return hEdmaResMgr;
     }
 
@@ -187,7 +191,7 @@ EDMA3_RM_Handle edma3init (unsigned int edma3Id, EDMA3_RM_Result *errorCode)
  *
   * \return  EDMA3_RM_SOK if success, else error code
  */
  *
   * \return  EDMA3_RM_SOK if success, else error code
  */
-EDMA3_RM_Result edma3deinit (unsigned int edma3Id, EDMA3_RM_Handle hEdmaResMgr)
+EDMA3_RM_Result edma3deinit (uint32_t edma3Id, EDMA3_RM_Handle hEdma)
     {
     EDMA3_RM_Result edma3Result = EDMA3_RM_SOK;
 
     {
     EDMA3_RM_Result edma3Result = EDMA3_RM_SOK;
 
@@ -203,7 +207,7 @@ EDMA3_RM_Result edma3deinit (unsigned int edma3Id, EDMA3_RM_Handle hEdmaResMgr)
         rmSemHandle[edma3Id] = NULL;
 
         /* Now, close the EDMA3 RM Instance */
         rmSemHandle[edma3Id] = NULL;
 
         /* Now, close the EDMA3 RM Instance */
-        edma3Result = EDMA3_RM_close (hEdmaResMgr, NULL);
+        edma3Result = EDMA3_RM_close (hEdma, NULL);
        }
        
     if (EDMA3_RM_SOK == edma3Result)
        }
        
     if (EDMA3_RM_SOK == edma3Result)