X-Git-Url: https://git.ti.com/gitweb?p=keystone-rtos%2Fedma3_lld.git;a=blobdiff_plain;f=examples%2Fedma3_driver%2Fsrc%2Fdma_poll_test.c;h=efd308ccd3ec0548902bbc070ee832f6dedbe557;hp=948dc1acf453385d965f1b59430ae51c79106b44;hb=5b09792e446378268175a200f998c2c155916ede;hpb=cfef0f5abb8227fb63512d4246323ebe613b2f57 diff --git a/examples/edma3_driver/src/dma_poll_test.c b/examples/edma3_driver/src/dma_poll_test.c old mode 100644 new mode 100755 index 948dc1a..efd308c --- a/examples/edma3_driver/src/dma_poll_test.c +++ b/examples/edma3_driver/src/dma_poll_test.c @@ -7,7 +7,7 @@ * to check the status of ongoing transfer. Interrupt will NOT occur in this * case. * -* Copyright (C) 2009 Texas Instruments Incorporated - http://www.ti.com/ +* Copyright (C) 2009-2018 Texas Instruments Incorporated - http://www.ti.com/ * * * Redistribution and use in source and binary forms, with or without @@ -48,6 +48,7 @@ extern signed char _dstBuff1[MAX_BUFFER_SIZE]; extern signed char *srcBuff1; extern signed char *dstBuff1; +#define EDMA3_DRV_DMA_CHANNEL_USR_REQ (10) /** * \brief EDMA3 mem-to-mem data copy test case, using a DMA channel. * This test case doesnot rely on the callback mechanism. @@ -78,6 +79,9 @@ EDMA3_DRV_Result edma3_test_poll_mode( uint32_t BRCnt = 0; int srcbidx = 0, desbidx = 0; int srccidx = 0, descidx = 0; +#ifdef EDMA3_RES_USER_REQ + uint32_t paRAMId = 0; +#endif srcBuff1 = (signed char*) GLOBAL_ADDR(_srcBuff1); @@ -139,7 +143,6 @@ EDMA3_DRV_Result edma3_test_poll_mode( tcc = EDMA3_DRV_TCC_ANY; chId = EDMA3_DRV_DMA_CHANNEL_ANY; - /* Request any DMA channel and any TCC */ if (result == EDMA3_DRV_SOK) { @@ -298,3 +301,276 @@ EDMA3_DRV_Result edma3_test_poll_mode( } return result; } + + +/** +* \brief EDMA3 mem-to-mem data copy test case with user requested paRAMId +* using a DMA channel. +* This test case doesnot rely on the callback mechanism. +* Instead, it Polls the IPR register to check the transfer +* completion status. +* +* \param edma3Instance [IN] EDMA3 Instance number +* \param acnt [IN] Number of bytes in an array +* \param bcnt [IN] Number of arrays in a frame +* \param ccnt [IN] Number of frames in a block +* \param syncType [IN] Synchronization type (A/AB Sync) +* +* \return EDMA3_DRV_SOK or EDMA3_DRV Error Code +*/ +EDMA3_DRV_Result edma3_test_user_req_paRAMId( + EDMA3_DRV_Handle hEdma, + uint32_t edmaInstance, + uint32_t acnt, + uint32_t bcnt, + uint32_t ccnt, + EDMA3_DRV_SyncType syncType) +{ + EDMA3_DRV_Result result = EDMA3_DRV_SOK; + uint32_t chId = 0; + uint32_t tcc = 0; + int i; + uint32_t count; + uint32_t Istestpassed = 0u; + uint32_t numenabled = 0; + uint32_t BRCnt = 0; + int srcbidx = 0, desbidx = 0; + int srccidx = 0, descidx = 0; + uint32_t paRAMId = 0; + + + srcBuff1 = (signed char*) GLOBAL_ADDR(_srcBuff1); + dstBuff1 = (signed char*) GLOBAL_ADDR(_dstBuff1); + + /* Initalize source and destination buffers */ + for (count = 0u; count < (acnt*bcnt*ccnt); count++) + { + srcBuff1[count] = (int)count+5; + /** + * No need to initialize the destination buffer as it is being invalidated. + dstBuff1[count] = initval; + */ + } + +#ifdef EDMA3_ENABLE_DCACHE + /* + * Note: These functions are required if the buffer is in DDR. + * For other cases, where buffer is NOT in DDR, user + * may or may not require the below functions. + */ + /* Flush the Source Buffer */ + if (result == EDMA3_DRV_SOK) + { + result = Edma3_CacheFlush((uint32_t)srcBuff1, (acnt*bcnt*ccnt)); + } + + /* Invalidate the Destination Buffer */ + if (result == EDMA3_DRV_SOK) + { + result = Edma3_CacheInvalidate((uint32_t)dstBuff1, (acnt*bcnt*ccnt)); + } +#endif /* EDMA3_ENABLE_DCACHE */ + + + /* Set B count reload as B count. */ + BRCnt = bcnt; + + /* Setting up the SRC/DES Index */ + srcbidx = (int)acnt; + desbidx = (int)acnt; + + if (syncType == EDMA3_DRV_SYNC_A) + { + /* A Sync Transfer Mode */ + srccidx = (int)acnt; + descidx = (int)acnt; + } + else + { + /* AB Sync Transfer Mode */ + srccidx = ((int)acnt * (int)bcnt); + descidx = ((int)acnt * (int)bcnt); + } + + + /* Setup for Channel 1*/ + tcc = EDMA3_DRV_TCC_ANY; + + chId = EDMA3_DRV_DMA_CHANNEL_USR_REQ; + + /* Request any DMA channel and any TCC */ + if (result == EDMA3_DRV_SOK) + { + result = EDMA3_DRV_requestChannel (hEdma, &chId, &tcc, + (EDMA3_RM_EventQueue)0, + NULL, NULL); + + result = EDMA3_DRV_getAllocatedPARAMId(hEdma, chId, &paRAMId); + if(result == EDMA3_DRV_SOK) + { + printf("\nReserved Channel ID Test\n"); + printf ("The Requested Channel ID: %d \nThe allocated PARAM Id:%d\n", (int)chId, (int)paRAMId); + + if (chId == paRAMId) + { + printf("The Requested Param ID is allocated for the given Channel\n"); + } + else + { + printf("The Requested Param ID is not allocated as same as the DMA channel\n"); + result = EDMA3_DATA_MISMATCH_ERROR; + } + printf("\n"); + } + } + + if (result == EDMA3_DRV_SOK) + { + result = EDMA3_DRV_setSrcParams (hEdma, chId, (uint32_t)(srcBuff1), + EDMA3_DRV_ADDR_MODE_INCR, + EDMA3_DRV_W8BIT); + } + + if (result == EDMA3_DRV_SOK) + { + result = EDMA3_DRV_setDestParams (hEdma, chId, (uint32_t)(dstBuff1), + EDMA3_DRV_ADDR_MODE_INCR, + EDMA3_DRV_W8BIT); + } + + if (result == EDMA3_DRV_SOK) + { + result = EDMA3_DRV_setSrcIndex (hEdma, chId, srcbidx, srccidx); + } + + if (result == EDMA3_DRV_SOK) + { + result = EDMA3_DRV_setDestIndex (hEdma, chId, desbidx, descidx); + } + + if (result == EDMA3_DRV_SOK) + { + if (syncType == EDMA3_DRV_SYNC_A) + { + result = EDMA3_DRV_setTransferParams (hEdma, chId, acnt, bcnt, ccnt, + BRCnt, EDMA3_DRV_SYNC_A); + } + else + { + result = EDMA3_DRV_setTransferParams (hEdma, chId, acnt, bcnt, ccnt, + BRCnt, EDMA3_DRV_SYNC_AB); + } + } + + if (result == EDMA3_DRV_SOK) + { + result = EDMA3_DRV_setOptField (hEdma, chId, + EDMA3_DRV_OPT_FIELD_TCINTEN, 1u); + } + + if (result == EDMA3_DRV_SOK) + { + result = EDMA3_DRV_setOptField (hEdma, chId, + EDMA3_DRV_OPT_FIELD_ITCINTEN, 1u); + } + + /* + * Since the transfer is going to happen in Manual mode of EDMA3 + * operation, we have to 'Enable the Transfer' multiple times. + * Number of times depends upon the Mode (A/AB Sync) + * and the different counts. + */ + if (result == EDMA3_DRV_SOK) + { + /*Need to activate next param*/ + if (syncType == EDMA3_DRV_SYNC_A) + { + numenabled = bcnt * ccnt; + } + else + { + /* AB Sync Transfer Mode */ + numenabled = ccnt; + } + + + for (i = 0; i < numenabled; i++) + { + /* + * Now enable the transfer as many times as calculated above. + */ + result = EDMA3_DRV_enableTransfer (hEdma, chId, + EDMA3_DRV_TRIG_MODE_MANUAL); + if (result != EDMA3_DRV_SOK) + { +#ifdef EDMA3_DRV_DEBUG + EDMA3_DRV_PRINTF ("edma3_test_user_req_paRAMId: EDMA3_DRV_enableTransfer " \ + "Failed, error code: %d\r\n", result); +#endif /* EDMA3_DRV_DEBUG */ + break; + } + + + /* Wait for the Completion Bit to be SET in the IPR/IPRH register. */ + result = EDMA3_DRV_waitAndClearTcc (hEdma, tcc); + if (result != EDMA3_DRV_SOK) + { +#ifdef EDMA3_DRV_DEBUG + EDMA3_DRV_PRINTF ("edma3_test_user_req_paRAMId: EDMA3_DRV_waitAndClearTcc " \ + "Failed, error code: %d\r\n", result); +#endif /* EDMA3_DRV_DEBUG */ + break; + } + } + } + + + /* Match the Source and Destination Buffers. */ + if (EDMA3_DRV_SOK == result) + { + for (i = 0; i < (acnt*bcnt*ccnt); i++) + { + if (srcBuff1[i] != dstBuff1[i]) + { + Istestpassed = 0u; +#ifdef EDMA3_DRV_DEBUG + EDMA3_DRV_PRINTF("edma3_test_user_req_paRAMId: Data write-read matching" \ + "FAILED at i = %d\r\n", i); +#endif /* EDMA3_DRV_DEBUG */ + break; + } + } + if (i == (acnt*bcnt*ccnt)) + { + Istestpassed = 1u; + } + + + /* Free the previously allocated channel. */ + result = EDMA3_DRV_freeChannel (hEdma, chId); + if (result != EDMA3_DRV_SOK) + { +#ifdef EDMA3_DRV_DEBUG + EDMA3_DRV_PRINTF("edma3_test_user_req_paRAMId: EDMA3_DRV_freeChannel() FAILED, " \ + "error code: %d\r\n", result); +#endif /* EDMA3_DRV_DEBUG */ + } + } + + + if(Istestpassed == 1u) + { +#ifdef EDMA3_DRV_DEBUG + EDMA3_DRV_PRINTF("edma3_test_user_req_paRAMId PASSED\r\n"); +#endif /* EDMA3_DRV_DEBUG */ + } + else + { +#ifdef EDMA3_DRV_DEBUG + EDMA3_DRV_PRINTF("edma3_test_user_req_paRAMId FAILED\r\n"); +#endif /* EDMA3_DRV_DEBUG */ + result = ((EDMA3_DRV_SOK == result) ? + EDMA3_DATA_MISMATCH_ERROR : result); + } + return result; +}