keystone-rtos/edma3_lld.git
9 years agoUpdated webgen makefile
Prasad Konnur [Wed, 16 Nov 2011 07:06:42 +0000 (12:36 +0530)]
Updated webgen makefile

9 years agoDocumentation changes for release 02.11.03.01
Prasad Konnur [Wed, 16 Nov 2011 06:57:55 +0000 (12:27 +0530)]
Documentation changes for release 02.11.03.01

9 years agoxdc compatibility key and eclipse folder updated for EDMA version 02.11.03.01
Prasad Konnur [Tue, 15 Nov 2011 09:26:01 +0000 (14:56 +0530)]
xdc compatibility key and eclipse folder updated for EDMA version 02.11.03.01

9 years agoRenamed Examples folder of Centaurus A8
Prasad Konnur [Mon, 14 Nov 2011 13:56:49 +0000 (19:26 +0530)]
Renamed Examples folder of Centaurus A8

9 years agoAdded Netra A8 Support
Prasad Konnur [Thu, 10 Nov 2011 14:57:55 +0000 (20:27 +0530)]
Added Netra A8 Support

9 years agoSingle cfg file for Netra and Centaurus in drv sample
Prasad Konnur [Thu, 10 Nov 2011 14:54:46 +0000 (20:24 +0530)]
Single cfg file for Netra and Centaurus in drv sample

9 years agoFixed possible thread safety issues
Prasad Konnur [Thu, 10 Nov 2011 13:55:36 +0000 (19:25 +0530)]
Fixed possible thread safety issues

10 years agoUpdated CCS project files for M3 Netra
prasad [Mon, 17 Oct 2011 08:07:18 +0000 (13:37 +0530)]
Updated CCS project files for M3 Netra

Examples folder for M3 Netra Renamed evmTI816x_ARM -> evmTI816x_M3

10 years agoCCS Project added to build the examples for M3 Centaurus
prasad [Fri, 14 Oct 2011 14:37:24 +0000 (20:07 +0530)]
CCS Project added to build the examples for M3 Centaurus

10 years agoAddition of M3 support for Centaurus
prasad [Fri, 14 Oct 2011 12:09:39 +0000 (17:39 +0530)]
Addition of M3 support for Centaurus

Added cfg files, makefiles and examples build using makefile

10 years agoAdded Webgen makefile to publish in the release webpage
Prasad Konnur [Mon, 10 Oct 2011 08:39:58 +0000 (14:09 +0530)]
Added Webgen makefile to publish in the release webpage

10 years agoUpdated Makefile to build for specific platform and Target, For libs and Examples
Prasad Konnur [Tue, 4 Oct 2011 14:10:26 +0000 (19:40 +0530)]
Updated Makefile to build for specific platform and Target, For libs and Examples

To build for all TARGETS supported by a PLATFORM provide only PLATFORM from command line
To build for a Specific target of a platform provide both PLATFORM and TARGET
If both are not specified it will build for all platform and targets supported.

Could be combined with libs, examples and clean makefile targets

Signed-off-by: Prasad Konnur <prasad.konnur@ti.com>
10 years agoUpdated package.xs to search library based on device name
Prasad Konnur [Wed, 21 Sep 2011 11:24:19 +0000 (16:54 +0530)]
Updated package.xs to search library based on device name

getlibs() function of xdc is edited to pick libraries based on device name insted of platform name.
For custom boards platform name is user defined.
Could not differentiate between Netra EVM and SIM libraries and SAIm libraries are never returned.

Signed-off-by: Prasad Konnur <prasad.konnur@ti.com>
10 years agoFix for IR SDOCM00084073
Prasad Konnur [Mon, 19 Sep 2011 14:50:10 +0000 (20:20 +0530)]
Fix for IR SDOCM00084073

Signed-off-by: Prasad Konnur <prasad.konnur@ti.com>
10 years agoDocumentation changes for version 02.11.02.04 DEV_EDMA3_LLD_02_11_02_04
Prasad Konnur [Wed, 8 Jun 2011 06:23:42 +0000 (11:53 +0530)]
Documentation changes for version 02.11.02.04

10 years agoUpdated eclipse folder for new version
Prasad Konnur [Thu, 9 Jun 2011 11:50:26 +0000 (17:20 +0530)]
Updated eclipse folder for new version

10 years agoFix Error in using EDMA as XDC package
Prasad Konnur [Tue, 7 Jun 2011 08:32:21 +0000 (14:02 +0530)]
Fix Error in using EDMA as XDC package

10 years agoFix for GENERIC defined for all release builds
Prasad Konnur [Tue, 7 Jun 2011 05:57:47 +0000 (11:27 +0530)]
Fix for GENERIC defined for all release builds

10 years agoDocuments updated with IRs implimented for 02.11.02.03 DEV_EDMA3_LLD_02_11_02_03
Prasad Konnur [Wed, 25 May 2011 06:22:11 +0000 (11:52 +0530)]
Documents updated with IRs implimented for 02.11.02.03

10 years agoAdding samples DEV_EDMA3_LLD_02_11_02_03_RC04
Jesse Villarreal [Tue, 24 May 2011 06:25:09 +0000 (11:55 +0530)]
Adding samples

10 years agoMacro.ini for out of box build
unknown [Thu, 19 May 2011 23:55:59 +0000 (19:55 -0400)]
Macro.ini for out of box build

10 years agoFixed bugs SDOCM00080618 and SDOCM00080034
Prasad Konnur [Thu, 19 May 2011 14:54:37 +0000 (20:24 +0530)]
Fixed bugs SDOCM00080618 and SDOCM00080034

10 years agoSupport of OMAP Tesla platform DEV_EDMA3_LLD_02_11_02_03_RC03
Villarreal Jesse [Thu, 19 May 2011 12:22:40 +0000 (17:52 +0530)]
Support of OMAP Tesla platform

10 years agoDocumentation changes for 02.11.02.03 DEV_EDMA3_LLD_02_11_02_03_RC01
Prasad Konnur [Tue, 17 May 2011 14:16:51 +0000 (19:46 +0530)]
Documentation changes for 02.11.02.03

10 years agomakefile related changes for support of M3
U-ENT\x0153534 [Wed, 6 Apr 2011 14:02:07 +0000 (19:32 +0530)]
makefile related changes for support of M3

10 years agoconfig files and examples added for supporting m3 video/vpss of netra
U-ENT\x0153534 [Wed, 6 Apr 2011 13:35:08 +0000 (19:05 +0530)]
config files and examples added for supporting m3 video/vpss of netra

10 years agoxdc compatibility key updated
U-ENT\x0153534 [Wed, 6 Apr 2011 11:09:30 +0000 (16:39 +0530)]
xdc compatibility key updated

10 years agoPatch II to add additional project files for CCSv5 project support for C66x examples
Raghu Nambiath [Sun, 15 May 2011 21:55:28 +0000 (17:55 -0400)]
Patch II to add additional project files for CCSv5 project support for C66x examples

10 years agoProject changes to resolve build issues.
unknown [Sun, 15 May 2011 20:04:55 +0000 (16:04 -0400)]
Project changes to resolve build issues.

10 years agoUpdated EDMA3 Driver version to 02.11.01.02 DEV_EDMA3_LLD_02_11_01_02
Raghu Nambiath [Tue, 15 Feb 2011 22:23:59 +0000 (17:23 -0500)]
Updated EDMA3 Driver version to 02.11.01.02

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoUpdated the Documentation for the release 02.11.01.02 DEV_EDMA3_LLD_02_11_01_02_RC02
Raghu Nambiath [Tue, 15 Feb 2011 12:18:47 +0000 (17:48 +0530)]
Updated the Documentation for the release 02.11.01.02

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoUpdated makefile to build C66x targets only with ELF DEV_EDMA3_LLD_02_11_01_02_RC01
Raghu Nambiath [Tue, 15 Feb 2011 01:10:22 +0000 (20:10 -0500)]
Updated makefile to build C66x targets only with ELF

- This is required if 7.0.x CGTOOL chain is used.
- Older CGTOOL 7.0.x tool chain for COFF does not support C66x target

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoUpdated the env.mk and the release batch file for release 02.11.01.02
Sundaram Raju [Mon, 14 Feb 2011 18:15:09 +0000 (23:45 +0530)]
Updated the env.mk and the release batch file for release 02.11.01.02

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoUpdated the Doxygen generated help files for the release 02.11.01.02
Sundaram Raju [Mon, 14 Feb 2011 13:08:15 +0000 (18:38 +0530)]
Updated the Doxygen generated help files for the release 02.11.01.02

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoUpdated the Doxygen cfg files for release 02.11.01.02
Sundaram Raju [Mon, 14 Feb 2011 13:07:24 +0000 (18:37 +0530)]
Updated the Doxygen cfg files for release 02.11.01.02

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoUpdated the release batch file to rename config.bld file
Sundaram Raju [Mon, 14 Feb 2011 09:43:02 +0000 (15:13 +0530)]
Updated the release batch file to rename config.bld file

- This removed buildforge dependancy on renaming the file

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoFix for bugs because of which generic RM library was not pulled for C64P targets
Sundaram Raju [Fri, 11 Feb 2011 12:32:54 +0000 (18:02 +0530)]
Fix for bugs because of which generic RM library was not pulled for C64P targets

- Refer IR# SDOCM00078797 for more details.
- for ISA c64p, library extensions that need to be generated are "64P"
- same way in getlibs() one has to check for "64P" to pull correct c64p libraries
- "-DGENERIC" flag has to be passed while building Generic RM library

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoFix for IR# SDOCM00078808 - EDMA LLD example fails for multi core run for TCI6486...
Raghu Nambiath [Fri, 11 Feb 2011 02:52:48 +0000 (21:52 -0500)]
Fix for IR# SDOCM00078808 - EDMA LLD example fails for multi core run for TCI6486 target

10 years agoUpdated the tools used for building the package in env.mk
Raghu Nambiath [Tue, 8 Feb 2011 02:25:35 +0000 (21:25 -0500)]
Updated the tools used for building the package in env.mk

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoAdded new top level makefile for the build of C66x platforms only
Raghu Nambiath [Mon, 14 Feb 2011 12:15:20 +0000 (17:45 +0530)]
Added new top level makefile for the build of C66x platforms only

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoUpdated XDC version and Compatibility key for the release 02.11.01.02
Raghu Nambiath [Mon, 14 Feb 2011 12:13:40 +0000 (17:43 +0530)]
Updated XDC version and Compatibility key for the release 02.11.01.02

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoC99 type modification
Raghu Nambiath [Mon, 14 Feb 2011 12:08:45 +0000 (17:38 +0530)]
C99 type modification

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoFix for multi-core execution of examples.
Raghu Nambiath [Mon, 14 Feb 2011 12:04:00 +0000 (17:34 +0530)]
Fix for multi-core execution of examples.

- Address would need to be global for EDMA transfer
- Testing version querry API added in the EDMA DRV module
- Adding of code to test default RM configuration

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoRemoved XDC and BIOS dependancy for DRV and RM module builds
Raghu Nambiath [Mon, 14 Feb 2011 11:23:19 +0000 (16:53 +0530)]
Removed XDC and BIOS dependancy for DRV and RM module builds

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoAdded support to Ny-Sh EVMs and Simulators.
Raghu Nambiath [Mon, 14 Feb 2011 11:15:05 +0000 (16:45 +0530)]
Added support to Ny-Sh EVMs and Simulators.

- Also removed the old Ny simulator TCI6498

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoUpdated Documentation for the release 02.11.00.01 DEV_EDMA3_LLD_02_11_00_01 DEV_EDMA3_LLD_02_11_00_01_RC05
Sundaram Raju [Wed, 2 Feb 2011 18:46:56 +0000 (00:16 +0530)]
Updated Documentation for the release 02.11.00.01

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoCommenting out the build of C66x generic RM library DEV_EDMA3_LLD_02_11_00_01_RC04
Sundaram Raju [Wed, 2 Feb 2011 11:04:34 +0000 (16:34 +0530)]
Commenting out the build of C66x generic RM library

- This support will properly be added in the next release of LLD

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoCommenting out the build of evmOMAPL138_ARM example from default build as it fails
Sundaram Raju [Sat, 29 Jan 2011 12:20:06 +0000 (17:50 +0530)]
Commenting out the build of evmOMAPL138_ARM example from default build as it fails

- Fix required in makerules of ARM-9

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoAllowing Cache invalidation for all buffers assuming they might be in DDR
Sundaram Raju [Tue, 1 Feb 2011 08:33:32 +0000 (14:03 +0530)]
Allowing Cache invalidation for all buffers assuming they might be in DDR

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoFixed bugs in the rules_*.mk files of Cortex A8 and ARM-9
Sundaram Raju [Fri, 28 Jan 2011 14:20:27 +0000 (19:50 +0530)]
Fixed bugs in the rules_*.mk files of Cortex A8 and ARM-9

- added the necessary compile & link flags for Sample applications

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoUpdated the Doxygen generated help files for the release 02.11.00.01
Sundaram Raju [Fri, 28 Jan 2011 13:34:34 +0000 (19:04 +0530)]
Updated the Doxygen generated help files for the release 02.11.00.01

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoUpdated the Doxygen cfg file for release 02.11.00.01
Sundaram Raju [Fri, 28 Jan 2011 13:23:12 +0000 (18:53 +0530)]
Updated the Doxygen cfg file for release 02.11.00.01

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoUpdated eclipse related files for the release 02.11.00.01
Sundaram Raju [Wed, 12 Jan 2011 15:33:23 +0000 (21:03 +0530)]
Updated eclipse related files for the release 02.11.00.01

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoUpdated XDC related files for release 02.11.00.01
Sundaram Raju [Sat, 29 Jan 2011 12:11:33 +0000 (17:41 +0530)]
Updated XDC related files for release 02.11.00.01

- changed the xdc compatibility key in the files
- added support for elf format in all platforms supported
- updated all package.bld files to fit new directory structure
- fixed many bugs (which never showed up) that were present earlier

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoModified the getlibs() to pick up the correct libraries in the new directory structure
Sundaram Raju [Thu, 27 Jan 2011 10:12:11 +0000 (15:42 +0530)]
Modified the getlibs() to pick up the correct libraries in the new directory structure

- The directory structure changed with the new make based build system
- The name of the libraries also changed
- The old extensions of the libraries are maintained

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoAdded a batch file that can be used for building of the LLD libraries
Sundaram Raju [Thu, 27 Jan 2011 13:07:26 +0000 (18:37 +0530)]
Added a batch file that can be used for building of the LLD libraries

- This is useful during a release and used by BuildForge project
- The batch file also generates XDC interface files required for the working of getlibs()
- It also removes unwanted XDC meta files that have build machine's local paths

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoUpdated evmOMAPL138_ARM example's Makefile to use ARM9 variables
Sundaram Raju [Wed, 2 Feb 2011 08:40:21 +0000 (14:10 +0530)]
Updated evmOMAPL138_ARM example's Makefile to use ARM9 variables

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoModified (DRV/RM) Sample libraries's Makefile to add specific flag for TI814X
Sundaram Raju [Fri, 28 Jan 2011 14:16:31 +0000 (19:46 +0530)]
Modified (DRV/RM) Sample libraries's Makefile to add specific flag for TI814X

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoFixed bug in Makefiles and made correct source files to be picked for compilation...
Sundaram Raju [Thu, 27 Jan 2011 13:26:10 +0000 (18:56 +0530)]
Fixed bug in Makefiles and made correct source files to be picked for compilation based on CORE

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoUpdated Top level Makefile and component.mk
Sundaram Raju [Wed, 2 Feb 2011 09:33:51 +0000 (15:03 +0530)]
Updated Top level Makefile and component.mk

- Added the ARM examples into default build
- Made build of ARM libraries and examples conditional to ELF format
- Added Generic RM libraries to default build

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoAdded support for Cortex A8 on evmTI814x
Sundaram Raju [Wed, 2 Feb 2011 08:45:17 +0000 (14:15 +0530)]
Added support for Cortex A8 on evmTI814x

- Added configuration for Cortex A8 on both DRV and RM Sample libraries
- Added example sample application evmTI814x_ARM

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoChanged evmTI814x example to older ccsv4 project version to suit makefile structure
Sundaram Raju [Wed, 2 Feb 2011 08:43:06 +0000 (14:13 +0530)]
Changed evmTI814x example to older ccsv4 project version to suit makefile structure

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoUpdated Makerules
Sundaram Raju [Wed, 2 Feb 2011 09:31:07 +0000 (15:01 +0530)]
Updated Makerules

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoAdded makefile for all examples and modified cfg file to remove loadpackage()
Sundaram Raju [Tue, 11 Jan 2011 14:37:53 +0000 (20:07 +0530)]
Added makefile for all examples and modified cfg file to remove loadpackage()

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoAdded makefile for each component and the top level makefile
Sundaram Raju [Tue, 11 Jan 2011 14:06:53 +0000 (19:36 +0530)]
Added makefile for each component and the top level makefile

Also added the component.mk file

Signed-off-by: Sundaram Raju <sundaram@ti.com>
10 years agoAdded makerules
Sundaram Raju [Tue, 11 Jan 2011 14:02:22 +0000 (19:32 +0530)]
Added makerules

Signed-off-by: Sundaram Raju <sundaram@ti.com>
11 years agoUpdated the Configuration for Tomahawk in RM only DEV_EDMA3_LLD_02_10_04_01
Sundaram Raju [Thu, 14 Oct 2010 06:14:37 +0000 (11:44 +0530)]
Updated the Configuration for Tomahawk in RM only

Signed-off-by: Sundaram Raju <sundaram@ti.com>
11 years agoUpdated Documents for the release 02.10.04.01
Sundaram Raju [Tue, 12 Oct 2010 07:18:37 +0000 (12:48 +0530)]
Updated Documents for the release 02.10.04.01

Signed-off-by: Sundaram Raju <sundaram@ti.com>
11 years agoModified XDC related files for the release 02.10.04.01
Sundaram Raju [Mon, 11 Oct 2010 09:50:48 +0000 (15:20 +0530)]
Modified XDC related files for the release 02.10.04.01

Signed-off-by: Sundaram Raju <sundaram@ti.com>
11 years agoAdded ELF support for C66x (both LE and BE) in the Generic library of RM
Sundaram Raju [Mon, 11 Oct 2010 09:48:53 +0000 (15:18 +0530)]
Added ELF support for C66x (both LE and BE) in the Generic library of RM

- Had to make some changes in XDC files to accomadate
  C66x in Generic and not in the platform specific libraries

Signed-off-by: Sundaram Raju <sundaram@ti.com>
11 years agoFix for the bug in Generic platform library in RM
Sundaram Raju [Tue, 5 Oct 2010 10:42:58 +0000 (16:12 +0530)]
Fix for the bug in Generic platform library in RM

- Refer to IR# SDOCM00074466 for more details

Signed-off-by: Sundaram Raju <sundaram@ti.com>
11 years agoUpdated Documents for the release 02.10.03.04 DEV_EDMA3_LLD_02_10_03_04
Sundaram Raju [Tue, 7 Sep 2010 18:33:47 +0000 (00:03 +0530)]
Updated Documents for the release 02.10.03.04

Signed-off-by: Sundaram Raju <sundaram@ti.com>
11 years agoModified the build related (XDC) files for adding support to TI814X
Sundaram Raju [Tue, 7 Sep 2010 12:00:55 +0000 (17:30 +0530)]
Modified the build related (XDC) files for adding support to TI814X

Signed-off-by: Sundaram Raju <sundaram@ti.com>
11 years agoAdded source files and example application project for supporting TI814X
Vinay K Nooji [Mon, 6 Sep 2010 12:48:55 +0000 (18:18 +0530)]
Added source files and example application project for supporting TI814X

Signed-off-by: Vinay K Nooji <x0101786@ti.com>
11 years agoAdding support for the Cross-bar in TI814X
Vinay K Nooji [Tue, 7 Sep 2010 11:10:50 +0000 (16:40 +0530)]
Adding support for the Cross-bar in TI814X

- Modified the DRV and RM source files for adding support for cross bar mapped events.

Signed-off-by: Sundaram Raju <sundaram@ti.com>
11 years agoChanged from 'ipc' module to 'knl' module in .cfg file of all example projects
Sundaram Raju [Tue, 7 Sep 2010 09:53:30 +0000 (15:23 +0530)]
Changed from 'ipc' module to 'knl' module in .cfg file of all example projects

Signed-off-by: Sundaram Raju <sundaram@ti.com>
11 years agoChanged from 'ipc' module to 'knl' module in all source files
Sundaram Raju [Tue, 7 Sep 2010 09:17:40 +0000 (14:47 +0530)]
Changed from 'ipc' module to 'knl' module in all source files

- due to the change in DSP/BIOS

Signed-off-by: Sundaram Raju <sundaram@ti.com>
11 years agoFix for BIOS.6.30.02.42 ECM issue
Sundaram Raju [Tue, 7 Sep 2010 07:22:26 +0000 (12:52 +0530)]
Fix for BIOS.6.30.02.42 ECM issue

- where the timer uses EVENT 7 instead of 14

Signed-off-by: Sundaram Raju <sundaram@ti.com>
11 years agoChanged memory location of ping pong buffers from EXT_RAM to DDR3_RAM
Sundaram Raju [Tue, 7 Sep 2010 07:19:29 +0000 (12:49 +0530)]
Changed memory location of ping pong buffers from EXT_RAM to DDR3_RAM

Merge on top of
c68ef - 2010-09-04 00:43:33 +0530 -Sundaram Raju - Changed DM740 --> TI816X

Signed-off-by: Sundaram Raju <sundaram@ti.com>
11 years agoFix for the platform TCI6498 moving from family c64p to c66 in DSP/BIOS.
Sundaram Raju [Sun, 5 Sep 2010 13:57:50 +0000 (19:27 +0530)]
Fix for the platform TCI6498 moving from family c64p to c66 in DSP/BIOS.

Signed-off-by: Sundaram Raju <sundaram@ti.com>
11 years agoAdded support for Netra EVM (evmTI816X).
Sundaram Raju [Sun, 5 Sep 2010 13:55:14 +0000 (19:25 +0530)]
Added support for Netra EVM (evmTI816X).

Signed-off-by: Sundaram Raju <sundaram@ti.com>
11 years agoAdd support for C6472 and TCI6486: update default RM configuration
Hongmei Gou [Fri, 3 Sep 2010 04:09:11 +0000 (09:39 +0530)]
Add support for C6472 and TCI6486: update default RM configuration

Signed-off-by: Hongmei Gou <h-gou@ti.com>
11 years agoChanged DM740 --> TI816X
Sundaram Raju [Fri, 3 Sep 2010 19:13:33 +0000 (00:43 +0530)]
Changed DM740 --> TI816X

Signed-off-by: Sundaram Raju <sundaram@ti.com>
11 years agoAdded new GENERIC platform for RM
Gunjan Dang [Tue, 17 Aug 2010 12:29:02 +0000 (17:59 +0530)]
Added new GENERIC platform for RM

- Added a new 'generic' platform in the Resource Manager library
that can be used for devices unsupported in the EDMA3 LLD

Signed-off-by: Sundaram Raju <sundaram@ti.com>
11 years agoAdd support for C6472 and TCI6486: tool version update for example projects
Hongmei Gou [Tue, 6 Jul 2010 22:14:19 +0000 (03:44 +0530)]
Add support for C6472 and TCI6486: tool version update for example projects

Signed-off-by: Hongmei Gou <h-gou@ti.com>
11 years agoAdd support for C6472 and TCI6486: build related files
Hongmei Gou [Mon, 14 Jun 2010 21:58:54 +0000 (03:28 +0530)]
Add support for C6472 and TCI6486: build related files

11 years agoAdd support for C6472 and TCI6486: source files
Hongmei Gou [Tue, 1 Jun 2010 19:44:26 +0000 (01:14 +0530)]
Add support for C6472 and TCI6486: source files

11 years agoFixed the CSL2_DAT_DEMO hang issue
Sundaram Raju [Mon, 28 Jun 2010 08:32:06 +0000 (14:02 +0530)]
Fixed the CSL2_DAT_DEMO hang issue

- Refer to IR# SDOCM00069906 for more details

Signed-off-by: Sundaram Raju <sundaram@ti.com>
11 years agoFixed the High Registers access bug in C6748/OMAPL138
Sundaram Raju [Mon, 28 Jun 2010 08:24:15 +0000 (13:54 +0530)]
Fixed the High Registers access bug in C6748/OMAPL138

- Refer to IR# SDOCM00071134 for more details

Signed-off-by: Sundaram Raju <sundaram@ti.com>
11 years agoFixed the bug that leads to assert when using allocAnyContigRes() function
Sundaram Raju [Fri, 28 May 2010 06:11:39 +0000 (11:41 +0530)]
Fixed the bug that leads to assert when using allocAnyContigRes() function

- When trying to request more contiguous resources than available assert is called
- Refer to IR# SDOCM00063765 for more details

Signed-off-by: Sundaram Raju <sundaram@ti.com>
11 years agoUpdated Documents (partial) for release edma3_lld_02_10_03_04 DEV_EDMA3_LLD_02_10_03_04_RC01
Sundaram Raju [Tue, 6 Jul 2010 07:45:31 +0000 (13:15 +0530)]
Updated Documents (partial) for release edma3_lld_02_10_03_04

Signed-off-by: Sundaram Raju <sundaram@ti.com>
11 years agoAdded Build related files to add support for Netra Simulator
Sundaram Raju [Mon, 5 Jul 2010 10:37:59 +0000 (16:07 +0530)]
Added Build related files to add support for Netra Simulator

Signed-off-by: Sundaram Raju <sundaram@ti.com>
11 years agoAdded source files to add support for Netra Simulator
Sundaram Raju [Mon, 5 Jul 2010 10:35:42 +0000 (16:05 +0530)]
Added source files to add support for Netra Simulator

Signed-off-by: Sundaram Raju <sundaram@ti.com>
11 years agoDocumentation changes DEV_EDMA3_LLD_02_10_02_03 DEV_EDMA3_LLD_02_10_02_03_RC04
Vinay K Nooji [Thu, 20 May 2010 08:59:09 +0000 (14:29 +0530)]
Documentation changes

Signed-off-by: Vinay K Nooji <x0101786@ti.com>
11 years agoAdd/Modify Build related files
Vinay K Nooji [Thu, 20 May 2010 08:57:37 +0000 (14:27 +0530)]
Add/Modify Build related files

Signed-off-by: Vinay K Nooji <x0101786@ti.com>
11 years agoAdded OMAPL138 ARM Support
Vinay K Nooji [Thu, 20 May 2010 08:49:32 +0000 (14:19 +0530)]
Added OMAPL138 ARM Support

Added/Modified source files

Signed-off-by: Vinay K Nooji <x0101786@ti.com>
11 years agoUpdated the data sheet for the memory usage statistics DEV.EDMA3.LLD.02.10.01.02_RC01 DEV_EDMA3_LLD_02_10_01_02
Imtiaz SMA [Mon, 12 Apr 2010 06:58:55 +0000 (12:28 +0530)]
Updated the data sheet for the memory usage statistics

Signed-off-by: Imtiaz SMA <imtiaz.syed@ti.com>
11 years agoreview comments fixed and test suite run on the code.
Imtiaz SMA [Mon, 12 Apr 2010 03:18:00 +0000 (08:48 +0530)]
review comments fixed and test suite run on the code.

Signed-off-by: Imtiaz SMA <imtiaz.syed@ti.com>
11 years agoSupport for the C6748 and OMAPL138 platforms.
Imtiaz SMA [Wed, 7 Apr 2010 10:16:33 +0000 (15:46 +0530)]
Support for the C6748 and OMAPL138 platforms.
This package only supports DSP and not ARM.
EDMA3 LLD changes after review comments FIX.

Signed-off-by: Imtiaz SMA <imtiaz.syed@ti.com>
11 years ago Updated Documents with PingPong buffer issue. DEV.EDMA3.LLD.02.10.00.01 EDMA3_LLD_BIOS6_02_10_00_01 EDMA3_LLD_BIOS6_02_10_00_01_RC04
Sundaram Raju [Mon, 7 Dec 2009 12:00:04 +0000 (17:30 +0530)]
Updated Documents with PingPong buffer issue.

PingPong Example is Failing for some EDMA Instances in some DSP cores
in Release mode only. It passes in Debug mode.
Refer IR# SDOCM00064758 for more details.