96c2e8c56d184b5e2f601f5bdf6fe626eabaf374
[keystone-rtos/fault_mgmt.git] / package.bld
1 /******************************************************************************
2  * FILE PURPOSE: Build description for the Fault Management
3  ******************************************************************************
4  * FILE NAME: package.bld
5  *
6  * DESCRIPTION: 
7  *  This file contains the build specification and description for the 
8  *  FM Library
9  *  
10  *  The file takes the following parameters from the command line through the
11  *  XDCARGS variable.
12  *      XDCARGS[0] = FM Install Type 
13  *      Valid Values are "TAR" or "SETUP"
14  *      DEFAULT is "SETUP"
15  *
16  *  Example for a valid command:
17  *      xdc XDCARGS="SETUP" release   
18  *
19  * Copyright (C) 2012-2015, Texas Instruments, Inc.
20  *****************************************************************************/
22 /* List of all subdirectories that combine to make the Fault Management Package. */
23 var subDirectories = ["src", "docs", "device", "include", "test", "util"];
25 /* Generate fault_mgmtlibver.h */
26 var tplt = xdc.loadTemplate("./fault_mgmtlibver.h.xdt");
27 tplt.genFile("./fault_mgmtlibver.h",lldReleaseVersion);   
29 /* Determine if we need to create the InstallJammer Application or not? 
30  * Fault Management Deliverables be either of the following formats:
31  *  - TAR Ball Package
32  *  - Setup Executable 
33  * DEFAULT is a TAR Executable. */
35 if ((arguments[0] != "TAR") && (arguments[0] != "SETUP"))
36     lldInstallType = "TAR";
37 else
38     lldInstallType = arguments[0];
40 /* Irrespective of the InstallType we always create a TAR Ball Package as a part
41  * of the RTSC Build. Here we determine the name of the TAR Ball Package
42  *  Format is as follows:
43  *      lld_<version> */
44 var lldRTSCFileName = "fault_mgmtlib" + "_" + lldPartNumber + "_" +
45                       lldReleaseVersion[0] + "_" +  lldReleaseVersion[1] + "_" + 
46                       lldReleaseVersion[2]  + "_" + lldReleaseVersion[3];
48 /******************************************************************
49  ************************ Release Banner **************************
50  ******************************************************************/
52 print ("************* Fault Management Library Build Information *************");
53 print ("Fault Management Lib Install : " + lldInstallType);
54 print ("Fault Management Lib Version : " + lldReleaseVersion);
55 print ("C66 Tools Directory          : " + c66ToolsBaseDir);
56 print ("RTSC File Name               : " + lldRTSCFileName);
57 print ("Fault Management Lib Path    : " + lldPath);
58 print ("Coverity Analysis            : " + (coverityAnalysis == "ON" ? "ON" : "OFF"));
59 print ("CC LE opts                   : " + C66LE.ccOpts.prefix);
60 print ("CC BE opts                   : " + C66BE.ccOpts.prefix);
61 print ("***********************************************************");
63 /* Create the release package for the Fault Management Library */
64 Pkg.defaultRelease = Pkg.addRelease (lldRTSCFileName, {prefix: "./packages/"});
66 /* Moving forward we need to set the Archiver of the package to be ZIP. This is currently
67  * not supported in the XDC tools being used. Currenly builds need to be done with the 
68  * following options:-
69  *   xdc MK_FIXLISTOPTS=-t release 
70  * ZIP is a better option as it works natively with INSTALL Jammer and we can remove the
71  * uncompression into a temporary directory. XDC Tools with xdc-rXX support the ZIP archiver. */
72 //Pkg.attrs = {archiver : "zip"};
74 /* Cycle through all the sub-directories and build all the files */
75 for (var i = 0; i < subDirectories.length; i++) 
76 {
77     /* Load the capsule in the sub directory. */
78     var caps = xdc.loadCapsule (subDirectories[i]+"/Module.xs");
80     print ("Building directory " + subDirectories[i]);
82     /* Build the capsule. */
83     caps.modBuild();
85     /* Package the module.xs files for building via package */
86     Pkg.otherFiles[Pkg.otherFiles.length++] = subDirectories[i]+"/Module.xs";
87 }
89 /* Package the remaining files */
90 Pkg.otherFiles[Pkg.otherFiles.length++] = "config.bld";
91 Pkg.otherFiles[Pkg.otherFiles.length++] = "package.bld";
92 Pkg.otherFiles[Pkg.otherFiles.length++] = "package.xdc";
93 Pkg.otherFiles[Pkg.otherFiles.length++] = "Settings.xdc";
94 Pkg.otherFiles[Pkg.otherFiles.length++] = "fault_mgmt.h";
95 Pkg.otherFiles[Pkg.otherFiles.length++] = "fault_mgmt_osal.h";
96 Pkg.otherFiles[Pkg.otherFiles.length++] = "fault_mgmtlibver.h";
97 Pkg.otherFiles[Pkg.otherFiles.length++] = "docs/Doxyfile";
98 Pkg.otherFiles[Pkg.otherFiles.length++] = "build/buildlib.xs";
99 Pkg.otherFiles[Pkg.otherFiles.length++] = "docs/ReleaseNotes_fault_mgmt.pdf";
100 Pkg.otherFiles[Pkg.otherFiles.length++] = "makefile";
102 /* Generate Users Manual Doxyfile */
103 var tplt = xdc.loadTemplate("./docs/doxyfile.xdt");
104 tplt.genFile("./docs/Doxyfile",lldReleaseVersion); 
106 /* Generate Settings.xdc */
107 var tplt = xdc.loadTemplate("./Settings.xdc.xdt");
108 tplt.genFile("./Settings.xdc",lldReleaseVersion); 
110 /* Check if we need to create the mini package? */
111 var miniBuild = java.lang.System.getenv("MINI_PACKAGE");
113 if (miniBuild == "ON")
115     /***************************************************************************
116      ********************************* MINI Package ****************************
117      ***************************************************************************/
118     /* Create the MINI RTSC Package */
119     var libUtility = xdc.loadCapsule ("build/buildlib.xs");
120     libUtility.createMiniPkg(lldRTSCFileName);
123 /********************************************************************* 
124  *********************** INSTALL-JAMMER Support **********************
125  * In order to create the InstallJammer Application; we need to UNTAR
126  * the package into a temporary directory. This is required because 
127  * currently the InstallJammer does not support the TAR Files and thus
128  * creating an UNTAR of the file. So to work-around the problem we will
129  * do the following in the EPILOGUE Section:-
130  *  (a) Create a temporary directory called 'tmp'
131  *  (b) UNTAR the package into 'tmp'
132  *  (c) Run the INSTALL Jammer on 'tmp'
133  *  (d) Remove the 'tmp' directory.
134  *
135  * This can be done only after the 'release' package has been created.
136  * Thus all of this work is being done in the EPILOGUE.
137  *********************************************************************/
138 if (lldInstallType == "SETUP")
140     /* Create the Install Jammer Version Variable. This is used inside the 
141      * MPI File to create the Final executable. 
142      *  The format supported is as follows:-
143      *   - setupwin32_fault_mgmtlib-<part_number>-<version>.exe 
144      *      This is for Fault Management Libraries and Header files
145      */
146     var InstallJammerVersion = "-DVersion " + lldPartNumber + "_" + lldReleaseVersion[0] + "_" +
147                                lldReleaseVersion[1] + "_" +  lldReleaseVersion[2]  + "_" + lldReleaseVersion[3];
149     /* This is the location where the tmp directory is located; this is used as 
150      * the input directory for the Install Jammer. */ 
151     var PackageBaseDir = " -DPackageBaseDir " + lldPath + "./tmp";
153     /* This is the location where the Fault Management will be installed by default. */
154     var WinInstallDir = " -DWinInstallDir C:/ti/fault_mgmtlib" + "_" + 
155                             lldPartNumber + "_" + 
156                             lldReleaseVersion[0] + "_" +  lldReleaseVersion[1] + "_" +  
157                             lldReleaseVersion[2]  + "_" + lldReleaseVersion[3];
159     /* Create the actual EPILOGUE Section for the INSTALLER */
160     Pkg.makeEpilogue += "release: install_application\n";
161     Pkg.makeEpilogue += "install_application:\n";
162     Pkg.makeEpilogue += "\t @echo -------------------------------------------------------\n";
163     Pkg.makeEpilogue += "\t @echo Creating the Install\n";
164     Pkg.makeEpilogue += "\t @echo -------------------------------------------------------\n";
165     Pkg.makeEpilogue += "\t -$(MKDIR) tmp\n";
166     Pkg.makeEpilogue += "\t -$(MKDIR) tmp/packages\n";
167     Pkg.makeEpilogue += "\t -$(MKDIR) tmp/eclipse\n";
168     Pkg.makeEpilogue += "\t -$(CP) -R eclipse tmp\n";
169     Pkg.makeEpilogue += "\t tar -xf ./packages/" + lldRTSCFileName + ".tar" + " -Ctmp/packages \n";
170     Pkg.makeEpilogue += "\t installjammer " + InstallJammerVersion + PackageBaseDir + WinInstallDir + 
171                         " --output-dir packages/ --build install/fault_mgmtlib.mpi\n";
172     Pkg.makeEpilogue += "\t -$(RMDIR) /S /Q tmp\n\n";
175 /* We need to clean after ourselves; extend the 'clean' target to take care of this. */
176 Pkg.makeEpilogue += "clean::\n";
177 Pkg.makeEpilogue += "\t -$(RM) docs/Doxyfile Settings.xdc fault_mgmtlibver.h\n";
178 Pkg.makeEpilogue += "\t -$(RM) makefile\n";
179 Pkg.makeEpilogue += "\t -$(RMDIR) docs/doxygen\n";
180 if (lldInstallType == "SETUP")
182     Pkg.makeEpilogue += "\t -$(RM) packages/*.exe\n";
183     Pkg.makeEpilogue += "\t -$(RM) packages/*.bin\n";
184     Pkg.makeEpilogue += "\t -$(RMDIR) eclipse\n\n";
186 if (miniBuild == "ON")
188     Pkg.makeEpilogue += "\t -$(RM) simpleC66LE.mak\n";
189     Pkg.makeEpilogue += "\t -$(RM) simpleC66BE.mak\n";