9 years agoAddressed SDOCM00107359 and partial SDOCM00108469 (minus compiler DEV.FFTC_LLD.02.02.00.03
Addressed SDOCM00107359 and partial SDOCM00108469 (minus compiler
upgrade) for debugging LLD with optimization (to get the call
stack).
upgrade) for debugging LLD with optimization (to get the call
stack).
Added correction for SDOCM00108333.
The API Fftc_getDeviceAccumulatorConfig()'s parameter pAccRxQNum
is now uint32_t * instead of uint16_t *.
The API Fftc_getDeviceAccumulatorConfig()'s parameter pAccRxQNum
is now uint32_t * instead of uint16_t *.
Made corrections for SDOCM00108271.
-The FFTC test cases for K2L didn't pass due to incorrect
eventId used for the accumulator channels chosen. Sprugr9f
was used as a reference, but it is incorrect. Version g
(sprugr9g) will contain the necessary corrections.
-Added System_exit() calls to complete execution of the
tests.
-The FFTC test cases for K2L didn't pass due to incorrect
eventId used for the accumulator channels chosen. Sprugr9f
was used as a reference, but it is incorrect. Version g
(sprugr9g) will contain the necessary corrections.
-Added System_exit() calls to complete execution of the
tests.
- Update of release notes for MCSDK 3.1.0.0 beta release.
- Additional changes related to the comparison of the code
to the documentation as was done for SDOCM00108143/144.
The eventIds needed corrections for queue numbers used in
the unit test code for K2K/K2H and K2L.
- changes made to the setupenv.bat file to bring it up to
the version numbers used in MCSDK 3.1.0.0 and also to
somewhat align it to other LLD setupenv.bat files.
to the documentation as was done for SDOCM00108143/144.
The eventIds needed corrections for queue numbers used in
the unit test code for K2K/K2H and K2L.
- changes made to the setupenv.bat file to bring it up to
the version numbers used in MCSDK 3.1.0.0 and also to
somewhat align it to other LLD setupenv.bat files.
Fix for SDOCM00108083 and SDOCM00108140.
FFTC power domain enabling for each instance is corrected for K2L
and added missing power domain enabling function call for K2K/K2H.
FFTC power domain enabling for each instance is corrected for K2L
and added missing power domain enabling function call for K2K/K2H.
Fix for SDOCM00108143. Accumulator RX queue number changed to 728
from 724 for K2L.
from 724 for K2L.
Fix for SDOCM00108144. Accumulator RX queue number changed to 728
from 724 for K2K/K2H.
from 724 for K2K/K2H.
Changes to the QMSS osal functions are made after the fix for
SDOCM00107127 was completed.
SDOCM00107127 was completed.
Fix for SDOCM00108083 implemented.
Update related to power domain with fixes during K2L EVM bringup verification
Merged latest changes 2.0.04 and 2.0.0.5 from master
Update
Fix for SDOCM00102292, FFTC driver not compatible with QMSS using RMv2
Testing limited to current unit test. For extended testing RM would need to be enabled to unit test and examples
Testing limited to current unit test. For extended testing RM would need to be enabled to unit test and examples
Update for version
Update for Nightly build failure to use Queue ID for second QMSS instance instead of Queue Number.
10 years agoUpdated paths. Newer version of XDC hangs the build during compilation. DEV.FFTC.02.02.00.00
Updated paths. Newer version of XDC hangs the build during compilation.
change FFTC_0 back to FFTC_A for compatbility with k2
add temp files to .gitignore
.gitignore to get rid of build files
Fix for SDOCM00098765
Removed incorrect device files
Support for Lamarr (TCI6630K2L) device
MCSDK 3.0: updated docs for Alpha-4
MCSDK 3.0: workaround to fix compilation issue for device specific CSL
MCSDK 3.0: device name change for Alpha-4
Commited by migration script
Commited by migration script
initial commit
initial commit