# File: fvid2_component.mk # This file is component include make file of FVID2 driver library. # List of variables set in this file and their purpose: # _RELPATH - This is the relative path of the module, typically from # top-level directory of the package # _PATH - This is the absolute path of the module. It derives from # absolute path of the top-level directory (set in env.mk) # and relative path set above # _INCLUDE - This is the path that has interface header files of the # module. This can be multiple directories (space separated) # _PKG_LIST - Names of the modules (and sub-modules) that are a part # part of this module, including itself. # _BOARD_DEPENDENCY - "yes": means the code for this module depends on # platform and the compiled obj/lib has to be kept # under directory # "no" or "" or if this variable is not defined: means # this module has no platform dependent code and hence # the obj/libs are not kept under dir. # _CORE_DEPENDENCY - "yes": means the code for this module depends on # core and the compiled obj/lib has to be kept # under directory # "no" or "" or if this variable is not defined: means # this module has no core dependent code and hence # the obj/libs are not kept under dir. # _APP_STAGE_FILES - List of source files that belongs to the module # , but that needs to be compiled at application # build stage (in the context of the app). This is # primarily for link time configurations or if the # source file is dependent on options/defines that are # application dependent. This can be left blank or # not defined at all, in which case, it means there # no source files in the module that are required # to be compiled in the application build stage. # ifeq ($(fvid2_component_make_include), ) fvid2_default_SOCLIST = j7 am65x fvid2_default_j7_CORELIST = mcu1_0 mcu1_1 fvid2_default_am65x_CORELIST = mcu1_0 mcu1_1 mpu1_0 ############################ # fvid2 package # List of components included under fvid2 lib # The components included here are built and will be part of fvid2 lib ############################ fvid2_LIB_LIST = fvid2 ############################ # fvid2 examples # List of examples under fvid2 (+= is used at each example definition) # All the tests mentioned in list are built when test target is called # List below all examples for allowed values ############################ fvid2_EXAMPLE_LIST = # # FVID2 Modules # # FVID2 library fvid2_COMP_LIST = fvid2 fvid2_RELPATH = ti/drv/fvid2 fvid2_PATH = $(PDK_FVID2_COMP_PATH) fvid2_LIBNAME = fvid2 fvid2_LIBPATH = $(PDK_FVID2_COMP_PATH)/lib fvid2_MAKEFILE = -fsrc/makefile export fvid2_MAKEFILE export fvid2_LIBNAME export fvid2_LIBPATH fvid2_BOARD_DEPENDENCY = no fvid2_CORE_DEPENDENCY = no export fvid2_COMP_LIST export fvid2_BOARD_DEPENDENCY export fvid2_CORE_DEPENDENCY fvid2_PKG_LIST = fvid2 fvid2_INCLUDE = $(fvid2_PATH) fvid2_SOCLIST = $(fvid2_default_SOCLIST) export fvid2_SOCLIST fvid2_$(SOC)_CORELIST = $(fvid2_default_$(SOC)_CORELIST) export fvid2_$(SOC)_CORELIST # # FVID2 Examples # export fvid2_LIB_LIST export fvid2_EXAMPLE_LIST FVID2_CFLAGS = # Enable asserts and prints FVID2_CFLAGS += -DFVID2_CFG_ASSERT_ENABLE #TODO: Enable for A53 after semi-hosting is enabled ifneq ($(CORE),$(filter $(CORE), mpu1_0 mpu1_1)) FVID2_CFLAGS += -DFVID2_CFG_USE_STD_ASSERT FVID2_CFLAGS += -DFVID2_CFG_PRINT_ENABLE endif export FVID2_CFLAGS fvid2_component_make_include := 1 endif