/* ============================================================================= * Copyright (c) Texas Instruments Incorporated 2012-2018 * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /** * \file fvid2_drvMgr.h * * \brief FVID2 driver manager header file. * * This file exposes internal functions of driver management functionality. * This is not used by application and is used by video drivers to register * itself to the FVID2. * */ #ifndef FVID2_DRVMGR_H_ #define FVID2_DRVMGR_H_ /* ========================================================================== */ /* Include Files */ /* ========================================================================== */ #include #ifdef __cplusplus extern "C" { #endif /* ========================================================================== */ /* Macros & Typedefs */ /* ========================================================================== */ /** \brief Number of driver object to allocate in FVID2 library. */ #define FVID2_CFG_FDM_NUM_DRV_OBJS (40U) /** \brief Number of channel object to allocate in FVID2 library. */ #define FVID2_CFG_FDM_NUM_CH_OBJS (80U) /** \brief FVID2 driver handle returned by individual drivers. */ typedef Ptr Fdrv_Handle; /** \brief Typedef for callback function parameters. */ typedef struct Fvid2_DrvCbParams_t Fvid2_DrvCbParams; /** * \brief Typedef for FVID2 driver callback function prototype. This will be * called by the driver and then the FVID2 driver manager will route the * callback to the application. * * fdmData: FVID2 driver manager internal data passed to driver during create * call. * * reserved: For future use. Not used currently. This will be set to NULL. */ typedef Int32 (*Fdm_CbFxn)(Ptr fdmData, Ptr reserved); /** * \brief Typedef for FVID2 driver error callback function prototype. * This will be called by the driver and then the FVID2 driver manager * will route the error callback to the application. * * fdmData: FVID2 driver manager internal data passed to driver during create * call. * * errList: Error data passed to the application. * * reserved: For future use. Not used currently. This will be set to NULL. */ typedef Int32 (*Fdm_ErrCbFxn)(Ptr fdmData, void *errList, Ptr reserved); /** \brief Typedef for FVID2 create function pointer. */ typedef Fdrv_Handle (*Fvid2_DrvCreate)(UInt32 drvId, UInt32 instanceId, Ptr createArgs, Ptr createStatusArgs, const Fvid2_DrvCbParams *fdmCbParams); /** \brief Typedef for FVID2 delete function pointer. */ typedef Int32 (*Fvid2_DrvDelete)(Fdrv_Handle handle, Ptr deleteArgs); /** \brief Typedef for FVID2 control function pointer. */ typedef Int32 (*Fvid2_DrvControl)(Fdrv_Handle handle, UInt32 cmd, Ptr cmdArgs, Ptr cmdStatusArgs); /** \brief Typedef for FVID2 queue function pointer. */ typedef Int32 (*Fvid2_DrvQueue)(Fdrv_Handle handle, Fvid2_FrameList *frameList, UInt32 streamId); /** \brief Typedef for FVID2 dequeue function pointer. */ typedef Int32 (*Fvid2_DrvDequeue)(Fdrv_Handle handle, Fvid2_FrameList *frameList, UInt32 streamId, UInt32 timeout); /** \brief Typedef for FVID2 process frames function pointer. */ typedef Int32 (*Fvid2_DrvProcessRequest)(Fdrv_Handle handle, Fvid2_FrameList *inProcessList, Fvid2_FrameList *outProcessList); /** \brief Typedef for FVID2 get processed frames function pointer. */ typedef Int32 (*Fvid2_DrvGetProcessedRequest)(Fdrv_Handle handle, Fvid2_FrameList *inProcessList, Fvid2_FrameList *outProcessList, UInt32 timeout); /* ========================================================================== */ /* Structure Declarations */ /* ========================================================================== */ /** * struct Fvid2_DrvCbParams_t * \brief Structure for setting callback function parameters. */ struct Fvid2_DrvCbParams_t { Fdm_CbFxn fdmCbFxn; /**< FDM callback function used by the driver to initimate any * operation has completed or not. */ Fdm_ErrCbFxn fdmErrCbFxn; /**< FDM error callback function used by the driver to initimate * any error occuring at the time of streaming. */ Fvid2_Handle handle; /**< FDM layer FVID2 handle. This can be used by the actual driver to call * application callback with proper FVID2 handle instead of routining * the call through FDM layer. */ void *errList; /**< Pointer to a valid framelist or processlist where the driver * copies the aborted/error packet. */ Ptr fdmData; /**< FDM specific data which is returned in the callback function * as it is. */ Ptr reserved; /**< For future use. Not used currently. Set this to NULL. */ }; /** * struct Fvid2_DrvOps * \brief Structure to store driver function pointers. */ typedef struct { UInt32 drvId; /**< Unique driver Id. */ Fvid2_DrvCreate createFxn; /**< FVID2 create function pointer. */ Fvid2_DrvDelete deleteFxn; /**< FVID2 delete function pointer. */ Fvid2_DrvControl controlFxn; /**< FVID2 control function pointer. */ Fvid2_DrvQueue queueFxn; /**< FVID2 queue function pointer. */ Fvid2_DrvDequeue dequeueFxn; /**< FVID2 dequeue function pointer. */ Fvid2_DrvProcessRequest processRequestFxn; /**< FVID2 process request function pointer. */ Fvid2_DrvGetProcessedRequest getProcessedRequestFxn; /**< FVID2 get processed request function pointer. */ } Fvid2_DrvOps; /* ========================================================================== */ /* Function Declarations */ /* ========================================================================== */ /** * Fvid2_registerDriver * \brief FVID2 register driver function. * * This function registers a driver with the FVID2 driver manager. * * \param drvOps Driver function table pointer containing driver * function pointers and driver name. The driver name * should be unique - two or more drivers can't have the * same driver name. * * \return Returns 0 on success else returns error value. */ Int32 Fvid2_registerDriver(const Fvid2_DrvOps *drvOps); /** * Fvid2_unRegisterDriver * \brief FVID2 unregister driver function. * * This function unregisters a driver from the FVID2 driver manager. * * \param drvOps Driver function table pointer containing driver * function pointers and driver name. * * \return Returns 0 on success else returns error value. */ Int32 Fvid2_unRegisterDriver(const Fvid2_DrvOps *drvOps); /** * Fvid2_checkFrameList * \brief Checks the FVID2 frame list for error and returns appropriate error. * * This is used by the drivers and not by the application. * * \param frameList Pointer to frame list to check for errors. * \param maxFrames Max frames to be checked against numFrames member * in frame list. * * \return Returns 0 on success else returns error value. */ Int32 Fvid2_checkFrameList(const Fvid2_FrameList *frameList, UInt32 maxFrames); /** * Fvid2_checkDqFrameList * \brief Checks the FVID2 frame list of dequeue call for error and returns * appropriate error. For dequeue operation, the frame pointers in the frames * should not be checked as this will be filled by the driver. * * This is used by the drivers and not by the application. * * \param frameList Pointer to frame list to check for errors. * \param maxFrames Max frames to be checked against numFrames member * in frame list. * * \return Returns 0 on success else returns error value. */ Int32 Fvid2_checkDqFrameList(const Fvid2_FrameList *frameList, UInt32 maxFrames); /** * Fvid2_copyFrameList * \brief Copies the source frame list to the destination frame list. * This also resets the frame pointers from the source frame list. * * This is used by the drivers and not by the application. * * \param dest Pointer to destination frame list. * \param src Pointer to source frame list. * * \return Returns 0 on success else returns error value. */ void Fvid2_copyFrameList(Fvid2_FrameList *dest, Fvid2_FrameList *src); /** * Fvid2_duplicateFrameList * \brief Duplicate the source frame list to the destination frame list. * This does not reset the frame pointers from the source frame list. * * This is used by the drivers and not by the application. * * \param dest Pointer to destination frame list. * \param src Pointer to source frame list. * * \return Returns 0 on success else returns error value. */ void Fvid2_duplicateFrameList(Fvid2_FrameList *dest, const Fvid2_FrameList *src); /** * \brief Fvid2_DrvOps structure init function. * * \param drvOps [IN] Pointer to #Fvid2_DrvOps structure. * */ static inline void Fvid2DrvOps_init(Fvid2_DrvOps *drvOps); /* ========================================================================== */ /* Static Function Definitions */ /* ========================================================================== */ static inline void Fvid2DrvOps_init(Fvid2_DrvOps *drvOps) { if (NULL != drvOps) { drvOps->drvId = 0U; drvOps->createFxn = NULL; drvOps->deleteFxn = NULL; drvOps->controlFxn = NULL; drvOps->queueFxn = NULL; drvOps->dequeueFxn = NULL; drvOps->processRequestFxn = NULL; drvOps->getProcessedRequestFxn = NULL; } return; } #ifdef __cplusplus } #endif #endif /* #ifndef FVID2_DRVMGR_H_ */