X-Git-Url: https://git.ti.com/gitweb?p=keystone-rtos%2Ffvid2.git;a=blobdiff_plain;f=include%2Ffvid2_drvMgr.h;h=0bf2cc86cd556ed1c43cdc3771b09d3676e3b795;hp=b49288c93305bc8e0f826f62b317500332baab5a;hb=bb79dfdc7a3095b0b3908d7204ee4f0d5d6c956c;hpb=43c54e1e3986ef555006091847e65bb9397717fa;ds=sidebyside diff --git a/include/fvid2_drvMgr.h b/include/fvid2_drvMgr.h index b49288c..0bf2cc8 100644 --- a/include/fvid2_drvMgr.h +++ b/include/fvid2_drvMgr.h @@ -1,5 +1,5 @@ -/* ============================================================================= - * Copyright (c) Texas Instruments Incorporated 2012-2018 +/* + * Copyright (c) Texas Instruments Incorporated 2018 * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions @@ -48,7 +48,7 @@ /* Include Files */ /* ========================================================================== */ -#include +#include #ifdef __cplusplus extern "C" { @@ -59,18 +59,16 @@ extern "C" { /* ========================================================================== */ /** \brief Number of driver object to allocate in FVID2 library. */ -#define FVID2_CFG_FDM_NUM_DRV_OBJS (40U) +#define FVID2_CFG_FDM_NUM_DRV_OBJS (40U) /** \brief Number of channel object to allocate in FVID2 library. */ -#define FVID2_CFG_FDM_NUM_CH_OBJS (80U) - - +#define FVID2_CFG_FDM_NUM_CH_OBJS (80U) /** \brief FVID2 driver handle returned by individual drivers. */ -typedef Ptr Fdrv_Handle; +typedef void *Fdrv_Handle; /** \brief Typedef for callback function parameters. */ -typedef struct Fvid2_DrvCbParams_t Fvid2_DrvCbParams; +typedef struct Fvid2_DrvCbParams_t Fvid2_DrvCbParams; /** * \brief Typedef for FVID2 driver callback function prototype. This will be @@ -79,10 +77,8 @@ typedef struct Fvid2_DrvCbParams_t Fvid2_DrvCbParams; * * fdmData: FVID2 driver manager internal data passed to driver during create * call. - * - * reserved: For future use. Not used currently. This will be set to NULL. */ -typedef Int32 (*Fdm_CbFxn)(Ptr fdmData, Ptr reserved); +typedef int32_t (*Fdm_CbFxn)(void *fdmData); /** * \brief Typedef for FVID2 driver error callback function prototype. @@ -94,48 +90,46 @@ typedef Int32 (*Fdm_CbFxn)(Ptr fdmData, Ptr reserved); * * errList: Error data passed to the application. * - * reserved: For future use. Not used currently. This will be set to NULL. */ -typedef Int32 (*Fdm_ErrCbFxn)(Ptr fdmData, void *errList, Ptr reserved); +typedef int32_t (*Fdm_ErrCbFxn)(void *fdmData, void *errList); /** \brief Typedef for FVID2 create function pointer. */ -typedef Fdrv_Handle (*Fvid2_DrvCreate)(UInt32 drvId, - UInt32 instanceId, - Ptr createArgs, - Ptr - createStatusArgs, +typedef Fdrv_Handle (*Fvid2_DrvCreate)(uint32_t drvId, + uint32_t instanceId, + void *createArgs, + void *createStatusArgs, const Fvid2_DrvCbParams *fdmCbParams); /** \brief Typedef for FVID2 delete function pointer. */ -typedef Int32 (*Fvid2_DrvDelete)(Fdrv_Handle handle, Ptr deleteArgs); +typedef int32_t (*Fvid2_DrvDelete)(Fdrv_Handle handle, void *deleteArgs); /** \brief Typedef for FVID2 control function pointer. */ -typedef Int32 (*Fvid2_DrvControl)(Fdrv_Handle handle, - UInt32 cmd, - Ptr cmdArgs, - Ptr cmdStatusArgs); +typedef int32_t (*Fvid2_DrvControl)(Fdrv_Handle handle, + uint32_t cmd, + void *cmdArgs, + void *cmdStatusArgs); /** \brief Typedef for FVID2 queue function pointer. */ -typedef Int32 (*Fvid2_DrvQueue)(Fdrv_Handle handle, - Fvid2_FrameList *frameList, - UInt32 streamId); +typedef int32_t (*Fvid2_DrvQueue)(Fdrv_Handle handle, + Fvid2_FrameList *frameList, + uint32_t streamId); /** \brief Typedef for FVID2 dequeue function pointer. */ -typedef Int32 (*Fvid2_DrvDequeue)(Fdrv_Handle handle, - Fvid2_FrameList *frameList, - UInt32 streamId, - UInt32 timeout); +typedef int32_t (*Fvid2_DrvDequeue)(Fdrv_Handle handle, + Fvid2_FrameList *frameList, + uint32_t streamId, + uint32_t timeout); /** \brief Typedef for FVID2 process frames function pointer. */ -typedef Int32 (*Fvid2_DrvProcessRequest)(Fdrv_Handle handle, - Fvid2_FrameList *inProcessList, - Fvid2_FrameList *outProcessList); +typedef int32_t (*Fvid2_DrvProcessRequest)(Fdrv_Handle handle, + Fvid2_FrameList *inProcessList, + Fvid2_FrameList *outProcessList); /** \brief Typedef for FVID2 get processed frames function pointer. */ -typedef Int32 (*Fvid2_DrvGetProcessedRequest)(Fdrv_Handle handle, - Fvid2_FrameList *inProcessList, - Fvid2_FrameList *outProcessList, - UInt32 timeout); +typedef int32_t (*Fvid2_DrvGetProcessedRequest)(Fdrv_Handle handle, + Fvid2_FrameList *inProcessList, + Fvid2_FrameList *outProcessList, + uint32_t timeout); /* ========================================================================== */ @@ -161,11 +155,9 @@ struct Fvid2_DrvCbParams_t void *errList; /**< Pointer to a valid framelist or processlist where the driver * copies the aborted/error packet. */ - Ptr fdmData; + void *fdmData; /**< FDM specific data which is returned in the callback function * as it is. */ - Ptr reserved; - /**< For future use. Not used currently. Set this to NULL. */ }; /** @@ -174,7 +166,7 @@ struct Fvid2_DrvCbParams_t */ typedef struct { - UInt32 drvId; + uint32_t drvId; /**< Unique driver Id. */ Fvid2_DrvCreate createFxn; /**< FVID2 create function pointer. */ @@ -209,7 +201,7 @@ typedef struct * * \return Returns 0 on success else returns error value. */ -Int32 Fvid2_registerDriver(const Fvid2_DrvOps *drvOps); +int32_t Fvid2_registerDriver(const Fvid2_DrvOps *drvOps); /** * Fvid2_unRegisterDriver @@ -222,7 +214,7 @@ Int32 Fvid2_registerDriver(const Fvid2_DrvOps *drvOps); * * \return Returns 0 on success else returns error value. */ -Int32 Fvid2_unRegisterDriver(const Fvid2_DrvOps *drvOps); +int32_t Fvid2_unRegisterDriver(const Fvid2_DrvOps *drvOps); /** * Fvid2_checkFrameList @@ -236,7 +228,8 @@ Int32 Fvid2_unRegisterDriver(const Fvid2_DrvOps *drvOps); * * \return Returns 0 on success else returns error value. */ -Int32 Fvid2_checkFrameList(const Fvid2_FrameList *frameList, UInt32 maxFrames); +int32_t Fvid2_checkFrameList(const Fvid2_FrameList *frameList, + uint32_t maxFrames); /** * Fvid2_checkDqFrameList @@ -252,8 +245,8 @@ Int32 Fvid2_checkFrameList(const Fvid2_FrameList *frameList, UInt32 maxFrames); * * \return Returns 0 on success else returns error value. */ -Int32 Fvid2_checkDqFrameList(const Fvid2_FrameList *frameList, - UInt32 maxFrames); +int32_t Fvid2_checkDqFrameList(const Fvid2_FrameList *frameList, + uint32_t maxFrames); /** * Fvid2_copyFrameList