Added an optional second ibl config area to the i2c eeprom There can now be two ibl configuration structures in the I2c rom. One is used by the big endian code, the other by the little. A single one can be used by simply referring to one reserved area in the I2C configuration file.
Debugged the IBL two stage load process The IBL now loads in two stages. The initial load from the boot ROM is an endian neutral image. This initial load determines the endian setting of the device and then loads the rest of the IBL using the correct endian image.