1 #ifndef __TIBOOT_H__
2 #define __TIBOOT_H__
3 /******************************************************************************
4 * FILE PURPOSE: Define Structures, MACROs and etc for TI Shared ROM Boot
5 ******************************************************************************
6 * FILE NAME: tiboot.h
7 *
8 * DESCRIPTION: Define structures, macros and etc for the TI Shared ROM boot
9 * process.
10 *
11 * TABS: NONE
12 *
13 * $Id: $
14 *
15 * REVISION HISTORY:
16 *
17 * $Log: $
18 *
19 * (C) Copyright 2004 TELOGY Networks, Inc.
20 ******************************************************************************/
21 #include "types.h"
23 /*******************************************************************************
24 * Utility Macro definitions
25 ******************************************************************************/
26 #define HEX_DIGIT(digit) ((digit) + '0')
27 #define BOOT_BIT_TO_MASK(bit) (1 << (bit))
29 /*******************************************************************************
30 * Data Definition: Error Handling relatBOOT_ENTRY_POINT_ADDRed definition:
31 *******************************************************************************
32 * Description: Define Handling related macros, constants
33 *
34 ******************************************************************************/
35 /* Define Module IDs */
36 #define BOOT_MODULE_ID_MAIN 0
37 #define BOOT_MODULE_ID_BTBL 1
38 #define BOOT_MODULE_ID_BETH 2
39 #define BOOT_MODULE_ID_I2C 3
40 #define BOOT_MODULE_ID_CHIP 4
41 #define BOOT_MODULE_ID_HW 5
43 /* Boot error codes */
44 enum {
45 BOOT_NOERR = 0,
46 BOOT_ERROR = 1, /* General error */
47 BOOT_INVALID_BOOT_MODE = 2,
48 BOOT_INVALID_I2C_DEV_ADDR = 3,
49 BOOT_INVALID_CHECKSUM = 4, /* Invalid checksum of the boot parameters */
50 BOOT_INVALID_PARAMS_SIZE = 5, /* the size of boot parameters is too big */
51 BOOT_RX_ETH_QUEUE_FULL = 6, /* ethmain.c, hw_rxPacket */
52 BOOT_CACHE_INIT_FAIL = 7, /* rmain.c, cache init failed */
53 BOOT_CACHE_DISABLE_FAIL = 8, /* rmain.c, cache disable failed */
54 BOOT_INVALID_CPPI_SIZE = 9, /* ethmain.c, invalid compile sizes */
55 BOOT_INVALID_CORE_ID = 10, /* Invalid core ID in cold boot */
56 BOOT_INVALID_MAC_ADDR = 11, /* Invalid MAC address (all 0's) */
57 BOOT_ETH_TX_SCRATCH = 12, /* tx scratch size invalid */
58 BOOT_ETH_TX_PACKET = 13, /* tx packet formation failure */
59 BOOT_ETH_MAC_INIT = 14 /* ethmain.c - mac init failed */
60 };
62 /* Error tracking prototypes (functions in rmain.c)*/
63 void bootException (UINT16 errorCode);
64 void bootError (UINT16 errorCode);
66 /* Error code = (module ID * 100) + module specific error */
67 #define BOOT_ERROR_CODE(id, code) ((UINT16)((id<<8) + code))
68 #define BOOT_EXCEPTION(error_code) bootException(error_code)
69 #define BOOT_ERROR(error_code) bootError(error_code)
71 /*******************************************************************************
72 * Begin Boot Parameter definitions
73 ******************************************************************************/
75 /*******************************************************************************
76 * Boot Parameter Common
77 ******************************************************************************/
78 typedef struct boot_params_common_s{
79 UINT16 length; /* size of the entire boot parameters in bytes */
80 UINT16 checksum; /* non-zero: 1's complement checksum of the boot
81 * parameters
82 * zero: checksum is not applicable
83 */
84 UINT16 boot_mode;
85 /*
86 * Specify the boot mode
87 * bit 02-00: Standard Boot Mode
88 * bit 15-03: Extended Boot Mode
89 */
91 } BOOT_PARAMS_COMMON_T;
93 typedef struct boot_params_ethernet_s{
95 /* common portion of the Boot parameters */
96 UINT16 length;
97 UINT16 checksum;
98 UINT16 boot_mode;
100 /* Etherent specific portion of the Boot Parameters */
101 UINT16 options;
102 /*
103 * Ethernet Specific Options
104 * Bit 0: GE:
105 * 0 - 10/100 Mb
106 * 1 - 1 Gb
107 * Bit 2: HD:
108 * 0 - Full Duplex
109 * 1 - Half Duplex
110 * Bit 3: SKIP TX
111 * 0 - Send the Ethernet Ready Frame
112 * 1 - Skip sending the Ethernet Ready Frame
113 * Bit 4: SKIP INIT
114 * 0 - Initialize the Ethernet MAC peripheral
115 * 1 - Skip initializing the Ethernet MAC peripheral
116 * Bit 5: FC
117 * 0 - Disable Flow Control
118 * 1 - Enable Flow Control
119 * Other bits: Reserved
120 */
121 #define BOOT_PARAMS_ETH_OPTIONS_GE 0x0001
122 #define BOOT_PARAMS_ETH_OPTIONS_HD 0x0004
123 #define BOOT_PARAMS_ETH_OPTIONS_SKIP_TX 0x0008
124 #define BOOT_PARAMS_ETH_OPTIONS_SKIP_INIT 0x0010
125 #define BOOT_PARAMS_ETH_OPTIONS_FC 0x0020
127 /*
128 * he device MAC address to be used for Boot:
129 * All zero mac address indicates that the device E-fuse address should
130 * be used.
131 */
132 UINT16 mac_addr_h;
133 UINT16 mac_addr_m;
134 UINT16 mac_addr_l;
136 /*
137 * The multicast or broadcast MAC address which should be accepted as
138 * a destination MAC address for boot table frames
139 */
140 UINT16 mmac_addr_h;
141 UINT16 mmac_addr_m;
142 UINT16 mmac_addr_l;
144 UINT16 src_port; /* Source UDP port number to be used during boot process */
145 /* 0: allow any SRC UDP port */
146 UINT16 dest_port; /* Destination UDP port number to be used during boot process */
148 /* The Device ID to be included in the boot ready announcement frame */
149 UINT16 device_id_12;
150 UINT16 device_id_34;
151 #define BOOT_PARAMS_DEVICE_ID_HIGH_MASK 0xFF00
152 #define BOOT_PARAMS_DEVICE_ID_HIGH_SHIFT 8
153 #define BOOT_PARAMS_DEVICE_ID_LOW_MASK 0x00FF
154 #define BOOT_PARAMS_DEVICE_ID_LOW_SHIFT 0
155 #define BOOT_PARAMS_GET_DEVICE_ID_13(device_id) \
156 (((device_id) & BOOT_PARAMS_DEVICE_ID_HIGH_MASK) > BOOT_PARAMS_DEVICE_ID_HIGH_SHIFT)
157 #define BOOT_PARAMS_GET_DEVICE_ID_24(device_id) \
158 (((device_id) & BOOT_PARAMS_DEVICE_ID_LOW_MASK) > BOOT_PARAMS_DEVICE_ID_LOW_SHIFT)
160 /*
161 * The destination MAC address used for the boot ready announce frame
162 */
163 UINT16 hmac_addr_h;
164 UINT16 hmac_addr_m;
165 UINT16 hmac_addr_l;
166 } BOOT_PARAMS_ETHERNET_T;
168 typedef struct boot_params_i2c_s{
170 /* common portion of the Boot parameters */
171 UINT16 length;
172 UINT16 checksum;
173 UINT16 boot_mode;
175 /* I2C specific portion of the Boot Parameters */
176 UINT16 options;
177 /*
178 * I2C Specific Options
179 * Bit 01-00: BT:
180 * 00 - Boot Parameter Mode
181 * 01 - Boot Table Mode
182 * 10 - Boot Config mode
183 * 11 - Slave receive boot config
184 * Bit 04-02: EETYPE: EEPROM type
185 * Other bits: Reserved
186 */
187 #define BOOT_PARAMS_I2C_OPTIONS_BP 0x0000
188 #define BOOT_PARAMS_I2C_OPTIONS_BT 0x0001
189 #define BOOT_PARAMS_I2C_OPTIONS_BC 0x0002
190 #define BOOT_PARAMS_I2C_OPTIONS_SLVOPT 0x0003
192 #define BOOT_PARAMS_I2C_OPTIONS_MASK 0x0003
193 #define BOOT_PARAMS_I2C_OPTIONS_SHIFT 0
195 #define BOOT_PARAMS_I2C_OPTIONS_EETYPE_MASK 0x001C
196 #define BOOT_PARAMS_I2C_OPTIONS_EETYPE_SHIFT 2
198 #define BOOT_PARAMS_I2C_IS_BOOTTBL_MODE(options) \
199 (((options) & BOOT_PARAMS_I2C_OPTIONS_MASK) == BOOT_PARAMS_I2C_OPTIONS_BT)
201 #define BOOT_PARAMS_I2C_IS_BOOTCONFIG_MODE(options) \
202 (((options) & BOOT_PARAMS_I2C_OPTIONS_MASK) == BOOT_PARAMS_I2C_OPTIONS_BC)
204 #define BOOT_PARAMS_I2C_IS_SLAVE_RCV_OPTIONS_MODE(options) \
205 (((options) & BOOT_PARAMS_I2C_OPTIONS_MASK) == BOOT_PARAMS_I2C_OPTIONS_SLVOPT)
207 #define BOOT_PARAMS_I2C_SET_BOOTTBL_MODE(options, mode) \
208 (options) = ((options) & ~BOOT_PARAMS_I2C_OPTIONS_MASK) | \
209 (((mode) & BOOT_PARAMS_I2C_OPTIONS_MASK) << \
210 BOOT_PARAMS_I2C_OPTIONS_SHIFT)
213 #define BOOT_PARAMS_I2C_GET_EETYPE(options) \
214 (((options) & BOOT_PARAMS_I2C_OPTIONS_EETYPE_MASK) >> BOOT_PARAMS_I2C_OPTIONS_EETYPE_SHIFT)
215 #define BOOT_PARAMS_I2C_SET_EETYPE(options, ee_type) \
216 (options) = (((options) & ~BOOT_PARAMS_I2C_OPTIONS_EETYPE_MASK) | \
217 (((ee_type) << BOOT_PARAMS_I2C_OPTIONS_EETYPE_SHIFT) & BOOT_PARAMS_I2C_OPTIONS_EETYPE_MASK))
219 /* The device address to be used for Boot */
220 UINT16 dev_addr; /* 16-bit device address (low) */
221 UINT16 dev_addr_ext; /* 16-bit extended device address (high)
222 * set to zero if not used
223 * Note: some I2C device requires 32-bit
224 * address
225 */
226 UINT16 multi_i2c_id; /* Multi device master write boot ID */
227 UINT16 my_i2c_id; /* This parts I2C address */
229 UINT16 core_freq_mhz; /* Core frequency, MHz */
230 UINT16 i2c_clk_freq_khz; /* Desired I2C clock frequency, kHz */
232 UINT16 next_dev_addr; /* Used only for the boot config mode. */
233 UINT16 next_dev_addr_ext; /* Copied into dev_addr* after config complete */
235 UINT16 address_delay; /* Rough number of cycles delay between address write
236 * and read to the i2c eeprom */
239 } BOOT_PARAMS_I2C_T;
241 /*
242 * UNION of boot parameter structures in all modes
243 * Note: We need to make sure that the structures genertaed by the C-compiler
244 * match with the boot parameter table data format i.e. a set of 16-bit
245 * data array.
246 */
247 #define BOOT_PARAMS_SIZE_IN_BYTES 256
248 typedef union {
249 BOOT_PARAMS_COMMON_T common;
250 BOOT_PARAMS_ETHERNET_T eth;
251 BOOT_PARAMS_I2C_T i2c;
252 UINT16 parameter[BOOT_PARAMS_SIZE_IN_BYTES/2];
253 } BOOT_PARAMS_T;
256 /*******************************************************************************
257 * Definition: The time stamp and version number are placed into the stats.
258 * This will be two characters packed per 16bits . The length
259 * value must be 32 bit divisible
260 *******************************************************************************/
261 #define BOOT_VERSION_LEN_UINT16 32
262 typedef struct BOOT_VERSION_S {
264 UINT16 vstring[BOOT_VERSION_LEN_UINT16];
266 } BOOT_VERSION_T;
267 extern BOOT_VERSION_T bootVersion;
270 /*******************************************************************************
271 * Definition: Runs time stats that are not initialized on cold boot entry
272 * !!!!!! boot.s assumes that the nonInit stats are at the top of the structure
273 * !!!!!! and that stage is the first element
274 *******************************************************************************/
275 typedef struct BOOT_STATS_NONINIT_S {
276 UINT16 stage; /* Record the SharedROM code execution stage */
277 #define BOOT_STAGE_ASM_START_UP 1
278 #define BOOT_STAGE_INIT_CACHE 2
279 #define BOOT_STAGE_CHCHE_INITED 3
280 #define BOOT_STAGE_ENTER_WARMBOOT 4
281 #define BOOT_STAGE_INIT_CPGMAC 5
282 #define BOOT_STAGE_SEND_ERA_FRAME 6
283 #define BOOT_STAGE_ETH_MAIN_LOOP 7
284 #define BOOT_STAGE_I2C_BOOTTBL_LOOP 8
285 #define BOOT_STAGE_I2C_BOOTPARAM_LOOP 9
286 #define BOOT_STAGE_DISABLE_CACHE 10
287 #define BOOT_STAGE_CHCHE_DISABLED 11
288 #define BOOT_STAGE_EXIT 12
289 #define BOOT_STAGE_ERROR_LOOP 13
290 #define BOOT_STAGE_I2C_BOOTCONFIG_LOOP 14
291 #define BOOT_STAGE_I2C_SLV_RCV_OPTIONS_LOOP 15
292 UINT16 coldBootEntries;
294 } BOOT_STATS_NONINIT_T;
296 /*******************************************************************************
297 * Definition: Run time statistics and error counts. These stats are
298 * initialized on cold boot entry.
299 ******************************************************************************/
300 typedef struct BOOT_STATS_MAIN_S {
301 UINT16 errorCode; /* (module ID <<8 ) + module specific error */
303 /* I2C operation related statistics */
304 UINT16 numI2Cpkts; /* number of I2C boot table packets processed */
305 UINT16 numI2CchksumError;/* number of I2C checksum errors */
306 UINT16 numI2CotherError; /* number of I2C section with invalid length and etc */
307 UINT16 numI2Cretrys; /* number of I2C retrys due to read access errors */
308 UINT16 numI2cWrites; /* number of I2C master writes to passive devices */
309 UINT16 numI2cWriteError; /* number of I2C master write errors */
311 UINT16 warmBootEntry; /* Count of entries into warm boot routine */
312 } BOOT_STATS_MAIN_T;
314 /*****************************************************************************
315 * Definition: I2C stats, Boot table and Ethernrt stats initialized
316 * on cold boot entry
317 *****************************************************************************/
318 typedef struct I2C_STATS_tag
319 {
320 UINT16 num_trans;
321 UINT16 num_trys;
322 UINT16 num_try_ok;
323 UINT16 num_try_lost_arb;
324 UINT16 num_try_idle_to;
325 UINT16 num_try_no_ack;
326 UINT16 num_try_other_err;
327 UINT32 extra_idle_waits;
328 UINT32 extra_clock_waits;
329 UINT32 tx_bytes;
330 UINT32 rx_bytes;
331 UINT32 data_re_reads;
332 } I2C_STATS_T;
334 typedef struct BTBL_STATS_tag
335 {
336 UINT16 num_sections; /* number of boot table sections received */
337 UINT16 num_pdma_copies; /* number of PDMA copies performed */
338 } BTBL_STATS_T;
340 typedef struct ETH_STATS_tag
341 {
342 /* MAC packets related statistics */
343 UINT16 uniMacPkts; /* Count of packets received with valid unicast mac
344 address */
345 UINT16 multiMacPkts; /* Count of packets received with valid multicast or
346 broadcast mac address */
347 UINT16 invalidMacPkts; /* Count of packets received with invalid mac
348 address */
349 UINT16 invalidLLCPkts; /* Count of 802.3 packets with wrong LLC/SNAP header */
350 UINT16 nonIpPkts; /* Count of non-IP packets received with valid
351 MAC address */
353 /* IP packets related statistics */
354 UINT16 nonIP4Pkts; /* Count of non-IP4 packets */
355 UINT16 ipfragments; /* Count of IP fragments received */
356 UINT16 ipTruncatedError; /* Count of truncated IP frame */
357 UINT16 nonUDPPkts; /* Count of IP packets with non-UDP paylaod */
359 /* UDP packets related statistics */
360 UINT16 udpSizeError; /* Count of UDP packet with invalid (odd) size */
361 UINT16 udpPortError; /* Count of UDP packets with invalid port number */
362 UINT16 udpChksumError; /* Count of UDP packets with checksum error */
364 /* Boot table packets related statistics */
365 UINT16 nonBtblPkts; /* Count of UDP packets with invalid boot table paylaod */
366 UINT16 outSeqPkts; /* Count of out of sequence boot table packets received
367 i.e. packets with unexpected seq_num */
368 UINT16 expSeqNum; /* Expected Sequence Number */
369 UINT16 lastSeqNum; /* Last sequence number received */
371 /* Driver errors */
372 UINT16 sizeZeroPackets; /* Count of packets arriving with 0 size */
373 } ETH_STATS_T;
375 typedef struct PCI_EEAI_STATS_tag
376 {
377 UINT16 pciI2cReads; /* Count of block reads of i2c eeprom */
378 UINT16 pciI2cRetries; /* Count of i2c read retries */
379 UINT16 pciChkSumErr; /* Count of block check sum errors */
380 UINT16 pciEeaiFail; /* Count of aborted pci attempts */
381 } PCI_EEAI_STATS_T;
383 /* Rapid I/O stats */
384 typedef struct RAPIDIO_STATS_tag
385 {
386 UINT16 rapidIoFailReady; /* If set rapid I/O peripheral failed to report ready */
387 } RAPIDIO_STATS_T;
389 /*******************************************************************************
390 * Definition: The statistics
391 *
392 * !!!!!! boot.s assumes that the nonInit stats are at the top of the structure!
393 *******************************************************************************/
394 typedef struct BOOT_STATS_S {
396 BOOT_STATS_NONINIT_T nonInit;
397 BOOT_STATS_MAIN_T main;
398 ETH_STATS_T eth;
399 I2C_STATS_T i2c;
400 BTBL_STATS_T btbl;
401 PCI_EEAI_STATS_T pci_eeai;
402 RAPIDIO_STATS_T rapidIo;
403 } BOOT_STATS_T;
405 extern BOOT_STATS_T bootStats;
407 /*******************************************************************************
408 * Definition: The magic start address, known to all modules
409 *******************************************************************************/
410 extern volatile UINT32 *p_boot_entry_addr;
412 #endif /* __TIBOOT_H__ */
414 /* nothing past this point */