]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - keystone-rtos/ibl.git/blob - src/device/c6457/tiboot_c6457.h
for loop for pll + ddr_ctr_config
[keystone-rtos/ibl.git] / src / device / c6457 / tiboot_c6457.h
1 #ifndef __TIBOOT_H__
2 #define __TIBOOT_H__
3 /******************************************************************************
4  * FILE PURPOSE: Define Structures, MACROs and etc for TI Shared ROM Boot
5  ******************************************************************************
6  * FILE NAME:   tiboot.h
7  *
8  * DESCRIPTION: Define structures, macros and etc for the TI Shared ROM boot
9  *              process.
10  *
11  * TABS: NONE
12  *
13  * $Id: $
14  *
15  * REVISION HISTORY:
16  *
17  * $Log: $
18  *
19  * (C) Copyright 2004 TELOGY Networks, Inc. 
20  ******************************************************************************/
21 #include "types.h"
23 /*******************************************************************************
24  * Utility Macro definitions
25  ******************************************************************************/
26 #define HEX_DIGIT(digit)        ((digit) + '0')
27 #define BOOT_BIT_TO_MASK(bit)   (1 << (bit))
29 /*******************************************************************************
30  * Data Definition: Error Handling relatBOOT_ENTRY_POINT_ADDRed definition:
31  *******************************************************************************
32  * Description: Define Handling related macros, constants
33  *
34  ******************************************************************************/
35 /* Define Module IDs */
36 #define BOOT_MODULE_ID_MAIN         0
37 #define BOOT_MODULE_ID_BTBL         1
38 #define BOOT_MODULE_ID_BETH         2
39 #define BOOT_MODULE_ID_I2C          3
40 #define BOOT_MODULE_ID_CHIP         4
41 #define BOOT_MODULE_ID_HW           5
43 /* Boot error codes */
44 enum {
45   BOOT_NOERR                = 0,
46   BOOT_ERROR                = 1,    /* General error */
47   BOOT_INVALID_BOOT_MODE    = 2,    
48   BOOT_INVALID_I2C_DEV_ADDR = 3,
49   BOOT_INVALID_CHECKSUM     = 4,    /* Invalid checksum of the boot parameters */
50   BOOT_INVALID_PARAMS_SIZE  = 5,    /* the size of boot parameters is too big */
51   BOOT_RX_ETH_QUEUE_FULL    = 6,    /* ethmain.c, hw_rxPacket */
52   BOOT_CACHE_INIT_FAIL      = 7,    /* rmain.c, cache init failed */
53   BOOT_CACHE_DISABLE_FAIL   = 8,    /* rmain.c, cache disable failed */
54   BOOT_INVALID_CPPI_SIZE    = 9,    /* ethmain.c, invalid compile sizes */
55   BOOT_INVALID_CORE_ID      = 10,   /* Invalid core ID in cold boot */
56   BOOT_INVALID_MAC_ADDR     = 11,   /* Invalid MAC address (all 0's) */
57   BOOT_ETH_TX_SCRATCH       = 12,   /* tx scratch size invalid */
58   BOOT_ETH_TX_PACKET        = 13,   /* tx packet formation failure */
59   BOOT_ETH_MAC_INIT         = 14,   /* ethmain.c - mac init failed */
60   BOOT_PERIPH_POWER         = 15,   /* peripheral failed to powerup */
61   BOOT_MAIN_FAIL            = 16,   /* Failed in initial boot setup (wrong core) */
62   BOOT_SK_REGISTERSCWP      = 17,   /* Failed at SK_registerSCWP */
63   BOOT_SK_ALLOCSC           = 18,   /* Failed at SK_allocSC */       
64   BOOT_CPSGMII_CONFIGINDEX  = 19,   /* Failed at wrong CPSGMII config index */
65   BOOT_SRIO_CONFIGINDEX     = 20    /* Failed at wrong SRIO config index */
66 };
68 /* Error tracking prototypes (functions in rmain.c)*/
69 void bootException (UINT16 errorCode);
70 void bootError (UINT16 errorCode);
72 /* Error code = (module ID *  100) + module specific error */
73 #define BOOT_ERROR_CODE(id, code)     ((UINT16)((id<<8) + code))
74 #define BOOT_EXCEPTION(error_code)     bootException(error_code)
75 #define BOOT_ERROR(error_code)         bootError(error_code) 
77 /*******************************************************************************
78  * Begin Boot Parameter definitions
79  ******************************************************************************/
81 /*******************************************************************************
82  * Boot Parameter Common 
83  ******************************************************************************/
84 typedef struct boot_params_common_s{
85    UINT16 length;       /* size of the entire boot parameters in bytes */
86    UINT16 checksum;     /* non-zero: 1's complement checksum of the boot 
87                          *           parameters
88                          * zero: checksum is not applicable
89                          */
90    UINT16 boot_mode;
91    UINT16 portNum;
92    UINT16 swPll;         /* CPU PLL multiplier */ 
93    
94     
95 } BOOT_PARAMS_COMMON_T;
97 typedef struct boot_params_ethernet_s{
99     /* common portion of the Boot parameters */
100     UINT16 length;
101     UINT16 checksum;
102     UINT16 boot_mode;
103     UINT16 portNum;
104     UINT16 swPll;         /* CPU PLL multiplier */ 
105      
106     /* Etherent specific portion of the Boot Parameters */
107     UINT16 options;
108     /*
109      * Ethernet Specific Options
110      *
111      * Bits 2:0 interface
112      *      000 - MII
113      *      001 - RMII
114      *      010 - GMII
115      *      011 - RGMII
116      *      100 - SMII
117      *      101 - S3MII
118      *
119      * Bit 3: HD:                                      
120      *        0 - Full Duplex                          
121      *        1 - Half Duplex                          
122      * Bit 4: SKIP TX                                           
123      *        0 - Send the Ethernet Ready Frame 
124      *        1 - Skip sending the Ethernet Ready Frame                                              
125      * Bit 5: SKIP INIT                                           
126      *        0 - Initialize the Ethernet MAC peripheral 
127      *        1 - Skip initializing the Ethernet MAC peripheral 
128      * Bit 6: FC
129      *        0 - Disable Flow Control
130      *        1 - Enable Flow Control                                               
131      *
132      * Other bits:  Reserved 
133      */ 
134      #define BOOT_PARAMS_ETH_OPTIONS_MII        0x0000
135      #define BOOT_PARAMS_ETH_OPTIONS_RMII       0x0001
136      #define BOOT_PARAMS_ETH_OPTIONS_GMII       0x0002
137      #define BOOT_PARAMS_ETH_OPTIONS_RGMII      0x0003
138      #define BOOT_PARAMS_ETH_OPTIONS_SMII       0x0004
139      #define BOOT_PARAMS_ETH_OPTIONS_S3MII      0x0005
140         
141         /* Faraday only supports SGMII */
142      #define BOOT_PARAMS_ETH_OPTIONS_SGMII      0x0006
143      
144      #define BOOT_PARAMS_ETH_OPTIONS_HD         0x0008
145      #define BOOT_PARAMS_ETH_OPTIONS_SKIP_TX    0x0010
146      #define BOOT_PARAMS_ETH_OPTIONS_SKIP_INIT  0x0020
147      #define BOOT_PARAMS_ETH_OPTIONS_FC         0x0040
148      
149      /* 
150       * he device MAC address to be used for Boot:
151       * All zero mac address indicates that the device E-fuse address should
152       *  be used.
153       */ 
154      UINT16 mac_addr_h;
155      UINT16 mac_addr_m;
156      UINT16 mac_addr_l;
157      
158      /* 
159       * The multicast or broadcast MAC address which should be accepted as
160       * a destination MAC address for boot table frames
161       */
162      UINT16 mmac_addr_h;
163      UINT16 mmac_addr_m;
164      UINT16 mmac_addr_l;
165         
166      UINT16 src_port;     /* Source UDP port number to be used during boot process */
167                           /* 0: allow any SRC UDP port */
168      UINT16 dest_port;    /* Destination UDP port number to be used during boot process */
169      
170      /* The Device ID to be included in the boot ready announcement frame */
171      UINT16 device_id_12;   
172      UINT16 device_id_34;   
173      #define BOOT_PARAMS_DEVICE_ID_HIGH_MASK     0xFF00
174      #define BOOT_PARAMS_DEVICE_ID_HIGH_SHIFT    8
175      #define BOOT_PARAMS_DEVICE_ID_LOW_MASK      0x00FF
176      #define BOOT_PARAMS_DEVICE_ID_LOW_SHIFT     0
177      #define BOOT_PARAMS_GET_DEVICE_ID_13(device_id)    \
178                (((device_id) & BOOT_PARAMS_DEVICE_ID_HIGH_MASK) > BOOT_PARAMS_DEVICE_ID_HIGH_SHIFT)
179      #define BOOT_PARAMS_GET_DEVICE_ID_24(device_id)    \
180                (((device_id) & BOOT_PARAMS_DEVICE_ID_LOW_MASK) > BOOT_PARAMS_DEVICE_ID_LOW_SHIFT)
181  
182      /* 
183       * The destination MAC address used for the boot ready announce frame
184       */
185      UINT16 hmac_addr_h;
186      UINT16 hmac_addr_m;
187      UINT16 hmac_addr_l;
189          /*
190       * The CPSGMII configurations for Faraday
191       */
193      UINT16 sgmiiConfig;
195      #define BOOT_PARAMS_SGMII_CONFIG_INDEX_MASK     0x0F     /* bit 3 to 0 is index */
196      #define BOOT_PARAMS_SGMII_CONFIG_DIRECT_CONFIG  (1<<4)   /* set to use direct configurations */
197      #define BOOT_PARAMS_SGMII_CONFIG_NO_CONFIG      (1<<5)   /* set to bypass CPSGMII config  */
199          UINT16 sgmiiControl;  
200      #define BOOT_PARAMS_SGMII_CONTROL_MASK 0x7F
202          UINT16 sgmiiMr_Adv_Ability;
203      #define BOOT_PARAMS_SGMII_ABILITY_MASK 0x0000FFFF
205          UINT16 sgmiiTx_Cfg_h;
206          UINT16 sgmiiTx_Cfg_l;
207          UINT16 sgmiiRx_Cfg_h;
208          UINT16 sgmiiRx_Cfg_l;
209          UINT16 sgmiiAux_Cfg_h;
210          UINT16 sgmiiAux_Cfg_l;
211      
212 }   BOOT_PARAMS_ETHERNET_T;
214 /**************************************************************************************
215  * Utopia boot options
216  **************************************************************************************/
217 typedef struct boot_params_utopia_s{
219     /* common portion of the Boot parameters */
220     UINT16 length;
221     UINT16 checksum;
222     UINT16 boot_mode;
223     UINT16 portNum;
224     UINT16 swPll;         /* CPU PLL multiplier */ 
225      
226     /* Utopia specific portion of the Boot Parameters */
227     /* Options 
228      *  ---------------------------------------------------------------
229      * | 15                          3  |    2    |    1    |    0    |
230      * ----------------------------------------------------------------
231      *          reserved                     |         |         \-> 0 = multi phy
232      *                                       |         |             1 = single phy
233      *                                       |         \-> 0 = 8 bit utopia
234      *                                       |             1 = 16 bit utopis
235      *                                       \-> 0 = Init port
236      *                                           1 = skip port init
237      */
238     UINT16 options;
239     
240     #define BOOT_PARAMS_UTOPIA_SINGLE_PHY    (1<<0)
241     #define BOOT_PARAMS_UTOPIA_16BIT         (1<<1)
242     #define BOOT_PARAMS_UTOPIA_SKIP_INIT     (1<<2)
243     
244     UINT16 cellSizeBytes;    /* Cell Size */
245     UINT16 busWidthBits;     /* Bus width (8 or 16) */
246     UINT16 slid;             /* Slave ID  */
247     UINT16 coreFreqMhz;      /* CPU frequency after pll mult */
248      
249     
250 } BOOT_PARAMS_UTOPIA_T;
252 typedef struct boot_params_i2c_s{
254     /* common portion of the Boot parameters */
255     UINT16 length;
256     UINT16 checksum;
257     UINT16 boot_mode;
258     UINT16 portNum;
259     UINT16 swPll;         /* CPU PLL multiplier */ 
260     
261     /* I2C specific portion of the Boot Parameters */
262     UINT16 options;
263     /*
264      * I2C Specific Options
265      * Bit 01-00: BT:                                      
266      *            00 - Boot Parameter Mode                            
267      *            01 - Boot Table Mode                     
268      *            10 - Boot Config mode
269      *            11 - Slave receive boot config
270      * Bit 04-02: EETYPE: EEPROM type             
271      * Other bits:  Reserved 
272      */ 
273      #define BOOT_PARAMS_I2C_OPTIONS_BP             0x0000
274      #define BOOT_PARAMS_I2C_OPTIONS_BT             0x0001
275      #define BOOT_PARAMS_I2C_OPTIONS_BC             0x0002
276      #define BOOT_PARAMS_I2C_OPTIONS_SLVOPT         0x0003
277      
278      #define BOOT_PARAMS_I2C_OPTIONS_MASK           0x0003
279      #define BOOT_PARAMS_I2C_OPTIONS_SHIFT          0
280      
281      #define BOOT_PARAMS_I2C_OPTIONS_EETYPE_MASK    0x001C
282      #define BOOT_PARAMS_I2C_OPTIONS_EETYPE_SHIFT   2 
283      
284      #define BOOT_PARAMS_I2C_IS_BOOTTBL_MODE(options) \
285              (((options) & BOOT_PARAMS_I2C_OPTIONS_MASK) == BOOT_PARAMS_I2C_OPTIONS_BT)
286              
287      #define BOOT_PARAMS_I2C_IS_BOOTCONFIG_MODE(options) \
288              (((options) & BOOT_PARAMS_I2C_OPTIONS_MASK) == BOOT_PARAMS_I2C_OPTIONS_BC)
289              
290      #define BOOT_PARAMS_I2C_IS_SLAVE_RCV_OPTIONS_MODE(options) \
291              (((options) & BOOT_PARAMS_I2C_OPTIONS_MASK) == BOOT_PARAMS_I2C_OPTIONS_SLVOPT)
292              
293      #define BOOT_PARAMS_I2C_IS_BOOTPARAM_MODE(options) \
294              (((options) & BOOT_PARAMS_I2C_OPTIONS_MASK) == BOOT_PARAMS_I2C_OPTIONS_BP)
295              
296      #define BOOT_PARAMS_I2C_SET_BOOTTBL_MODE(options, mode)               \
297              (options) = ((options) & ~BOOT_PARAMS_I2C_OPTIONS_MASK) |     \
298                          (((mode)   &  BOOT_PARAMS_I2C_OPTIONS_MASK) <<    \
299                                        BOOT_PARAMS_I2C_OPTIONS_SHIFT)
300              
301              
302      #define BOOT_PARAMS_I2C_GET_EETYPE(options)    \
303              (((options) & BOOT_PARAMS_I2C_OPTIONS_EETYPE_MASK) >> BOOT_PARAMS_I2C_OPTIONS_EETYPE_SHIFT)
304      #define BOOT_PARAMS_I2C_SET_EETYPE(options, ee_type)         \
305              (options) = (((options) & ~BOOT_PARAMS_I2C_OPTIONS_EETYPE_MASK) |  \
306                          (((ee_type) << BOOT_PARAMS_I2C_OPTIONS_EETYPE_SHIFT) & BOOT_PARAMS_I2C_OPTIONS_EETYPE_MASK))          
307         
308      /* The device address to be used for Boot */
309      UINT16 dev_addr;           /* 16-bit device address (low) */
310      UINT16 dev_addr_ext;       /* 16-bit extended device address (high) 
311                                  * set to zero if not used
312                                  * Note: some I2C device requires 32-bit 
313                                  * address
314                                  */ 
315      UINT16 multi_i2c_id;      /* Multi device master write boot ID */
316      UINT16 my_i2c_id;         /* This parts I2C address            */
317      
318      UINT16 core_freq_mhz;     /* Core frequency, MHz               */
319      UINT16 i2c_clk_freq_khz;  /* Desired I2C clock frequency, kHz  */
320      
321      UINT16 next_dev_addr;      /* Used only for the boot config mode.         */
322      UINT16 next_dev_addr_ext;  /* Copied into dev_addr* after config complete */
323      
324      UINT16 address_delay;      /* Rough number of cycles delay between address write
325                                  * and read to the i2c eeprom */
326      
327      
328 } BOOT_PARAMS_I2C_T;   
331 typedef struct boot_params_rapidio_s{
333     /* common portion of the Boot parameters */
334     UINT16 length;
335     UINT16 checksum;
336     UINT16 boot_mode;
337     UINT16 portNum;
338     UINT16 swPll;         /* CPU PLL multiplier */ 
339     
340     /* Options */
341     UINT16 options;
342     
343     #define BOOT_PARAMS_RIO_OPTIONS_TX_ENABLE  (1<<0)   /* set to enable transmit    */
344     #define BOOT_PARAMS_RIO_OPTIONS_BOOT_TABLE (1<<1)   /* set to use boot tables    */
345     #define BOOT_PARAMS_RIO_OPTIONS_NO_CONFIG  (1<<2)   /* set to bypass port config */
346     
347     UINT16 cfg_index;       /* General configuration index to use      */
348     UINT16 node_id;         /* The node id for this device             */
349     UINT16 serdes_ref_clk;  /* The serdes reference clock freq, in MHz */
350     UINT16 link_rate;       /* Data link rate (mega bits per second    */
351     UINT16 pf_low;          /* Packet forward range, low               */
352     UINT16 pf_high;         /* Packet forward range, high              */
353     
354 } BOOT_PARAMS_RIO_T;
356 /*
357  * UNION of boot parameter structures in all modes
358  * Note: We need to make sure that the structures genertaed by the C-compiler
359  *       match with the boot parameter table data format i.e. a set of 16-bit
360  *       data array.
361  */ 
362 #define BOOT_PARAMS_SIZE_IN_BYTES       128
363 typedef union {
364    BOOT_PARAMS_COMMON_T    common;  
365    BOOT_PARAMS_ETHERNET_T  eth;
366    BOOT_PARAMS_I2C_T       i2c;
367    BOOT_PARAMS_UTOPIA_T    utopia;
368    BOOT_PARAMS_RIO_T       rio;
369    UINT16                  parameter[BOOT_PARAMS_SIZE_IN_BYTES/2]; 
370 } BOOT_PARAMS_T;
373 /*******************************************************************************
374  * Definition: The time stamp and version number are placed into the stats. 
375  *             This will be two characters packed per 16bits . The length
376  *             value must be 32 bit divisible
377  *******************************************************************************/
378 #define BOOT_VERSION_LEN_UINT16    32 
379 typedef struct BOOT_VERSION_S {
381   UINT16 vstring[BOOT_VERSION_LEN_UINT16];
382   
383 } BOOT_VERSION_T;
384 extern BOOT_VERSION_T bootVersion;
385   
387 /*******************************************************************************
388  * Definition: Runs time stats that are not initialized on cold boot entry
389  *   !!!!!! boot.s assumes that the nonInit stats are at the top of the structure
390  *   !!!!!! and that stage is the first element
391  *******************************************************************************/
392 typedef struct BOOT_STATS_NONINIT_S {
393   UINT16  stage;            /* Record the SharedROM code execution stage */
394   #define BOOT_STAGE_ASM_START_UP               1
395   #define BOOT_STAGE_INIT_CACHE                 2
396   #define BOOT_STAGE_CHCHE_INITED               3
397   #define BOOT_STAGE_ENTER_WARMBOOT             4
398   #define BOOT_STAGE_INIT_CPGMAC                5
399   #define BOOT_STAGE_SEND_ERA_FRAME             6
400   #define BOOT_STAGE_ETH_MAIN_LOOP              7
401   #define BOOT_STAGE_I2C_BOOTTBL_LOOP           8
402   #define BOOT_STAGE_I2C_BOOTPARAM_LOOP         9
403   #define BOOT_STAGE_DISABLE_CACHE             10
404   #define BOOT_STAGE_CHCHE_DISABLED            11
405   #define BOOT_STAGE_EXIT                      12
406   #define BOOT_STAGE_ERROR_LOOP                13  
407   #define BOOT_STAGE_I2C_BOOTCONFIG_LOOP       14
408   #define BOOT_STAGE_I2C_SLV_RCV_OPTIONS_LOOP  15
409   #define BOOT_STAGE_UTOPIA_MAIN_LOOP          16
410   UINT16  coldBootEntries;
411   
412 } BOOT_STATS_NONINIT_T;
414 /*******************************************************************************
415  * Definition: Run time statistics and error counts. These stats are 
416  *             initialized on cold boot entry.
417  ******************************************************************************/
418  
419 typedef struct BOOT_STATS_COMMON_S  {
420   UINT32    bootStatus;
421   UINT16    nColdBootEntries;
422   UINT16    nBootReentries;
423   UINT16    nPllWarns;
424   UINT16    nResetWarns;
425 } BOOT_STATS_COMMON_T;
426  
427  
428 typedef struct BOOT_STATS_MAIN_S {
429   UINT16  errorCode;        /* (module ID <<8 ) + module specific error */
430   
431   /* I2C operation related statistics */
432   UINT16  numI2Cpkts;       /* number of I2C boot table packets processed */
433   UINT16  numI2CchksumError;/* number of I2C checksum errors */
434   UINT16  numI2ClengthError;/* number of I2C block length errors */
435   UINT16  numI2CotherError; /* number of I2C section with invalid length and etc */
436   UINT16  numI2Cretrys;     /* number of I2C retrys due to read access errors */
437   UINT16  numI2cWrites;     /* number of I2C master writes to passive devices */
438   UINT16  numI2cWriteError; /* number of I2C master write errors              */
439   
440   UINT16  warmBootEntry;    /* Count of entries into warm boot routine   */
441 } BOOT_STATS_MAIN_T;
445 /*****************************************************************************
446  * Definition: I2C stats, Boot table and Ethernrt stats initialized 
447  *             on cold boot entry
448  *****************************************************************************/
449 typedef struct I2C_STATS_tag
451     UINT16      num_trans;
452     UINT16      num_trys;
453     UINT16      num_try_ok;
454     UINT16      num_try_lost_arb;
455     UINT16      num_try_idle_to;
456     UINT16      num_try_no_ack;
457     UINT16      num_try_other_err;
458     UINT32      extra_idle_waits;
459     UINT32      extra_clock_waits;
460     UINT32      tx_bytes;
461     UINT32      rx_bytes;
462     UINT32      data_re_reads;
463 } I2C_STATS_T;
465 typedef struct BTBL_STATS_tag
467   UINT16  num_sections;     /* number of boot table sections received */
468   UINT16  num_pdma_copies;  /* number of PDMA copies performed */
469 } BTBL_STATS_T;
471 typedef struct ETH_STATS_tag
473   /* MAC packets related statistics */
474   UINT16  uniMacPkts;       /* Count of packets received with valid unicast mac 
475                                address   */
476   UINT16  multiMacPkts;     /* Count of packets received with valid multicast or
477                                broadcast mac address   */
478   UINT16  invalidMacPkts;   /* Count of packets received with invalid mac 
479                                address   */
480   UINT16  invalidLLCPkts;   /* Count of 802.3 packets with wrong LLC/SNAP header */
481   UINT16  nonIpPkts;        /* Count of non-IP packets received with valid 
482                                MAC address   */
483                                
484   /* IP packets related statistics */                             
485   UINT16  nonIP4Pkts;       /* Count of non-IP4 packets        */
486   UINT16  ipfragments;      /* Count of IP fragments received      */
487   UINT16  ipTruncatedError; /* Count of truncated IP frame */
488   UINT16  nonUDPPkts;       /* Count of IP packets with non-UDP paylaod  */
489   
490   /* UDP packets related statistics */
491   UINT16  udpSizeError;     /* Count of UDP packet with invalid (odd) size */
492   UINT16  udpPortError;     /* Count of UDP packets with invalid port number */
493   UINT16  udpChksumError;   /* Count of UDP packets with checksum error */
494   
495   /* Boot table packets related statistics */
496   UINT16  nonBtblPkts;      /* Count of UDP packets with invalid boot table paylaod */
497   UINT16  outSeqPkts;       /* Count of out of sequence boot table packets received       
498                                i.e. packets with unexpected seq_num      */
499   UINT16  expSeqNum;        /* Expected Sequence Number */
500   UINT16  lastSeqNum;       /* Last sequence number received */                             
502   /* Driver errors */
503   UINT16  sizeZeroPackets;  /* Count of packets arriving with 0 size */
504 } ETH_STATS_T;
506 typedef struct PCI_EEAI_STATS_tag
508   UINT16  pciI2cReads;         /* Count of block reads of i2c eeprom */
509   UINT16  pciI2cRetries;       /* Count of i2c read retries          */
510   UINT16  pciChkSumErr;        /* Count of block check sum errors    */
511   UINT16  pciEeaiFail;         /* Count of aborted pci attempts      */
512 } PCI_EEAI_STATS_T;
514 /* Rapid I/O stats */
515 typedef struct RAPIDIO_STATS_tag
517   UINT16 rapidIoFailReady;     /* If set rapid I/O peripheral failed to report ready */
518   UINT16 rapidIoBtblBlocks;    /* Count of number of boot table blocks received */
519   UINT16 rapidIoBtblBadBlocks; /* Count of boot table blocks rejected */
520 } RAPIDIO_STATS_T;
522 typedef struct HPI_STATS_Tag
524   UINT16 hpiBtblBlocks;        /* Count of boot table blocks received */
525   UINT16 hpiBtblBadBlocks;     /* Count of boot table blocks rejected */
526 } HPI_STATS_T;
528 /* Utopia stats */
529 typedef struct UTOPIA_STATS_tag
531   UINT16 cellCount;            /* Count of cells received   */
532   UINT16 invalidPtr;           /* Count of invalid pointers received in processing */
533   UINT16 invalidSize;          /* Count of cells that were too small               */
534   UINT16 cellMagicCount;       /* Count of cells received with valid magic         */
535   UINT16 cellMagicFailed;      /* Count of cells received with invalid magic       */
536   UINT16 trapNoCellMem;        /* Trapped due to no cell space in memory           */
537   UINT16 possibleOverrun;      /* Count of possible cell buffer overruns           */
538 } UTOPIA_STATS_T;
540 /*******************************************************************************
541  * Definition: The statistics
542  *
543  *   !!!!!! boot.s assumes that the nonInit stats are at the top of the structure!
544  *******************************************************************************/
545 typedef struct BOOT_STATS_S {
547  BOOT_STATS_COMMON_T   common;
548  BOOT_STATS_NONINIT_T  nonInit;
549  BOOT_STATS_MAIN_T     main;
550  I2C_STATS_T           i2c;
551  BTBL_STATS_T          btbl;
552  union  {
553    ETH_STATS_T           eth;
554    PCI_EEAI_STATS_T      pci_eeai;
555    RAPIDIO_STATS_T       rapidIo;
556    UTOPIA_STATS_T        utopia;
557    HPI_STATS_T           hpi;
558  } u;
559 } BOOT_STATS_T;
561 extern BOOT_STATS_T bootStats;
563 /*******************************************************************************
564  * Definition: The magic start address, known to all modules
565  *******************************************************************************/
566 extern volatile UINT32 *p_boot_entry_addr;
568 #endif  /* __TIBOOT_H__ */
570 /* nothing past this point */