]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - keystone-rtos/ibl.git/blob - src/device/c6472/tiboot_c6472.h
Cleanup unused MACROS
[keystone-rtos/ibl.git] / src / device / c6472 / tiboot_c6472.h
1 #ifndef __TIBOOT_H__
2 #define __TIBOOT_H__
3 /******************************************************************************
4  * FILE PURPOSE: Define Structures, MACROs and etc for TI Shared ROM Boot
5  ******************************************************************************
6  * FILE NAME:   tiboot.h
7  *
8  * DESCRIPTION: Define structures, macros and etc for the TI Shared ROM boot
9  *              process.
10  *
11  * TABS: NONE
12  *
13  * $Id: $
14  *
15  * REVISION HISTORY:
16  *
17  * $Log: $
18  *
19  * (C) Copyright 2004 TELOGY Networks, Inc. 
20  ******************************************************************************/
21 #include "types.h"
23 /*******************************************************************************
24  * Utility Macro definitions
25  ******************************************************************************/
26 #define HEX_DIGIT(digit)        ((digit) + '0')
27 #define BOOT_BIT_TO_MASK(bit)   (1 << (bit))
29 /*******************************************************************************
30  * Data Definition: Error Handling relatBOOT_ENTRY_POINT_ADDRed definition:
31  *******************************************************************************
32  * Description: Define Handling related macros, constants
33  *
34  ******************************************************************************/
35 /* Define Module IDs */
36 #define BOOT_MODULE_ID_MAIN         0
37 #define BOOT_MODULE_ID_BTBL         1
38 #define BOOT_MODULE_ID_BETH         2
39 #define BOOT_MODULE_ID_I2C          3
40 #define BOOT_MODULE_ID_CHIP         4
41 #define BOOT_MODULE_ID_HW           5
43 /* Boot error codes */
44 enum {
45   BOOT_NOERR                = 0,
46   BOOT_ERROR                = 1,    /* General error */
47   BOOT_INVALID_BOOT_MODE    = 2,    
48   BOOT_INVALID_I2C_DEV_ADDR = 3,
49   BOOT_INVALID_CHECKSUM     = 4,    /* Invalid checksum of the boot parameters */
50   BOOT_INVALID_PARAMS_SIZE  = 5,    /* the size of boot parameters is too big */
51   BOOT_RX_ETH_QUEUE_FULL    = 6,    /* ethmain.c, hw_rxPacket */
52   BOOT_CACHE_INIT_FAIL      = 7,    /* rmain.c, cache init failed */
53   BOOT_CACHE_DISABLE_FAIL   = 8,    /* rmain.c, cache disable failed */
54   BOOT_INVALID_CPPI_SIZE    = 9,    /* ethmain.c, invalid compile sizes */
55   BOOT_INVALID_CORE_ID      = 10,   /* Invalid core ID in cold boot */
56   BOOT_INVALID_MAC_ADDR     = 11,   /* Invalid MAC address (all 0's) */
57   BOOT_ETH_TX_SCRATCH       = 12,   /* tx scratch size invalid */
58   BOOT_ETH_TX_PACKET        = 13,   /* tx packet formation failure */
59   BOOT_ETH_MAC_INIT         = 14,   /* ethmain.c - mac init failed */
60   BOOT_PERIPH_POWER         = 15,   /* peripheral failed to powerup */
61   BOOT_MAIN_FAIL            = 16    /* Failed in initial boot setup (wrong core) */
62 };
64 /* Error tracking prototypes (functions in rmain.c)*/
65 void bootException (UINT16 errorCode);
66 void bootError (UINT16 errorCode);
68 /* Error code = (module ID *  100) + module specific error */
69 #define BOOT_ERROR_CODE(id, code)     ((UINT16)((id<<8) + code))
70 #define BOOT_EXCEPTION(error_code)     bootException(error_code)
71 #define BOOT_ERROR(error_code)         bootError(error_code) 
73 /*******************************************************************************
74  * Begin Boot Parameter definitions
75  ******************************************************************************/
77 /*******************************************************************************
78  * Boot Parameter Common 
79  ******************************************************************************/
80 typedef struct boot_params_common_s{
81    UINT16 length;       /* size of the entire boot parameters in bytes */
82    UINT16 checksum;     /* non-zero: 1's complement checksum of the boot 
83                          *           parameters
84                          * zero: checksum is not applicable
85                          */
86    UINT16 boot_mode;
87    UINT16 portNum;
88    UINT16 swPll;         /* CPU PLL multiplier */ 
89    
90     
91 } BOOT_PARAMS_COMMON_T;
93 typedef struct boot_params_ethernet_s{
95     /* common portion of the Boot parameters */
96     UINT16 length;
97     UINT16 checksum;
98     UINT16 boot_mode;
99     UINT16 portNum;
100     UINT16 swPll;         /* CPU PLL multiplier */ 
101      
102     /* Etherent specific portion of the Boot Parameters */
103     UINT16 options;
104     /*
105      * Ethernet Specific Options
106      *
107      * Bits 2:0 interface
108      *      000 - MII
109      *      001 - RMII
110      *      010 - GMII
111      *      011 - RGMII
112      *      100 - SMII
113      *      101 - S3MII
114      *      110 - RMII 10Mbs
115      *      111 - RMII 100Mbs
116      *
117      * Bit 3: HD:                                      
118      *        0 - Full Duplex                          
119      *        1 - Half Duplex                          
120      * Bit 4: SKIP TX                                           
121      *        0 - Send the Ethernet Ready Frame 
122      *        1 - Skip sending the Ethernet Ready Frame                                              
123      * Bit 5: SKIP INIT                                           
124      *        0 - Initialize the Ethernet MAC peripheral 
125      *        1 - Skip initializing the Ethernet MAC peripheral 
126      * Bit 6: FC
127      *        0 - Disable Flow Control
128      *        1 - Enable Flow Control                                               
129      *
130      * Other bits:  Reserved 
131      */ 
132      #define BOOT_PARAMS_ETH_OPTIONS_MII        0x0000
133      #define BOOT_PARAMS_ETH_OPTIONS_RMII       0x0001
134      #define BOOT_PARAMS_ETH_OPTIONS_GMII       0x0002
135      #define BOOT_PARAMS_ETH_OPTIONS_RGMII      0x0003
136      #define BOOT_PARAMS_ETH_OPTIONS_SMII       0x0004
137      #define BOOT_PARAMS_ETH_OPTIONS_S3MII      0x0005
138      #define BOOT_PARAMS_ETH_OPTIONS_RMII_10    0x0006
139      #define BOOT_PARAMS_ETH_OPTIONS_RMII_100   0x0007
140      
141      #define BOOT_PARAMS_ETH_OPTIONS_HD         0x0008
142      #define BOOT_PARAMS_ETH_OPTIONS_SKIP_TX    0x0010
143      #define BOOT_PARAMS_ETH_OPTIONS_SKIP_INIT  0x0020
144      #define BOOT_PARAMS_ETH_OPTIONS_FC         0x0040
145      
146      /* 
147       * he device MAC address to be used for Boot:
148       * All zero mac address indicates that the device E-fuse address should
149       *  be used.
150       */ 
151      UINT16 mac_addr_h;
152      UINT16 mac_addr_m;
153      UINT16 mac_addr_l;
154      
155      /* 
156       * The multicast or broadcast MAC address which should be accepted as
157       * a destination MAC address for boot table frames
158       */
159      UINT16 mmac_addr_h;
160      UINT16 mmac_addr_m;
161      UINT16 mmac_addr_l;
162         
163      UINT16 src_port;     /* Source UDP port number to be used during boot process */
164                           /* 0: allow any SRC UDP port */
165      UINT16 dest_port;    /* Destination UDP port number to be used during boot process */
166      
167      /* The Device ID to be included in the boot ready announcement frame */
168      UINT16 device_id_12;   
169      UINT16 device_id_34;   
170      #define BOOT_PARAMS_DEVICE_ID_HIGH_MASK     0xFF00
171      #define BOOT_PARAMS_DEVICE_ID_HIGH_SHIFT    8
172      #define BOOT_PARAMS_DEVICE_ID_LOW_MASK      0x00FF
173      #define BOOT_PARAMS_DEVICE_ID_LOW_SHIFT     0
174      #define BOOT_PARAMS_GET_DEVICE_ID_13(device_id)    \
175                (((device_id) & BOOT_PARAMS_DEVICE_ID_HIGH_MASK) > BOOT_PARAMS_DEVICE_ID_HIGH_SHIFT)
176      #define BOOT_PARAMS_GET_DEVICE_ID_24(device_id)    \
177                (((device_id) & BOOT_PARAMS_DEVICE_ID_LOW_MASK) > BOOT_PARAMS_DEVICE_ID_LOW_SHIFT)
178  
179      /* 
180       * The destination MAC address used for the boot ready announce frame
181       */
182      UINT16 hmac_addr_h;
183      UINT16 hmac_addr_m;
184      UINT16 hmac_addr_l;
185      
186 }   BOOT_PARAMS_ETHERNET_T;
188 /**************************************************************************************
189  * Utopia boot options
190  **************************************************************************************/
191 typedef struct boot_params_utopia_s{
193     /* common portion of the Boot parameters */
194     UINT16 length;
195     UINT16 checksum;
196     UINT16 boot_mode;
197     UINT16 portNum;
198     UINT16 swPll;         /* CPU PLL multiplier */ 
199      
200     /* Utopia specific portion of the Boot Parameters */
201     /* Options 
202      *  ---------------------------------------------------------------
203      * | 15                          3  |    2    |    1    |    0    |
204      * ----------------------------------------------------------------
205      *          reserved                     |         |         \-> 0 = multi phy
206      *                                       |         |             1 = single phy
207      *                                       |         \-> 0 = 8 bit utopia
208      *                                       |             1 = 16 bit utopis
209      *                                       \-> 0 = Init port
210      *                                           1 = skip port init
211      */
212     UINT16 options;
213     
214     #define BOOT_PARAMS_UTOPIA_SINGLE_PHY    (1<<0)
215     #define BOOT_PARAMS_UTOPIA_16BIT         (1<<1)
216     #define BOOT_PARAMS_UTOPIA_SKIP_INIT     (1<<2)
217     
218     UINT16 cellSizeBytes;    /* Cell Size */
219     UINT16 busWidthBits;     /* Bus width (8 or 16) */
220     UINT16 slid;             /* Slave ID  */
221     UINT16 coreFreqMhz;      /* CPU frequency after pll mult */
222      
223     
224 } BOOT_PARAMS_UTOPIA_T;
226 typedef struct boot_params_i2c_s{
228     /* common portion of the Boot parameters */
229     UINT16 length;
230     UINT16 checksum;
231     UINT16 boot_mode;
232     UINT16 portNum;
233     UINT16 swPll;         /* CPU PLL multiplier */ 
234     
235     /* I2C specific portion of the Boot Parameters */
236     UINT16 options;
237     /*
238      * I2C Specific Options
239      * Bit 01-00: BT:                                      
240      *            00 - Boot Parameter Mode                            
241      *            01 - Boot Table Mode                     
242      *            10 - Boot Config mode
243      *            11 - Slave receive boot config
244      * Bit 04-02: EETYPE: EEPROM type             
245      * Other bits:  Reserved 
246      */ 
247      #define BOOT_PARAMS_I2C_OPTIONS_BP             0x0000
248      #define BOOT_PARAMS_I2C_OPTIONS_BT             0x0001
249      #define BOOT_PARAMS_I2C_OPTIONS_BC             0x0002
250      #define BOOT_PARAMS_I2C_OPTIONS_SLVOPT         0x0003
251      
252      #define BOOT_PARAMS_I2C_OPTIONS_MASK           0x0003
253      #define BOOT_PARAMS_I2C_OPTIONS_SHIFT          0
254      
255      #define BOOT_PARAMS_I2C_OPTIONS_EETYPE_MASK    0x001C
256      #define BOOT_PARAMS_I2C_OPTIONS_EETYPE_SHIFT   2 
257      
258      #define BOOT_PARAMS_I2C_IS_BOOTTBL_MODE(options) \
259              (((options) & BOOT_PARAMS_I2C_OPTIONS_MASK) == BOOT_PARAMS_I2C_OPTIONS_BT)
260              
261      #define BOOT_PARAMS_I2C_IS_BOOTCONFIG_MODE(options) \
262              (((options) & BOOT_PARAMS_I2C_OPTIONS_MASK) == BOOT_PARAMS_I2C_OPTIONS_BC)
263              
264      #define BOOT_PARAMS_I2C_IS_SLAVE_RCV_OPTIONS_MODE(options) \
265              (((options) & BOOT_PARAMS_I2C_OPTIONS_MASK) == BOOT_PARAMS_I2C_OPTIONS_SLVOPT)
266              
267      #define BOOT_PARAMS_I2C_IS_BOOTPARAM_MODE(options) \
268              (((options) & BOOT_PARAMS_I2C_OPTIONS_MASK) == BOOT_PARAMS_I2C_OPTIONS_BP)
269              
270      #define BOOT_PARAMS_I2C_SET_BOOTTBL_MODE(options, mode)               \
271              (options) = ((options) & ~BOOT_PARAMS_I2C_OPTIONS_MASK) |     \
272                          (((mode)   &  BOOT_PARAMS_I2C_OPTIONS_MASK) <<    \
273                                        BOOT_PARAMS_I2C_OPTIONS_SHIFT)
274              
275              
276      #define BOOT_PARAMS_I2C_GET_EETYPE(options)    \
277              (((options) & BOOT_PARAMS_I2C_OPTIONS_EETYPE_MASK) >> BOOT_PARAMS_I2C_OPTIONS_EETYPE_SHIFT)
278      #define BOOT_PARAMS_I2C_SET_EETYPE(options, ee_type)         \
279              (options) = (((options) & ~BOOT_PARAMS_I2C_OPTIONS_EETYPE_MASK) |  \
280                          (((ee_type) << BOOT_PARAMS_I2C_OPTIONS_EETYPE_SHIFT) & BOOT_PARAMS_I2C_OPTIONS_EETYPE_MASK))          
281         
282      /* The device address to be used for Boot */
283      UINT16 dev_addr;           /* 16-bit device address (low) */
284      UINT16 dev_addr_ext;       /* 16-bit extended device address (high) 
285                                  * set to zero if not used
286                                  * Note: some I2C device requires 32-bit 
287                                  * address
288                                  */ 
289      UINT16 multi_i2c_id;      /* Multi device master write boot ID */
290      UINT16 my_i2c_id;         /* This parts I2C address            */
291      
292      UINT16 core_freq_mhz;     /* Core frequency, MHz               */
293      UINT16 i2c_clk_freq_khz;  /* Desired I2C clock frequency, kHz  */
294      
295      UINT16 next_dev_addr;      /* Used only for the boot config mode.         */
296      UINT16 next_dev_addr_ext;  /* Copied into dev_addr* after config complete */
297      
298      UINT16 address_delay;      /* Rough number of cycles delay between address write
299                                  * and read to the i2c eeprom */
300      
301      
302 } BOOT_PARAMS_I2C_T;   
305 typedef struct boot_params_rapidio_s{
307     /* common portion of the Boot parameters */
308     UINT16 length;
309     UINT16 checksum;
310     UINT16 boot_mode;
311     UINT16 portNum;
312     UINT16 swPll;         /* CPU PLL multiplier */ 
313     
314     /* Options */
315     UINT16 options;
316     
317     #define BOOT_PARAMS_RIO_OPTIONS_TX_ENABLE  (1<<0)   /* set to enable transmit    */
318     #define BOOT_PARAMS_RIO_OPTIONS_BOOT_TABLE (1<<1)   /* set to use boot tables    */
319     #define BOOT_PARAMS_RIO_OPTIONS_NO_CONFIG  (1<<2)   /* set to bypass port config */
320     
321     UINT16 cfg_index;       /* General configuration index to use             */
322     UINT16 node_id;         /* The node id for this device                    */
323     UINT16 serdes_ref_clk;  /* The serdes reference clock freq, in hundredths
324                              * of MHz (1 MHz would be 100)                    */
325     UINT16 link_rate;       /* Data link rate (mega bits per second           */
326     UINT16 pf_low;          /* Packet forward range, low                      */
327     UINT16 pf_high;         /* Packet forward range, high                     */
328     
329 } BOOT_PARAMS_RIO_T;
331 /*
332  * UNION of boot parameter structures in all modes
333  * Note: We need to make sure that the structures genertaed by the C-compiler
334  *       match with the boot parameter table data format i.e. a set of 16-bit
335  *       data array.
336  */ 
337 #define BOOT_PARAMS_SIZE_IN_BYTES       128
338 typedef union {
339    BOOT_PARAMS_COMMON_T    common;  
340    BOOT_PARAMS_ETHERNET_T  eth;
341    BOOT_PARAMS_I2C_T       i2c;
342    BOOT_PARAMS_UTOPIA_T    utopia;
343    BOOT_PARAMS_RIO_T       rio;
344    UINT16                  parameter[BOOT_PARAMS_SIZE_IN_BYTES/2]; 
345 } BOOT_PARAMS_T;
348 /*******************************************************************************
349  * Definition: The time stamp and version number are placed into the stats. 
350  *             This will be two characters packed per 16bits . The length
351  *             value must be 32 bit divisible
352  *******************************************************************************/
353 #define BOOT_VERSION_LEN_UINT16    32 
354 typedef struct BOOT_VERSION_S {
356   UINT16 vstring[BOOT_VERSION_LEN_UINT16];
357   
358 } BOOT_VERSION_T;
359 extern BOOT_VERSION_T bootVersion;
360   
362 /*******************************************************************************
363  * Definition: Runs time stats that are not initialized on cold boot entry
364  *   !!!!!! boot.s assumes that the nonInit stats are at the top of the structure
365  *   !!!!!! and that stage is the first element
366  *******************************************************************************/
367 typedef struct BOOT_STATS_NONINIT_S {
368   UINT16  stage;            /* Record the SharedROM code execution stage */
369   #define BOOT_STAGE_ASM_START_UP               1
370   #define BOOT_STAGE_INIT_CACHE                 2
371   #define BOOT_STAGE_CHCHE_INITED               3
372   #define BOOT_STAGE_ENTER_WARMBOOT             4
373   #define BOOT_STAGE_INIT_CPGMAC                5
374   #define BOOT_STAGE_SEND_ERA_FRAME             6
375   #define BOOT_STAGE_ETH_MAIN_LOOP              7
376   #define BOOT_STAGE_I2C_BOOTTBL_LOOP           8
377   #define BOOT_STAGE_I2C_BOOTPARAM_LOOP         9
378   #define BOOT_STAGE_DISABLE_CACHE             10
379   #define BOOT_STAGE_CHCHE_DISABLED            11
380   #define BOOT_STAGE_EXIT                      12
381   #define BOOT_STAGE_ERROR_LOOP                13  
382   #define BOOT_STAGE_I2C_BOOTCONFIG_LOOP       14
383   #define BOOT_STAGE_I2C_SLV_RCV_OPTIONS_LOOP  15
384   #define BOOT_STAGE_UTOPIA_MAIN_LOOP          16
385   UINT16  coldBootEntries;
386   
387 } BOOT_STATS_NONINIT_T;
389 /*******************************************************************************
390  * Definition: Run time statistics and error counts. These stats are 
391  *             initialized on cold boot entry.
392  ******************************************************************************/
393  
394 typedef struct BOOT_STATS_COMMON_S  {
395   UINT32    bootStatus;
396   UINT16    nColdBootEntries;
397   UINT16    nBootReentries;
398   UINT16    nPllWarns;
399   UINT16    nResetWarns;
400 } BOOT_STATS_COMMON_T;
401  
402  
403 typedef struct BOOT_STATS_MAIN_S {
404   UINT16  errorCode;        /* (module ID <<8 ) + module specific error */
405   
406   /* I2C operation related statistics */
407   UINT16  numI2Cpkts;       /* number of I2C boot table packets processed */
408   UINT16  numI2CchksumError;/* number of I2C checksum errors */
409   UINT16  numI2ClengthError;/* number of I2C block length errors */
410   UINT16  numI2CotherError; /* number of I2C section with invalid length and etc */
411   UINT16  numI2Cretrys;     /* number of I2C retrys due to read access errors */
412   UINT16  numI2cWrites;     /* number of I2C master writes to passive devices */
413   UINT16  numI2cWriteError; /* number of I2C master write errors              */
414   
415   UINT16  warmBootEntry;    /* Count of entries into warm boot routine   */
416 } BOOT_STATS_MAIN_T;
420 /*****************************************************************************
421  * Definition: I2C stats, Boot table and Ethernrt stats initialized 
422  *             on cold boot entry
423  *****************************************************************************/
424 typedef struct I2C_STATS_tag
426     UINT16      num_trans;
427     UINT16      num_trys;
428     UINT16      num_try_ok;
429     UINT16      num_try_lost_arb;
430     UINT16      num_try_idle_to;
431     UINT16      num_try_no_ack;
432     UINT16      num_try_other_err;
433     UINT32      extra_idle_waits;
434     UINT32      extra_clock_waits;
435     UINT32      tx_bytes;
436     UINT32      rx_bytes;
437     UINT32      data_re_reads;
438 } I2C_STATS_T;
440 typedef struct BTBL_STATS_tag
442   UINT16  num_sections;     /* number of boot table sections received */
443   UINT16  num_pdma_copies;  /* number of PDMA copies performed */
444 } BTBL_STATS_T;
446 typedef struct ETH_STATS_tag
448   /* MAC packets related statistics */
449   UINT16  uniMacPkts;       /* Count of packets received with valid unicast mac 
450                                address   */
451   UINT16  multiMacPkts;     /* Count of packets received with valid multicast or
452                                broadcast mac address   */
453   UINT16  invalidMacPkts;   /* Count of packets received with invalid mac 
454                                address   */
455   UINT16  invalidLLCPkts;   /* Count of 802.3 packets with wrong LLC/SNAP header */
456   UINT16  nonIpPkts;        /* Count of non-IP packets received with valid 
457                                MAC address   */
458                                
459   /* IP packets related statistics */                             
460   UINT16  nonIP4Pkts;       /* Count of non-IP4 packets        */
461   UINT16  ipfragments;      /* Count of IP fragments received      */
462   UINT16  ipTruncatedError; /* Count of truncated IP frame */
463   UINT16  nonUDPPkts;       /* Count of IP packets with non-UDP paylaod  */
464   
465   /* UDP packets related statistics */
466   UINT16  udpSizeError;     /* Count of UDP packet with invalid (odd) size */
467   UINT16  udpPortError;     /* Count of UDP packets with invalid port number */
468   UINT16  udpChksumError;   /* Count of UDP packets with checksum error */
469   
470   /* Boot table packets related statistics */
471   UINT16  nonBtblPkts;      /* Count of UDP packets with invalid boot table paylaod */
472   UINT16  outSeqPkts;       /* Count of out of sequence boot table packets received       
473                                i.e. packets with unexpected seq_num      */
474   UINT16  expSeqNum;        /* Expected Sequence Number */
475   UINT16  lastSeqNum;       /* Last sequence number received */                             
477   /* Driver errors */
478   UINT16  sizeZeroPackets;  /* Count of packets arriving with 0 size */
479 } ETH_STATS_T;
481 typedef struct PCI_EEAI_STATS_tag
483   UINT16  pciI2cReads;         /* Count of block reads of i2c eeprom */
484   UINT16  pciI2cRetries;       /* Count of i2c read retries          */
485   UINT16  pciChkSumErr;        /* Count of block check sum errors    */
486   UINT16  pciEeaiFail;         /* Count of aborted pci attempts      */
487 } PCI_EEAI_STATS_T;
489 /* Rapid I/O stats */
490 typedef struct RAPIDIO_STATS_tag
492   UINT16 rapidIoFailReady;     /* If set rapid I/O peripheral failed to report ready */
493   UINT16 rapidIoBtblBlocks;    /* Count of number of boot table blocks received */
494   UINT16 rapidIoBtblBadBlocks; /* Count of boot table blocks rejected */
495 } RAPIDIO_STATS_T;
497 typedef struct HPI_STATS_Tag
499   UINT16 hpiBtblBlocks;        /* Count of boot table blocks received */
500   UINT16 hpiBtblBadBlocks;     /* Count of boot table blocks rejected */
501 } HPI_STATS_T;
503 /* Utopia stats */
504 typedef struct UTOPIA_STATS_tag
506   UINT16 cellCount;            /* Count of cells received   */
507   UINT16 invalidPtr;           /* Count of invalid pointers received in processing */
508   UINT16 invalidSize;          /* Count of cells that were too small               */
509   UINT16 cellMagicCount;       /* Count of cells received with valid magic         */
510   UINT16 cellMagicFailed;      /* Count of cells received with invalid magic       */
511   UINT16 trapNoCellMem;        /* Trapped due to no cell space in memory           */
512   UINT16 possibleOverrun;      /* Count of possible cell buffer overruns           */
513 } UTOPIA_STATS_T;
515 /*******************************************************************************
516  * Definition: The statistics
517  *
518  *   !!!!!! boot.s assumes that the nonInit stats are at the top of the structure!
519  *******************************************************************************/
520 typedef struct BOOT_STATS_S {
522  BOOT_STATS_COMMON_T   common;
523  BOOT_STATS_NONINIT_T  nonInit;
524  BOOT_STATS_MAIN_T     main;
525  I2C_STATS_T           i2c;
526  BTBL_STATS_T          btbl;
527  union  {
528    ETH_STATS_T           eth;
529    PCI_EEAI_STATS_T      pci_eeai;
530    RAPIDIO_STATS_T       rapidIo;
531    UTOPIA_STATS_T        utopia;
532    HPI_STATS_T           hpi;
533  } u;
534 } BOOT_STATS_T;
536 extern BOOT_STATS_T bootStats;
538 /*******************************************************************************
539  * Definition: The magic start address, known to all modules
540  *******************************************************************************/
541 extern volatile UINT32 *p_boot_entry_addr;
543 #endif  /* __TIBOOT_H__ */
545 /* nothing past this point */