Merge branch 'tmp-mike2'
[keystone-rtos/ibl.git] / src / device / c6474l / c6474l.c
1 /*
2  *
3  * Copyright (C) 2010 Texas Instruments Incorporated - http://www.ti.com/ 
4  * 
5  * 
6  *  Redistribution and use in source and binary forms, with or without 
7  *  modification, are permitted provided that the following conditions 
8  *  are met:
9  *
10  *    Redistributions of source code must retain the above copyright 
11  *    notice, this list of conditions and the following disclaimer.
12  *
13  *    Redistributions in binary form must reproduce the above copyright
14  *    notice, this list of conditions and the following disclaimer in the 
15  *    documentation and/or other materials provided with the   
16  *    distribution.
17  *
18  *    Neither the name of Texas Instruments Incorporated nor the names of
19  *    its contributors may be used to endorse or promote products derived
20  *    from this software without specific prior written permission.
21  *
22  *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
23  *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
24  *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
25  *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
26  *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
27  *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
28  *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
29  *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
30  *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
31  *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
32  *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
33  *
34 */
38 /************************************************************************************
39  * FILE PURPOSE: C6474 Device Specific functions
40  ************************************************************************************
41  * FILE NAME: c6474l.c
42  *
43  * DESCRIPTION: Implements the device specific functions for the IBL
44  *
45  * @file c6474l.c
46  *
47  * @brief
48  *  This file implements the device specific functions for the IBL
49  *
50  ************************************************************************************/
51 #include "ibl.h"
52 #include "device.h"
53 #include "pllapi.h"
54 #include "emif31api.h"
55 #include "pscapi.h"
56 #include "gpio.h"
57 #include <string.h>
59 extern cregister unsigned int DNUM;
62 /**
63  *  @brief Determine if an address is local
64  *
65  *  @details
66  *    Examines an input address to determine if it is a local address
67  */
68 bool address_is_local (Uint32 addr)
69 {
70     /* L2 */
71     if ((addr >= 0x00800000) && (addr < 0x00898000))
72         return (TRUE);
74     /* L1P */
75     if ((addr >= 0x00e00000) && (addr < 0x00e08000))
76         return (TRUE);
78     /* L2D */
79     if ((addr >= 0x00f00000) && (addr < 0x00f08000))
80         return (TRUE);
82     return (FALSE);
84 }
87 /**
88  * @brief  Convert a local l1d, l1p or l2 address to a global address
89  *
90  * @details
91  *  The global address is formed. If the address is not local then
92  *  the input address is returned
93  */
94 Uint32 deviceLocalAddrToGlobal (Uint32 addr)
95 {
97     if (address_is_local (addr))
98         addr = (1 << 28) | (DNUM << 24) | addr;
100     return (addr);
103         
104         
105 /**
106  * @brief Configure the PLLs
107  *
108  * @details
109  *   Only the main PLL can be configured here. The DDR pll is enabled by default,
110  *   and the network PLL is enabled through serdes configuration.
111  *   the multiplier and dividers.
112  */
113 void devicePllConfig (void)
115     if (ibl.pllConfig[ibl_MAIN_PLL].doEnable == TRUE)
116         hwPllSetPll (MAIN_PLL, 
117                      ibl.pllConfig[ibl_MAIN_PLL].prediv,
118                      ibl.pllConfig[ibl_MAIN_PLL].mult,
119                      ibl.pllConfig[ibl_MAIN_PLL].postdiv);
123 /**
124  * @brief
125  *   Enable the DDR
126  *
127  * @details
128  *   The DDR controller on the c6474 is an emif 3.1. The controller is
129  *   initialized directly with the supplied values
130  */
131 void deviceDdrConfig (void)
133     if (ibl.ddrConfig.configDdr != 0)
134         hwEmif3p1Enable (&ibl.ddrConfig.uEmif.emif3p1);
137         
139 /**
140  *  @brief Power up a peripheral
141  *
142  *  @details
143  *    Boot peripherals are powered up
144  */
145 int32 devicePowerPeriph (int32 modNum)
147     /* If the input value is < 0 there is nothing to power up */
148     if (modNum < 0)
149         return (0);
152     if (modNum >= TARGET_PWR_MAX_MOD)
153         return (-1);
155     return ((int32)pscEnableModule(modNum));
156         
160 /**
161  *  @brief  Enable the pass through version of the nand controller
162  *
163  *  @details  On the evm the nand controller is enabled by setting 
164  *            gpio 14 high
165  */
166 #if 0
167 int32 deviceConfigureForNand(void)
169         hwGpioSetDirection(NAND_MODE_GPIO, GPIO_OUT);
170         hwGpioSetOutput(NAND_MODE_GPIO);
171     return (0);
174 #endif
177 /**
178  *  @brief
179  *    The e-fuse mac address is loaded
180  */
181 void deviceLoadDefaultEthAddress (uint8 *maddr)
183     uint32 macA, macB;
185     /* Read the e-fuse mac address */
186     macA = *((uint32 *)0x2880834);
187     macB = *((uint32 *)0x2880838);
189     maddr[0] = (macB >>  8) & 0xff;
190     maddr[1] = (macB >>  0) & 0xff;
191     maddr[2] = (macA >> 24) & 0xff;
192     maddr[3] = (macA >> 16) & 0xff;
193     maddr[4] = (macA >>  8) & 0xff;
194     maddr[5] = (macA >>  0) & 0xff;