1 /************************************************************************************
2 * FILE PURPOSE: C6474 Device Specific functions
3 ************************************************************************************
4 * FILE NAME: c6474l.c
5 *
6 * DESCRIPTION: Implements the device specific functions for the IBL
7 *
8 * @file c6474l.c
9 *
10 * @brief
11 * This file implements the device specific functions for the IBL
12 *
13 ************************************************************************************/
14 #include "ibl.h"
15 #include "device.h"
16 #include "pllapi.h"
17 #include "emif31api.h"
18 #include "pscapi.h"
19 #include "gpio.h"
20 #include <string.h>
22 extern cregister unsigned int DNUM;
25 /**
26 * @brief Determine if an address is local
27 *
28 * @details
29 * Examines an input address to determine if it is a local address
30 */
31 bool address_is_local (Uint32 addr)
32 {
33 /* L2 */
34 if ((addr >= 0x00800000) && (addr < 0x00898000))
35 return (TRUE);
37 /* L1P */
38 if ((addr >= 0x00e00000) && (addr < 0x00e08000))
39 return (TRUE);
41 /* L2D */
42 if ((addr >= 0x00f00000) && (addr < 0x00f08000))
43 return (TRUE);
45 return (FALSE);
47 }
50 /**
51 * @brief Convert a local l1d, l1p or l2 address to a global address
52 *
53 * @details
54 * The global address is formed. If the address is not local then
55 * the input address is returned
56 */
57 Uint32 deviceLocalAddrToGlobal (Uint32 addr)
58 {
60 if (address_is_local (addr))
61 addr = (1 << 28) | (DNUM << 24) | addr;
63 return (addr);
65 }
68 /**
69 * @brief Configure the PLLs
70 *
71 * @details
72 * Only the main PLL can be configured here. The DDR pll is enabled by default,
73 * and the network PLL is enabled through serdes configuration.
74 * the multiplier and dividers.
75 */
76 void devicePllConfig (void)
77 {
78 if (ibl.pllConfig[ibl_MAIN_PLL].doEnable == TRUE)
79 hwPllSetPll (MAIN_PLL,
80 ibl.pllConfig[ibl_MAIN_PLL].prediv,
81 ibl.pllConfig[ibl_MAIN_PLL].mult,
82 ibl.pllConfig[ibl_MAIN_PLL].postdiv);
84 }
86 /**
87 * @brief
88 * Enable the DDR
89 *
90 * @details
91 * The DDR controller on the c6474 is an emif 3.1. The controller is
92 * initialized directly with the supplied values
93 */
94 void deviceDdrConfig (void)
95 {
96 if (ibl.ddrConfig.configDdr != 0)
97 hwEmif3p1Enable (&ibl.ddrConfig.uEmif.emif3p1);
99 }
102 /**
103 * @brief Power up a peripheral
104 *
105 * @details
106 * Boot peripherals are powered up
107 */
108 int32 devicePowerPeriph (int32 modNum)
109 {
110 /* If the input value is < 0 there is nothing to power up */
111 if (modNum < 0)
112 return (0);
115 if (modNum >= TARGET_PWR_MAX_MOD)
116 return (-1);
118 return ((int32)pscEnableModule(modNum));
120 }
123 /**
124 * @brief Enable the pass through version of the nand controller
125 *
126 * @details On the evm the nand controller is enabled by setting
127 * gpio 14 high
128 */
129 #if 0
130 int32 deviceConfigureForNand(void)
131 {
132 hwGpioSetDirection(NAND_MODE_GPIO, GPIO_OUT);
133 hwGpioSetOutput(NAND_MODE_GPIO);
134 return (0);
136 }
137 #endif
140 /**
141 * @brief
142 * The e-fuse mac address is loaded
143 */
144 void deviceLoadDefaultEthAddress (uint8 *maddr)
145 {
146 uint32 macA, macB;
148 /* Read the e-fuse mac address */
149 macA = *((uint32 *)0x2880834);
150 macB = *((uint32 *)0x2880838);
152 maddr[0] = (macB >> 8) & 0xff;
153 maddr[1] = (macB >> 0) & 0xff;
154 maddr[2] = (macA >> 24) & 0xff;
155 maddr[3] = (macA >> 16) & 0xff;
156 maddr[4] = (macA >> 8) & 0xff;
157 maddr[5] = (macA >> 0) & 0xff;
158 }