new pll sequence of 1.main 2.pa 3.ddr
[keystone-rtos/ibl.git] / src / device / c66x / c66x.c
1 /*
2  *
3  * Copyright (C) 2010 Texas Instruments Incorporated - http://www.ti.com/ 
4  * 
5  * 
6  *  Redistribution and use in source and binary forms, with or without 
7  *  modification, are permitted provided that the following conditions 
8  *  are met:
9  *
10  *    Redistributions of source code must retain the above copyright 
11  *    notice, this list of conditions and the following disclaimer.
12  *
13  *    Redistributions in binary form must reproduce the above copyright
14  *    notice, this list of conditions and the following disclaimer in the 
15  *    documentation and/or other materials provided with the   
16  *    distribution.
17  *
18  *    Neither the name of Texas Instruments Incorporated nor the names of
19  *    its contributors may be used to endorse or promote products derived
20  *    from this software without specific prior written permission.
21  *
22  *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
23  *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
24  *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
25  *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
26  *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
27  *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
28  *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
29  *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
30  *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
31  *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
32  *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
33  *
34 */
38 /************************************************************************************
39  * FILE PURPOSE: C66x Device Specific functions
40  ************************************************************************************
41  * FILE NAME: c66x.c
42  *
43  * DESCRIPTION: Implements the device specific functions for the IBL
44  *
45  * @file c66x.c
46  *
47  * @brief
48  *  This file implements the device specific functions for the IBL
49  *
50  ************************************************************************************/
51 #include "ibl.h"
52 #include "iblloc.h"
53 #include "iblcfg.h"
54 #include "device.h"
55 #include "pllapi.h"
56 #include "emif31api.h"
57 #include "pscapi.h"
58 #include "gpio.h"
59 #include "qm_api.h"
60 #include "cpdma_api.h"
61 #include "pa_api.h"
62 #include "serdes_api.h"
63 #include "net.h"
64 #include "nandhwapi.h"
65 #include "nor_api.h"
66 #include "spi_api.h"
67 #include <string.h>
69 extern cregister unsigned int DNUM;
71 /**
72  *  @brief Determine if an address is local
73  *
74  *  @details
75  *    Examines an input address to determine if it is a local address. Using the largest
76  *    L2 size on the C6670.
77  */
78 bool address_is_local (Uint32 addr)
79 {
80     /* L2 */
81     if ((addr >= 0x00800000) && (addr < 0x00900000))
82         return (TRUE);
84     /* L1P */
85     if ((addr >= 0x00e00000) && (addr < 0x00e08000))
86         return (TRUE);
88     /* L2D */
89     if ((addr >= 0x00f00000) && (addr < 0x00f08000))
90         return (TRUE);
92     return (FALSE);
94 }
97 /**
98  * @brief  Convert a local l1d, l1p or l2 address to a global address
99  *
100  * @details
101  *  The global address is formed. If the address is not local then
102  *  the input address is returned
103  */
104 Uint32 deviceLocalAddrToGlobal (Uint32 addr)
107     if (address_is_local (addr))
108         addr = (1 << 28) | (DNUM << 24) | addr;
110     return (addr);
113         
114         
115 /**
116  * @brief
117  *   Enable the DDR
118  *
119  * @details
120  *   The DDR controller on the c66x is an emif 4.0. The controller is
121  *   initialized directly with the supplied values
122  */
123 void deviceDdrConfig (void)
125     /* The emif registers must be made visible. MPAX mapping 2 is used */
126     DEVICE_REG_XMPAX_L(2) =  0x10000000 | 0xff;     /* replacement addr + perm*/
127     DEVICE_REG_XMPAX_H(2) =  0x2100000B;         /* base addr + seg size (64KB)*/       
129     if (ibl.ddrConfig.configDdr != 0)
130         hwEmif4p0Enable (&ibl.ddrConfig.uEmif.emif4p0);
133         
136 /**
137  *  @brief  Enable EMIF25 or SPI interface to the NAND
138  *
139  */
140 int32 deviceConfigureForNand(void)
143     return (0);
147 /**
148  *  @brief
149  *      Return the base memory address for emif25 in a given chip select space
150  */
151 uint32 deviceEmif25MemBase (int32 cs)
153     switch (cs)  {
155         case 2:  return (TARGET_MEM_NAND_CS_2);
157         case 3:  return (TARGET_MEM_NAND_CS_3);
159         case 4:  return (TARGET_MEM_NAND_CS_4);
161         case 5:  return (TARGET_MEM_NAND_CS_5);
163     }
165     return (0xffffffff);
170 /**
171  *  @brief
172  *      Return the PSC number for NAND/NOR through emif. Only 6678 has the emif
173  */
174 Int32 deviceEmifPscNum (void)
176     Uint32 v;
178     v = *((Uint32 *)DEVICE_JTAG_ID_REG);
179     v &= DEVICE_JTAG_ID_MASK;
180     if (v == DEVICE_C6678_JTAG_ID_VAL)
181         return (TARGET_PWR_EMIF_C6678);
183     /* Return a negative number to indicate no PSC module is associated with NAND */
184     return (-1);
190 /**
191  *  @brief
192  *    The e-fuse mac address is loaded
193  */
194 void deviceLoadDefaultEthAddress (uint8 *maddr)
196     uint32 macA, macB;
198     /* Read the e-fuse mac address */
199     macA = *((uint32 *)0x2620110);
200     macB = *((uint32 *)0x2620114);
202     maddr[0] = (macB >>  8) & 0xff;
203     maddr[1] = (macB >>  0) & 0xff;
204     maddr[2] = (macA >> 24) & 0xff;
205     maddr[3] = (macA >> 16) & 0xff;
206     maddr[4] = (macA >>  8) & 0xff;
207     maddr[5] = (macA >>  0) & 0xff;
211 /**
212  *  @brief
213  *    Compile time queue manager information
214  */
215 #define DEVICE_NUM_RX_CPPIS     1
216 #define DEVICE_NUM_TX_CPPIS     1
217 #define DEVICE_NUM_CPPIS        (DEVICE_NUM_RX_CPPIS + DEVICE_NUM_TX_CPPIS)
219 /* The linking RAM */
220 #pragma DATA_SECTION(qm_linkram_buf, ".linkram")
221 #pragma DATA_ALIGN(qm_linkram_buf, 16)
222 uint8 qm_linkram_buf[DEVICE_NUM_CPPIS * 2 * (sizeof(uint32)/sizeof(uint8))];
225 /* The CPPI RAM */
226 #pragma DATA_SECTION(qm_cppi_buf, ".cppi")
227 #pragma DATA_ALIGN(qm_cppi_buf, 16)
228 uint8 qm_cppi_buf[QM_DESC_SIZE_BYTES * DEVICE_NUM_CPPIS];
231 /* The rx data buffers */
232 #pragma DATA_SECTION(qm_buffer, ".mac_buffer")
233 #pragma DATA_ALIGN(qm_buffer, 16)
234 uint8 qm_buffer[MAX_SIZE_STREAM_BUFFER * DEVICE_NUM_RX_CPPIS];
236 const qmConfig_t qmConfig =  {
237     (UINT32) qm_linkram_buf,
238     sizeof  (qm_cppi_buf),
239     (UINT32) qm_cppi_buf,
241     DEVICE_NUM_CPPIS,
242     DEVICE_QM_FREE_Q
243 };
245 /**
246  *  @brief
247  *      Return the queue manager memory configuration information
248  */
249 void *targetGetQmConfig (void)
251     return ((void *)&qmConfig);
254 /**
255  *  @brief
256  *      Attach a packet buffer to each descriptor and push onto the linked buffer queue
257  */
258 void targetInitQs (void)
260     int32 i;
261     qmHostDesc_t *hd;
263     for (i = 0; i < DEVICE_NUM_RX_CPPIS; i++)  {
265         hd                = hwQmQueuePop (DEVICE_QM_FREE_Q);
266         hd->buffLen       = sizeof (qm_buffer) / DEVICE_NUM_CPPIS;
267         hd->buffPtr       = (UINT32) &(qm_buffer[MAX_SIZE_STREAM_BUFFER * i]);
268         hd->nextBDPtr     = 0;
269         hd->origBufferLen = MAX_SIZE_STREAM_BUFFER;
270         hd->origBuffPtr   = hd->buffPtr;
272         hwQmQueuePush (hd, DEVICE_QM_LNK_BUF_Q, QM_DESC_SIZE_BYTES);
274     }
277     for (i = 0; i < DEVICE_NUM_TX_CPPIS; i++)  {
279         hd                = hwQmQueuePop (DEVICE_QM_FREE_Q);
280         hd->buffLen       = 0;
281         hd->buffPtr       = 0;
282         hd->nextBDPtr     = 0;
283         hd->origBufferLen = 0;
284         hd->origBuffPtr   = 0;
286         hwQmQueuePush (hd, DEVICE_QM_TX_Q, QM_DESC_SIZE_BYTES);
288     }
295 const cpdmaRxCfg_t cpdmaEthRxCfg =  {
297     DEVICE_PA_CDMA_RX_CHAN_CFG_BASE,    /* Base address of PA CPDMA rx config registers */
298     DEVICE_PA_CDMA_RX_NUM_CHANNELS,     /* Number of rx channels */
300     DEVICE_PA_CDMA_RX_FLOW_CFG_BASE,    /* Base address of PA CPDMA rx flow registers */
301     DEVICE_PA_CDMA_RX_NUM_FLOWS,        /* Number of rx flows */
303     0,                                  /* Queue manager for descriptor / buffer for received packets */
304     DEVICE_QM_LNK_BUF_Q,                /* Queue of descriptors /buffers for received packets */
306     0,                                  /* Queue manager for received packets */
307     DEVICE_QM_RCV_Q,                    /* Queue for received packets (overridden by PA)  */
309     DEVICE_RX_CDMA_TIMEOUT_COUNT        /* Teardown maximum loop wait */
310 };
313 /**
314  *  @brief
315  *      Return the cpdma configuration information
316  */
317 void *targetGetCpdmaRxConfig (void)
319     return ((void *)&cpdmaEthRxCfg);
324 const cpdmaTxCfg_t cpdmaEthTxCfg = {
326     DEVICE_PA_CDMA_GLOBAL_CFG_BASE,     /* Base address of global config registers      */
327     DEVICE_PA_CDMA_TX_CHAN_CFG_BASE,    /* Base address of PA CPDMA tx config registers */
328     DEVICE_PA_CDMA_TX_NUM_CHANNELS      /* Number of tx channels */
330 };
333 /**
334  *  @brief
335  *      return the tx cpdma configuration information
336  */
337 void *targetGetCpdmaTxConfig (void)
339     return ((void *)&cpdmaEthTxCfg);
343 /**
344  *  @brief
345  *     Configure the PA
346  */
347 void targetPaConfig (uint8 *macAddr)
349     paConfig_t     paCfg;
350     qmHostDesc_t  *hd;
351     SINT16         ret;
353     /* Filter everything except the desired mac address and the broadcast mac */
354     paCfg.mac0ms = ((uint32)macAddr[0] << 24) | ((uint32)macAddr[1] << 16) | ((uint32)macAddr[2] << 8) | (uint32)(macAddr[3]);
355     paCfg.mac0ls = ((uint32)macAddr[4] << 24) | ((uint32)macAddr[5] << 16);
357     paCfg.mac1ms = 0xffffffff;
358     paCfg.mac1ls = 0xffff0000;
360     paCfg.rxQnum = DEVICE_QM_RCV_Q;
362     /* Form the configuration command in a buffer linked to a descriptor */
363     hd = hwQmQueuePop (DEVICE_QM_LNK_BUF_Q);
364     paCfg.cmdBuf = (uint8 *)hd->origBuffPtr;
366     ret = hwPaEnable (&paCfg);
367     if (ret != 0)  {
368         iblStatus.iblFail = ibl_FAIL_CODE_PA;
369         return;
370     }
373     /* Send the command to the PA through the QM */
374     hd->softwareInfo0 = PA_MAGIC_ID;
375     hd->buffLen = 16;
376     QM_DESC_DESCINFO_SET_PKT_LEN(hd->descInfo, 16);
378     /* Set the return Queue */
379     QM_DESC_PINFO_SET_QM    (hd->packetInfo, 0);
380     QM_DESC_PINFO_SET_QUEUE (hd->packetInfo, DEVICE_QM_LNK_BUF_Q);
382     hwQmQueuePush (hd, DEVICE_QM_PA_CFG_Q, QM_DESC_SIZE_BYTES);
387 /**
388  *  @brief
389  *      Chip level SGMII serdes configuration
390  *
391  *  @details
392  *      Both lanes are always setup, regardless of the port value
393  */
394 void targetSgmiiSerdesConfig (int32 port, void *viblSgmii)
396   serdesConfig_t scfg;
397   iblSgmii_t     *sgmii = (iblSgmii_t *)viblSgmii;
399   scfg.cfg      = sgmii->auxConfig;
400   scfg.nLanes   = 2;
401   scfg.rxCfg[0] = scfg.rxCfg[1] = sgmii->rxConfig;
402   scfg.txCfg[0] = scfg.txCfg[1] = sgmii->txConfig;
404   hwSerdesConfig (TARGET_SGMII_SERDES_BASE, &scfg);
406   hwSerdesWaitLock (TARGET_SGMII_SERDES_STATUS_BASE);
411 Int32 targetMacSend (void *vptr_device, Uint8* buffer, int num_bytes) 
413     qmHostDesc_t   *hd;
414     NET_DRV_DEVICE *ptr_device = (NET_DRV_DEVICE *)vptr_device;
415     int             i;
418     /* Must always setup the descriptor to have the minimum packet length */
419     if (num_bytes < 64)
420         num_bytes = 64;
423     for (i = 0, hd = NULL; hd == NULL; i++, chipDelay32 (1000)) 
424         hd = hwQmQueuePop (DEVICE_QM_TX_Q);
425     
426     if (hd == NULL)
427         return (-1);
429     QM_DESC_DESCINFO_SET_PKT_LEN(hd->descInfo, num_bytes);
431     hd->buffLen       = num_bytes;
432     hd->origBufferLen = num_bytes;
434     hd->buffPtr     = deviceLocalAddrToGlobal((UINT32)buffer);
435     hd->origBuffPtr = deviceLocalAddrToGlobal((UINT32)buffer);
437     
438     /* Return the descriptor back to the transmit queue */
439     QM_DESC_PINFO_SET_QM(hd->packetInfo, 0);
440     QM_DESC_PINFO_SET_QUEUE(hd->packetInfo, DEVICE_QM_TX_Q);
442     hwQmQueuePush (hd, DEVICE_QM_ETH_TX_Q, QM_DESC_SIZE_BYTES);
444     return (0);
449 Int32 targetMacRcv (void *vptr_device, UINT8 *buffer)
451     Int32           pktSizeBytes; 
452     qmHostDesc_t   *hd;
453     NET_DRV_DEVICE *ptr_device = (NET_DRV_DEVICE *)vptr_device;
455     hd = hwQmQueuePop (DEVICE_QM_RCV_Q);
456     if (hd == NULL)
457         return (0);
459     pktSizeBytes = QM_DESC_DESCINFO_GET_PKT_LEN(hd->descInfo);
460     iblMemcpy ((void *)buffer, (void *)hd->buffPtr, pktSizeBytes);
462     hd->buffLen = hd->origBufferLen;
463     hd->buffPtr = hd->origBuffPtr;
465     hwQmQueuePush (hd, DEVICE_QM_LNK_BUF_Q, QM_DESC_SIZE_BYTES);
467     return (pktSizeBytes);
471 void targetFreeQs (void)
473     qmHostDesc_t   *hd;
475     do  {
477         hd = hwQmQueuePop (DEVICE_QM_FREE_Q);
479     } while (hd != NULL);
481     do  {
483         hd = hwQmQueuePop (DEVICE_QM_LNK_BUF_Q);
485     } while (hd != NULL);
486     
487     do  {
489         hd = hwQmQueuePop (DEVICE_QM_RCV_Q);
491     } while (hd != NULL);
492     
493     do  {
495         hd = hwQmQueuePop (DEVICE_QM_TX_Q);
497     } while (hd != NULL);
498     
499 }    
501 extern nandCtbl_t nandEmifCtbl;
502 /**
503  *  @brief Return the NAND interface (GPIO, EMIF25 or SPI) used based on the value
504  *         of interface
505  */
506 #ifndef EXCLUDE_NAND_GPIO
507 nandCtbl_t nandGpioCtbl =  {
509     nandHwGpioDriverInit,
510     nandHwGpioDriverReadBytes,
511     nandHwGpioDriverReadPage,
512     nandHwGpioDriverClose
514 };
515 #endif
517 #ifndef EXCLUDE_NAND_EMIF
518 extern Int32 nandHwEmifDriverInit (int32 cs, void *vdevInfo);
519 extern Int32 nandHwEmifDriverReadBytes (Uint32 block, Uint32 page, Uint32 byte, Uint32 nbytes, Uint8 *data);
520 extern Int32 nandHwEmifDriverReadPage (Uint32 block, Uint32 page, Uint8 *data);
521 extern Int32 nandHwEmifDriverClose (void);
523 nandCtbl_t nandEmifCtbl =  {
525     nandHwEmifDriverInit,
526     nandHwEmifDriverReadBytes,
527     nandHwEmifDriverReadPage,
528     nandHwEmifDriverClose
530 };
531 #endif
533 #ifndef EXCLUDE_NAND_SPI
534 nandCtbl_t nandSpiCtbl =  {
537     nandHwSpiDriverInit,
538     nandHwSpiDriverReadBytes,
539     nandHwSpiDriverReadPage,
540     nandHwSpiDriverClose
542 };
543 #endif
545 nandCtbl_t *deviceGetNandCtbl (int32 interface)
547 #ifndef EXCLUDE_NAND_GPIO
549     if (interface == ibl_PMEM_IF_GPIO)
550         return (&nandGpioCtbl);
552 #endif
554 #ifndef EXCLUDE_NAND_SPI
556     if (interface == ibl_PMEM_IF_SPI)
557         return (&nandSpiCtbl);
559 #endif
561 #ifndef EXCLUDE_NAND_EMIF
563     if ((interface >= ibl_PMEM_IF_CHIPSEL_2) && (interface <= ibl_PMEM_IF_CHIPSEL_5))
564         return (&nandEmifCtbl);
566 #endif
568     return (NULL);
573 /**
574  * @brief
575  *      Get the nor call table for the specified nor interface
576  */
578 #ifndef EXCLUDE_NOR_EMIF
579 norCtbl_t norEmifCtbl = {
580     
581     norHwEmifDriverInit,
582     norHwEmifDriverReadBytes,
583     norHwEmifDriverClose
585 };
587 #endif
589 #ifndef EXCLUDE_NOR_SPI
591 norCtbl_t norSpiCtbl = {
592     
593     norHwSpiDriverInit,
594     norHwSpiDriverReadBytes,
595     norHwSpiDriverClose
597 };
599 #endif
601 norCtbl_t *deviceGetNorCtbl (int32 interface)
604 #ifndef EXCLUDE_NOR_SPI
605     
606     if (interface == ibl_PMEM_IF_SPI)
607         return (&norSpiCtbl);
609 #endif
611 #ifndef EXCLUDE_NOR_EMIF
612    
613     if ((interface >= ibl_PMEM_IF_CHIPSEL_2) && (interface <= ibl_PMEM_IF_CHIPSEL_5))
614         return (&norEmifCtbl);
616 #endif
618     return (NULL);
621     
624     
630