763207ff7dc019f01b63a66cc3d0fb9e2f3d5bdf
[keystone-rtos/ibl.git] / src / device / c66x / target.h
1 /*
2  *
3  * Copyright (C) 2010 Texas Instruments Incorporated - http://www.ti.com/ 
4  * 
5  * 
6  *  Redistribution and use in source and binary forms, with or without 
7  *  modification, are permitted provided that the following conditions 
8  *  are met:
9  *
10  *    Redistributions of source code must retain the above copyright 
11  *    notice, this list of conditions and the following disclaimer.
12  *
13  *    Redistributions in binary form must reproduce the above copyright
14  *    notice, this list of conditions and the following disclaimer in the 
15  *    documentation and/or other materials provided with the   
16  *    distribution.
17  *
18  *    Neither the name of Texas Instruments Incorporated nor the names of
19  *    its contributors may be used to endorse or promote products derived
20  *    from this software without specific prior written permission.
21  *
22  *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
23  *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
24  *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
25  *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
26  *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
27  *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
28  *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
29  *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
30  *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
31  *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
32  *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
33  *
34 */
38 /**************************************************************************
39  * FILE PURPOSE: Target specific definitions
40  **************************************************************************
41  * FILE NAME: target.h
42  *
43  * DESCRIPTION: This file defines target specific values used by low level
44  *                              drivers.
45  *
46  * @file target.h
47  *
48  * @brief
49  *  Low level target specific values are defined
50  *
51  ***************************************************************************/
52 #ifndef _TARGET_H
53 #define _TARGET_H
54 #include "types.h"
55 #include <stdint.h>
56 #include <stdio.h>
57 #include <string.h>
58 #include <stdlib.h>
60  
61 /** 
62  *  @brief
63  *   Device EMAC definitions
64  */
65  
67 /**
68  *  @brief
69  *    Device Timer definitions
70  */
71 #define TIMER0_BASE             0x02200000u
73 #define TIMER_INPUT_DIVIDER     6           /* Timer driven from cpu clock / 6 */
76 /**
77  *  @def MAIN_PLL
78  */
79 #define MAIN_PLL        0   /**< The index to the main PLL */
81 /**
82  * @def NET_PLL
83  */
84 #define NET_PLL         1   /**< The index to the network PLL */
86 /**
87  *  @def DDR_PLL
88  */
89 #define DDR_PLL         2   /**< The index to the DDR PLL */
92 /**
93  *  @brief
94  *    Device PLL definitions
95  */
96 #define DEVICE_PLL_BASE(x)      ((x) == MAIN_PLL ? 0x2310000 : ((x) == NET_PLL ? 0x2620338 : 0x2620330))
97 #define DEVICE_MAIN_PLL_CTL_0       0x2620328
98 #define DEVICE_MAIN_PLL_CTL_1       0x262032c
101 /**
102  *  @brief
103  *   The c66x devices use a register external to the PLL controller for prediv configuration
104  */
105 #define chipPllExternalPrediv(x)    TRUE
107 /**
108  * @brief 
109  *  Device PSC definitions
110  */
111 #define DEVICE_PSC_BASE     0x02350000u
113 /**
114  *  @brief
115  *    The SPI module base and module divider
116  */
117 #define DEVICE_SPI_BASE(x)          0x20bf0000u
118 #define DEVICE_SPI_MOD_DIVIDER      6
119 #define DEVICE_SPI_MAX_DIVIDER      0xff     
121 /**
122  * @brief
123  *  The PSC number for the PA sub-system */
124 #define TARGET_PWR_PA       7
126 /**
127  * @brief
128  *  The PSC number for the SGMII */
129 #define TARGET_PWR_ETH(x)   8
131 /** 
132  * @brief
133  *   The PSC numbers for EMIF16 and SPI vary between devices. The devices are run time
134  *   identified by reading the JTAG ID register,
135  *   NOTE: Have the variant bits as zero while defining the JTAG ID 
136  */
137 #define DEVICE_C6678_JTAG_ID_VAL   0x9e02f      /* C6678 */     
138 #define DEVICE_C6670_JTAG_ID_VAL   0xb94102f    /* C6670 */     
140 #define DEVICE_JTAG_ID_REG          0x2620018
141 #define DEVICE_JTAG_ID_MASK         0x0fffffff /* exclude variant bits(31:28) */
144 /**
145  *  @brief
146  *    The PSC number for NAND depends on the device
147  */
148 #define TARGET_PWR_EMIF         deviceEmifPscNum()
149 #define TARGET_PWR_EMIF_C6678   3
151 /*
152  *  @brief
153  *     The PSC number for SPI depends on the device
154  */
155 #define TARGET_PWR_SPI      deviceSpiPscNum()
157 /**
158  *  @brief
159  *      The PSC number for GPIO. GPIO is in the always on domain
160  */
161 #define TARGET_PWR_GPIO     -1
163 /**
164  *  @brief
165  *      The LPSC number for PCIe. PCIe is 10 for C6678/C6770
166  */
167 #define TARGET_PWR_PCIE    10 
169 /**
170  * @brief
171  *  Flag to indicate timer 0 power up requested. The time is always on in the 6472
172  */
173 #define TARGET_PWR_TIMER_0  -1
175 /**
176  *  @brief
177  *    Device DDR controller definitions
178  */
179 #define DEVICE_EMIF4_BASE  0x21000000
180 #define targetEmifType()   ibl_EMIF_TYPE_40
182 /**
183  *  @brief
184  *     Device EMIF 2.5 controller definitions
185  */
186 #define DEVICE_EMIF25_BASE  0x20c00000
188 /** 
189  *  @brief
190  *      NAND memory regions
191  */
192 #define TARGET_MEM_NAND_CS_2    0x70000000 
193 #define TARGET_MEM_NAND_CS_3    0x74000000 
194 #define TARGET_MEM_NAND_CS_4    0x78000000 
195 #define TARGET_MEM_NAND_CS_5    0x7c000000 
196 uint32 deviceNandMemBase (int32 cs);
197 #define TARGET_SHFL(x)  _shfl(x)  /* The shuffle intrinsic */
200 /**
201  * @brief
202  *  The highest module number. The value for nyquist is used
203  */
204 #define TARGET_PWR_MAX_MOD  30
205  
207 /**
208  * @brief
209  *   The base address of MDIO 
210  */
211 #define TARGET_MDIO_BASE    0x2090300
213 /**
214  * @brief
215  *   The number of external ethernet ports
216  */
217 #define TARGET_EMAC_N_PORTS     2
219 /**
220  *  @brief
221  *    GPIO address
222  */
223 #define GPIO_GPIOPID_REG        0x02320000
224 #define GPIO_GPIOEMU_REG        0x02320004
225 #define GPIO_BINTEN_REG         0x02320008
226 #define GPIO_DIR_REG            0x02320010
227 #define GPIO_OUT_DATA_REG       0x02320014
228 #define GPIO_SET_DATA_REG       0x02320018
229 #define GPIO_CLEAR_DATA_REG     0x0232001C
230 #define GPIO_IN_DATA_REG        0x02320020
231 #define GPIO_SET_RIS_TRIG_REG   0x02320024
232 #define GPIO_CLR_RIS_TRIG_REG   0x02320028
233 #define GPIO_SET_FAL_TRIG_REG   0x0232002C
234 #define GPIO_CLR_FAL_TRIG_REG   0x02320030
236 /**
237  *  @brief
238  *      The base address of the I2C peripheral, and the module divisor of the cpu clock
239  */
240 #define DEVICE_I2C_BASE                 0x02530000
241 #define DEVICE_I2C_MODULE_DIVISOR       6
242  
243 /**
244  * @brief
245  *      The address of the DEVSTAT register
246  */
247 #define DEVICE_REG_DEVSTAT              0x02620020
249 /**
250  * @brief
251  *     Prototypes for the PLL functions handled outside the main PLL registers
252  */
253 SINT16 chipPllSetExternalPrediv(UINT16 pllNum, UINT32 predivRegVal);
254 SINT16 chipPllExternalBwAdj (UINT16 pllNum, UINT16 mult);
255 UINT32 chipPllExternalMult (UINT16 pllNum, UINT16 mult);
258 /**
259  *  @brief
260  *      Hardware network subsystem support, ethernet switch
261  */
262 #define DEVICE_CPSW
263 #define DEVICE_CPSW_NUM_PORTS       3                    /* 3 switch ports */
264 #define DEVICE_CPSW_BASE            (0x02090800)
265 #define targetGetSwitchCtl()        CPSW_CTL_P0_ENABLE   /* Enable port 0 */
266 #define targetGetSwitchMaxPktSize() 9000
268 #define DEVICE_QM
269 #define DEVICE_QM_MANAGER_BASE          0x02a68000
270 #define DEVICE_QM_DESC_SETUP_BASE       0x02a6a000
271 #define DEVICE_QM_MANAGER_QUEUES_BASE   0x02a20000
272 #define DEVICE_QM_MANAGER_Q_PROXY_BASE  0x02a40000
273 #define DEVICE_QM_QUEUE_STATUS_BASE             0x02a00000
274 #define DEVICE_QM_NUM_LINKRAMS          2
275 #define DEVICE_QM_NUM_MEMREGIONS        20
276 void    *targetGetQmConfig(void);
277 void     targetInitQs (void);
279 #define chipLmbd(x,y) _lmbd(x,y)
284 #define DEVICE_CPDMA
286 #define DEVICE_PA_CDMA_GLOBAL_CFG_BASE   0x02004000
287 #define DEVICE_PA_CDMA_TX_CHAN_CFG_BASE  0x02004400
288 #define DEVICE_PA_CDMA_RX_CHAN_CFG_BASE  0x02004800
289 #define DEVICE_PA_CDMA_RX_FLOW_CFG_BASE  0x02005000
291 #define DEVICE_PA_CDMA_RX_NUM_CHANNELS   24
292 #define DEVICE_PA_CDMA_RX_NUM_FLOWS      32
293 #define DEVICE_PA_CDMA_TX_NUM_CHANNELS   9
296 #define DEVICE_QM_FREE_Q                910
297 #define DEVICE_QM_LNK_BUF_Q             911
298 #define DEVICE_QM_RCV_Q                 912
299 #define DEVICE_QM_TX_Q                  913
300 #define DEVICE_QM_PA_CFG_Q              640
301 #define DEVICE_QM_ETH_TX_Q              648
303 #define DEVICE_RX_CDMA_TIMEOUT_COUNT    1000
307 #define DEVICE_PA
308 #define DEVICE_PA_BASE                  0x02000000
309 #define DEVICE_PA_NUM_PDSPS             6
310 #define DEVICE_PA_RUN_CHECK_COUNT       100         /* Number of loops to verify PA firmware is running */
311 #define DEVICE_PA_PLL_BASE              0x02620338
312 #define chipLower8(x)                   ((x) & 0x00ff)
315 #define TARGET_SGMII_EXTERNAL_SERDES
316 #define TARGET_SGMII_TYPE_2             /* Use second sgmii setup sequence */
317 #define TARGET_SGMII_BASE_ADDRESSES    { 0x02090100, 0x02090200 }
318 #define TARGET_SGMII_SERDES_BASE        0x2620340
319 #define TARGET_SGMII_SERDES_STATUS_BASE 0x2620158
320 #define TARGET_SGMII_SOFT_RESET         0x04
321 #define TARGET_SGMII_CONTROL            0x10
322 #define TARGET_SGMII_MR_ADV_ABILITY     0x18
323 void targetSgmiiSerdesConfig (int32 port, void *cfg);
324 #define chipKickOpenSerdes(x)           *((uint32 *)0x2620038) = 0x83e70b13; *((uint32 *)0x262003c) = 0x95a4f1e0
325 #define chipKickClosedSerdes(x)         ;       /* never lock the registers */
326 #define TARGET_SERDES_LOCK_DELAY        (1600*1000)
328 #define DEVICE_EMACSL_BASE(x)           (0x02090900 + (x)*0x040)
329 #define DEVICE_N_GMACSL_PORTS           2
330 #define DEVICE_EMACSL_RESET_POLL_COUNT  100
331 Int32 targetMacSend (void *ptr_device, Uint8* buffer, int num_bytes);
332 Int32 targetMacRcv (void *ptr_device, UINT8 *buffer);
334 #define DEVICE_SS
335 #define DEVICE_PSTREAM_CFG_REG_ADDR                 0x2000604
336 #define DEVICE_PSTREAM_CFG_REG_VAL_ROUTE_PDSP0      0
337 #define hwConfigStreamingSwitch()                   DEVICE_REG32_W(DEVICE_PSTREAM_CFG_REG_ADDR, DEVICE_PSTREAM_CFG_REG_VAL_ROUTE_PDSP0);
339 #define ECC_BLOCK_SIZE                  256
341 /* NAND address pack macro */
342 #define PACK_ADDR(col, page, block) \
343         ((col & 0x000000ff) | ((page & 0x0000001f) << 9) | ((block & 0x00000fff) << 14))
345 /**
346  *  @brief
347  *      Register access macros
348  */
349 #define DEVICE_REG32_W(x,y)   *(volatile unsigned int *)(x)=(y)
350 #define DEVICE_REG32_R(x)    (*(volatile unsigned int *)(x))
352 #define BOOTBITMASK(x,y)      (   (   (  ((UINT32)1 << (((UINT32)x)-((UINT32)y)+(UINT32)1) ) - (UINT32)1 )   )   <<  ((UINT32)y)   )
353 #define BOOT_READ_BITFIELD(z,x,y)   (((UINT32)z) & BOOTBITMASK(x,y)) >> (y)
354 #define BOOT_SET_BITFIELD(z,f,x,y)  (((UINT32)z) & ~BOOTBITMASK(x,y)) | ( (((UINT32)f) << (y)) & BOOTBITMASK(x,y) )
356 /** 
357  *  @brief
358  *      Mpax configuration registers 
359  */
360 #define DEVICE_REG_XMPAX_L(x) *((volatile unsigned int *)(0x08000000 + (8*(x))))
361 #define DEVICE_REG_XMPAX_H(x) *((volatile unsigned int *)(0x08000004 + (8*(x))))
364 /**
365  *  @brief
366  *      ROM boot loader boot modes and table locations
367  */
368 #define BOOT_MODE_I2C               40
369 #define BOOT_MODE_SPI               50
372 #define ROM_BOOT_PARAMS_ADDR_C6678   0x873680
373 #define ROM_BOOT_PARAMS_ADDR_C6670   0x8f3680
375 /**
376  *  @brief
377  *      No device specific configuration required for NOR boot, so
378  *      the function call is defined to return success.
379  */
380 #define deviceConfigureForNor()    0
383 /****************************************************************
384  *
385  * NOTE: Following build flags enable DEVICE specific workarounds
386  * and have code which is specific to C6670/C6678 LC EVMs
387  *
388  ****************************************************************/
390 /**
391  *  @brief
392  *      Support for PLL workaround to re-enter ROM boot loader.
393  */
394 #define IBL_ENTER_ROM              1
396 /**
397  *  @brief
398  *      Support for enabling EDC for internal memory.
399  */
400 #define IBL_ENABLE_EDC             1 
402 /**
403  *  @brief
404  *      Support for enabling PCIe workarond for C6678/C6670.
405  */
406 #define IBL_ENABLE_PCIE_WORKAROUND 1
408 /**
409  *  @brief
410  *     DDR start and end address needed for DDR memory test 
411  */
412 #define DDR3_TEST_START_ADDRESS 0x80000000
413 #define DDR3_TEST_END_ADDRESS   (DDR3_TEST_START_ADDRESS + (128 *1024))
415 /**
416  *  @brief
417  *     Software workaround for DDR3 memory corruption is to re-init the PLL's and DDR controller. This flag enables the workaround
418  */
419 #define PLL_REINIT_WORKAROUND
421 extern int32_t ddr3_memory_test();
423 #endif /* _TARGET_H */