5ee3ddffae9e81cc8975d0c461e111180be9d969
1 /********************************************************************************************************
2 * FILE PURPOSE: Config level PLL driver
3 ********************************************************************************************************
4 * FILE NAME: cfgpll.c
5 *
6 * DESCRIPTION: The boot driver for PLLs that dont have a pll controller, but are controlled
7 * by registers in config space.
8 *
9 *********************************************************************************************************/
10 #include "types.h"
11 #include "target.h"
12 #include "pllapi.h"
14 #define DEVICE_REG32_W(x,y) *(volatile unsigned int *)(x)=(y)
15 #define DEVICE_REG32_R(x) (*(volatile unsigned int *)(x))
17 #define BOOTBITMASK(x,y) ( ( ( ((UINT32)1 << (((UINT32)x)-((UINT32)y)+(UINT32)1) ) - (UINT32)1 ) ) << ((UINT32)y) )
18 #define BOOT_READ_BITFIELD(z,x,y) (((UINT32)z) & BOOTBITMASK(x,y)) >> (y)
19 #define BOOT_SET_BITFIELD(z,f,x,y) (((UINT32)z) & ~BOOTBITMASK(x,y)) | ( (((UINT32)f) << (y)) & BOOTBITMASK(x,y) )
22 /*********************************************************************************************************
23 * FUNCTION PURPOSE: Configure and enable a pll
24 *********************************************************************************************************
25 * DESCRIPTION: The PLL is configured. If the existing configuration matches the requested one no
26 * register write is made.
27 *********************************************************************************************************/
28 SINT16 hwPllSetCfgPll (UINT32 base, UINT32 prediv, UINT32 mult, UINT32 postdiv, UINT32 chipFreqMhz, UINT32 pllFreqMhz)
29 {
30 UINT32 reg;
31 UINT32 regb;
32 UINT32 bwAdj;
34 UINT16 currentPrediv;
35 UINT16 currentMult;
36 UINT16 currentPostdiv;
37 UINT16 currentBypass;
38 UINT16 currentBwAdj;
39 UINT16 currentEnable;
40 UINT16 currentClkOut;
42 reg = DEVICE_REG32_R (base);
43 regb = DEVICE_REG32_R (base + 4);
45 currentPrediv = 1 + BOOT_READ_BITFIELD (reg, 5, 0);
46 currentMult = 1 + BOOT_READ_BITFIELD (reg, 18, 6);
47 currentPostdiv = 1 + BOOT_READ_BITFIELD (reg, 22, 19);
48 currentBypass = BOOT_READ_BITFIELD (reg, 23, 23);
49 currentBwAdj = 1 + BOOT_READ_BITFIELD (reg, 31, 24) + ((BOOT_READ_BITFIELD (regb, 3, 0)) << 8);
50 currentEnable = BOOT_READ_BITFIELD(regb, 14, 14);
51 currentClkOut = BOOT_READ_BITFIELD(regb, 13, 13);
53 /* The PLL is currently enabled and connected if bypass == 0, enable == 1, clkout == 1 */
55 if ( (currentBypass == 0) &&
56 (currentPrediv == prediv) &&
57 (currentMult == mult) &&
58 (currentPostdiv == postdiv) &&
59 (currentEnable == 0) &&
60 (currentClkOut == 1) &&
61 (currentBwAdj == (mult >> 1)) )
62 return (0);
65 /* bwAdj is based only on the mult value */
66 bwAdj = (mult >> 1) - 1;
68 /* Multiplier / divider values are input as 1 less then the desired value */
69 if (prediv > 0)
70 prediv -= 1;
72 if (mult > 0)
73 mult -= 1;
75 if (postdiv > 0)
76 postdiv -= 1;
78 regb = BOOT_SET_BITFIELD(regb, 1, 6, 6);
79 DEVICE_REG32_W (base + 4, regb);
81 /* Setup the PLL. Assert bypass */
82 reg = BOOT_SET_BITFIELD (reg, 1, 23, 23); /* Bypass must be enabled */
83 DEVICE_REG32_W (base, reg);
85 /* Set bit 14 in register 1 to disable the PLL (assert reset) */
86 regb = BOOT_SET_BITFIELD(regb, 1, 14, 14);
87 DEVICE_REG32_W (base + 4, regb);
89 reg = BOOT_SET_BITFIELD (reg, prediv, 5, 0);
90 reg = BOOT_SET_BITFIELD (reg, mult, 18, 6);
91 reg = BOOT_SET_BITFIELD (reg, postdiv, 22, 19);
92 reg = BOOT_SET_BITFIELD (reg, (bwAdj & 0xff), 31, 24);
94 DEVICE_REG32_W (base, reg);
96 /* The 4 MS Bits of bwadj */
97 regb = BOOT_SET_BITFIELD (regb, (bwAdj >> 8), 3, 0);
98 DEVICE_REG32_W (base + 4, regb);
101 /* Reset must be asserted for at least 5us. Give a huge amount of padding here to be safe
102 * (the factor of 100) */
103 chipDelay32 (5 * chipFreqMhz * 100);
106 /* Clear bit 14 in register 1 to re-enable the pll */
107 regb = BOOT_SET_BITFIELD(regb, 0, 14, 14);
108 DEVICE_REG32_W (base + 4, regb);
110 /* Need to wait 100,000 output PLL cycles before releasing bypass and setting
111 * up the clk output */
112 chipDelay32 (chipFreqMhz * 100000 / pllFreqMhz);
115 /* Disable the bypass */
116 reg = BOOT_SET_BITFIELD (reg, 0, 23, 23); /* The value 0 disables the bypass */
117 DEVICE_REG32_W (base, reg);
119 /* Enable the output source (set bit 13) */
120 regb = BOOT_SET_BITFIELD(regb, 1, 13, 13);
121 DEVICE_REG32_W (base + 4, regb);
123 return (0);
125 } /* hwPllSetCfgPll */