8de03f6ce1bf075709ead16ebce57cac01ceb4cb
[keystone-rtos/ibl.git] / src / hw / plls / pll014phi / pll.c
1 /*************************************************************************************
2  * FILE PURPOSE: Provide PLL control functions
3  *************************************************************************************
4  * FILE NAME: pll.c
5  *
6  * DESCRIPTION: Provides functions to control the pll
7  *
8  *************************************************************************************/
9 #include "types.h"
10 #include "ibl.h"
11 #include "pllloc.h"
12 #include "pllapi.h"
13 #include "target.h"
15 #define DEVICE_REG32_W(x,y)   *(volatile unsigned int *)(x)=(y)
16 #define DEVICE_REG32_R(x)    (*(volatile unsigned int *)(x))
18 #define BOOTBITMASK(x,y)      (   (   (  ((UINT32)1 << (((UINT32)x)-((UINT32)y)+(UINT32)1) ) - (UINT32)1 )   )   <<  ((UINT32)y)   )
19 #define BOOT_READ_BITFIELD(z,x,y)   (((UINT32)z) & BOOTBITMASK(x,y)) >> (y)
20 #define BOOT_SET_BITFIELD(z,f,x,y)  (((UINT32)z) & ~BOOTBITMASK(x,y)) | ( (((UINT32)f) << (y)) & BOOTBITMASK(x,y) )
23 typedef enum  {
24     HW_PLL_DO_NOT_ENABLE_PLL,
25     HW_PLL_ENABLE_PLL
26 } hwPllEnable_t;
28 /*********************************************************************************
29  * FUNCTION PURPOSE: Provide a delay loop
30  *********************************************************************************
31  * DESCRIPTION: Generates a delay, units of cycles
32  *********************************************************************************/
33 void hw_pll_delay (UINT32 del)
34 {
35   UINT32 i;
36   volatile UINT32 j;
38   for (i = j = 0; i < del; i++)
39     asm (" nop ");
41 } /* hw_pll_delay */
44 /**********************************************************************************
45  * FUNCTION PURPOSE: Enables the pll to the specified multiplier
46  **********************************************************************************
47  * DESCRIPTION: Sets up the pll
48  **********************************************************************************/
49 /* latest Sequence as provided by Tom during 10/27 */
50 SINT16 hwPllSetPll (UINT32 pllNum, UINT32 prediv, UINT32 mult, UINT32 postdiv)
51 {
52   UINT32 ctl, reg;
53   UINT32 secctl;
54   UINT32 status;
55   UINT32 alnctl;
56   UINT32 pmult;
57   UINT32 pdiv;
58   UINT32 pllBase;
59   UINT32 i;
60   SINT16 ret = 0;
61   UINT32 pllm_min = 10, plld_min =0, outputdiv = 9;
62   UINT32 div2=3, div5=5, div8=64;
64   /* Mutliplier/divider values of 0 are invalid */
65   if (prediv == 0)
66     prediv = 1;
68   if (mult == 0)
69     mult = 1;
71   if (postdiv == 0)
72     postdiv = 1;
74   /* Get the base address of the pll */
75   pllBase = (UINT32) DEVICE_PLL_BASE(pllNum);
77  /* Wait for Stabilization time (min 100 us) */
78  /* assuming max device speed, 1.4GHz, 1 cycle = 0.714 ns *
79   * so, 100 us = 100000 ns = 140056 cycles */
80   hw_pll_delay (140056);
82   /* Program pllen=0 (pll bypass), pllrst=1 (reset pll), pllsrc = 0 */
83   ctl = DEVICE_REG32_R (pllBase + PLL_REG_CTL);
85  /* Check if PLL BYPASS is turned off previously */
86   secctl = DEVICE_REG32_R (pllBase + PLL_REG_SECCTL);
88   if ( (secctl & PLL_REG_SECCTL_FIELD_BYPASS) != 0 ) {
89     /* PLL BYPASS is turned on */
91     /* Clear the PLLENSRC bit */
92      ctl = ctl & ~(PLL_REG_CTL_FIELD_PLLENSRC);
93      DEVICE_REG32_W (pllBase + PLL_REG_CTL, ctl);
95     /* Clear the PLLEN bit */
96      ctl = ctl & ~(PLL_REG_CTL_FIELD_PLLEN);
97      DEVICE_REG32_W (pllBase + PLL_REG_CTL, ctl);
99      /* Wait for 4 Ref clocks */
100      /* The slowest clock can be at 24MHz, so min:160ns delay */
101      hw_pll_delay(225);
103      /* Put the PLL in Bypass mode to perform the power down mode */
104      secctl = secctl | PLL_REG_SECCTL_FIELD_BYPASS;
105      DEVICE_REG32_W (pllBase + PLL_REG_SECCTL, secctl);
107      /* Advisory 8: Multiple PLLs May Not Lock After Power-on Reset Issue         *  
108       * In order to ensure proper PLL startup, the PLL power_down pin needs to be *  
109       * toggled. This is accomplished by toggling the PLLPWRDN bit in the PLLCTL  *  
110       * register. This needs to be done before the main PLL initialization        *  
111       * sequence                                                                  */
112       ctl = ctl | 2;
113       DEVICE_REG32_W (pllBase + PLL_REG_CTL, ctl);
115       /* Stay in a loop such that the bit is set for 5 µs (minimum) and           *   
116        * then clear the bit.                                                      */
117       hw_pll_delay (14005); /* waiting 10 us */
119       /* Power up the PLL */
120       ctl = ctl & ~2;
121       DEVICE_REG32_W (pllBase + PLL_REG_CTL, ctl);
123       /* Set the ENSAT Bit */
124      /* Usage Note 9: For optimal PLL operation, the ENSAT bit in the PLL control *  
125       * registers for the Main PLL, DDR3 PLL, and PA PLL should be set to 1.      *  
126       * The PLL initialization sequence in the boot ROM sets this bit to 0 and    *  
127       * could lead to non-optimal PLL operation. Software can set the bit to the  *  
128       * optimal value of 1 after boot                                             */
129         reg = DEVICE_REG32_R (DEVICE_MAIN_PLL_CTL_1);
130         reg = reg | (1 << 6);
131         DEVICE_REG32_W (DEVICE_MAIN_PLL_CTL_1, reg);
132   }
134   /* Program the necessary multipliers/dividers and BW adjustments            */
135    /* This routine will subtract 1 from the mult value */
136   pmult = chipPllExternalMult(pllNum, mult);
137   pmult   = pmult & PLL_REG_PLLM_FIELD_MULTm1;
138   DEVICE_REG32_W (pllBase + PLL_REG_PLLM, pmult);
140   /* Set the PLL Divider */
141   chipPllSetExternalPrediv(pllNum, prediv - 1);  
143   /* set the output divide */
144   secctl = BOOT_SET_BITFIELD(secctl, 1 & 0x000f, 22, 19);
145   DEVICE_REG32_W (pllBase + PLL_REG_SECCTL, secctl); 
146       
147   /* set the BWADJ */
148   chipPllExternalBwAdj (pllNum, mult);
150   /* WAIT FOR THE go STAT BIT HERE (50 us) */
151     hw_pll_delay (140056 >> 1);   
152   /* wait for the GOSTAT, but don't trap if lock is never read */
153   for (i = 0; i < 100; i++)  {
154     hw_pll_delay (300);
155     status = DEVICE_REG32_R (pllBase + PLL_REG_PLLSTAT);
156     if ( (status & PLL_REG_STATUS_FIELD_GOSTAT) == 0 )
157       break;
158   }
159   /* Enable the pll even if the lock failed. Return a warning. */
160   if (i == 100)  
161     ret = -1;
162   
163   /* Set PLL dividers if needed */
164   reg = 0x8000 | (div2 -1);
165   DEVICE_REG32_W (pllBase + PLL_REG_DIV2, reg);
167   reg = 0x8000 | (div5 -1);
168   DEVICE_REG32_W (pllBase + PLL_REG_DIV5, reg);
170   reg = 0x8000 | (div8 -1);
171   DEVICE_REG32_W (pllBase + PLL_REG_DIV8, reg);
173   /* Program ALNCTLn registers */
174   alnctl = DEVICE_REG32_R (pllBase + PLL_REG_ALNCTL);
175   alnctl = alnctl | ((1 << 1) | (1 << 4) | (1 << 7));
176   DEVICE_REG32_W (pllBase + PLL_REG_ALNCTL, alnctl);
178   /* Set GOSET bit in PLLCMD to initiate the GO operation to change the divide *   
179    * values and align the SYSCLKs as programmed                                */
180   reg = DEVICE_REG32_R (pllBase + PLL_REG_CMD);
181   reg = reg | 1;
182   DEVICE_REG32_W (pllBase + PLL_REG_CMD, reg);
184   /* wait for the GOSTAT, but don't trap if lock is never read */
185   for (i = 0; i < 100; i++)  {
186     hw_pll_delay (300);
187     status = DEVICE_REG32_R (pllBase + PLL_REG_PLLSTAT);
188     if ( (status & PLL_REG_STATUS_FIELD_GOSTAT) == 0 )
189       break;
190   }
192   /* Wait for the PLL Reset duration time (min: 1000 ns)                      */
193     hw_pll_delay (1400);
195   /* Release PLL from Reset */
196     ctl = ctl & ~(PLL_REG_CTL_FIELD_PLLRST);
197     DEVICE_REG32_W (pllBase + PLL_REG_CTL, ctl);
199   /* Wait for PLL Lock time (min 50 us) */
200     hw_pll_delay (140056 >> 1);  
201    
202   /* wait for the pll to lock, but don't trap if lock is never read */
203   for (i = 0; i < 100; i++)  {
204     hw_pll_delay (2000/7);
205     status = DEVICE_REG32_R (pllBase + PLL_REG_PLLSTAT);
206     if ( (status & PLL_REG_STATUS_FIELD_LOCK) != 0 )
207       break;
208   }
210   /* Enable the pll even if the lock failed. Return a warning. */
211   if (i == 100)  
212     ret = -1;
214   /* Clear the secondary controller bypass bit */
215   secctl = secctl & ~PLL_REG_SECCTL_FIELD_BYPASS;
216   DEVICE_REG32_W (pllBase + PLL_REG_SECCTL, secctl);
219   /* Set pllen to 1 to enable pll mode */
220   ctl = ctl | PLL_REG_CTL_FIELD_PLLEN;
221   DEVICE_REG32_W (pllBase + PLL_REG_CTL, ctl);
222   
223   return (ret);
224 } /* hwPllSetPll */