1 #ifndef _QM_API_H
2 #define _QM_API_H
3 /*******************************************************************************************
4 * FILE PURPOSE: Boot loader queue manager API definition
5 *******************************************************************************************
6 * FILE NAME: qm_api.h
7 *
8 * DESCRIPTION: Defines the stripped down QM driver API to the boot loader.
9 *
10 ********************************************************************************************/
12 /* return values */
13 #define QM_OK 0
14 #define QM_INVALID_LINKRAM_ALIGNMENT -1
15 #define QM_INVALID_MEMREGION_ALIGNMENT -2
16 #define QM_INVALID_LINKRAM_SIZE -3
17 #define QM_INVALID_LINKRAM_RAM_SIZE -4 /* Not enough link ram for the number of descriptors */
20 /* Memory alignment requirements (bytes) */
21 #define QM_LINKRAM_ALIGN 4
22 #define QM_MEMR_ALIGN 16 /* Not specified in the doc */
24 /* The driver supports only a single descriptor size */
25 #define QM_DESC_SIZE_BYTES 64
27 /* QM setup configuration */
28 typedef struct qmConfig_s {
30 UINT32 linkRamBase;
31 UINT32 linkRamSize;
33 UINT32 memRegionBase;
34 UINT32 memRegNumDescriptors;
36 UINT32 destQ; /* Where the initialized descriptors are placed */
38 } qmConfig_t;
40 typedef struct qmHostDesc_s {
41 /** Descriptor type, packet type, protocol specific region location, packet length */
42 UINT32 descInfo;
43 /** Source tag, Destination tag */
44 UINT32 tagInfo;
45 /** EPIB present, PS valid word count, error flags, PS flags, return policy, return push policy,
46 * packet return QM number, packet return queue number */
47 UINT32 packetInfo;
48 /** Number of valid data bytes in the buffer */
49 UINT32 buffLen;
50 /** Byte aligned memory address of the buffer associated with this descriptor */
51 UINT32 buffPtr;
52 /** 32-bit word aligned memory address of the next buffer descriptor */
53 UINT32 nextBDPtr;
54 /** Completion tag, original buffer size */
55 UINT32 origBufferLen;
56 /** Original buffer pointer */
57 UINT32 origBuffPtr;
58 /** Optional EPIB word0 */
59 UINT32 timeStamp;
60 /** Optional EPIB word1 */
61 UINT32 softwareInfo0;
62 /** Optional EPIB word2 */
63 UINT32 softwareInfo1;
64 /** Optional EPIB word3 */
65 UINT32 softwareInfo2;
66 /** Optional protocol specific data */
67 UINT32 psData;
68 } qmHostDesc_t;
71 /* Descriptor values */
72 /* Descriptor Info: Descriptor type is host with any protocol specific info in the descriptor */
73 #define QM_DESC_TYPE_HOST 0
74 #define QM_DESC_PSINFO_IN_DESCR 0
75 #define QM_DESC_DEFAULT_DESCINFO (QM_DESC_TYPE_HOST << 30) | \
76 (QM_DESC_PSINFO_IN_DESCR << 22)
77 #define QM_DESC_INFO_GET_PSINFO_LOC(x) BOOT_READ_BITFIELD((x), 22, 22)
79 #define QM_DESC_DESCINFO_SET_PKT_LEN(x,v) (x) = BOOT_SET_BITFIELD((x), (v), 21, 0)
80 #define QM_DESC_DESCINFO_GET_PKT_LEN(x) BOOT_READ_BITFIELD((x), 21, 0)
83 /* Packet Info */
84 #define QM_DESC_PINFO_EPIB 1
85 #define QM_DESC_PINFO_RETURN_OWN 1
86 #define QM_DESC_DEFAULT_PINFO (QM_DESC_PINFO_EPIB << 31) | \
87 (QM_DESC_PINFO_RETURN_OWN << 15)
88 #define QM_PKT_INFO_GET_EPIB(x) BOOT_READ_BITFIELD((x), 31, 31)
89 #define QM_PKT_INFO_SET_PSINFO_SIZE(x,v) (x) = BOOT_SET_BITFIELD((x), (v), 29, 24)
93 #define QM_DESC_PINFO_SET_QM(x,v) (x) = BOOT_SET_BITFIELD((x), (v), 13, 12)
94 #define QM_DESC_PINFO_SET_QUEUE(x,v) (x) = BOOT_SET_BITFIELD((x), (v), 11, 0)
97 /* prototypes */
98 qmHostDesc_t *hwQmQueuePop (UINT32 qnum);
99 void hwQmQueuePush (qmHostDesc_t *hd, UINT32 qnum, UINT32 descSize);
100 SINT16 hwQmSetup (qmConfig_t *cfg);
101 UINT32 hwQmQueueCount (UINT32 qnum);
102 void hwQmTeardown (void);
103 SINT16 hwQmInitThreshold (UINT32 qnum);
108 #endif /* _QM_API_H */